Last edited 2 months ago

Linux Mailbox framework overview

<noinclude


> This article gives information about the Linux® mailbox framework. The mailbox framework is involved in interprocessor communication in heterogeneous multicore systems.

1. Framework purpose[edit | edit source]

The mailbox framework is used in interprocessor communication to exchange messages or signals between Arm®Cortex®-A and Cortex®-M. The mailbox framework is based on:

  • A mailbox controller that is platform dependent:
    • It is in charge of configuring and handling IRQ from the IPCC peripheral.
    • It provides a generic API to the mailbox client.
  • A mailbox client that is in charge of the message to send or receive.


A general presentation of the mailbox framework is available in the Linux mailbox documentation [1].

2. System overview[edit | edit source]

Mailbox overview.png

2.1. Component description[edit | edit source]

  • Mailbox controller
The mailbox controller is the stm32_ipcc. It configures and controls the IPCC peripheral
  • Mailbox client
The user can define their own mailbox client.
A mailbox client character device driver is provided as an example to demonstrate communication using a mailbox and shared memory ([2]).
Another example is the RPMsg framework, which uses a mailbox for interprocessor communication. In this case, the mailbox client is the remoteproc driver that forwards services from/to the RPMsg framework.

2.2. API description[edit | edit source]

The APIs are described in the Mailbox client API [3]

3. Configuration[edit | edit source]

3.1. Kernel Configuration[edit | edit source]

The following kernel configurations can be enabled using the Linux Menuconfig tool: Menuconfig or how to configure kernel :

  • Activate STM32 IPCC mailbox controller driver
Device drivers  --->
    -*- Mailbox Hardware Support  --->
        <*> STM32 IPCC Mailbox
  • Activate MAILBOX CDEV mailbox client driver
Device drivers  --->
    -*- Mailbox Hardware Support  --->
        <*> mailbox client char device

3.2. Device tree configuration[edit | edit source]

Please refer to the IPCC device tree configuration.

4. How to use the framework[edit | edit source]

The Linux mailbox documentation [1] provides with a very simple example of use.

5. How to trace and debug the framework[edit | edit source]

5.1. How to trace[edit | edit source]

Dynamic debug traces can be added using the following commands:

echo -n 'file stm32-ipcc.c +p' > /sys/kernel/debug/dynamic_debug/control
echo -n 'file mailbox.c +p' > /sys/kernel/debug/dynamic_debug/control

6. Source code location[edit | edit source]

7. References[edit | edit source]