1. Article purpose[edit | edit source]
This article provides simple examples for the Developer Package of the OpenSTLinux distribution, that illustrate cross-compilation with the SDK:
- modification of software elements delivered as source code (for example the Linux kernel)
- addition of software (for example the Linux kernel module or user-space applications)
These examples also show how to deploy the results of the cross-compilation on the target, through a network connection to the host machine.
![]() |
There are many ways to achieve the same result; this article aims to provide at least one solution per example. You are free to explore other methods that are better adapted to your development constraints. |
2. Prerequisites[edit | edit source]
The prerequisites from the Cross-compile with OpenSTLinux SDK article must be executed, and the cross-compilation and deployment of any piece of software, as explained in that article, is known.
The board and the host machine are connected through an Ethernet link, and a remote terminal program is started on the host machine: see How to get Terminal.
The target is started, and its IP address (<board ip address>) is known.
![]() |
If you encounter a problem with any of the commands in this article, remember that the README.HOW_TO.txt helper files, from the Linux kernel, Optee-OS, TF-A and U-Boot installation directories, are the build references. |
![]() |
Regarding the Linux kernel examples, it is considered that the Linux kernel has been setup, configured and built a first time in a dedicated build directory (<Linux kernel build directory> later in this page) different from the source code directory (<Linux kernel source directory> later in this document). |
3. Modifying the Linux kernel configuration[edit | edit source]
3.1. Preamble[edit | edit source]
The Linux kernel configuration option that you want to modify might be used by external out-of-tree Linux kernel modules (for example the GPU kernel driver), and these should then be recompiled. These modules are, by definition, outside the kernel tree structure, and are not delivered in the Developer Package source code; it is not possible to recompile them with the Developer Package. Consequently, if the Linux kernel is reconfigured and recompiled with this option then deployed on the board, the external out-of-tree Linux kernel modules might no longer be loaded.
There are two possible situations:
- This is not a problem for the use cases on which you are currently working. In this case you can use the Developer Package to modify and recompile the Linux kernel.
- This is a problem for the use cases on which you are currently working. In this case you need to switch on the STM32MPU Distribution Package, and after having modified the Linux kernel configuration, use it to rebuild the whole image (that is, not only the Linux kernel but also the external out-of-tree Linux kernel modules).
Example:
- Let's assume that the FUNCTION_TRACER and FUNCTION_GRAPH_TRACER options are activated to install the ftrace Linux kernel feature
- This feature is used to add tracers in the whole kernel, including the external out-of-tree Linux kernel modules
- The Developer Package is used to reconfigure and recompile the Linux kernel, and to deploy it on the board
- The external out-of-tree Linux kernel modules are not recompiled. This is the case for the GPU kernel driver
- Consequently, the Linux kernel fails to load the GPU kernel driver module. However, even if the display no longer works, the Linux kernel boot succeeds, and the setup is sufficient, for example, to debug use cases involving an Ethernet or USB connection
- The Distribution Package is used to reconfigure the Linux kernel, and to rebuild and deploy the whole image on the board
- The external out-of-tree Linux kernel modules are recompiled, including the GPU kernel driver
- Consequently, the Linux kernel succeeds in loading the GPU kernel driver module. The display is available.
3.2. Simple example[edit | edit source]
This simple example modifies the value defined for the contiguous memory area (CMA) size.
- Get the current value of the CMA size through the analysis of the target boot log
dmesg | grep -i cma
Note that dmesg information provides indication regarding CMA size configuration:
- - With cma: Reserved message: the CMA size configuration is made via the kernel configuration
- - With Reserved memory: created CMA memory pool message: the CMA size configuration is declared on kernel devicetree
Thus, in our example for modifying the Linux kernel configuration, we will only consider the STM32MP135F-DK and STM32MP157F-DK2
boards.
- Go to the Linux kernel build directory
<Linux kernel build directory>cd
- Start the Linux kernel configuration menu: see Menuconfig or how to configure kernel
- Navigate to "Device Drivers - Generic Driver Options"
- select "Size in Megabytes"
- modify its value to 256
- exit and save the new configuration
- Check that the configuration file (.config) has been modified
grep -i CONFIG_CMA_SIZE_MBYTES .config
CONFIG_CMA_SIZE_MBYTES=256
- Cross-compile the Linux kernel: see Menuconfig or how to configure kernel
- Update the Linux kernel image on board: see Menuconfig or how to configure kernel
- Reboot the board: see Menuconfig or how to configure kernel
- Get the new value of the CMA size (256 Mbytes) through the analysis of the target boot log
dmesg | grep -i cma
STM32MP135F-DK ![]() |
256 MiB at 0xd8800000[ 0.000000] cma: Reserved |
STM32MP157F-DK2 ![]() |
256 MiB at 0xd9800000[ 0.000000] cma: Reserved |
4. Modifying the Linux kernel device tree[edit | edit source]
4.1. STM32MP135F-DK
and STM32MP157F-DK2
simple example[edit | edit source]
This simple example modifies the default status of a user LED.
- With the board started; check that the user green LED (LD4 for STM32MP135F-DK
, LD5 for STM32MP157F-DK2
) is disabled
- Go to the Linux kernel source directory
<Linux kernel source directory>cd
- Edit the device tree source file to add the lines highlighted below
- Go to the Linux kernel build directory
<Linux kernel build directory>cd
- Generate the device tree blobs (*.dtb) from Linux repository tree repository usage.
make dtbs
or see STM32MP257F-EV1 Evaluation board with external device tree to generate the dtb from external device
then
cp arch/<arm architecture>/boot/dts/stm32mp*.dtb install_artifact/boot/
- Update the device tree blobs on the board
<board ip address>:/boot/scp install_artifact/boot/stm32mp*.dtb root@
- Reboot the board
reboot
- Check that the user green LED (LD4 for STM32MP135F-DK
, LD5 for STM32MP157F-DK2
) is enabled (green)
4.2. STM32MP257F-EV1
simple example[edit | edit source]
This simple example modifies the value defined for the contiguous memory area (CMA) size.
- Get the current value of the CMA size through the analysis of the target boot log
dmesg | grep -i cma
Note that dmesg information provides indication regarding CMA size configuration:
- - With cma: Reserved message: the CMA size configuration is made via the kernel configuration
- - With Reserved memory: created CMA memory pool message: the CMA size configuration is declared on kernel devicetree
Thus, in our example for modifying the Linux kernel device tree, we will only consider the STM32MP257F-EV1 boards.
- Go to the Linux kernel source directory
<Linux kernel source directory>cd
- Edit the device tree source file to modify the highlighted CMA size value below
- Modify the current 128MB size to match with 256MB one: 256MB = 0x10000000
- Go to the Linux kernel build directory
<Linux kernel build directory>cd
- Generate the device tree blobs (*.dtb)
make dtbs
or see STM32MP257F-EV1 Evaluation board with external device tree to generate the dtb from external device tree
then
cp arch/<arm architecture>/boot/dts/stm32mp*.dtb install_artifact/boot/
- Update the device tree blobs on the board
<board ip address>:/boot/scp install_artifact/boot/stm32mp*.dtb root@
- Reboot the board
reboot
- Get the new value of the CMA size (256 Mbytes) through the analysis of the target boot log
dmesg | grep -i cma
STM32MP257F-EV1 ![]() |
256 MiB[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000f2800000, size |
4.3. STM32MP257F-EV1 Evaluation board
with external device tree[edit | edit source]
For compilation of external device tree (aka OSTL device tree) in the external git, linux/stm32mp257f-ev1-ca35tdcid-ostl.dts , you can add this git inside Linux® kernel tree or outside Linux® kernel tree.
4.3.1. External git inside Linux® kernel tree[edit | edit source]
https://github.com/STMicroelectronics/dt-stm32mp.git arch/arm64/boot/dts/st/external-dtgit submodule add
dtbs or make stm32mp257f-ev1-ca35tdcid-ostl.dtbmake
4.3.2. External git outside Linux® kernel tree with KBUILD_EXTDTS[edit | edit source]
https://github.com/STMicroelectronics/dt-stm32mp.git <External device tree directory>git clone
dtbs KBUILD_EXTDTS=<External device tree directory>/linux or make stm32mp257f-ev1-ca35tdcid-ostl.dtb KBUILD_EXTDTS=<External device tree directory>/linuxmake
5. Modifying a built-in Linux kernel device driver[edit | edit source]
This simple example adds unconditional log information when the display driver is probed.
- Check that there's no log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
- Go to the Linux kernel source directory
<Linux kernel source directory>cd
- Edit the ./drivers/gpu/drm/stm/drv.c source file
- Add a log information in the stm_drm_platform_probe function
DRM_INFO("Simple example - %s\n", __func__); return 0; [...] }static int stm_drm_platform_probe(struct platform_device *pdev) { struct device *dev = &pdev->dev; struct drm_device *ddev; int ret; [...]
- Go to the Linux kernel build directory
<Linux kernel build directory>cd
- Cross-compile the Linux kernel (please check the load address in the README.HOW_TO.txt helper file)
0xC2000040 cp arch/<arm architecture>/boot/${imgtarget} install_artifact/boot/[ "${ARCH}" = "arm" ] && imgtarget="uImage" || imgtarget="Image.gz" make ${imgtarget} LOADADDR=
- Update the Linux kernel image on board
<board ip address>:/boot/scp -r install_artifact/boot/* root@
- Reboot the board
reboot
- Check that there is now log information when the display driver is probed
Simple example - stm_drm_platform_probedmesg | grep -i stm_drm_platform_probe [ 2.995125] [drm]
6. Modifying/adding an external Linux kernel module[edit | edit source]
Most device drivers (modules) in the Linux kernel can be compiled either into the kernel itself (built-in/internal module) or as Loadable Kernel Modules (LKM/external module) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure).
6.1. Modifying an external in-tree Linux kernel module[edit | edit source]
This simple example adds an unconditional log information when the virtual video test driver (vivid) kernel module is probed or removed.
- Go to the Linux kernel source directory
<Linux kernel source directory>cd
- Edit the ./drivers/media/test-drivers/vivid/vivid-core.c source file
- Add log information in the vivid_probe and vivid_remove functions
pr_info("Simple example - %s\n", __func__); return ret; }static int vivid_probe(struct platform_device *pdev) { const struct font_desc *font = find_font("VGA8x16"); int ret = 0, i; [...] /* n_devs will reflect the actual number of allocated devices */ n_devs = i;
pr_info("Simple example - %s\n", __func__); }static void vivid_remove(struct platform_device *pdev) { struct vivid_dev *dev; unsigned int i, j; [...]
- Go to the Linux kernel build directory
<Linux kernel build directory>cd
- Cross-compile the Linux kernel modules
make modules
make INSTALL_MOD_PATH="./install_artifact" modules_install
- Remove the link on install_artifact/lib/modules/<kernel version>/
<kernel version>/build rm install_artifact/lib/modules/<kernel version>/sourcerm install_artifact/lib/modules/
- Optionally, strip kernel modules (to reduce the size of each kernel modules)
find . -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
- Update the vivid kernel module on the board (please check the kernel version <kernel version>)
"<kernel version>"/kernel/drivers/media/test-drivers/vivid/vivid.ko root@<board ip address>:/lib/modules/<kernel version>/kernel/drivers/media/test-drivers/vivid/scp install_artifact/lib/modules/
OR
<board ip address>:/lib/modules/scp -r install_artifact/lib/modules/* root@
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a
sync
- Insert the vivid kernel module into the Linux kernel
Simple example - vivid_probemodprobe vivid [...] [ 3412.784638]
- Remove the vivid kernel module from the Linux kernel
Simple example - vivid_removermmod vivid [...] [ 3423.708517]
6.2. Adding an external out-of-tree Linux kernel module[edit | edit source]
This simple example adds a "Hello World" external out-of-tree Linux kernel module to the Linux kernel.
- Prerequisite: the Linux source code is installed, and the Linux kernel has been cross-compiled
- Go to the working directory that contains all the source code (that is, the directory that contains the Linux kernel, Optee-OS, TF-A and U-Boot source code directories)
<tag>/sources/<arm architecture>-<distro>-linux*cd
- Export to KERNEL_SRC_PATH the path to the Linux kernel build directory that contains both the Linux kernel source code and the configuration file (.config)
<Linux kernel build directory>/export KERNEL_SRC_PATH=$PWD/
- Create a directory for this kernel module example
mkdir kernel_module_example
cd kernel_module_example
- Create the source code file for this kernel module example: kernel_module_example.c
Linux kernel module example"); MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>"); MODULE_LICENSE("GPL v2");// SPDX-identifier: GPL-2.0 /* * Copyright (C) STMicroelectronics SA 2018 * * Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com> * */ #include <linux/module.h> /* for all kernel modules */ #include <linux/kernel.h> /* for KERN_INFO */ #include <linux/init.h> /* for __init and __exit macros */ static int __init kernel_module_example_init(void) { printk(KERN_INFO "Kernel module example: hello world from STMicroelectronics\n"); return 0; } static void __exit kernel_module_example_exit(void) { printk(KERN_INFO "Kernel module example: goodbye from STMicroelectronics\n"); } module_init(kernel_module_example_init); module_exit(kernel_module_example_exit); MODULE_DESCRIPTION("STMicroelectronics simple external out-of-tree
- Create the makefile for this kernel module example: Makefile
![]() |
All the indentations in a makefile are tabulations |
Linux kernel module example # Object file(s) to be built obj-m := kernel_module_example.o # Path to the directory that contains the Linux kernel source code # and the configuration file (.config) KERNEL_DIR ?= $(KERNEL_SRC_PATH) # Path to the directory that contains the generated objects DESTDIR ?= $(KERNEL_DIR)/install_artifact # Path to the directory that contains the source file(s) to compile PWD := $(shell pwd) default: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules install: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install clean: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean# Makefile for simple external out-of-tree
- Cross-compile the kernel module example
make clean
make
make install
- Go to the Linux kernel build directory
<Linux kernel build directory>cd
- The generated kernel module example is in: install_artifact/lib/modules/"<kernel version>"/extra/kernel_module_example.ko
- Remove the link on "install_artifact/lib/modules/<kernel version>/"
<kernel version>/build rm install_artifact/lib/modules/<kernel version>/sourcerm install_artifact/lib/modules/
- Optionally, strip kernel modules (to reduce the size of each kernel modules)
find . -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
- Push this kernel module example on board (please check the kernel version "<kernel version>")
<board ip address> mkdir -p /lib/modules/"<kernel version>"/extra scp install_artifact/lib/modules/<kernel version>/extra/kernel_module_example.ko root@<board ip address>:/lib/modules/<kernel version>/extrassh root@
OR
<board ip address>:/lib/modules/scp -r install_artifact/lib/modules/* root@
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a
sync
- Insert the kernel module example into the Linux kernel
Kernel module example: hello world from STMicroelectronicsmodprobe kernel_module_example [18167.821725]
- Remove the kernel module example from the Linux kernel
Kernel module example: goodbye from STMicroelectronicsrmmod kernel_module_example [18180.086722]
7. Modifying the U-Boot[edit | edit source]
This simple example adds unconditional log information when U-Boot starts. Within the scope of the optee boot chain, U-Boot is used as second stage boot loader (SSBL).
- Have a look at the U-Boot log information when the board reboots
reboot
- Go to the U-Boot source directory
<U-Boot source directory>cd
- Edit the source file to add the lines highlighted below in the checkboard function
- Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk help
- FIP image case building
The "FIP_artifacts" folder should be specified to allow to update the FIP binary with the new U-Boot binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "FIP_DEPLOYDIR_ROOT" variable should be set as below:
FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifactsexport
Note that to keep the original FIP binary, the "FIP_DEPLOYDIR_FIP" variable should be set as below:
FIP_DEPLOYDIR_FIP=$PWD/../deploy/fipexport
- Cross-compile the U-Boot to generate FIP binary update:
make -f $PWD/../Makefile.sdk all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp15_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp157f-ev1 stm32mp157f-dk2"
make -f $PWD/../Makefile.sdk all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp13_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp135f-dk"
make -f $PWD/../Makefile.sdk all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp25_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp257f-ev1"
- Go to the directory where the compilation results are stored
FIP_DEPLOYDIR_FIPcd $
- Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot: 0
STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
![]() |
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot |
- On the host machine, check the partition associated with the secondary stage boot loader that contains the FIP binary: fip-a
sdb5ls -l /dev/disk/by-partlabel/ | grep 'fip-a' lrwxrwxrwx 1 root root 10 Feb 8 08:57 fip-a -> ../../
- Copy the FIP binary to the dedicated partition
fip-<device tree>-<boot chain mode>.bin of=/dev/sdb5 bs=1M conv=fdatasyncdd if=
![]() |
In case you get a permission denied you can set more permission on /dev/sdb5:
sudo chmod 777 /dev/sdb5
|
- Reset the U-Boot shell: in the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset
- Have a look at the new U-Boot log information when the board reboots
8. Modifying the TF-A[edit | edit source]
8.1. TF-A modification example[edit | edit source]
This simple example adds unconditional log information when the TF-A starts. Within the scope of the optee boot chain, TF-A is used as first stage boot loader (FSBL).
- Have a look at the TF-A log information when the board reboots
reboot
- Go to the TF-A source directory
<TF-A source directory>cd
- Edit the source file to add the lines highlighted below in the print_reset_reason function
- Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk help
![]() |
According to the modification done on TF-A source code, both TF-A FSBL and FIP binaries may need to be updated. You will find below the steps to follow for both update |
8.2. TF-A image case building[edit | edit source]
- Cross-compile the TF-A:
make -f $PWD/../Makefile.sdk TF_A_DEVICETREE="stm32mp157f-ev1 stm32mp157f-dk2" TF_A_CONFIG="optee-sdcard" stm32
make -f $PWD/../Makefile.sdk TF_A_DEVICETREE="stm32mp135f-dk" TF_A_CONFIG="optee-sdcard" stm32
make -f $PWD/../Makefile.sdk TF_A_DEVICETREE="stm32mp257f-ev1" TF_A_CONFIG="optee-sdcard" stm32
- Go to the directory in which the compilation results are stored
cd ../deploy
- Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot: 0
STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
![]() |
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot |
- On the host machine, check the FSBL partition associated with the first stage boot loader
ls -l /dev/disk/by-partlabel/ | grep fsbl
Note that there are two FSBL partitions to ensure first stage boot loader binary backup.
- Copy the TF-A binary to the dedicated partition; to test the new TF-A binary, it might be useful to keep the old TF-A binary in the backup FSBL (fsbl2 or fsbla2)
tf-a-<device tree>-sdcard.stm32 of=/dev/sdb1 bs=1M conv=fdatasyncdd if=
![]() |
In case you get a permission denied you can set more permission on /dev/sdb1 :
sudo chmod 777 /dev/sdb1
|
- Reset the U-Boot shell: in the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset
8.3. FIP image case building[edit | edit source]
The "FIP_artifacts" folder should be specified to allow to update the FIP binary with the new U-Boot binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "FIP_DEPLOYDIR_ROOT" var should be set as below:
FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifactsexport
Note that to keep the original FIP binary, the "FIP_DEPLOYDIR_FIP" var should be set as below:
FIP_DEPLOYDIR_FIP=$PWD/../deploy/fipexport
- Cross-compile the TF-A to generate FIP binary update:
make -f $PWD/../Makefile.sdk TF_A_DEVICETREE="stm32mp157f-ev1 stm32mp157f-dk2" TF_A_CONFIG="optee-sdcard" fip
make -f $PWD/../Makefile.sdk TF_A_DEVICETREE="stm32mp135f-dk" TF_A_CONFIG="optee-sdcard" fip
make -f $PWD/../Makefile.sdk TF_A_DEVICETREE="stm32mp257f-ev1" TF_A_CONFIG="optee-sdcard" fip
- Go to the directory in which the compilation results are stored
FIP_DEPLOYDIR_FIPcd $
- Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot: 0
STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
![]() |
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot |
- On the host machine, check the partition associated with the secondary stage boot loader that contains the FIP binary: fip-a
sdb5ls -l /dev/disk/by-partlabel/ | grep 'fip-a' lrwxrwxrwx 1 root root 10 Feb 8 08:57 fip-a -> ../../
- Copy the FIP binary to the dedicated partition
fip-<device tree>-<boot chain mode>.bin of=/dev/sdb5 bs=1M conv=fdatasyncdd if=
![]() |
In case you get a permission denied you can set more permission on /dev/sdb5:
sudo chmod 777 /dev/sdb5
|
- Reset the U-Boot shell: In the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset
8.4. TF-A modification results[edit | edit source]
- Have a look at the new TF-A log information when the board reboots
9. Modifying the OP-TEE OS[edit | edit source]
This simple example adds unconditional log information when the OP-TEE OS starts.
- Have a look at the OP-TEE OS log information when the board reboots
DTB found I/TC: OP-TEE version: <OP-TEE OS version> (gcc version <GCC version>) [...] I/TC: WARNING: This OP-TEE configuration might be insecure! [...]reboot [...] I/TC: Embedded
- Go to the OP-TEE OS source directory
<OP-TEE OS source directory>cd
- Edit the ./core/arch/arm/kernel/boot.c source file to add the lines highlighted below in the __weak boot_init_primary_late function
OP-TEE version: %s", core_v_str); IMSG("OP-TEE OS simple example"); [...] }void __weak boot_init_primary_late(unsigned long fdt, unsigned long manifest) { init_external_dt(fdt); [...] IMSG("
- Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk help
- FIP images case building
The "FIP_artifacts" folder should be specified to allow to update the FIP binary with the new U-Boot binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "FIP_DEPLOYDIR_ROOT" var should be set as below:
FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifactsexport
Note that to keep the original FIP binary, the "FIP_DEPLOYDIR_FIP" var should be set as below:
FIP_DEPLOYDIR_FIP=$PWD/../deploy/fipexport
- Cross-compile the OP-TEE OS to generate FIP binary update:
DTB_SOURCE_FILE="stm32mp157F-ev1 stm32mp157f-dk2"make -f $PWD/../Makefile.sdk all OPTEE_CONFIG=optee CFG_EMBED_
DTB_SOURCE_FILE="stm32mp135f-dk"make -f $PWD/../Makefile.sdk all OPTEE_CONFIG=optee CFG_EMBED_
DTB_SOURCE_FILE="stm32mp257f-ev1"make -f $PWD/../Makefile.sdk all OPTEE_CONFIG=optee CFG_EMBED_
- Go to the directory where the compilation results are stored
FIP_DEPLOYDIR_FIPcd $
- Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot: 0
STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
![]() |
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot |
- On the host machine, check the partition associated with the secondary stage boot loader that contains the FIP binary: fip-a
fip-a -> ../../sdb5ls -l /dev/disk/by-partlabel/ | grep 'fip-a' lrwxrwxrwx 1 root root 10 Feb 8 08:57
- Copy the FIP binary to the dedicated partition
fip-<device tree>-<boot chain mode>.bin of=/dev/sdb5 bs=1M conv=fdatasyncdd if=
![]() |
In case you get a permission denied you can set more permission on /dev/sdb5:
sudo chmod 777 /dev/sdb5
|
- Reset the U-Boot shell: In the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset
- Have a look at the new OP-TEE OS log information when the board reboots
DTB found I/TC: OP-TEE version: <OP-TEE OS version> (gcc version <GCC version>) [...] I/TC: OP-TEE OS simple example I/TC: WARNING: This OP-TEE configuration might be insecure! [...][...] I/TC: Embedded
10. Adding a "hello world" user space example[edit | edit source]
Thanks to the OpenSTLinux SDK, it is easy to develop a project outside of the OpenEmbedded build system. This chapter shows how to compile and execute a simple "hello world" example.
10.1. Source code file[edit | edit source]
- Go to the working directory that contains all the source codes (i.e. directory that contains the Linux kernel, Optee-os, TF-A and U-Boot source code directories)
<tag>/sources/<arm architecture>-<distro>-linux*cd
- Create a directory for this user space example
mkdir hello_world_example
cd hello_world_example
- Create the source code file for this user space example: hello_world_example.c
// SPDX-identifier: GPL-2.0
/*
* Copyright (C) STMicroelectronics SA 2018
*
* Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com>
*
*/
#include <stdio.h>
#include <unistd.h>
int main(int argc, char **argv)
{
int i =11;
printf("\nUser space example: hello world from STMicroelectronics\n");
setbuf(stdout,NULL);
while (i--) {
printf("%i ", i);
sleep(1);
}
printf("\nUser space example: goodbye from STMicroelectronics\n");
return(0);
}
10.2. Cross-compilation[edit | edit source]
Three ways to use the OpenSTLinux SDK to cross-compile this user space example are proposed below: (1) command line (2) makefile-based project (3) autotools-based project.
10.2.1. Command line[edit | edit source]
This method allows quick cross-compilation of a single-source code file. It applies if the project has only one file.
The cross-development toolchain is associated with the sysroot that contains the header files and libraries needed for generating binaries that run on the target architecture (see SDK for OpenSTLinux distribution#Native and target sysroots).
The sysroot location is specified with the --sysroot option.
The sysroot location must be specified using the --sysroot option. The CC environment variable created by the SDK already includes the --sysroot option that points to the SDK sysroot location.
<SDK installation directory>/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabiecho $CC arm-ostl-linux-gnueabi-gcc -march=armv7ve -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=
- Create the directory in which the generated binary is to be stored
mkdir -p install_artifact install_artifact/usr install_artifact/usr/local install_artifact/usr/local/bin
- Cross-compile the single source code file for the user space example
$CC hello_world_example.c -o ./install_artifact/usr/local/bin/hello_world_example
10.2.2. Makefile-based project[edit | edit source]
For this method, the cross-toolchain environment variables established by running the cross-toolchain environment setup script are subject to general make rules.
For example, see the following environment variables:
<SDK installation directory>/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi echo $CFLAGS -O2 -pipe -g -feliminate-unused-debug-types echo $LDFLAGS -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed echo $LD arm-ostl-linux-gnueabi-ld --sysroot=<SDK installation directory>/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabiecho $CC arm-ostl-linux-gnueabi-gcc -march=armv7ve -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=
- Create the makefile for this user space example: Makefile
![]() |
All the indentations in a makefile are tabulations |
PROG = hello_world_example
SRCS = hello_world_example.c
OBJS = $(SRCS:.c=.o)
CLEANFILES = $(PROG)
INSTALL_DIR = ./install_artifact/usr/local/bin
# Add / change option in CFLAGS if needed
# CFLAGS += <new option>
$(PROG): $(OBJS)
$(CC) $(CFLAGS) -o $(PROG) $(OBJS)
.c.o:
$(CC) $(CFLAGS) -c $< -o $@
all: $(PROG)
clean:
rm -f $(CLEANFILES) $(patsubst %.c,%.o, $(SRCS)) *~
install: $(PROG)
mkdir -p $(INSTALL_DIR)
install $(PROG) $(INSTALL_DIR)
- Cross-compile the project
make
make install
10.2.3. Autotools-based project[edit | edit source]
This method creates a project based on GNU autotools.
- Create the makefile for this user space example: Makefile.am
bin_PROGRAMS = hello_world_example
hello_world_example_SOURCES = hello_world_example.c
- Create the configuration file for this user space example: configure.ac
AC_INIT(hello_world_example,0.1)
AM_INIT_AUTOMAKE([foreign])
AC_PROG_CC
AC_PROG_INSTALL
AC_OUTPUT(Makefile)
- Generate the local aclocal.m4 files and create the configure script
aclocal
autoconf
- Generate the files needed by GNU coding standards (for compliance)
touch NEWS README AUTHORS ChangeLog
- Generate the links towards SDK scripts
automake -a
- Cross-compile the project
./configure ${CONFIGURE_FLAGS}
make
make install DESTDIR=./install_artifact
10.3. Deploy and execute on board[edit | edit source]
- Check that the generated binary for this user space example is in: ./install_artifact/usr/local/bin/hello_world_example
- Push this binary onto the board
scp -r install_artifact/* root@<board ip address>:/
- Execute this user space example
User space example: hello world from STMicroelectronics 10 9 8 7 6 5 4 3 2 1 0 User space example: goodbye from STMicroelectronicscd /usr/local/bin ./hello_world_example