STM32PRGFW-UTIL release note

Revision as of 14:12, 12 September 2024 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

The STM32PRGFW-UTIL is an STMicroelectronics original initiative to manage the One-time Programmable (OTP) memories and also supports STPMIC programming.

More information can be found in the detailed release notes referenced later in this article.

1. STM32PRGFW-UTIL - version 1.1.0.rc6[edit source]

Warning white.png Warning
It is mandatory to use STM32PRGFW-UTIL version 1.1.0.rc6 and above, to avoid bricking of your device.
Info white.png Information
This new version has some dependencies with STM32CubeIDE 1.16.0.24w19 (at least) and STM32CubeProgrammer v2.17.0-A02 minimum (at least) , it is then highly recommended to update also those 2 other ST tools
STM32PRGFW-UTIL for Linux® and Windows® host PC
Download

Version 1.1.0.rc6

  • STM32PRGFW-UTIL firmware package is available here .
Installing the STM32PRGFW-UTIL
  • To use STM32PRGFW-UTIL, unzip the package on computer..
  • Then refer to READMED.md , to use this tool .
Detailed release note
  • Full details about the content of this tool release are available here .