Last edited 9 months ago

How to modify the panel backlight: Difference between revisions


Latest revision as of 09:41, 8 October 2024



First identify the backlight device linked to your panel, thanks to the sysfs:

ls /sys/class/backlight
5a000000.dsi.0

In the above example, there is a single entry named "5a000000.dsi.0", which is replaced by "*" in the below command.


To adjust the panel backlight, enter the following command:

echo 32 > /sys/class/backlight/*/brightness    # set the dsi panel backlight to the value 32

Note: Only values between 0 and max_brightness must be used.

To get the maximum panel backlight value, enter:

cat /sys/class/backlight/*/max_brightness
255

To get the actual panel backlight value, enter:

cat /sys/class/backlight/*/actual_brightness
32


Use one of the following commands to quickly test the panel backlight:

export bl=/sys/class/backlight/5a000000.dsi.0/brightness
export max=/sys/class/backlight/5a000000.dsi.0/max_brightness

# switch on/off test
(while true; do echo 0 > $bl; sleep 0.5; echo $max > $bl; sleep 0.5; done)

# slow 32-step tests (only for pwm-based backlights)
(i=0; while true; do i=$(((i+32)%256)); echo $i > $bl; sleep 0.5; done)

# fast 1-step test  (only for pwm-based backlights)
(i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done)