Last edited 9 months ago

STM32MP13 SRAM internal memory: Difference between revisions


Latest revision as of 16:22, 7 October 2024



1. Article purpose[edit | edit source]

The purpose of this article is to:

  • briefly introduce the SRAM internal memory peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit | edit source]

The SRAM peripheral is 32-Kbyte wide, split into three separate banks:

  • SRAM1 (16 Kbytes)
  • SRAM2 (8 Kbytes)
  • SRAM3 (8 Kbytes)

Those banks have individual security control (see security support in the runtime assignment table below) and automatic clock gating (for power management optimization), but they are not supplied when the system goes to Standby low power mode, so their content is lost in that case.

Refer to the STM32MP13 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit | edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit | edit source]

3.1.1. On STM32MP13x lines More info.png[edit | edit source]

The ROM code uses:

  • the SRAM1 and SRAM2 to store internal data
  • the SRAM3 to store the FSBL header

This ROM code mapping strategy aims to leave the whole SYSRAM internal memory free for FSBL binary loading then execution.

The TF-A BL2 uses:

  • the SRAM1 to store boot NAND 4kB scratch buffer
  • the SRAM2 to store MbedTLS in case of secure boot
  • the SRAM3 to store fw-config DT


Click on How to.png to expand or collapse the legend...

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
nonsecure
(U-Boot)
Core/RAM SRAM Any instance SRAM first used by ROM code, then TF-A BL2. After assignment free to user

3.2. Runtime assignment[edit | edit source]

3.2.1. On STM32MP13x lines More info.png[edit | edit source]

Click on How to.png to expand or collapse the legend...

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
nonsecure
(Linux)
Core/RAM SRAM SRAM1 Assignment (between A7 S and A7 NS)
SRAM2 Assignment (between A7 S and A7 NS)
SRAM3 Assignment (between A7 S and A7 NS)

4. Software frameworks and drivers[edit | edit source]

Below are listed the software frameworks and drivers managing the XXX peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit | edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.