Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 12: | Line 12: | ||
=== Install sources === | === Install sources === | ||
==== From the Developer package ==== | ==== From the Developer package ==== | ||
The Developer Package contains OpenSTLinux and TF-A sources: [[STM32MP1_Developer_Package# | The Developer Package contains OpenSTLinux and TF-A sources: [[STM32MP1_Developer_Package#Installing_the_OpenSTLinux_BSP_packages|TF-A Installation]] | ||
==== Official source tree ==== | ==== Official source tree ==== |
Revision as of 18:03, 26 October 2022
1. Article purpose[edit | edit source]
This section details the TF-A BL2 stage (Trusted Firmware-A Boot Loader stage 2) used as FSBL (First Stage Boot Loader).
It explains how to configure and build BL2 in STM32 MPU context, describes the build process from sources, and shows how to deploy it on your target.
2. Source code access and build process[edit | edit source]
2.1. Cross compilation[edit | edit source]
Cross compilation of TF-A BL2 is only required if it needs to be modified.
Refer to Setup Cross compile environment.
The build process creates an STM32 image. This binary is built in a single step during the build process.
2.2. Install sources[edit | edit source]
2.2.1. From the Developer package[edit | edit source]
The Developer Package contains OpenSTLinux and TF-A sources: TF-A Installation
2.2.2. Official source tree[edit | edit source]
Download the source code from the official Trusted Firmware-A git repository.
https://git.trustedfirmware.org/TF-A/trusted-firmware-a.gitgit clone
For a full-featured software, go to STMicroelectronics github:
https://github.com/STMicroelectronics/arm-trusted-firmware.gitgit clone
2.2.3. Distribution Package[edit | edit source]
It is possible to use the distribution package to download and rebuid TF-A BL2
2.3. Build process[edit | edit source]
2.3.1. TF-A Build flags[edit | edit source]
Generic build flags for TF-A are described in the Build Options page of the official TF-A documentation[1].
Specific STM32MP1 platform flags can be found in the build instruction chapter of the official TF-A documentation [2] and in STMicroelectronics TF-A repository: docs/plat/stm32mp1.rst
Other optional flags:
- STM32MP_FORCE_MTD_START_OFFSET = <value>: overrides the default start offset to read FIP on MTD devices (need to be aligned with FlashLayout).
2.4. Build command[edit | edit source]
2.4.1. Build command details[edit | edit source]
The BL2 generation depends on the selected storage device. By default, only one storage device is supported.
:
Then compile the TF-A BL2.
For example, default build command for STM32MP15 is:
DTB_FILE_NAME=<board_name>.dtbmake ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \ <Selected storage> STM32MP15=1
Example with sdcard:
STM32MP_SDMMC=1 \ STM32MP15=1 DTB_FILE_NAME=stm32mp157c-ev1.dtbmake ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1
Replace STM32MP_SDMMC with the chosen device.
2.4.2. Secure boot support[edit | edit source]
To enable secure boot, you have to add TRUSTED_BOARD_BOOT=1 flag:
Example with secure boot on stm32mp135f-dk:
MBEDTLS_DIR=<path_to_mbedtls_directory> make ARM_ARCH_MAJOR=7 \ ARCH=aarch32 PLAT=stm32mp1 STM32MP_SDMMC=1 TRUSTED_BOARD_BOOT=1 \ STM32MP13=1 DTB_FILE_NAME=stm32mp135f-dk.dtb
To enable secure boot with encryption support, you have to add DECRYPTION_SUPPORT=aes_gcm with the ENCRYPT_BLx to specify the encrypted binary.
Example with encrypted BL32 on stm32mp135f-dk:
MBEDTLS_DIR=<path_to_mbedtls_directory> make ARM_ARCH_MAJOR=7 \ ARCH=aarch32 PLAT=stm32mp1 STM32MP_SDMMC=1 TRUSTED_BOARD_BOOT=1 \ ENCRYPT_BL32=1 DECRYPTION_SUPPORT=aes_gcm \ STM32MP13=1 DTB_FILE_NAME=stm32mp135f-dk.dtb
2.4.3. Troubleshooting[edit | edit source]
If you use developer package SDK, you have to unset these flags:
unset LDFLAGS;
unset CFLAGS;
2.5. Final image[edit | edit source]
The final image is available for Flash memory or SDCard update in the corresponding folder:
<BUILD_PLAT>/tf-a-<board>.stm32
Ex:
build/release/tf-a-stm32mp157c-ev1.stm32
3. Updating the software on board[edit | edit source]
3.1. Partitioning of binaries[edit | edit source]
The TF-A build provides a binary named tf-a-<board>.stm32 that MUST be copied to a dedicated partition named "fsblX" (X depends on the number of needed backups in the Flash).
3.2. Updating via SDCard[edit | edit source]
If you use an SDCard, simply update TF-A using the dd command on your host.
Plug your SDCard into the computer and copy the binary to the dedicated partition; on an SDCard/USB disk the "fsbl1" partition is partition 1:
- SDCard: /dev/mmcblkXp1 (where X is the instance number)
- SDCard via USB reader: /dev/sdX1 (where X is the instance number)
- Under Linux®
dd if=<tf-a file>.stm32 of=/dev/<device partition> bs=1M conv=fdatasync
- Under Windows®
CoreUtils [3] that includes the dd command is available for Windows.
3.3. Updating via USB mass storage on U-boot[edit | edit source]
See How to use USB mass storage in U-Boot.
Refer to the previous section to put tf-a-<board>.stm32 into SDCard/USB disk.
3.4. Updating your boot device via STM32CubeProgrammer[edit | edit source]
Refer to the STM32CubeProgrammer documentation to update your target.
- ↑ Unsupported domain!
- ↑ Unsupported domain!
- ↑ http://gnuwin32.sourceforge.net/packages/coreutils.htm