deleted>Frq08988 m (moved Linux directory structure to OpenSTLinux directory structure: Dedicated to OpenSTLinux) |
Registered User mNo edit summary |
||
(41 intermediate revisions by 7 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
{{ | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
}} | |||
<noinclude></noinclude> | |||
This article aims at presenting, '''as example''', the directory structure of the Linux root file system available on STM32 board. | |||
[[ | All files and directories are located under the root directory (''/''), in compliance with the [[File Hierarchy Standard (FHS)|File system Hierarchy Standard]]. | ||
This | This root directory corresponds to the Linux root file system (rootfs partition), as defined in [[STM32 MPU Flash mapping#Flash partitions|Flash partitions]]. Note also that the user file system (userfs partition), the boot file system (bootfs partition) and the vendor file system (vendorfs partition) can be accessed through the ''/usr/local'' mounting point, through the ''/boot'' mounting point, and through the ''/vendor'' mounting point respectively. | ||
{{info|In practice, this article uses the release '''STM32MP15-Ecosystem-{{EcosystemRelease/Revision | revision=6.1.0}}''' for the STM32MPU Embedded Software distribution as an example to illustrate the Linux directory structure. If you are using a different release, the names of the directories and files might differ.}}{{UpdateNeededForNewRelease|The trees below shall be updated periodically, even if the information banner specifies that they might not be up-to-date}} | |||
The directories are shown in {{STLightGreen|green}}, while the files are in black. | |||
{{ | |||
{{STLightGreen|/}} {{Highlight|'''Root directory (rootfs partition)'''}} | |||
├── {{STLightGreen|bin}} {{Highlight|Essential user binaries (e.g. ''/bin/cat'', ''/bin/ls'', ''/bin/cp''...)}} | |||
{{ | |||
├── {{ | |||
│ └── [...] | │ └── [...] | ||
├── {{ | ├── {{STLightGreen|boot}} {{Highlight|Mounting point for the boot file system (bootfs partition): see below}} | ||
├── {{ | ├── {{STLightGreen|dev}} {{Highlight|Device files (e.g. ''/dev/null'', ''/dev/tty0'', ''/dev/video0''...)}} | ||
├── {{STLightGreen|etc}} {{Highlight|System-wide configuration files (e.g. ''/etc/xdg/weston/weston.ini'' Weston configuration file...)}} | |||
├── {{ | ├── {{STLightGreen|home}} {{Highlight|Users' home directories (containing saved files, personal settings...)}} | ||
├── {{ | ├── {{STLightGreen|lib}} {{Highlight|Essential system libraries for the binaries in ''/bin'' and ''/sbin'' (e.g. ''libncurses.so.*''...)}} | ||
├── {{ | │ ├── {{STLightGreen|modules}} | ||
│ ├── {{ | │ │ └── ''{{STLightGreen|{{EcosystemRelease/Component | revision=latest | component=Linux kernel | name=release}}}}'' {{Highlight|The directory name is the linux version (i.e. {{EcosystemRelease/Component | revision=latest | component=Linux kernel | name=release}})}} | ||
│ │ └── {{ | │ │ ├── {{STLightGreen|kernel}} {{Highlight|Linux kernel modules}} | ||
│ │ ├── {{ | |||
│ │ │ └── [...] | │ │ │ └── [...] | ||
│ │ ├── modules.dep {{Highlight|List of module dependencies (generated by ''depmod'')}} | │ │ ├── modules.dep {{Highlight|List of module dependencies (generated by ''depmod'')}} | ||
│ │ └── [...] | │ │ └── [...] | ||
│ └── [...] | │ └── [...] | ||
├── {{ | ├── {{STLightGreen|lost+found}} | ||
├── {{ | ├── {{STLightGreen|media}} {{Highlight|Mount points for removable media devices}} | ||
├── {{STLightGreen|mnt}} {{Highlight|Temporarily mounted file systems}} | |||
├── {{ | ├── {{STLightGreen|proc}} {{Highlight|[[Pseudo filesystem|Pseudo filesystem]] providing process and kernel information as files (e.g. ''/proc/cpuinfo'', ''/proc/version''...)}} | ||
├── {{ | ├── {{STLightGreen|root}} {{Highlight|Home directory for the root user)}} | ||
├── {{ | ├── {{STLightGreen|run}} {{Highlight|Run-time variable data (information about the running system since last boot)}} | ||
├── {{ | ├── {{STLightGreen|sbin}} {{Highlight|Essential system binaries (e.g. ''/sbin/fsck'', ''/sbin/init'', ''/sbin/modprobe''...)}} | ||
├── {{ | ├── {{STLightGreen|sys}} {{Highlight|Information about devices, drivers, and some kernel features (e.g. ''/sys/kernel/debug'' aka''debgufs''...)}} | ||
├── {{ | ├── {{STLightGreen|tmp}} {{Highlight|Temporary files}} | ||
├── {{ | ├── {{STLightGreen|usr}} {{Highlight|User utilities and applications}} | ||
│ ├── {{ | │ ├── {{STLightGreen|bin}} {{Highlight|Non-essential user binaries (e.g. ''/usr/bin/lsusb'', ''/usr/bin/weston''...)}} | ||
│ ├── {{ | │ ├── {{STLightGreen|lib}} {{Highlight|Non-essential system libraries for the binaries in ''/usr/bin'' and ''/usr/sbin''}} | ||
│ ├── {{ | │ ├── {{STLightGreen|local}} {{Highlight|Mounting point for the user file system (userfs partition): see below}} | ||
│ ├── {{ | │ ├── {{STLightGreen|sbin}} {{Highlight|Non-essential system binaries (e.g. ''/usr/sbin/alsactl'', ''/usr/sbin/weston.sh''...)}} | ||
│ ├── {{ | │ ├── {{STLightGreen|share}} {{Highlight|Architecture-independent (shared) data}} | ||
│ └── [...] | │ └── [...] | ||
├── {{STLightGreen|var}} {{Highlight|Variable files}} | |||
└── {{STLightGreen|vendor}} {{Highlight|Mounting point for the vendor file system (vendorfs partition): see below}} | |||
* Boot file system mounting point | * Boot file system mounting point | ||
{{ | {{STLightGreen|/boot}} {{Highlight|'''bootfs partition'''}} | ||
├── | ├── stm32{{HighlightParam|<soc>}}-dk[*].dtb {{Highlight|Linux kernel device tree blob files for discovery board(s)}} | ||
├── | ├── stm32{{HighlightParam|<soc>}}-ev[*].dtb {{Highlight|Linux kernel device tree blob files for evaluation board(s)}} | ||
├── uImage | ├── [...] | ||
├── uImage {{Highlight|Linux kernel binary image file (with U-Boot wrapper)}} | |||
└── [...] | └── [...] | ||
* User file system mounting point | * User file system mounting point | ||
{{ | {{STLightGreen|/usr/local}} {{Highlight|'''userfs partition'''}} | ||
├── {{ | ├── {{STLightGreen|Cube-{{HighlightParam|[M4|M33]}}-examples}} {{Highlight|Examples for M4 {{HighlightParam|(STM32CubeMP1)}} Package or M33 {{HighlightParam|(STM32CubeMP2)}} running on Arm<sup>®</sup> Cortex<sup>®</sup>M}} | ||
│ ├── {{ | │ ├── {{STLightGreen|STM32MP{{HighlightParam|<soc>}}-DK}} {{Highlight|Examples of firmwares running on Arm Cortex-M4 or Cortex-M33 }} | ||
│ │ ├── {{ | │ │ ├── {{STLightGreen|Applications}} | ||
│ │ │ ├── | │ │ │ ├── {{STLightGreen|<Applications Name>}} | ||
│ │ │ ├── {{ | │ │ | | ├── {{STLightGreen|<Application Name>}} {{Highlight|OpenAMP TTY echo application}} | ||
│ │ │ │ └── {{ | │ │ │ | | ├── <script name>.sh {{Highlight|Script to start/stop this application}} | ||
│ │ │ │ └── | │ │ │ | | ├── {{STLightGreen|lib}} | ||
│ │ │ └── README | │ │ │ | | │ └── {{STLightGreen|firmware}} | ||
│ │ | │ │ │ | | │ └── <Application Name>.elf {{Highlight|Firmware for this application}} | ||
│ │ │ | | └── README {{Highlight|Helper file for this application}} | |||
│ │ │ ├── {{ | │ │ │ │ └── [...] {{Highlight|Others applications with the same structure (script, helper file and firmware)}} | ||
│ │ │ │ └── {{ | │ │ │ └── [...] {{Highlight|Others applications with the same structure (script, helper file and firmware)}} | ||
│ │ │ | │ │ ├── {{STLightGreen|Demonstrations}} | ||
│ │ │ ├── {{STLightGreen|AI_Character_Recognition}} {{Highlight|Artificial intelligence character recognition demonstration}} | |||
│ | │ │ │ └── {{STLightGreen|lib}} | ||
│ │ | │ │ │ └── {{STLightGreen|firmware}} | ||
│ │ | │ │ │ └── AI_Character_Recognition.elf {{Highlight|Firmware for this demonstration}} | ||
│ | . . . | ||
│ │ │ | . . . | ||
│ | . . . | ||
{{ReviewsComments|-- [[User:Jean Christophe Trotin|Jean Christophe Trotin]] ([[User talk:Jean Christophe Trotin|talk]]) 15:51, 10 June 2025 (CEST)<br />The following directory shall either only be present for the boards of the STM32MP1 series, or be named "Linux-A7-examples" for the boards of the STM32MP1 series and "Linux-A35-examples" for the boards of the STM32MP2 series.}} | |||
├── {{STLightGreen|Linux-A7-examples}} {{Highlight|Examples for Linux<sup>®</sup> running on Arm<sup>®</sup> Cortex<sup>®</sup>-A7}} | |||
│ ├── {{STLightGreen|GPIO}} {{Highlight|GPIO examples}} | |||
│ │ ├── {{STLightGreen|buttons}} | |||
│ │ │ ├── button_gpio_exti.sh {{Highlight|Script for this example}} | |||
│ │ | └── README.md {{Highlight|Helper file for this example}} | |||
│ │ └── {{STLightGreen|leds}} {{Highlight|Same structure for this example relative to the leds}} | |||
│ │ └── [...] | |||
│ └── [...] {{Highlight|Same structure for all the examples}} | |||
├── {{STLightGreen|demo}} {{Highlight|All files needed (e.g. Python scripts, pictures, media files...) for the GTK demo launcher}} | |||
│ └── [...] | |||
├── {{STLightGreen|lost+found}} | |||
└── {{STLightGreen|weston-start-at-startup}} | |||
└── start_up_demo_launcher.sh {{Highlight|Script to start the GTK demo launcher}} | |||
* Vendor file system mounting point | |||
{{STLightGreen|/vendor}} {{Highlight|'''vendorfs partition'''}} | |||
├── [*].so {{Highlight|Specific vendor libraries (e.g. Vivante libraries OpenGL ES, OpenVG and EGL)}} | |||
└── [...] | |||
<noinclude> | |||
[[Category:OpenSTLinux filesystem]] | |||
{{PublicationRequestId | 7653 | 2018-06-11 | AnneJ}} | |||
</noinclude> | |||
Latest revision as of 14:10, 30 June 2025
This article aims at presenting, as example, the directory structure of the Linux root file system available on STM32 board.
All files and directories are located under the root directory (/), in compliance with the File system Hierarchy Standard.
This root directory corresponds to the Linux root file system (rootfs partition), as defined in Flash partitions. Note also that the user file system (userfs partition), the boot file system (bootfs partition) and the vendor file system (vendorfs partition) can be accessed through the /usr/local mounting point, through the /boot mounting point, and through the /vendor mounting point respectively.
Template:InfoTemplate:UpdateNeededForNewRelease
The directories are shown in green, while the files are in black.
/ Template:Highlight ├── bin Template:Highlight │ └── [...] ├── boot Template:Highlight ├── dev Template:Highlight ├── etc Template:Highlight ├── home Template:Highlight ├── lib Template:Highlight │ ├── modules │ │ └── 6.6.78 Template:Highlight │ │ ├── kernel Template:Highlight │ │ │ └── [...] │ │ ├── modules.dep Template:Highlight │ │ └── [...] │ └── [...] ├── lost+found ├── media Template:Highlight ├── mnt Template:Highlight ├── proc Template:Highlight ├── root Template:Highlight ├── run Template:Highlight ├── sbin Template:Highlight ├── sys Template:Highlight ├── tmp Template:Highlight ├── usr Template:Highlight │ ├── bin Template:Highlight │ ├── lib Template:Highlight │ ├── local Template:Highlight │ ├── sbin Template:Highlight │ ├── share Template:Highlight │ └── [...] ├── var Template:Highlight └── vendor Template:Highlight
- Boot file system mounting point
/boot Template:Highlight ├── stm32<soc>-dk[*].dtb Template:Highlight ├── stm32<soc>-ev[*].dtb Template:Highlight ├── [...] ├── uImage Template:Highlight └── [...]
- User file system mounting point
/usr/local Template:Highlight ├── Cube-[M4|M33]-examples Template:Highlight │ ├── STM32MP<soc>-DK Template:Highlight │ │ ├── Applications │ │ │ ├── <Applications Name> │ │ | | ├── <Application Name> Template:Highlight │ │ │ | | ├── <script name>.sh Template:Highlight │ │ │ | | ├── lib │ │ │ | | │ └── firmware │ │ │ | | │ └── <Application Name>.elf Template:Highlight │ │ │ | | └── README Template:Highlight │ │ │ │ └── [...] Template:Highlight │ │ │ └── [...] Template:Highlight │ │ ├── Demonstrations │ │ │ ├── AI_Character_Recognition Template:Highlight │ │ │ └── lib │ │ │ └── firmware │ │ │ └── AI_Character_Recognition.elf Template:Highlight . . . . . . . . .
Linux-A7-examples Template:Highlight │ ├── GPIO Template:Highlight │ │ ├── buttons │ │ │ ├── button_gpio_exti.sh Template:Highlight │ │ | └── README.md Template:Highlight │ │ └── leds Template:Highlight │ │ └── [...] │ └── [...] Template:Highlight ├── demo Template:Highlight │ └── [...] ├── lost+found └── weston-start-at-startup └── start_up_demo_launcher.sh Template:Highlight├──
- Vendor file system mounting point
/vendor Template:Highlight ├── [*].so Template:Highlight └── [...]