Last edited 6 months ago

STM32MP1 power overview: Difference between revisions


Latest revision as of 11:19, 20 January 2025


This article gives information about the support power management in OpenSTlinux for STM32MP1 series.

1. Framework purpose[edit | edit source]

The purpose of this article is to explain how OpenSTlinux components handle the STM32MP1 series power management:

  • Software overview
  • Peripheral power support
  • Low-power modes available on the device

See also the page How to define your low-power strategy.

2. Software overview[edit | edit source]

Power mgt.png

The system power request is handled with the PSCI support and OP-TEE.

The power requests associated to each device (clock, regulator, operation point) are consolidated by the Linux frameworks, and can be handled by a Linux driver or by OP-TEE through SCMI requests.


2.1. Component description[edit | edit source]

The OpenSTLinux components for low-power modes are:

Nonsecure world (Linux):

  • Power management frameworks: See Power overview for details
  • PSCI library: this is a set of standardized functions to request a low-power service to the secure monitor.
  • SCMI drivers: driver for system resources (clock, regulators, power domain,...), exposed by OP-TEE with SCMI protocol.
  • Device driver: any peripheral driver which needs to control power.
    • RCC driver for clock and reset managed by nonsecure world.

Secure monitor and secure world components (OP-TEE):

  • Low-power driver: the role of this driver is to choose the low-power mode according to the programmed wake-up source(s).
  • PWR driver: this driver is responsible for configuring the low-power mode.
  • RCC driver: this driver handles the circuit secure clocks.
  • PSCI libray: generic PSCI stack.

STM32 peripherals (hardware):

2.2. API description[edit | edit source]

The OpenSTLinux power management support is based on Arm® interface specifications:

  • Power state coordination interface (PSCI) [1] defines many messages (see identifiers in TF-A include/lib/psci/psci.h or in Linux include/kvm/arm_psci.h ), for examples:
    • CPU_ON/CPU_OFF : used for hotplug feature.
    • SYSTEM_OFF : used for power off.
    • SYSTEM_RESET : used for system reset.
    • SYSTEM_SUSPEND : used to system suspend (deep).
    • PSCI_VERSION : return the supported version of the PSCI specication, v1.1 is supported by TF-A.
  • System Control and Management Interface (SCMI)[2], see SCMI overview for details.

3. Configuration[edit | edit source]

The objective of this chapter is to explain how to configure OpenSTLinux for low-power modes.

See the page power overview for kernel configuration details.

3.1. Supported power modes in OP-TEE[edit | edit source]

The default system low-power mode mapping can be modified through the secure monitor device tree, as described in OP-TEE documentation/devicetree/bindings/regulator/st,stm32mp1-pwr-reg.yaml .

Find below an example in OP-TEE core/arch/arm/dts/stm32mp135f-dk.dts

 &pwr_regulators {
 	system_suspend_supported_soc_modes = <
 		STM32_PM_CSLEEP_RUN
 		STM32_PM_CSTOP_ALLOW_LP_STOP
 		STM32_PM_CSTOP_ALLOW_LPLV_STOP
 		STM32_PM_CSTOP_ALLOW_LPLV_STOP2
 		STM32_PM_CSTOP_ALLOW_STANDBY_DDR_SR
 	>;
 
 	system_off_soc_mode = <STM32_PM_SHUTDOWN>;
 };

3.2. STPMIC configuration for low-power mode in OP-TEE[edit | edit source]

Refer to PMIC OP-TEE page for details of PMIC configuration in OP-TEE for each power mode, and to application note AN5260 and AN5587 for configuration examples.

In OpenSTLinux, the selected PSCI power level is indicated to OP-TEE with Secure-EL1 Payload Dispatcher (SPD) PSCI hooks. The power level is then consolidated with the genPD power domains state and indicated with pm_hint to each OP-TEE drivers to save/restore the device configuration (see core/include/kernel/pm.h and core/arch/arm/plat-stm32mp1/stm32mp_pm.h for details).

This hook is used by the STPMIC1 driver in OP-TEE to configure each regulators according to the selected low-power mode as described in device tree by subnodes.

See OP-TEE device tree in core/arch/arm/dts/stm32mp135f-dk.dts for configuration example:

			vddcpu: buck1 {
				regulator-name = "vddcpu";
				regulator-min-microvolt = <1250000>;
				regulator-max-microvolt = <1350000>;
				regulator-always-on;
				regulator-over-current-protection;

				lp-stop {
					regulator-suspend-microvolt = <1250000>;
				};
				lplv-stop {
					regulator-suspend-microvolt = <900000>;
				};
				lplv-stop2 {
					regulator-off-in-suspend;
				};
				standby-ddr-sr {
					regulator-off-in-suspend;
				};
				standby-ddr-off {
					regulator-off-in-suspend;
				};
			};

4. How to use the framework[edit | edit source]

4.1. Low-power modes[edit | edit source]

Refer to STM32MP13 reference manuals or STM32MP15 reference manuals for the full description of low-power modes.

The modes are handled by the RCC and the PWR peripherals.

Only the Suspend-to-RAM (S2RAM) target is supported for STM32MP1 series: the whole system activity is stopped and a low-power mode is entered. The software selects the deepest mode according to the activated wake-up source(s).

STM32MP1 series STMicroelectronics deliveries propose a default mapping of the low-power modes for each type of board, this default mapping can be changed thanks to the device tree as explain in a paragraph above.

4.1.1. On STM32MP13x lines More info.png[edit | edit source]

The AN5565 STM32MP13 lines using low-power modes gives more information on these modes and on associated the wake-up sources.

The table below summarizes the device hardware states corresponding to each low-power mode.

MPU mode Platform mode VDDCORE state VDDCPU state Clocks state
CRun Run On On On
CStop Stop/LPLV-Stop On/Retention On/Retention Off/Off
CStandby Stop/LPLV-Stop/LPLVL-STOP2/Standby On/Retention/Retention/Off On/Retention/Off/Off Off/Off/Off/Off

The following tables give the list of wake-up sources available in each mode.

Platform mode Available wake-up sources
Stop/LP-Stop Group1 : Group2 + HSE CSS USBH, OTG, CEC, ETH
LPLV-Stop
LPLV-Stop2
Group2 : Group3 + PVD, AVD, USART, I2C, SPI, DTS, LPTIM, GPIO
Standby Group3 : BOR, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, Wakeup pins (from PWR)

4.1.2. On STM32MP15x lines More info.png[edit | edit source]

The AN5109 low-power application note also gives more information on these modes, including:

  • the detailed description of the operating modes
  • the low-power mode entry and exit sequences
  • the low-power mode control registers
  • the wake-up sources and the software mechanism that ensures the consistency between the low-power mode and the activated wake-up source

The table below summarizes the device hardware states corresponding to each low-power mode.

The term "subsystem" either refers to Arm® Cortex®-A7 (also called MPU) or to Arm® Cortex®-M4 (also called MCU). A mode prefixed by 'C' corresponds to a subsystem mode.

Level Mode VDDCORE state Subsystem Clocks state
MPU Subsystem MPU CRun On On
MPU CStop On Off
MPU CStandby On Off
MCU Subsystem MCU CRun On On
MCU CStop On Off

A platform mode is the combination of MPU and MCU modes.

MPU mode MCU mode Platform mode VDDCORE state Clocks state
CRun/CStop/CStandby CRun Run On On
CStop/CStandby CStop Stop (LPDS = 0) On Off
CStop/CStandby CStop LP-Stop or LPLV-Stop (LPDS = 1) Retention Off
CStandby CStop
MCU PDDS = 1
Standby Off Off

The following tables give the list of wake-up sources available in each mode.

Plaform mode Available wake-up sources
Stop
LP-Stop
Group1 : Group2 + USB, CEC, ETH, USART, I²C, SPI, LPTIM
LPLV-Stop Group2 : Group3 + PVD, AVD, GPIO
Standby Group3: BOR, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, Wakeup pins (from PWR)

This list of Wake-up capability peripheral for each mode is defined in the Table 35. Functionalities depending on system operating mode of the STM32MP15 reference manuals.

5. Source code location[edit | edit source]

Below are listed the software frameworks and drivers managing the OpenSTLinux power management.

  • And drivers for each internal peripheral or external component are described in the associated pages:

6. How to trace and debug[edit | edit source]

See How to debug TF-A BL2 and How_to_debug_OP-TEE to activate the traces.

7. To go further[edit | edit source]

Refer to reference manual for a detailed description of low-power modes and peripheral wake-up sources:

The following application notes gives additional information on the hardware settings used for low-power management:

8. References[edit | edit source]

  1. Arm Power State Coordination Interface (PSCI):
    https://developer.arm.com/documentation/den0022
  2. Arm System Control and Management Interface Platform Design Document (SCMI) specification:
    https://developer.arm.com/documentation/den0056