Last edited 2 weeks ago

PWM overview: Difference between revisions

Registered User
mNo edit summary
Registered User
Tag: 2017 source edit
(2 intermediate revisions by 2 users not shown)
Line 1: Line 1:
<noinclude>{{ApplicableFor
{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x, STM32MP25x
|MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x
|MPUs checklist=STM32MP13x,STM32MP15x, STM32MP25x
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x
}}</noinclude>
}}
<noinclude></noinclude>
This article gives information about the Linux<sup>&reg;</sup> PWM framework.<br />
This article gives information about the Linux<sup>&reg;</sup> PWM framework.<br />
It explains how to activate the PWM interface and, based on examples, how to use it.<br />
It explains how to activate the PWM interface and, based on examples, how to use it.<br />
Line 74: Line 75:
===How to use PWM with sysfs interface===
===How to use PWM with sysfs interface===
The available PWM controllers are listed in sysfs:
The available PWM controllers are listed in sysfs:
  {{Board$}} ls /sys/class/pwm
  {{Board$}}ls /sys/class/pwm
  '''pwmchip0'''
  '''pwmchip0'''


The number of channels per controller can be read in npwm (read-only)
The number of channels per controller can be read in npwm (read-only)
  {{Board$}} cd /sys/class/pwm/pwmchip0
  {{Board$}}cd /sys/class/pwm/pwmchip0
  {{Board$}} cat npwm
  {{Board$}}cat npwm
  '''4'''
  '''4'''


Line 88: Line 89:


As an example, proceed as follows to export the first channel (TIMx_CH1, e.g. channel 0):
As an example, proceed as follows to export the first channel (TIMx_CH1, e.g. channel 0):
  {{Board$}} echo '''0''' > export
  {{Board$}}echo '''0''' > export
  {{Board$}} ls
  {{Board$}}ls
  device  export  '''npwm'''  power  '''pwm0'''  subsystem  uevent  unexport
  device  export  '''npwm'''  power  '''pwm0'''  subsystem  uevent  unexport


Line 95: Line 96:


As an example, proceed as follows to set a period of 100 ms with a duty cycle of 60% on channel 0:
As an example, proceed as follows to set a period of 100 ms with a duty cycle of 60% on channel 0:
  {{Board$}} echo 100000000 > pwm0/period
  {{Board$}}echo 100000000 > pwm0/period
  {{Board$}} echo 60000000 > pwm0/duty_cycle
  {{Board$}}echo 60000000 > pwm0/duty_cycle
  {{Board$}} echo 1 > pwm0/enable
  {{Board$}}echo 1 > pwm0/enable


The polarity can be inverted or set to normal by using the polarity entry:
The polarity can be inverted or set to normal by using the polarity entry:
  {{Board$}} echo "'''inversed'''" > pwm0/polarity
  {{Board$}}echo "'''inversed'''" > pwm0/polarity
  {{Board$}} cat pwm0/polarity
  {{Board$}}cat pwm0/polarity
  '''inversed'''
  '''inversed'''
   
   
  {{Board$}} echo "'''normal'''" > pwm0/polarity
  {{Board$}}echo "'''normal'''" > pwm0/polarity
  {{Board$}} cat pwm0/polarity
  {{Board$}}cat pwm0/polarity
  '''normal'''
  '''normal'''


Line 112: Line 113:
{{Info|PWM output and capture mode are mutually exclusive on a TIM instance}}
{{Info|PWM output and capture mode are mutually exclusive on a TIM instance}}
  # First export a channel (e.g. 0), then capture PWM input on it:
  # First export a channel (e.g. 0), then capture PWM input on it:
  {{Board$}} cd /sys/class/pwm/pwmchip0
  {{Board$}}cd /sys/class/pwm/pwmchip0
  {{Board$}} echo '''0''' > export
  {{Board$}}echo '''0''' > export
   
   
  {{Board$}} cd pwm0
  {{Board$}}cd pwm0
  {{Board$}} ls
  {{Board$}}ls
  '''capture'''  duty_cycle  enable  period  polarity  power  uevent
  '''capture'''  duty_cycle  enable  period  polarity  power  uevent
   
   
  {{Board$}} cat capture
  {{Board$}}cat capture
  '''10000 1002'''              {{highlight|# capture result is in nano-seconds, e.g.: 100KHz, 10% duty cycle}}
  '''10000 1002'''              {{highlight|# capture result is in nano-seconds, e.g.: 100KHz, 10% duty cycle}}
===Example of PWM usage with kernel PWM API===
===Example of PWM usage with kernel PWM API===
Several in-kernel drivers use [[PWM_overview#Kernel_PWM_API|kernel PWM API]]. Below a few examples:
Several in-kernel drivers use [[PWM_overview#Kernel_PWM_API|kernel PWM API]]. Below a few examples:
* pwm-beeper: ''drivers/input/misc/pwm-beeper.c''<ref>{{CodeSource | Linux kernel | drivers/input/misc/pwm-beeper.c | drivers/input/misc/pwm-beeper.c}}, Example to use kernel PWM API</ref> driver, {{CodeSource | Linux kernel | Documentation/devicetree/bindings/input/pwm-beeper.txt | Documentation/devicetree/bindings/input/pwm-beeper.txt}} DT binding documentation.
* pwm-beeper: ''drivers/input/misc/pwm-beeper.c''<ref>{{CodeSource | Linux kernel | drivers/input/misc/pwm-beeper.c | drivers/input/misc/pwm-beeper.c}}, Example to use kernel PWM API</ref> driver, {{CodeSource | Linux kernel | Documentation/devicetree/bindings/input/pwm-beeper.yaml | Documentation/devicetree/bindings/input/pwm-beeper.yaml}} DT binding documentation.
* pwm-vibrator: ''drivers/input/misc/pwm-vibra.c''<ref>{{CodeSource | Linux kernel | drivers/input/misc/pwm-vibra.c | drivers/input/misc/pwm-vibra.c}}, Example to use kernel PWM API</ref> driver, {{CodeSource | Linux kernel | Documentation/devicetree/bindings/input/pwm-vibrator.yaml | Documentation/devicetree/bindings/input/pwm-vibrator.yaml}} DT binding documentation.
* pwm-vibrator: ''drivers/input/misc/pwm-vibra.c''<ref>{{CodeSource | Linux kernel | drivers/input/misc/pwm-vibra.c | drivers/input/misc/pwm-vibra.c}}, Example to use kernel PWM API</ref> driver, {{CodeSource | Linux kernel | Documentation/devicetree/bindings/input/pwm-vibrator.yaml | Documentation/devicetree/bindings/input/pwm-vibrator.yaml}} DT binding documentation.


Line 129: Line 130:
=== How to monitor with debugfs ===
=== How to monitor with debugfs ===
PWM usage can be monitored from [[Debugfs|debugfs]] 'pwm' entry. For example:
PWM usage can be monitored from [[Debugfs|debugfs]] 'pwm' entry. For example:
  {{Board$}} cd /sys/kernel/debug/
  {{Board$}}cd /sys/kernel/debug/
  {{Board$}} cat pwm
  {{Board$}}cat pwm
  platform/44000000.timer:pwm, 4 PWM devices                                                              {{highlight|<-- One timer instance exposes 4 PWM channels.}}
  platform/44000000.timer:pwm, 4 PWM devices                                                              {{highlight|<-- One timer instance exposes 4 PWM channels.}}
   pwm-0  (sysfs              ): requested enabled period: 1000000 ns duty: 500000 ns polarity: normal  {{highlight|<-- Channel 0 has been exported, enabled and configured via sysfs}}
   pwm-0  (sysfs              ): requested enabled period: 1000000 ns duty: 500000 ns polarity: normal  {{highlight|<-- Channel 0 has been exported, enabled and configured via sysfs}}
Line 139: Line 140:
Here are some clues on how to debug possible errors in PWM capture mode.<br/>
Here are some clues on how to debug possible errors in PWM capture mode.<br/>
See [[#How to use PWM capture with sysfs interface|How to use PWM capture with sysfs interface]] as a pre-requisite.
See [[#How to use PWM capture with sysfs interface|How to use PWM capture with sysfs interface]] as a pre-requisite.
  {{Board$}} cat capture  
  {{Board$}}cat capture  
  cat: capture: Connection timed out
  cat: capture: Connection timed out
This may be due to:
This may be due to:
* the input signal isn't recognized as a PWM input (or there's no input signal to capture).
* the input signal isn't recognized as a PWM input (or there's no input signal to capture).
* a wrong alternate function number is used for the input pin configuration in the device-tree.<br/>See "[[TIM_device_tree_configuration#TIM configured in PWM input capture mode|TIM configured in PWM input capture mode]]" for further details.
* a wrong alternate function number is used for the input pin configuration in the device-tree.<br/>See "[[TIM_device_tree_configuration#TIM configured in PWM input capture mode|TIM configured in PWM input capture mode]]" for further details.
  {{Board$}} cat capture  
  {{Board$}}cat capture  
  cat: capture: Device or resource busy
  cat: capture: Device or resource busy
This may be due to:
This may be due to:
* a PWM channel on the same TIM instance is already running (in capture or output mode)
* a PWM channel on the same TIM instance is already running (in capture or output mode)
  {{Board$}} cat capture  
  {{Board$}}cat capture  
  cat: capture: No such device
  cat: capture: No such device
This may be due to:
This may be due to:
* the DMA isn't configured properly in the device-tree.<br/>See "[[TIM_device_tree_configuration#TIM configured in PWM input capture mode|TIM configured in PWM input capture mode]]" for further details.
* the DMA isn't configured properly in the device-tree.<br/>See "[[TIM_device_tree_configuration#TIM configured in PWM input capture mode|TIM configured in PWM input capture mode]]" for further details.
  {{Board$}} cat capture
  {{Board$}}cat capture
  cat: capture: Function not implemented
  cat: capture: Function not implemented
This may be due to:
This may be due to:

Revision as of 18:04, 23 October 2024

Applicable for STM32MP13x lines, STM32MP15x lines, Unknown MPU, Unknown MPU, Unknown MPU

This article gives information about the Linux® PWM framework.
It explains how to activate the PWM interface and, based on examples, how to use it.

1. Framework purpose[edit | edit source]

PWM (Pulse Width Modulation) framework offers a unified interface for the users to:

  • control PWM output(s) such as period, duty cycle and polarity.
  • capture a PWM signal and report its period and duty cycle (e.g. input).

The interface can be used from:

  • user space (sysfs)
  • kernel space (API)

PWMs can be used in various use cases, as mentioned in How to use the framework to control LEDs, beepers, vibrators or fans...

2. System overview[edit | edit source]

PWM sysfs interfacePWM kernel interfaceSTM32 TIM Linux driverSTM32 LPTIM Linux driverSTM32 TIM internal peripheralSTM32 LPTIM internal peripheral
PWM Implementation architecture

2.1. Component description[edit | edit source]

  • PWM user (User space)

The user can use PWM sysfs interface, from a user terminal or a custom application, to control PWM device(s) from user space.

  • PWM user (Kernel space)

User drivers can use PWM API to control PWM external device(s) from kernel space (such as back-light, vibrator, LED or fan drivers).

  • PWM framework (Kernel space)

The PWM core provides sysfs interface and PWM API. They can be used to implement PWM user and PWM controller drivers.

  • PWM drivers (Kernel space)

Provider drivers such as STM32 TIM Linux driver and STM32 LPTIM Linux driver that expose PWM controller(s) to the core.

  • PWM hardware

PWM controller(s) such as TIM internal peripheral[1] and LPTIM internal peripheral[2] used to drive external PWM controlled devices.

2.2. API description[edit | edit source]

Documentation on PWM interface can be found under kernel Documentation/driver-api/pwm.rst[3]

2.2.1. Kernel PWM API[edit | edit source]

The main useful user API are the following:

  • devm_pwm_get() or pwm_get() / pwm_put(): this API is used to look up, request, then free a PWM device.
  • pwm_init_state(), pwm_get_state(), pwm_apply_state(): this API is used to initialize, retrieve and apply the current PWM device state.
  • pwm_config(): this API updates the PWM device configuration (period and duty cycle).
  • ...

2.2.2. Sysfs interface[edit | edit source]

In addition to Documentation/driver-api/pwm.rst[3], details on ABI are available in Documentation/ABI/testing/sysfs-class-pwm[4].

3. Configuration[edit | edit source]

3.1. Kernel configuration[edit | edit source]

Activate PWM framework in the kernel configuration through the Linux menuconfig tool, Menuconfig or how to configure kernel (CONFIG_PWM=y):

Device Drivers  --->
   [*] Pulse-Width Modulation (PWM) Support  --->

Activate PWM drivers for STM32 PWM drivers: STM32 TIM Linux driver and/or STM32 LPTIM Linux driver

3.2. Device tree configuration[edit | edit source]

  • PWM generic DT bindings:

PWM DT bindings documentation[5] describes device tree properties related to standard PWM user nodes and PWM controller nodes.

  • Detailed DT configuration for STM32 internal peripherals:

TIM device tree configuration and/or LPTIM device tree configuration

4. How to use the framework[edit | edit source]

PWM can be used either from the user or the kernel space.

4.1. How to use PWM with sysfs interface[edit | edit source]

The available PWM controllers are listed in sysfs:

ls /sys/class/pwm
pwmchip0

The number of channels per controller can be read in npwm (read-only)

cd /sys/class/pwm/pwmchip0
cat npwm
4

Each channel is exported (requested for sysfs activation) by writing the corresponding number in 'export'.

Info white.png Information
TIMx_CH1 is exported as "pwm0", TIMx_CH2 as "pwm1", and so on:
  • PWM channels are numbered from 0 to 'npwm' - 1
  • TIM[1] channels are numbered from 1 to 'npwm'.

As an example, proceed as follows to export the first channel (TIMx_CH1, e.g. channel 0):

echo 0 > export
ls
device  export  npwm  power  pwm0  subsystem  uevent  unexport

The period and duty cycle must be configured before enabling any channel.

As an example, proceed as follows to set a period of 100 ms with a duty cycle of 60% on channel 0:

echo 100000000 > pwm0/period
echo 60000000 > pwm0/duty_cycle
echo 1 > pwm0/enable

The polarity can be inverted or set to normal by using the polarity entry:

echo "inversed" > pwm0/polarity
cat pwm0/polarity
inversed

echo "normal" > pwm0/polarity
cat pwm0/polarity
normal

4.2. How to use PWM capture with sysfs interface[edit | edit source]

PWM capture is available on some PWM controllers such as TIM internal peripheral[1] (see TIM configured in PWM input capture mode ).

Info white.png Information
PWM output and capture mode are mutually exclusive on a TIM instance
# First export a channel (e.g. 0), then capture PWM input on it:
cd /sys/class/pwm/pwmchip0
echo 0 > export

cd pwm0
ls
capture  duty_cycle  enable  period  polarity  power  uevent

cat capture
10000 1002               # capture result is in nano-seconds, e.g.: 100KHz, 10% duty cycle

4.3. Example of PWM usage with kernel PWM API[edit | edit source]

Several in-kernel drivers use kernel PWM API. Below a few examples:

5. How to trace and debug the framework[edit | edit source]

5.1. How to monitor with debugfs[edit | edit source]

PWM usage can be monitored from debugfs 'pwm' entry. For example:

cd /sys/kernel/debug/
cat pwm
platform/44000000.timer:pwm, 4 PWM devices                                                               <-- One timer instance exposes 4 PWM channels.
 pwm-0   (sysfs               ): requested enabled period: 1000000 ns duty: 500000 ns polarity: normal   <-- Channel 0 has been exported, enabled and configured via sysfs
 pwm-1   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
 pwm-2   ((null)              ): period: 0 ns duty: 0 ns polarity: normal                                <-- Other channels aren't used currently
 pwm-3   ((null)              ): period: 0 ns duty: 0 ns polarity: normal

5.2. Troubleshooting PWM capture[edit | edit source]

Here are some clues on how to debug possible errors in PWM capture mode.
See How to use PWM capture with sysfs interface as a pre-requisite.

cat capture 
cat: capture: Connection timed out

This may be due to:

  • the input signal isn't recognized as a PWM input (or there's no input signal to capture).
  • a wrong alternate function number is used for the input pin configuration in the device-tree.
    See "TIM configured in PWM input capture mode" for further details.
cat capture 
cat: capture: Device or resource busy

This may be due to:

  • a PWM channel on the same TIM instance is already running (in capture or output mode)
cat capture 
cat: capture: No such device

This may be due to:

cat capture
cat: capture: Function not implemented

This may be due to:

  • a wrong TIM instance is being used (e.g. "/sys/class/pwm/pwmchip/pwmchipN"), and it doesn't support capture (like LPTIM)
  • the DMA support isn't enabled (CONFIG_DMA_ENGINE)

6. References[edit | edit source]

  1. 1.0 1.1 1.2 TIM internal peripheral
  2. LPTIM internal peripheral
  3. 3.0 3.1 Documentation/driver-api/pwm.rst , Pulse Width Modulation interface
  4. Documentation/ABI/testing/sysfs-class-pwm , Pulse Width Modulation ABI
  5. Documentation/devicetree/bindings/pwm/pwm.txt , PWM DT bindings documentation
  6. drivers/input/misc/pwm-beeper.c , Example to use kernel PWM API
  7. drivers/input/misc/pwm-vibra.c , Example to use kernel PWM API