Last edited 3 weeks ago

Which STM32MPU Embedded Software Package better suits your needs

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This article gives an overview of the STM32 MPU embedded software offer, and details the content of the flagship distribution that is the Yocto-based OpenSTLinux embedded software.

1. Overview of the STM32 MPU embedded software offer[edit | edit source]

The STM32 MPU embedded software offer includes several distributions (provided by STMicroelectronics or by partners) that run over all or part of the STM32 MPU microprocessor devices, and that are supported for all or part of the STM32 MPU boards (Evaluation boards and Discovery kits). The STM32 MPU ecosystem release note describes the content of the most recent ecosystem release, and therefore lists the delivered distributions, microprocessor devices and boards.

For each distribution, up to three software packages are delivered:

  • The Starter Package (software image) to quickly and easily start with any STM32 MPU microprocessor device. The Starter Package is generated from the Distribution Package.
  • The Developer Package (SDK for cross-development, source code for the BSP of the distribution) to add your own developments on top of the STM32 MPU Embedded Software distribution, or to replace the Starter Package pre-built binaries. The Developer Package is generated from the Distribution Package.
  • The Distribution Package (build framework on host PC, source code for the whole distribution) to create your own distribution, your own Starter Package and your own Developer Package.
STM32 MPU embedded software distribution Packages

The rest of the article details the above Packages for the Yocto-based OpenSTLinux embedded software, the flagship distribution that is supported for all the STM32 MPU boards. It helps finding the one that best fits your use case. Packages are standalone, but they are not isolated one from the others: there are gateways between them.

The next chapter is an overview of the Yocto-based OpenSTLinux embedded software components. The last chapter concludes by providing an example of production cycle based on the three Packages.

2. Overview of the Yocto-based OpenSTLinux embedded software components[edit | edit source]

The STM32MPU Embedded Software distribution includes the following components (as illustrated in the figure below):

  • Binaries: software images
  • Software development kit (SDK):
    • Cross-development toolchain
    • Libraries, headers and symbols
    • Environment setup scripts
  • Source code for:
    • The OpenSTLinux distribution running on Arm® Cortex®-A processor(s): U-Boot, TF-A, OP-TEE, Linux® kernel, application frameworks
    • The FwST-M Packages (firmwares) running on Arm® Cortex®-M processor: STM32Cube MPU Package (only supported for STM32MP15x lines More info.png and STM32MP2 series), TF-M (only supported for STM32MP2 series), MCUboot (only supported for the M33-TD flavor More info green.png of STM32MP2 series)
  • Build framework for embedded Linux® (based on OpenEmbedded that is the recommended build system of the Yocto Project):
    • BitBake: a make-like build tool
    • Recipes: a recipe specifies how a particular package is built
    • Layers: a layer is a collection of recipes and/or configurations used on top of the OpenEmbedded core
  • Documentation and tools such as:
    • The present wiki
    • The STM32CubeProgrammer
    • Integrated development environments (IDE)


STM32MPU Embedded Software distribution components
Nota: Documentation and tools are cross-Package components. They are not described in this article: consequently, they are implicitly present in all the figures of this article.


Each of the three Packages described below is made of some of the above components.

3. Starter Package for the Yocto-based OpenSTLinux embedded software[edit | edit source]

This Package allows to quickly and easily get any STM32 microprocessor development platform up and running.
An STM32 microprocessor development platform (such as STM32MP157x-EV1 Evaluation board) and a microSD card (populated with the software image delivered for this platform) are all what is required to discover the platform capabilities. No integrated development environment (IDE), no software development kit (SDK) are needed: just use the development platform as a "micro-PC" running Linux®.
The software image also contains the firmwares running on Arm® Cortex®-M processor (only supported for STM32MP15x lines More info.png and STM32MP2 series).


STM32 MPU Embedded Software Starter Package.png


What are the main use cases that can be covered with this Package?

  • Evaluation of the STM32 microprocessor device and development platform (such as internal peripherals and performance)
  • Execution of the STM32Cube MPU firmware projects delivered with each STM32Cube MPU Package (only supported for STM32MP15x lines More info.png and STM32MP2 series)
read Starter Package for STM32CubeMP15 to get started with running STM32Cube MPU firmware for Arm Cortex-M4,
read Starter Package for STM32CubeMP2 to get started with running STM32Cube MPU firmware for Arm Cortex-M33.
  • Direct development on the development platform of simple user examples in different languages (Shell, Python...)


For more information on the Starter Package depending on your development platform, refer to the corresponding Starter Package article named Your_development_platform - Starter Package.
Example: STM32MP15 Evaluation boards - Starter Package for the STM32MP15 Evaluation boards.
All Starter Package articles belong to the Category:Starter Package.


Switch to the next Package if you need to:

  • modify or tune any piece of software of the STM32MPU Embedded Software distribution (e.g. Linux® kernel)
  • integrate pieces of software from open-source communities or third parties
  • develop and integrate your own applications
  • benefit from a software development kit (e.g. for powerful cross-development toolchain)
  • take advantage of an integrated development environment (IDE)

4. Developer Package for the Yocto-based OpenSTLinux embedded software[edit | edit source]

This Package allows the modification of some pieces of software of the STM32MPU Embedded Software distribution, as well as the addition of your applications in your platform software image.
The Developer Package provides on top of the Starter Package:

  • a software development kit (SDK) for cross-development on an host PC
  • the following pieces of software of the OpenSTLinux distribution in source code:
    • U-Boot
    • Trusted Firmware-A (TF-A)
    • Linux® kernel
    • Optionally, Open source Trusted Execution Environment (OP-TEE)
  • the source code for the following firmwares running on the Arm® Cortex®-M processor:
    • STM32Cube MPU Package (only supported for STM32MP15x lines More info.png and STM32MP2 series)
    • Trusted Firmware-M (TF-M) (only supported for STM32MP2 series)
    • MCUboot (only supported for the M33-TD flavor More info green.png of STM32MP2 series)
  • Initialization code generator (STM32CubeMX). This tool makes it possible to
    • generate device tree for OpenSTLinux distribution
    • generate the peripheral initialization C code and IDE project creation files for STM32Cube MPU package
  • An Eclipse-based integrated development environment (IDE) - STM32CubeIDE
    • STM32Cube MPU firmware projects are supported by STM32CubeIDE
    • Projects files generated by STM32CubeMX can be directly opened by this IDE to continue STM32Cube MPU firmware development
    • STM32CubeIDE integrates STM32CubeMX for an easier user experience
    • IDE is optional for OpenSTLinux development since all actions can be achieved through a command line
Info white.png Information
The Developer Package doesn't include the application frameworks (Linux® user space applications, U-Boot applications and OP-TEE user space applications) in source code.


Developer Package components


What are the main use cases that can be covered with this Package?

  • Modification and tuning of the pieces of software delivered as source code (see above list):
    • Code modification
    • Efficient development cycle (compile, push on target, debug)
    • Tuning of the configuration options (e.g. for the Linux® kernel)
    • Adaptation of the device tree files for the microprocessor device and development platform
  • Development of the firmwares running on the Arm® Cortex®-M processor (only supported for STM32MP15x lines More info.png and STM32MP2 series)
read Developer Package for STM32CubeMP15 to get started with building and running STM32Cube MPU firmware for Arm Cortex-M4,
read Developer Package for STM32CubeMP2 to get started with building and running STM32Cube MPU firmware for Arm Cortex-M33.
  • Addition of your own Linux® applications or Linux® application frameworks
  • Addition of your own trusted applications (TA) (if OP-TEE is part of the software release)
  • Addition of your own U-Boot applications


For more information on the Developer Package for any STM32 microprocessors series, refer to the STM32MPU Developer Package article.
All Developer Package articles belong to the Category:Developer Package.


Switch to the next Package if you need to:

  • modify or tune the (U-Boot, OP-TEE and Linux®) application frameworks of the OpenSTLinux distribution
  • create your own distribution (e.g. to integrate and share pieces of software from open source communities or third parties)
  • generate your own software development kit (SDK) and images

5. Distribution Package for the Yocto-based OpenSTLinux embedded software[edit | edit source]

This Package allows the creation of a new distribution with a final objective of productization.
It includes the source code of all the pieces of software of the STM32MPU Embedded Software distribution (including the application frameworks), plus a build framework based on OpenEmbedded (aka distribution builder). A host PC is required to operate this Package (a Linux® host PC is even strongly recommended).


Distribution Package components


What are the main use cases that can be covered with this Package?

  • Creation of your own Linux® distribution
    • to tune the system configuration options (such as memory sizes or debug options)
    • to share all the developments within your team (software baseline)
    • to prepare the final software for productization
  • Integration of the following software in this distribution:
    • your developments made thanks to the Developer Package
    • pieces of software coming from open source communities or third parties
    • Integrate your STM32Cube MPU firmware projects in your own distribution (binary or source code) (only supported for STM32MP15x lines More info.png and STM32MP2 series)
read Distribution Package for STM32CubeMP15 to understand how STM32Cube MPU firmware (for Arm Cortex-M4) projects have been installed in STM32MPU Embedded software distribution,
read Distribution Package for STM32CubeMP2 to understand how STM32Cube MPU firmware (for Arm Cortex-M33) projects have been installed in STM32MPU Embedded software distribution.
  • Generation of your own Starter Package images
  • Generation of your own Developer Package SDK


Generally speaking, few dedicated people from the project team use this Distribution Package to create and regularly enrich the project Linux® distribution and generate the project Developer Package. Most of developers will use this Developer Package for their developments, since it is a light weighted and efficient (short development cycle) environment.

For more information on the Distribution Package for any STM32 microprocessor series, refer to the STM32MPU Distribution Package article.
All Distribution Package articles belong to the Category:Distribution Package.

6. Example of production cycle for the Yocto-based OpenSTLinux embedded software[edit | edit source]

The following figures give an example of gateways between the different Packages, that might be seen as a production cycle.

STM32MPU Embedded Software distribution: evaluation, development and integration


In the example given above, the developers use the Developer Package of the STM32MPU Embedded Software distribution to create an add-on piece of software (e.g. Linux® application on top of the Linux® application frameworks) and modify the Linux® kernel. Their deliveries are integrated on top of the Distribution Package of the STM32MPU Embedded Software distribution, together with pieces of software from an open source community and a third party. The result is your own Distribution Package.

Your distribution: generating, improving and productizing


In the example given above, your new images (binaries) and your new Developer Package are generated from this new Distribution Package. The developers base their additional developments on this new Developer Package. The production cycle is then initiated.