Last edited 8 months ago

How to build Qt applications using Qt Creator

(Redirected from How To build Qt applications using Qt Creator)
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

Important
This version of X-LINUX-QT expansion package is validated against the ecosystem release v6.2.0 .
It has not been ported yet on ecosystem release v6.2.1 .
Important
This article has not been updated yet for the (ecosystem release v6.2.1 ).
The subject of this article is not part of STM32MPU ecosystem releases, for which ST provides some support. This article only provides, as example, some helper guidelines (tips): you may need to make some adaptations depending on your system setup.

This article explains how to use the X-LINUX-QT developer package to build Qt applications for the STM32 microprocessor series. It has been written for STM32MP2 series but it can be adapted easily to STM32MP1 series.

The validation and snapshots of this article have been made with X-LINUX-QT expansion package v2.1.0, but can be easily translated to other releases.

1. Prerequisites[edit | edit source]

Check first, detailed prerequisites in X-LINUX-QT_expansion_package#Prerequisites and X-LINUX-QT Developer Package#Prerequisites.

The Qt™ Creator[1] tool is used to build, debug and run applications demos on target.

The X-LINUX-QT developer package is up and running on your board. For that, follow information provided in X-LINUX-QT Developer Package article.

2. Install the Qt Creator[edit | edit source]

  • The Qt™ Creator can be downloaded and installed following this link.
  • The Qt™ online installer can be downloaded following this link.
  • Installing the X-LINUX-QT developer package configures also the new STM32MPU Kit for the already installed Qt™ Creator IDE.

IMPORTANT: this new STM32MPU Kit is only created when installing X-LINUX-QT v2.1.0 developer package (see #Install_the_X-LINUX-QT_developer_package_v2.1.0) over Yocto-based OpenSTLinux embedded software v6.0.0

But if X-LINUX-QT developer package v2.1.0 have been installed, this kit can be easily cloned inside Qt Creator to a new kit targeting the SDK generated from distribution package v2.3.0 or v2.2.0.

3. Select the new kit installed by the X-LINUX-QT developer package[edit | edit source]

Information
Qt6 6.6.3 must be installed in order to have the list of examples for that Qt version.

Once the Qt™ Creator is launched and the Welcome to Qt™ Creator is displayed:

  • Go to the Examples from the list on the left,
  • Then select the new Qt6 6.6.3 from the dropdown list.

The supported examples are then displayed.

Qt™ Creator Welcome Screen - Qt6 Examples - Picture is not contractual (based on previous Qt6 6.5.3 version)

4. Select the project example[edit | edit source]

  • Search for a specific example in the Search bar in front of the selected kit.
  • Select the example you are looking for (just a simple click on it).
Qt™ Creator Welcome Screen - Select the example - Picture is not contractual (based on previous Qt6 6.5.3 version)
  • Close the "Help window" if not needed.
Qt™ Creator Welcome Screen - The example's Help window - Picture is not contractual (based on previous Qt6 6.5.3 and OpenSTLinux versions)

5. Configure the project example[edit | edit source]

  • Make sure that the new kit added by X-LINUX-QT developer package is selected
  • Press the Configure Project button:
Qt™ Creator - Configure Project - Picture is not contractual (based on previous Qt6 6.5.3 and OpenSTLinux versions)
  • Make sure all configuration steps are successfully done (green bars):
Qt™ Creator - Project Configuration Status

6. Configure the STM32 MPU Kit[edit | edit source]

  • Select the Configure Project button from the vertical bar on the left.
  • Select the new Kit added by the X-LINUX-QT developer package.
  • Select Run Settings.
  • On the right panel, scroll down till the Environment section.
  • Press the Details button.
  • Add the below environment variables:
XDG_RUNTIME_DIR=/run/user/1000
QT_QPA_PLATFORM=wayland
QT_VULKAN_LIB=/usr/lib/libvulkan.so.1
Qt™ Creator - Configure Run Settings - Picture is not contractual (based on previous Qt6 6.5.3 and OpenSTLinux versions)

7. Build and run the project[edit | edit source]

  • Make sure that the board is connected to the host machine via the USB DRD TypeC connector. for that, follow the instructions from the X-LINUX-QT expansion package#Hardware prerequisites section and check how to get your board connected to the host machine.
  • Once in the Run Setting panel, the notice below should not appear at the bottom of the screen.
Qt™ Creator - Run Project - Picture is not contractual (based on previous Qt6 6.5.3 and OpenSTLinux versions)
  • Press the Run button from the vertical bar on the left to build, deploy and run the selected example on the connected board.
Qt™ Creator - Run Project - Picture is not contractual (based on previous Qt6 6.5.3 and OpenSTLinux versions
  • If everything went well, then the example will be running on the connected board.
The Quick Items example running on the target