Last edited 4 months ago

X-LINUX-QT Developer Package


This article aims to give the following information:

  • How to download and install the latest X-LINUX-QT Developer Package for the STM32 microprocessor series.
  • Where to find the previous releases (archives).
1. Prerequisites[edit | edit source]

Check detailed prerequisites here.


2. Install the STM32MPU OpenSTLinux Developer Package[edit | edit source]

To download and install the STM32MPU OpenSTLinux Developer Package, follow the instructions from here.

3. Install the X-LINUX-QT Developer Package[edit | edit source]
  • Download and install the X-LINUX-QT Developer Package
The X-LINUX-QT Developer Package is delivered through two tarball files named:
  • en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz for x86_64 host architecture
  • en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz for arm64 host architecture

  • Download and install the X-LINUX-QT Developer Package
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
X-LINUX-QT Developer Package v2.0.0 release
Download
  • Go on st.com to download
    • en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz file for x86_64 host architecture
    • en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz file for arm64 host architecture
Installation

For x86_64 host architecture

  • Uncompress the tarball file to get the Developer Package installation script.
 mkdir -p ~/MySDK
 tar xvf en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz -C ~/MySDK
  • If needed, change the permissions on the SDK installation script so that it is executable.
 chmod +x ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
  • Run the SDK installation script.
 cd <working directory absolute path>/Developer-Package/SDK
 ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
  • A successful installation outputs the following log:
===============================================================================================================================================
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06 - X-LINUX-QT version 2.0.0 SDK-Addon installer
===============================================================================================================================================
Extracting X-LINUX-QT-Addon SDK................................................................................................Done.
Setting it up... Done.
Do you want to configure the Qt Creator for this SDK [y/n]? n
Qt Creator configuration will be ignored.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.

Alternative : If the preliminary the Qt Creator has been installed as explained in the "Prerequisites" chapter, it is now possible to configure it. For that, answer y to the next question:

Do you want to configure the Qt Creator for this SDK [y/n]? y
Please enter the directory where Qt Tools are installed (default: "/usr/lib, /usr/libexec"): /usr/libexec
Using /home/USER/Qt/Tools/sdktool/libexec/qtcreator/sdktool
Adding "Qt https://code.qt.io/yocto/meta-qt6.git,6.5.3 for STM32MP25 ( 5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06, X-LINUX-QT v2.0.0)" kit for Qt Creator... Done.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.

For arm64 host architecture

  • Uncompress the tarball file to get the Developer Package installation script.
 mkdir -p ~/MySDK
 tar xvf en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz -C ~/MySDK
  • If needed, change the permissions on the SDK installation script so that it is executable.
 chmod +x ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
 cd <working directory absolute path>/Developer-Package/SDK
 ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk/{{X-
  • A successful installation outputs the following log:
==================================================================================================================================================
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06 - X-LINUX-QT version 2.0.0 SDK-Addon installer
===================================================================================================================================================
Extracting X-LINUX-QT-Addon SDK......................................................................................................... Done.
Setting it up... Done.
Do you want to configure the Qt Creator for this SDK [y/n]? n
Qt Creator configuration will be ignored.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.

Alternative: If the Qt Creator has been installed preliminary as explained in the "Prerequisites" chapter, it is now possible to configure it. For that, answer y to the next question:

Do you want to configure the Qt Creator for this SDK [y/n]? y 
Please enter the directory where Qt Tools are installed (default: "/usr/lib, /usr/libexec"): /usr/libexec
Using /home/USER/Qt/Tools/sdktool/libexec/qtcreator/sdktool
Adding "Qt https://code.qt.io/yocto/meta-qt6.git,6.5.3 for STM32MP25 ( 5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06, X-LINUX-QT v2.0.0)" kit for Qt Creator... Done.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.
  • Older versions of X-LINUX-QT Developer Package can be found here.

4. Archives Archive box.png[edit | edit source]

X-LINUX-QT release Developer Package
X-LINUX-QT v1.0.0 X-LINUX-QT Developer Package v1.0.0