Last edited 7 months ago

X-LINUX-QT Expansion Package


X-LINUX-QT-Expansion Package-logo.png


1. Article purpose[edit | edit source]

Purpose of this article is to:

  • Introduce the X-LINUX-QT Expansion Package[1],
  • Define the hardware & software deliverables to use the X-LINUX-QT packages,
  • Describe all steps to integrate the X-LINUX-QT packages and associated expected results,
  • Give some use case examples enabled by the X-LINUX-QT package,
  • Explain how to create a Qt™ application using the X-LINUX-QT Developer Package
  • Describe all steps to use Qt™ Creator with the X-LINUX-QT Developer Package and associated expected results.
QT Expansion Package In STM32MPU Embedded Software.png


2. X-LINUX-QT Expansion Package description[edit | edit source]

2.1. Overview[edit | edit source]

X-LINUX-QT is an STM32 MPU OpenSTLinux Expansion Package that targets Qt based application and graphical user interface (GUI) development for STM32MP25x lines More info.png.
It contains Linux® Qt frameworks, as well as an ST Application Launcher based on Qt Framework and application examples to get started with Qt application development.

The Qt framework contains a comprehensive set of highly intuitive and modularized C++ library classes and is loaded with APIs to simplify your application development. Qt produces highly readable, easily maintainable and reusable code with high runtime performance and small footprint – and it's cross-platform.

This expansion package is a complete ecosystem that allows developers working with OpenSTLinux to create Qt based application very easily.

  • All-in-one Qt solutions for the STM32MP2 series supporting Wayland and Weston.
  • Pre-integrated into Linux® distribution based on ST environment
  • Include Qt frameworks to build UIs and Applications
  • Include ST Application Launcher based on Qt framework forSTM32 MPU devices (see supported platforms list)


2.2. Main restrictions[edit | edit source]

This first version of X-LINUX-QT Expansion Package is not yet functional with STM32MP1 series.

2.3. Versioning[edit | edit source]

Latest version of X-LINUX-QT is 2.0.0. The X-LINUX-QT Expansion Package is based to be used with OpenSTLinux distribution ecosystem release v5.1.0 More info.png .

The generic versioning X-LINUX-QT vx.y.z is built as follows:

  • x: major version depending on Qt major versions. Each new major version is incompatible with previous Qt versions. Initial major version 1.0.0 is for Qt 5.x and current version 2.0.0 is for Qt 6.x
  • y: minor version depending on the OpenSTLinux distribution major versions. Each new major version is incompatible with previous OpenSTLinux distribution versions. Initial minor version will be for OpenSTLinux Distribution v5.x
  • z: patch version is changed when new functionalities, bug fixes and/or modules are added to the X-LINUX-QT Expansion Package in a backward compatible manner.

3. Associated licenses[edit | edit source]

Associated licenses are available in the wiki article X-LINUX-QT_licenses.

4. Prerequisites[edit | edit source]

4.1. Hardware prerequisites[edit | edit source]

  • STM32MP257F-EV1 Evaluation board More info green.png

STM32MP257x-EV1 assembled.jpg

  • STM32MP257F-DK Discovery kit More info green.png

STM32MP257x-DK assembled.jpg

4.2. Software prerequisites[edit | edit source]

The X-LINUX-QT Expansion Package runs with OpenSTLinux ecosystem release v5.1.0 More info.png .

The X-LINUX-QT Expansion Package can be used in standalone or with the Qt™ Creator[2] tool.
The Qt™ Creator[2] tool can be used to build, debug and run applications demos on target. If you want to use it, you need to make following prerequisites:

  • You will need to create a Qt™ account then download and install the Qt™ Creator
  • The Qt™ online installer is available from here

5. Hardware setup[edit | edit source]

5.1. STM32MP257x-EV1 Evaluation board[edit | edit source]

The STM32MP257x-EV1 - hardware description describes how to set up the STM32MP257F-EV1 Evaluation board More info green.png: it explains how to assemble the boards, set the right power jumper configuration, connect the display to the board and connect the board to your development environment.

5.2. STM32MP257x-DK Discovery Discovery kit[edit | edit source]

The STM32MP257x-DKx_-_hardware_description describes how to set up the STM32MP257F-DK Discovery kit More info green.png: it explains how to connect the display to the board and connect the board to your development environment.

6. Software setup[edit | edit source]

6.1. How to get software[edit | edit source]

There are 3 possibilities to install the additional X-LINUX-QT Expansion Package software to port on top of OpenSTLinux.

Select the one corresponding to your needs amongst :

6.1.1. How to install the Starter Package[edit | edit source]

6.1.1.1. Install OpenSTLinux Starter Package[edit | edit source]

Before developing with the Developer Package, it is essential to start up your board thanks to its Starter Package. All articles relative to Starter Packages are found in Category:Starter Package: find the one that corresponds to your board, and follow the installation instructions (if not yet done), before going further.

Thanks to the Starter Package, all Flash partitions are populated.

6.1.1.2. Install the X-LINUX-QT Starter Package[edit | edit source]

The packagegroup-x-linux-qt package must be installed on top of the STM32MPU Starter Package to bring the "Qt framework" as graphics solution.

Once the board is booted, make sure it is connected to the internet then execute the following commands in the console to install the X-LINUX-QT packages:

  • First of all , you may need to update date and time on your connected board before running the below commands. Date and Time on your connected board can be updated by this command:
date +%y%m%d -s "20250701"
date +%T -s "00:00:00"
  • Refresh the apt database to access the Qt package repository:
apt-get update

.

  • Install the package with the apt configuration to access the Qt packages :
CollapseFor Qt6:
cd /var/cache/apt/archives
wget http://extra.packages.openstlinux.st.com/Qt/5.1/pool/config/a/apt-openstlinux-x-linux-qt/apt-openstlinux-x-linux-qt_2.0_all.deb
apt-get install ./apt-openstlinux-x-linux-qt_2.0_all.deb
For Qt5:
cd /var/cache/apt/archives
wget http://extra.packages.openstlinux.st.com/Qt/5.1/pool/config/a/apt-openstlinux-x-linux-qt/apt-openstlinux-x-linux-qt_1.0_all.deb
apt-get install ./apt-openstlinux-x-linux-qt_1.0_all.deb
  • Update the apt database to read the Qt package repository :
apt-get update
  • Install the package group for the X-LINUX-QT package
apt-get install -y packagegroup-x-linux-qt
  • Restart the Weston graphical services with the new ST-Launcher
systemctl restart weston-graphical-session.service
6.1.1.3. Starter Package expected results[edit | edit source]

Once the X-LINUX-QT Starter Package is installed and the Weston graphical service is restarted, the new STLauncher is displayed.

  • The STLauncher Splash Screen is displayed for few seconds
STLauncher Splash screen
  • The Main Window displays all compatible installed applications
  • To display more information about the running hardware and software:
    • Click on the Settings button on the top right of the screen
STLauncher Main window
  • The SETTINGS screen is displayed
STLauncher Settings window
  • Click on the INFORMATIONS button
  • The INFORMATIONS screen is displayed
STLauncher Information window
6.1.1.4. Run examples from the starter package[edit | edit source]
6.1.1.4.1. Legacy demonstrations[edit | edit source]

Demos, which are available via the GTK demo launcher, are still supported by the new QT STLauncher.
For example, you can run the 3D Cube Demo from the new Qt STLauncher:

  • Select the demo's icon (Selected icon will be in Yellow)
STLauncher - Selected 3D Cube Icon
  • Click on the demo's icon again to run the demo
Running 3D Cube Demo
6.1.1.4.2. New Qt examples[edit | edit source]
  • Qt OpenGL Cube example
The Qt OpenGL Cube example is now displayed in the new STLauncher.
In order to run the examples, select its icon first then click on it again to start it
  • Select the Qt OpenGL Cube example icon (Selected icon will be in Yellow)
STLauncher - Selected OpenGL Cube Icon
  • Click on the demo's icon again to run the demo
Running OpenGL Cube Demo
6.1.1.4.3. New Qt demonstrations[edit | edit source]

The new Medical and RobotArm3D demonstrations are displayed in the new STLauncher. In order to run the demonstration, select its icon first then click on it again to start it.

  • ST Medical
ST Medical Demo - Startup screen



Running ST Medical Demo
  • ST RobotArm3D Demo
ST RobotArm3D Demo - Startup screen



Running ST RobotArm3D Demo


6.1.2. How to install Developer Package[edit | edit source]

6.1.2.1. Install the STM32MPU OpenSTLinux Developer Package[edit | edit source]

To download and install the STM32MPU OpenSTLinux Developer Package, you need to follow instructions from here

6.1.2.2. Install the X-LINUX-QT Developer Package[edit | edit source]
  • Download and install the X-LINUX-QT Developer Package
The X-LINUX-QT Developer Package is delivered through two tarball files named :
  • en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz for x86_64 host architecture
  • en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz for arm64 host architecture

  • Download and install the X-LINUX-QT Developer Package
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
X-LINUX-QT Developer Package v2.0.0 release
Download
  • Go on st.com to download
    • en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz file for x86_64 host architecture
    • en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz file for arm64 host architecture
Installation
Collapse

For x86_64 host architecture

  • Uncompress the tarball file to get the Developer Package installation script.
 mkdir -p ~/MySDK
 tar xvf en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz -C ~/MySDK
  • If needed, change the permissions on the SDK installation script so that it is executable.
 chmod +x ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
  • Run the SDK installation script.
 cd <working directory absolute path>/Developer-Package/SDK
 ~/MySDK/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk/st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
  • A successful installation outputs the following log:
===============================================================================================================================================
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26 - X-LINUX-QT version 2.0.0 SDK-Addon installer
===============================================================================================================================================
Extracting X-LINUX-QT-Addon SDK................................................................................................Done.
Setting it up... Done.
Do you want to configure the Qt Creator for this SDK [y/n]? n
Qt Creator configuration will be ignored.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.

Alternative : If you have installed preliminary the Qt Creator as explained in the "Prerequisites" chapter, you can now configure it. For that, you need to answer y to the next question

Do you want to configure the Qt Creator for this SDK [y/n]? y
Please enter the directory where Qt Tools are installed (default: "/usr/lib, /usr/libexec"): /usr/libexec
Using /home/USER/Qt/Tools/sdktool/libexec/qtcreator/sdktool
Adding "Qt https://code.qt.io/yocto/meta-qt6.git,6.5.3 for STM32MP25 ( 4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26, X-LINUX-QT v2.0.0)" kit for Qt Creator... Done.
X-LINUX-QT-Addon SDK has been successfully set up and is ready to be used.

For arm64 host architecture

  • Older versions of X-LINUX-QT Developer Package can be found here.

6.1.3. How to install Distribution Package[edit | edit source]

6.1.3.1. Install the STM32MPU OpenSTLinux Distribution Package[edit | edit source]

As prerequisite to X-LINUX-QT Distribution Package, you need to get and install the STM32MPU OpenSTLinux Distribution Package v5.1.0.

The way to proceed is given in STM32MPU_Distribution_Package article.

6.1.3.2. Install X-LINUX-QT Distribution Package[edit | edit source]

To install the X-LINUX-QT Distribution Package follow the below steps

6.1.3.2.1. Clone the meta-st-x-linux-qt git repository[edit | edit source]
 cd <Distribution Package installation directory>
CollapseFor Qt6:
 git clone -b v2.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt
For Qt5:
 git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt
6.1.3.2.2. Clone the meta-qt git repository[edit | edit source]
CollapseFor Qt6:
 git clone -b 6.5.3 https://code.qt.io/yocto/meta-qt6.git layers/meta-qt6
For Qt5:
 git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5
6.1.3.2.3. Setup the build environment[edit | edit source]
CollapseFor Qt6:
  • For a new environment
Source the build environment with the correct board and layers:
CollapseFor STM32MP25x lines More info.png:
 DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt6 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh
  • For an already installed environment
Add the layers to the Yocto environment:
 cd <Distribution Package installation directory>
 source layers/meta-st/scripts/envsetup.sh
 bitbake-layers add-layer ../layers/meta-qt6 ../layers/meta-st/meta-st-x-linux-qt
For Qt5:
  • For a new environment
Source the build environment with the correct board and layers:
CollapseFor STM32MP25x lines More info.png:
 DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt5 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh
  • For an already installed environment
Add the layers to the Yocto environment:
 cd <Distribution Package installation directory>
 source layers/meta-st/scripts/envsetup.sh
 bitbake-layers add-layer ../layers/meta-qt5 ../layers/meta-st/meta-st-x-linux-qt
6.1.3.3. Re-build the X-LINUX-QT Starter Package[edit | edit source]
X-LINUX-QT-Starter Package-Overview.png

To rebuild the X-LINUX-QT Starter Package, user must install the X-LINUX-QT Distribution Package (as explained in previous chapter), set up the environment and run the adequate bitbake command as below:

 bitbake st-image-qt package-index

The output will be the "full image" files for the st-image-qt.

6.1.3.4. Re-build the X-LINUX-QT Developer Package[edit | edit source]
X-LINUX-QT-Developer Package-Overview.png


To rebuild the X-LINUX-QT Developer Package, user must install the X-LINUX-QT Distribution Package (as explained in previous chapter), set up the environment and run the adequate bitbake command as below:

 bitbake st-image-qt -c do_populate_sdk

The output will be the full SDK installer for the st-image-qt.




7. How to create QT applications using the X-LINUX-QT Developer Package[edit | edit source]


7.1. Building QT application using CMake[edit source]

7.1.1. Update the SDK environment for CMake[edit | edit source]

Follow below steps if you need to add the missing OE_CMAKE_TOOLCHAIN_FILE variable to your SDK configuration

  • Open terminal and load the environment setup
 source /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/environment-setup-cortexa35-ostl-linux
  • Export the OE_CMAKE_TOOLCHAIN_FILE variable
 export OE_CMAKE_TOOLCHAIN_FILE="$OECORE_NATIVE_SYSROOT/usr/lib/cmake/Qt6/qt.toolchain.cmake"
7.1.2. Download the Demo example source code[edit | edit source]
 mkdir -p /opt/st/demos/Qt
 cd /opt/st/demos/Qt
 git clone https://github.com/KDABLabs/KDBoatDemo.git -b qt6
7.1.3. Build the Demo example[edit | edit source]
 cd KDBoatDemo
 cmake -S . -B config_default
-- Toolchain file defaulted to '/opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/x86_64-ostl_sdk-linux/usr/lib/cmake/Qt6/qt.toolchain.cmake'
-- The C compiler identification is GNU 12.3.0
-- The CXX compiler identification is GNU 12.3.0
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/x86_64-ostl_sdk-linux/usr/bin/aarch64-ostl-linux/aarch64-ostl-linux-gcc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - done
-- Check for working CXX compiler: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/x86_64-ostl_sdk-linux/usr/bin/aarch64-ostl-linux/aarch64-ostl-linux-g++ - skipped
-- Detecting CXX compile features
-- Detecting CXX compile features - done
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD - Success
-- Found Threads: TRUE  
-- Performing Test HAVE_STDATOMIC
-- Performing Test HAVE_STDATOMIC - Success
-- Found WrapAtomic: TRUE  
-- Performing Test HAVE_EGL
-- Performing Test HAVE_EGL - Success
-- Found EGL: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/cortexa35-ostl-linux/usr/include (found version "1.5") 
-- Performing Test HAVE_GLESv2
-- Performing Test HAVE_GLESv2 - Success
-- Found GLESv2: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/cortexa35-ostl-linux/usr/include  
-- Found XKB: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/cortexa35-ostl-linux/usr/lib/libxkbcommon.so (found suitable version "1.5.0", minimum required is "0.5.0") 
-- Could NOT find WrapVulkanHeaders (missing: Vulkan_INCLUDE_DIR) 
-- Could NOT find WrapVulkanHeaders (missing: Vulkan_INCLUDE_DIR) 
-- Configuring done
-- Generating done
-- Build files have been written to: /opt/st/demos/Qt/KDBoatDemo/config_default
 cmake --build config_default --target all
[  7%] Running qmlimportscanner for KDABBoatDemo
[  7%] Built target KDABBoatDemo_qmlimportscan
[ 15%] Automatic MOC for target KDABBoatDemo
[ 15%] Built target KDABBoatDemo_autogen
[ 23%] Automatic RCC for imagesMaps2.qrc
[ 30%] Automatic RCC for data.qrc
[ 38%] Automatic RCC for images.qrc
[ 46%] Automatic RCC for imagesMaps.qrc
[ 53%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/mocs_compilation.cpp.o
[ 61%] Building CXX object CMakeFiles/KDABBoatDemo.dir/main.cpp.o
[ 69%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_imagesMaps.cpp.o
[ 76%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_imagesMaps2.cpp.o
[ 84%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_images.cpp.o
[ 92%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_data.cpp.o
[100%] Linking CXX executable KDABBoatDemo
[100%] Built target KDABBoatDemo
7.1.4. Deploy the Demo example to your running board[edit | edit source]
  • Copy the Example's binary into your connected board
 cd /opt/st/demos/Qt
 scp config_default/KDABBoatDemo root@192.168.7.1:/home/root/.
7.1.5. Run the Demo example on your board[edit | edit source]
  • Connect to your running board
 ssh root@192.168.7.1
  • Run the Demo's example (windowed mode)
 ./KDABBoatDemo
  • Check the running Demo example on your board's display
Running KDAB Boat Demo on target (Windowed Mode)
  • Run the Demo's example (Full screen mode)
 ./KDABBoatDemo --fullscreen
  • Check the running Demo example on your board's display
Running KDAB Boat Demo on target (Full screen Mode)


7.2. Building QT application using STM32CubeIDE[edit source]

7.2.1. Update the SDK environment for CMake[edit | edit source]

Please follow below steps if you need to add the missing OE_CMAKE_TOOLCHAIN_FILE variable to your SDK configuration

  • Open terminal and load the environment setup
 source /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/environment-setup-cortexa35-ostl-linux
  • Add the missing OE_CMAKE_TOOLCHAIN_FILE variable to the qt6 environment file
 echo "export OE_CMAKE_TOOLCHAIN_FILE=\"\$OECORE_NATIVE_SYSROOT/usr/lib/cmake/Qt6/qt.toolchain.cmake\"" >> $OECORE_NATIVE_SYSROOT/environment-setup.d/qt6.sh
7.2.2. Install the STM32CubeIDE[edit | edit source]
  • Please follow instructions from here to know how to install and use the STM32CubeIDE.
7.2.3. Select the updated OpenSTLinux SDK by the X-LINUX-QT Developer Package[edit | edit source]
  • Please follow instructions from here to know how to install the STM32MPU OpenSTLinux Developper Package for the STM32CubeIDE.
  • Please select the updated STM32MPU OpenSTLinux Developper Package by the X-LINUX-QT Developer Package.
7.2.4. Download the Demo example source code[edit | edit source]
 mkdir -p /opt/st/demos/Qt
 cd /opt/st/demos/Qt
 git clone https://github.com/KDABLabs/KDBoatDemo.git -b qt6
7.2.5. Build the Demo example[edit | edit source]
  • Import the Project from STM32CubeIDE
  • Start a new STM32 CMake Project
STM32CubeIDE New CMake Project 01.png


  • Select Project with existing CMake sources
STM32CubeIDE New CMake Project 02.png


  • Fill the Project name and source directory
  • Project name = KDBoatDemo
  • Source directory = /opt/st/demos/Qt/KDBoatDemo
STM32CubeIDE New CMake Project 03.png


  • Configure default toolchain
  • Select OpenSTLinux SDK for the Toolchain field
  • Select your installed OpenSTLinux SDK (openstlinux-6.1-yocto-mickledore-mpu-v24.06.26) for the Version field
STM32CubeIDE New CMake Project 04.png


  • Build the Project
  • Select the project from the list and press the Build button
STM32CubeIDE Build CMake Project 01.png
  • Wait until the build is finished and make sure it is done successfully
STM32CubeIDE Build CMake Project 02.png
7.2.6. Deploy the Demo example to your running board[edit | edit source]
  • Copy the Example's binary into your connected board
 cd /opt/st/demos/Qt
 scp config_default/KDABBoatDemo root@192.168.7.1:/home/root/.
7.2.7. Run the Demo example on your board[edit | edit source]
  • Connect to your running board
 ssh root@192.168.7.1
  • Run the Demo's example (windowed mode)
 ./KDABBoatDemo
  • Check the running Demo example on your board's display
Running KDAB Boat Demo on target (Windowed Mode)
  • Run the Demo's example (Full screen mode)
 ./KDABBoatDemo --fullscreen
  • Check the running Demo example on your board's display
Running KDAB Boat Demo on target (Full screen Mode)


7.3. Building Qt applications using Qt Creator[edit source]

The Qt™ Creator[2] tool is used to build, debug and run applications demos on target.

7.3.1. Install the Qt Creator[edit | edit source]
  • The Qt™ Creator can be downloaded and installed following this link
  • The Qt™ online installer can be dowloaded cliking on this link
  • Installing the X-LINUX-QT Developer Package configures also the new STM32MPU Kit for the already installed Qt™ Creator IDE.
7.3.2. Select the new Kit installed by the X-LINUX-QT Developer Package[edit | edit source]

Once the Qt™ Creator is launched and the Welcome to Qt™ Creator is displayed:

  • Go to the Examples from the list on the left ,
  • Then select the new Qt6 6.5.3 from the dropdown list.

The supported examples are then displayed.

Qt™ Creator Welcome Screen - Qt 6.5.3 Examples
7.3.3. Select the project example[edit | edit source]
  • You may search for a specific example in the Search bar in front of the selected Kit
  • Select the example you are looking for (just a simple click on it)
Qt™ Creator Welcome Screen - Select the example
  • Close the Help window if not needed
Qt™ Creator Welcome Screen - The example's Help window
7.3.4. Configure the project example[edit | edit source]
  • Make sure the new added Kit by X-LINUX-QT Developer Package is selected
  • Press the Configure Project button
Qt™ Creator - Configure Project
  • Make sure all configuration steps are successfully done (Green Bars)
Qt™ Creator - Project Configuration Status
7.3.5. Configure the STM32 MPU Kit[edit | edit source]
  • Select the Configure Project button from the vertical bar on the left
  • Select the new Kit added by the X-LINUX-QT Developer Package
  • Select Run Settings
  • On the right panel, scroll down till the Environment section
  • Press the Details button
  • Add the below environment variables
XDG_RUNTIME_DIR=/run/user/1000
QT_QPA_PLATFORM=wayland
QT_VULKAN_LIB=/usr/lib/libvulkan.so.1
Qt™ Creator - Configure Run Settings
7.3.6. Build and run the project[edit | edit source]
  • Make sure your board is connected to your host machine via the USB DRD TypeC connector.
  • Follow instructions from the Hardware setup section and check how to get your board connected to your host machine.
  • Once in the Run Setting panel, you shouldn't have the below notice at the bottom of the screen.
Qt™ Creator - Run Project
  • Press the Run button from the vertical bar on the left
  • That will build, deploy and run the selected example on the connected board.
Qt™ Creator - Run Project
  • If everything went well, then the example will be running on the connected board.
The Quick Items example running on the target




8. References[edit | edit source]