Last edited 9 months ago

Ethtool


1. Article purpose[edit | edit source]

This article provides the basic information needed to start using the Linux® command tool: ethtool [1].

2. Introduction[edit | edit source]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
ethtool Monitoring tools ethtool[1] allows to query or control network driver and hardware settings, in particular for wired Ethernet devices. Yes Yes Yes No No No

3. Installing the trace and debug tool on your target board[edit | edit source]

3.1. Using the STM32MPU Embedded Software distribution[edit | edit source]

ethtool is installed by default and ready to be used with all STM32MPU Embedded Software Packages.

 which ethtool
/usr/sbin/ethtool

It is integrated in weston image distribution through the meta-st package: meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools-base.bb.

RDEPENDS:packagegroup-framework-tools-base-network = "\
    ethtool         \
    iproute2        \
    curl            \
"

4. Getting started[edit | edit source]

The Ethernet links available on your board can be listed by using the IP Linux command line:

ip link | grep end
3: end0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP mode DEFAULT group default qlen 1000
  • Get information about the end0 network device:
ethtool end0
Settings for end0:
        Supported ports: [ TP    MII ]
        Supported link modes:   10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Half 1000baseT/Full
        Supported pause frame use: Symmetric Receive-only
        Supports auto-negotiation: Yes
        Supported FEC modes: Not reported
        Advertised link modes:  10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Half 1000baseT/Full
        Advertised pause frame use: Symmetric Receive-only
        Advertised auto-negotiation: Yes
        Advertised FEC modes: Not reported
        Link partner advertised link modes:  10baseT/Half 10baseT/Full
                                             100baseT/Half 100baseT/Full
                                             1000baseT/Full
        Link partner advertised pause frame use: No
        Link partner advertised auto-negotiation: Yes
        Link partner advertised FEC modes: Not reported
        Speed: 1000Mb/s
        Duplex: Full
        Auto-negotiation: on
        master-slave cfg: preferred slave
        master-slave status: slave
        Port: Twisted Pair
        PHYAD: 0
        Transceiver: external
        MDI-X: Unknown
        Supports Wake-on: ug
        Wake-on: d
        Current message level: 0x0000003f (63)
                               drv probe link timer ifdown ifup
        Link detected: yes
  • Display Ethernet driver settings for end0
ethtool -i end0
driver: st_gmac
version: 6.1.82
firmware-version: 
expansion-rom-version: 
bus-info: 
supports-statistics: yes
supports-test: no
supports-eeprom-access: no
supports-register-dump: yes
supports-priv-flags: no
  • Display network statistics for end0:
 ethtool -S end0
NIC statistics:
     mmc_tx_octetcount_gb: 0
     mmc_tx_framecount_gb: 0
     mmc_tx_broadcastframe_g: 0
     mmc_tx_multicastframe_g: 0
     mmc_tx_64_octets_gb: 0
     mmc_tx_65_to_127_octets_gb: 0
     mmc_tx_128_to_255_octets_gb: 0
     mmc_tx_256_to_511_octets_gb: 0
     mmc_tx_512_to_1023_octets_gb: 0
     mmc_tx_1024_to_max_octets_gb: 0
     mmc_tx_unicast_gb: 0
     mmc_tx_multicast_gb: 0
     mmc_tx_broadcast_gb: 0
     mmc_tx_underflow_error: 0
     mmc_tx_singlecol_g: 0
     mmc_tx_multicol_g: 0
     mmc_tx_deferred: 0
     mmc_tx_latecol: 0
     mmc_tx_exesscol: 0
     mmc_tx_carrier_error: 0
     mmc_tx_octetcount_g: 0
     mmc_tx_framecount_g: 314
     mmc_tx_excessdef: 0
     mmc_tx_pause_frame: 0
     mmc_tx_vlan_frame_g: 0
     mmc_rx_framecount_gb: 0
     mmc_rx_octetcount_gb: 0
     mmc_rx_octetcount_g: 0
     mmc_rx_broadcastframe_g: 0
     mmc_rx_multicastframe_g: 0
     mmc_rx_crc_error: 0
     mmc_rx_align_error: 0
     mmc_rx_run_error: 0
     mmc_rx_jabber_error: 0
     mmc_rx_undersize_g: 0
     mmc_rx_oversize_g: 0
     mmc_rx_64_octets_gb: 0
     mmc_rx_65_to_127_octets_gb: 0
     mmc_rx_128_to_255_octets_gb: 0
     mmc_rx_256_to_511_octets_gb: 0
     mmc_rx_512_to_1023_octets_gb: 0
     mmc_rx_1024_to_max_octets_gb: 0
     mmc_rx_unicast_g: 75
     mmc_rx_length_error: 0
     mmc_rx_autofrangetype: 0
     mmc_rx_pause_frames: 0
     mmc_rx_fifo_overflow: 0
     mmc_rx_vlan_frames_gb: 0
     mmc_rx_watchdog_error: 0
     mmc_rx_ipc_intr_mask: 0
     mmc_rx_ipc_intr: 0
     mmc_rx_ipv4_gd: 0
     mmc_rx_ipv4_hderr: 0
     mmc_rx_ipv4_nopay: 0
     mmc_rx_ipv4_frag: 0
     mmc_rx_ipv4_udsbl: 0
     mmc_rx_ipv4_gd_octets: 0
     mmc_rx_ipv4_hderr_octets: 0
     mmc_rx_ipv4_nopay_octets: 0
     mmc_rx_ipv4_frag_octets: 0
     mmc_rx_ipv4_udsbl_octets: 0
     mmc_rx_ipv6_gd_octets: 0
     mmc_rx_ipv6_hderr_octets: 0
     mmc_rx_ipv6_nopay_octets: 0
     mmc_rx_ipv6_gd: 0
     mmc_rx_ipv6_hderr: 0
     mmc_rx_ipv6_nopay: 0
     mmc_rx_udp_gd: 0
     mmc_rx_udp_err: 0
     mmc_rx_tcp_gd: 0
     mmc_rx_tcp_err: 0
     mmc_rx_icmp_gd: 0
     mmc_rx_icmp_err: 0
     mmc_rx_udp_gd_octets: 0
     mmc_rx_udp_err_octets: 0
     mmc_rx_tcp_gd_octets: 0
     mmc_rx_tcp_err_octets: 0
     mmc_rx_icmp_gd_octets: 0
     mmc_rx_icmp_err_octets: 0
     mmc_tx_fpe_fragment_cntr: 0
     mmc_tx_hold_req_cntr: 0
     mmc_rx_packet_assembly_err_cntr: 0
     mmc_rx_packet_smd_err_cntr: 0
     mmc_rx_packet_assembly_ok_cntr: 0
     mmc_rx_fpe_fragment_cntr: 0
     tx_underflow: 0
     tx_carrier: 0
     tx_losscarrier: 0
     vlan_tag: 0
     tx_deferred: 0
     tx_vlan: 0
     tx_jabber: 0
     tx_frame_flushed: 0
     tx_payload_error: 0
     tx_ip_header_error: 0
     rx_desc: 0
     sa_filter_fail: 0
     overflow_error: 0
     ipc_csum_error: 0
     rx_collision: 0
     rx_crc_errors: 0
     dribbling_bit: 0
     rx_length: 0
     rx_mii: 0
     rx_multicast: 0
     rx_gmac_overflow: 0
     rx_watchdog: 0
     da_rx_filter_fail: 0
     sa_rx_filter_fail: 0
     rx_missed_cntr: 0
     rx_overflow_cntr: 0
     rx_vlan: 0
     rx_split_hdr_pkt_n: 0
     tx_undeflow_irq: 0
     tx_process_stopped_irq: 0
     tx_jabber_irq: 0
     rx_overflow_irq: 0
     rx_buf_unav_irq: 0
     rx_process_stopped_irq: 0
     rx_watchdog_irq: 0
     tx_early_irq: 0
     fatal_bus_error_irq: 0
     rx_early_irq: 0
     threshold: 1
     tx_pkt_n: 314
     rx_pkt_n: 2816
     normal_irq_n: 2696
     rx_normal_irq_n: 2684
     napi_poll: 5676
     tx_normal_irq_n: 12
     tx_clean: 2992
     tx_set_ic_bit: 12
     irq_receive_pmt_irq_n: 0
     mmc_tx_irq_n: 0
     mmc_rx_irq_n: 0
     mmc_rx_csum_offload_irq_n: 0
     irq_tx_path_in_lpi_mode_n: 0
     irq_tx_path_exit_lpi_mode_n: 0
     irq_rx_path_in_lpi_mode_n: 0
     irq_rx_path_exit_lpi_mode_n: 0
     phy_eee_wakeup_error_n: 0
     ip_hdr_err: 0
     ip_payload_err: 0
     ip_csum_bypassed: 1026
     ipv4_pkt_rcvd: 1487
     ipv6_pkt_rcvd: 263
     no_ptp_rx_msg_type_ext: 2816
     ptp_rx_msg_type_sync: 0
     ptp_rx_msg_type_follow_up: 0
     ptp_rx_msg_type_delay_req: 0
     ptp_rx_msg_type_delay_resp: 0
     ptp_rx_msg_type_pdelay_req: 0
     ptp_rx_msg_type_pdelay_resp: 0
     ptp_rx_msg_type_pdelay_follow_up: 0
     ptp_rx_msg_type_announce: 0
     ptp_rx_msg_type_management: 0
     ptp_rx_msg_pkt_reserved_type: 0
     ptp_frame_type: 0
     ptp_ver: 0
     timestamp_dropped: 0
     av_pkt_rcvd: 0
     av_tagged_pkt_rcvd: 0
     vlan_tag_priority_val: 0
     l3_filter_match: 0
     l4_filter_match: 0
     l3_l4_filter_no_match: 0
     irq_pcs_ane_n: 0
     irq_pcs_link_n: 0
     irq_rgmii_n: 0
     mtl_tx_status_fifo_full: 0
     mtl_tx_fifo_not_empty: 0
     mmtl_fifo_ctrl: 0
     mtl_tx_fifo_read_ctrl_write: 0
     mtl_tx_fifo_read_ctrl_wait: 0
     mtl_tx_fifo_read_ctrl_read: 0
     mtl_tx_fifo_read_ctrl_idle: 0
     mac_tx_in_pause: 0
     mac_tx_frame_ctrl_xfer: 0
     mac_tx_frame_ctrl_idle: 0
     mac_tx_frame_ctrl_wait: 0
     mac_tx_frame_ctrl_pause: 0
     mac_gmii_tx_proto_engine: 0
     mtl_rx_fifo_fill_level_full: 0
     mtl_rx_fifo_fill_above_thresh: 0
     mtl_rx_fifo_fill_below_thresh: 0
     mtl_rx_fifo_fill_level_empty: 0
     mtl_rx_fifo_read_ctrl_flush: 0
     mtl_rx_fifo_read_ctrl_read_data: 0
     mtl_rx_fifo_read_ctrl_status: 0
     mtl_rx_fifo_read_ctrl_idle: 0
     mtl_rx_fifo_ctrl_active: 0
     mac_rx_frame_ctrl_fifo: 0
     mac_gmii_rx_proto_engine: 0
     tx_tso_frames: 0
     tx_tso_nfrags: 0
     mtl_est_cgce: 0
     mtl_est_hlbs: 0
     mtl_est_hlbf: 0
     mtl_est_btre: 0
     mtl_est_btrlm: 0
     q0_tx_pkt_n: 314
     q0_tx_irq_n: 12
     q0_rx_pkt_n: 2816
     q0_rx_irq_n: 2684

5. To go further[edit | edit source]

Lots of documentation exists on Internet about ethtool.

Refer to ethtool man page[1] for more details on command options.

6. References[edit | edit source]


  • Useful external links
Document link Document Type Description
ethtool Standard Wikipedia article
ethtool-command User guide thegeekstuff web page