Last edited 10 months ago

STM32DDRFW-UTIL release note


The STM32DDRFW-UTIL is an STMicroelectronics original initiative required for DDR configurations and tests. The objective of this firmware is to configure the DDR Subsystem (DDRSS) on STMicroelectronics boards and test the DDR configuration.

More information can be found in the detailed release notes referenced later in this article.

1. STM32DDRFW-UTIL - Version v1.1.0[edit | edit source]

STM32DDRFW-UTIL for Linux® and Windows® host PC
Download

Version v1.1.0

  • STM32DDRFW-UTIL firmware package is available: here .
Installing the STM32DDRFW-UTIL
  • To use STM32DDRFW-UTIL, unzip the package on computer..
  • Then refer to README.md , to use this tool .
Detailed release note
  • Full details about the content of this tool release are available here: here .