Last edited 8 months ago

MB1605


MB1605 board overview.

1. Board overview[edit | edit source]

Main board MB1605, revision C-01: part of the STM32MP257x-DK Discovery kit More info green.png.

STM32MP257x-DK Discovery kit front side
STM32MP257F-DK shown here (picture is not contractual)


Details about some LEDs:

  • The LD11: turns green if power connection established (the power cable is inserted into the CN21 connector).
  • Two general-purpose color LEDs (LED1 and LD9) are available as light indicators:
    • The blue LED (LED1) is used as the Linux® Heartbeat LED, which is blinking as long as Linux® is alive on the Cortex®-A.
    • The orange LED (LD9) is used as a STM32Cube example verdict LED.
  • The two LEDs, the LD7 (red) and LD8 (green) are either connected to the STM32MP257 MPU ??? sentence coming form UM, not enough clear
  • The LEDs (LD5 and LD6) are used as ST-LINK indicator status.


STM32MP257x-DK Discovery kit back side
STM32MP257F-DK shown here (picture is not contractual)




2. Links[edit | edit source]

MB1605 schematics