1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the DCMIPP peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The DCMIPP (digital camera memory interface pixel processor) peripheral is used to receive video data from an external parallel camera sensor device, or from any other digital video equipment supporting a parallel interface.
The DCMIPP hardware block can receive various frame data formats such as: RAW8, RGB565, YUV422 and other formats, as well as compressed data such as JPEG.
Moreover, on STM32MP2 series:
- the DCMIPP is also connected to the CSI internal peripheral that provides an interface to communicate with MIPI® CSI-compliant camera sensors: the DCMIPP is able to get pixels from the parallel or MIPI® CSI interface.
- the DCMIPP embeds 3 dedicated pixel pipelines named "dump", "main" and "auxiliary": camera sensor data go into these pixel pipelines before they are sent to memory for further processing or display purposes.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP1 series[edit | edit source]
The DCMIPP peripheral is not used at boot time.
3.1.2. On STM32MP2 series[edit | edit source]
3.1.2.1. Cortex-A35 master boot[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Visual | DCMIPP | DCMIPP | ⬚ |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Visual | DCMIPP | DCMIPP | ☑ |
3.2.2. On STM32MP21 unknown microprocessor device[edit | edit source]
| rowspan="1" | Visual | rowspan="1" | DCMIPP | DCMIPP | ⬚OP-TEE | ☑ | ⬚ | ☐ | |-
|}
3.2.3. On STM32MP23 unknown microprocessor device[edit | edit source]
| rowspan="1" | Visual | rowspan="1" | DCMIPP | DCMIPP | ⬚OP-TEE | ☑ | ⬚ | ☐ | |-
|}
3.2.4. On STM32MP25x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Visual | DCMIPP | DCMIPP | ⬚OP-TEE | ☑ | ⬚ | ☐ |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the DCMIPP peripheral for the embedded software components listed in the above tables.
- Linux®: V4L2 framework
- STM32Cube:
- for STM32MP13x lines
: DCMIPP HAL driver and header file of DCMIPP HAL module
- for STM32MP2 series: DCMIPP HAL driver and header file of DCMIPP HAL module
- for STM32MP13x lines
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
See also additional information in the DCMIPP device tree configuration article for Linux®.