X-LINUX-QT How To




This article aims to explain How to use the the latest X-LINUX-QT Developer Package for the STM32 microprocessor series.

1. Prerequisites[edit source]

Refer to the detailed prerequisites here.

2. Building QT application using CMake[edit source]

2.1. Update the SDK environment for CMake[edit | edit source]

Follow the steps bellow in case it is necessary to add the missing OE_CMAKE_TOOLCHAIN_FILE variable to the SDK configuration.

  • Open the terminal and load the environment setup:
 source /opt/st/stm32mp2/5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/environment-setup-cortexa35-ostl-linux
  • Export the OE_CMAKE_TOOLCHAIN_FILE variable:
 export OE_CMAKE_TOOLCHAIN_FILE="$OECORE_NATIVE_SYSROOT/usr/lib/cmake/Qt6/qt.toolchain.cmake"
2.2. Download the demo example source code[edit | edit source]
 mkdir -p /opt/st/demos/Qt
 cd /opt/st/demos/Qt
 git clone https://github.com/KDABLabs/KDBoatDemo.git -b qt6
2.3. Build the demo example[edit | edit source]
 cd KDBoatDemo
 cmake -S . -B config_default
-- Toolchain file defaulted to '/opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/x86_64-ostl_sdk-linux/usr/lib/cmake/Qt6/qt.toolchain.cmake'
-- The C compiler identification is GNU 12.3.0
-- The CXX compiler identification is GNU 12.3.0
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/x86_64-ostl_sdk-linux/usr/bin/aarch64-ostl-linux/aarch64-ostl-linux-gcc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - done
-- Check for working CXX compiler: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/x86_64-ostl_sdk-linux/usr/bin/aarch64-ostl-linux/aarch64-ostl-linux-g++ - skipped
-- Detecting CXX compile features
-- Detecting CXX compile features - done
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD - Success
-- Found Threads: TRUE  
-- Performing Test HAVE_STDATOMIC
-- Performing Test HAVE_STDATOMIC - Success
-- Found WrapAtomic: TRUE  
-- Performing Test HAVE_EGL
-- Performing Test HAVE_EGL - Success
-- Found EGL: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/cortexa35-ostl-linux/usr/include (found version "1.5") 
-- Performing Test HAVE_GLESv2
-- Performing Test HAVE_GLESv2 - Success
-- Found GLESv2: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/cortexa35-ostl-linux/usr/include  
-- Found XKB: /opt/st/stm32mp2/4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26_x-linux-qt_v2.0.0/sysroots/cortexa35-ostl-linux/usr/lib/libxkbcommon.so (found suitable version "1.5.0", minimum required is "0.5.0") 
-- Could NOT find WrapVulkanHeaders (missing: Vulkan_INCLUDE_DIR) 
-- Could NOT find WrapVulkanHeaders (missing: Vulkan_INCLUDE_DIR) 
-- Configuring done
-- Generating done
-- Build files have been written to: /opt/st/demos/Qt/KDBoatDemo/config_default
 cmake --build config_default --target all
[  7%] Running qmlimportscanner for KDABBoatDemo
[  7%] Built target KDABBoatDemo_qmlimportscan
[ 15%] Automatic MOC for target KDABBoatDemo
[ 15%] Built target KDABBoatDemo_autogen
[ 23%] Automatic RCC for imagesMaps2.qrc
[ 30%] Automatic RCC for data.qrc
[ 38%] Automatic RCC for images.qrc
[ 46%] Automatic RCC for imagesMaps.qrc
[ 53%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/mocs_compilation.cpp.o
[ 61%] Building CXX object CMakeFiles/KDABBoatDemo.dir/main.cpp.o
[ 69%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_imagesMaps.cpp.o
[ 76%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_imagesMaps2.cpp.o
[ 84%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_images.cpp.o
[ 92%] Building CXX object CMakeFiles/KDABBoatDemo.dir/KDABBoatDemo_autogen/EWIEGA46WW/qrc_data.cpp.o
[100%] Linking CXX executable KDABBoatDemo
[100%] Built target KDABBoatDemo
2.4. Deploy the demo example to the running board[edit | edit source]
  • Copy the Example's binary into the connected board:
 cd /opt/st/demos/Qt
 scp config_default/KDABBoatDemo root@192.168.7.1:/home/root/.
2.5. Run the demo example on the board[edit | edit source]
  • Connect to the running board:
 ssh root@192.168.7.1
  • Run the demo's example (windowed mode):
 ./KDABBoatDemo
  • Check the running demo example on the board's display:
Running KDAB Boat Demo on target (Windowed Mode)
  • Run the demo's example (full screen mode):
 ./KDABBoatDemo --fullscreen
  • Check the running demo example on the board's display:
Running KDAB Boat Demo on target (Full screen Mode)


3. Building QT application using STM32CubeIDE[edit source]

3.1. Update the SDK environment for CMake[edit | edit source]

Please follow the steps below if it is necessary to add the missing OE_CMAKE_TOOLCHAIN_FILE variable to the SDK configuration.

  • Open the terminal and load the environment setup:
 source /opt/st/stm32mp2/5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/environment-setup-cortexa35-ostl-linux
  • Add the missing OE_CMAKE_TOOLCHAIN_FILE variable to the qt6 environment file:
 echo "export OE_CMAKE_TOOLCHAIN_FILE=\"\$OECORE_NATIVE_SYSROOT/usr/lib/cmake/Qt6/qt.toolchain.cmake\"" >> $OECORE_NATIVE_SYSROOT/environment-setup.d/qt6.sh
3.2. Install the STM32CubeIDE[edit | edit source]
  • Follow the instructions from here to know how to install and use the STM32CubeIDE.
3.3. Select the updated OpenSTLinux SDK by the X-LINUX-QT Developer Package.[edit | edit source]
  • Follow the instructions from here to know how to install the STM32MPU OpenSTLinux Developper Package for the STM32CubeIDE.
  • Select the updated STM32MPU OpenSTLinux Developper Package by the X-LINUX-QT Developer Package.
3.4. Download the demo example source code[edit | edit source]
 mkdir -p /opt/st/demos/Qt
 cd /opt/st/demos/Qt
 git clone https://github.com/KDABLabs/KDBoatDemo.git -b qt6
3.5. Build the demo example[edit | edit source]
  • Import the Project from STM32CubeIDE.
  • Start a new STM32 CMake Project:
STM32CubeIDE New CMake Project 01.png


  • Select Project with existing CMake sources:
STM32CubeIDE New CMake Project 02.png


  • Fill the Project name and source directory.
  • Project name = KDBoatDemo
  • Source directory = /opt/st/demos/Qt/KDBoatDemo
STM32CubeIDE New CMake Project 03.png


  • Configure the default toolchain.
  • Select OpenSTLinux SDK for the Toolchain field.
  • Select the installed OpenSTLinux SDK (openstlinux-6.1-yocto-mickledore-mpu-v24.06.26) for the Version field.
STM32CubeIDE New CMake Project 04.png


  • Build the Project.
  • Select the project from the list and press the Build button:
STM32CubeIDE Build CMake Project 01.png
  • Wait until the build is finished and make sure it is done successfully:
STM32CubeIDE Build CMake Project 02.png
3.6. Deploy the demo example to your running board[edit | edit source]
  • Copy the example's binary into your connected board:
 cd /opt/st/demos/Qt
 scp config_default/KDABBoatDemo root@192.168.7.1:/home/root/.
3.7. Run the demo example on the board[edit | edit source]
  • Connect to the running board:
 ssh root@192.168.7.1
  • Run the demo's example (windowed mode):
 ./KDABBoatDemo
  • Check the running demo example on the board's display:
Running KDAB Boat demo on target (Windowed Mode)
  • Run the demo's example (Full screen mode):
 ./KDABBoatDemo --fullscreen
  • Check the running demo example on the board's display:
Running KDAB Boat demo on target (Full screen Mode)


4. Building Qt applications using Qt Creator[edit source]

The Qt™ Creator[1] tool is used to build, debug and run applications demos on target.

4.1. Install the Qt Creator[edit | edit source]
  • The Qt™ Creator can be downloaded and installed following this link.
  • The Qt™ online installer can be downloaded following this link.
  • Installing the X-LINUX-QT Developer Package configures also the new STM32MPU Kit for the already installed Qt™ Creator IDE.
4.2. Select the new Kit installed by the X-LINUX-QT Developer Package[edit | edit source]

Once the Qt™ Creator is launched and the Welcome to Qt™ Creator is displayed:

  • Go to the Examples from the list on the left,
  • Then select the new Qt6 6.5.3 from the dropdown list.

The supported examples are then displayed.

Qt™ Creator Welcome Screen - Qt 6.5.3 Examples
4.3. Select the project example[edit | edit source]
  • Search for a specific example in the Search bar in front of the selected kit.
  • Select the example you are looking for (just a simple click on it).
Qt™ Creator Welcome Screen - Select the example
  • Close the Help window if not needed.
Qt™ Creator Welcome Screen - The example's Help window
4.4. Configure the project example[edit | edit source]
  • Make sure that the new added Kit by X-LINUX-QT Developer Package is selected.
  • Press the Configure Project button:
Qt™ Creator - Configure Project
  • Make sure all configuration steps are successfully done (green bars):
Qt™ Creator - Project Configuration Status
4.5. Configure the STM32 MPU Kit[edit | edit source]
  • Select the Configure Project button from the vertical bar on the left.
  • Select the new Kit added by the X-LINUX-QT Developer Package.
  • Select Run Settings.
  • On the right panel, scroll down till the Environment section.
  • Press the Details button.
  • Add the below environment variables:
XDG_RUNTIME_DIR=/run/user/1000
QT_QPA_PLATFORM=wayland
QT_VULKAN_LIB=/usr/lib/libvulkan.so.1
Qt™ Creator - Configure Run Settings
4.6. Build and run the project[edit | edit source]
  • Make sure that the board is connected to the host machine via the USB DRD TypeC connector.
  • Follow the instructions from the Hardware setup section and check how to get your board connected to the host machine.
  • Once in the Run Setting panel, the notice below shouldn't appear at the bottom of the screen.
Qt™ Creator - Run Project
  • Press the Run button from the vertical bar on the left.
  • That will build, deploy and run the selected example on the connected board.
Qt™ Creator - Run Project
  • If everything went well, then the example will be running on the connected board.
The Quick Items example running on the target



5. References[edit source]