1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the RISAB peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit source]
The RISAB peripheral is part of the RIF. It is used to protect internal SRAM access.
Its main features are:
- Configuration at fixed size memory blocks (512B) and pages (4kB)
- Access filtering per:
- secure level
- CID filtering
- privilege level per CID
- read-only, write-only or read/write per CID
- Possibility to delegate page configuration to a specified execution context defined by delegated configuration CID. Useful to manage memory region access right at SW component level instead of requiring changes to TDCID secure OS.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
On STM32MP25x lines , there are 6 RISAB instances. The following table shows RISAB - Internal SRAM mapping and provides information regarding RISAB programming owner and default HW configuration.
RISAB registers are accessible in read by all execution context to check memory can be accessed or not.
RISAB instance | Internal SRAM | Owner | Default configuration |
---|---|---|---|
RISAB1 | SYSRAM1 (lower 128kB) | Cortex-A35 Secure | Secure, unprivileged, any CID |
RISAB2 | SYSRAM2 (upper 128kB) | Cortex-A35 Secure | Secure, unprivileged, any CID |
RISAB3 | MCURAM1 (lower 128kB) | TDCID Secure | Non-secure, unprivileged, any CID |
RISAB4 | MCURAM2 (upper128kB) | TDCID Secure | Non-secure, unprivileged, any CID |
RISAB5 | RETRAM | TDCID Secure | Secure, unprivileged, any CID |
RISAB6 | VDERAM | TDCID Secure | Non-secure, unprivileged, any CID |
RISAB configurations are done during bootflow according to memory usage. The ROM code, the FSBL configures RISAB to perform an initial RISAB configuration to allow and secure their execution. The RISAB configuration for run time execution is applied by TDCID secure OS.
3.1. Boot time assignment[edit source]
3.1.1. On STM32MP25x lines
[edit source]
Click on to expand or collapse the legend...
- ☐ means that the peripheral can be assigned to the given boot time context.
- ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Security | RISAB | RISAB1 | ✓ | ✓ | ⬚ | |
RISAB2 | ✓ | ✓ | ⬚ | |||
RISAB3 | ⬚ | ⬚ | ||||
RISAB4 | ⬚ | ⬚ | ||||
RISAB5 | ✓ | ⬚ | ⬚ | Used by ROM code only during cold boot | ||
RISAB6 | ⬚ | ⬚ |
3.2. Runtime assignment[edit source]
3.2.1. On STM32MP25x lines
[edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Security | RISAB | RISAB1 | ☑OP-TEE | ⬚ | ☐ | ☐ | ||
RISAB2 | ☑OP-TEE | ⬚ | ☐ | ☐ | ||||
RISAB3 | ☑OP-TEE | ⬚ | ☐ | ☐ | ||||
RISAB4 | ☑OP-TEE | ⬚ | ☐ | ☐ | ||||
RISAB5 | ☑OP-TEE | ⬚ | ☐ | ☐ | ||||
RISAB6 | ☑OP-TEE | ⬚ | ☐ | ☐ |
4. Software frameworks and drivers[edit source]
Below are listed the software frameworks and drivers managing the OTFDEC peripheral for the embedded software components listed in the above tables.
![]() |
Coming soon |
5. How to assign and configure the peripheral[edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:
- partial device trees (pin control and clock tree) for the OpenSTLinux software components,
- HAL initialization code for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
![]() |
Coming soon |
6. How to go further[edit source]
![]() |
Coming soon |
7. References[edit source]