Last edited 3 days ago

DCMIPP internal peripheral: Difference between revisions


Latest revision as of 11:35, 28 March 2025


1. Article purpose

The purpose of this article is to:

  • briefly introduce the DCMIPP peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview

The DCMIPP (digital camera memory interface pixel processor) peripheral is used to receive video data from an external camera sensor device, or from any other digital video equipment supporting its interfaces.

2.1. On STM32MP13x lines More info.png

The DCMIPP peripheral main features are:

  • Parallel input interface: up to 16 bits in parallel
  • Pipe0 (for data dump): for a direct dump from the camera to the memory without processing
    • Input pixel format: RGB565, RGB888, YUV422, raw Bayer/Mono 8/10/12/14, and ByteStream (JPEG)
    • Output pixel format: any data as-is, Y/Rb: 8/10/12/14 statistics, bit streams
    • Flow selection and frame control: Capture mode in Continuous vs. Snapshot mode
    • Crop and basic decimation

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

2.2. On STM32MP23x lines More info.png and STM32MP25x lines More info.png

The DCMIPP peripheral main features are the same as on STM32MP13x lines More info.png, with the following extra ones:

  • CSI-2 host input interface: MIPI CSI-2 v1.3, Interleaved packets, four virtual channels. Please refer to CSI internal peripheral for more details
  • Flow selection and frame control: CSI-2 interleaved packets supported, Capture mode in Continuous vs. Snapshot mode
  • Pipe1 (for main usage): with ISP, crop, downsize, ColorConv, decimation, multi-planar
    • Statistic removal
    • Bad pixel removal
    • Integrated image signal processing (ISP) block, which makes possible to connect very low cost camera modules without any embedded ISP: Black level calibration, Statistics extraction, Exposure control, Raw Bayer to RGB conversion (demosaicing), Color conversion to adapt to the sensor and tune the illumination, Contrast enhancement
    • Byte-to-pixel conversion
    • Output pixel format: 888, 565, 422-1, Y8, ARGB and RGBA (coplanar) and 422-2 / 420-2 / 420-3 (multi-planar)
  • Pipe2 (for ancillary usage): with crop, downsize, decimation, coplanar
    • Byte-to-pixel conversion
    • Output pixel format: 888, 565, 422-1, Y8, ARGB and RGBA (coplanar only)
  • Test pattern generator: Color bar or square pattern, up to 16k x 16k, YUV, raw, or Mono

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

2.3. On STM32MP21x lines More info.png

The DCMIPP peripheral main features are the same as on STM32MP23x lines More info.png and STM32MP25x lines More info.png, with the following extra ones:

  • Pipe1 (for main usage)
    • Integrated image signal processing (ISP) block: Statistics extraction supports the histogram extraction

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment

3.1.1. On STM32MP1 series

The DCMIPP peripheral is not used at boot time.

3.1.2. On STM32MP2 series

Click on How to.png to expand or collapse the legend...

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Visual DCMIPP DCMIPP

3.2. Runtime assignment

3.2.1. On STM32MP13x lines More info.png

Click on How to.png to expand or collapse the legend...

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Visual DCMIPP DCMIPP

3.2.2. On STM32MP21x lines More info.png

Click on How to.png to expand or collapse the legend...

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Visual DCMIPP DCMIPP OP-TEE

3.2.3. On STM32MP23x lines More info.png

Click on How to.png to expand or collapse the legend...

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Visual DCMIPP DCMIPP OP-TEE

3.2.4. On STM32MP25x lines More info.png

Click on How to.png to expand or collapse the legend...

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Visual DCMIPP DCMIPP OP-TEE

4. Software frameworks and drivers

Below are listed the software frameworks and drivers managing the DCMIPP peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the DCMIPP device tree configuration article for Linux®.