Registered User m (Linux-6.6.48 OV5640 command lines) |
Registered User (DV6.0 changes) |
||
Line 33: | Line 33: | ||
|} | |} | ||
Capture the JPEG pictures then decode and display them: | Capture the JPEG pictures then decode and display them: | ||
{{Board$}} | {{Board$}}v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --set-parm=30 --stream-mmap --stream-count=-1 {{highlight|'''--stream-to{{=}}-'''}} {{HighlightParam|2>/dev/null}} {{highlight|'''<nowiki>|</nowiki>'''}} gst-play-1.0 {{highlight|'''"fd://0"'''}} | ||
{{highlight|'''--stream-to{{=}}-'''}} tells [[V4l2-ctl]] to output binary captured content to standard output, which is then sent to pipe {{highlight|'''<nowiki>|</nowiki>'''}}. | {{highlight|'''--stream-to{{=}}-'''}} tells [[V4l2-ctl]] to output binary captured content to standard output, which is then sent to pipe {{highlight|'''<nowiki>|</nowiki>'''}}. | ||
Line 75: | Line 75: | ||
Then fill the {{HighlightParam|'''host{{=}}'''}} udpsink property with this IP address on the remote side: | Then fill the {{HighlightParam|'''host{{=}}'''}} udpsink property with this IP address on the remote side: | ||
{{Board$}} | {{Board$}}v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --set-parm=30 --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink {{HighlightParam|'''host{{=}}'''}}{{highlight|'''aa.bb.cc.dd'''}} port=5000 | ||
Then play the UDP stream on the host PC: | Then play the UDP stream on the host PC: |
Latest revision as of 16:48, 25 November 2024
1. Overview[edit | edit source]
This article explains how to stream camera content over network thanks to GStreamer application on top of V4L2 Linux® kernel framework.
Capturing compressed JPEG pictures is an efficient way to send camera images to any local or remote player. JPEG pictures require a limited bandwidth while being fully interoperable.
![]() |
This article focus on camera sensors that can directly output JPEG content, if it is not the case refer to How to stream RAW camera over network. |
Find below some examples of command lines allowing to capture a continuous JPEG stream while playing it using various multimedia players, either local or remote.
2. Local streaming[edit | edit source]
Here is an example of a local preview involving V4l2-ctl for JPEG pictures capture and gst-play GStreamer player for JPEG decoding and display. JPEG pictures are sent over a standard Linux pipe.
ExpandFor STM32MP135 line ![]() |
Capture the JPEG pictures then decode and display them:
--stream-to=- 2>/dev/null | gst-play-1.0 "fd://0"v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --set-parm=30 --stream-mmap --stream-count=-1
--stream-to=- tells V4l2-ctl to output binary captured content to standard output, which is then sent to pipe |.
Special URI fd://0 tells gst-play GStreamer player to read data from the pipe.
Note the 2>/dev/null right after the V4l2-ctl command to remove the logs from console output.
3. UDP streaming[edit | edit source]
An internet connection is required, for example, by plugging an Ethernet cable on the:
STM32MP135x-DK Discovery kit ![]() |
CN4 Ethernet connector 1 or CN15 Ethernet connector 2 |
STM32MP157x-DKx Discovery kit ![]() |
CN8 Ethernet connector |
STM32MP157x-EV1 Evaluation board ![]() |
CN3 Ethernet connector |
![]() |
On the STM32MP135x-DK board, the GC2145 camera sensor is not capable of streaming JPEG data, hence JPEG based network streaming is not possible with this sensor. The example below is given using a CSI based OV5640 sensor, capable of JPEG output. |
ExpandFor STM32MP135 line ![]() |
Get the IP addressaa.bb.cc.dd of the host PC using the ifconfig command:
aa.bb.cc.dd Bcast:10.201.23.255 Mask:255.255.252.0 inet addr:127.0.0.1 Mask:255.0.0.0ifconfig | grep "inet" inet addr:
Then fill the host= udpsink property with this IP address on the remote side:
host=aa.bb.cc.dd port=5000v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --set-parm=30 --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink
Then play the UDP stream on the host PC:
gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink
A new window appears on the host PC displaying the camera content.
![]() |
Due to SDP protocol signaling, this solution is not fully interoperable because it needs a dedicated GStreamer command line to be played on the host side. |