Registered User mNo edit summary |
Registered User |
||
Line 61: | Line 61: | ||
| rowspan="1" | [[FMC internal peripheral|FMC]] | | rowspan="1" | [[FMC internal peripheral|FMC]] | ||
| FMC | | FMC | ||
| <span title=" | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | | <span title="assignable peripheral" style="font-size:21px">☐</span> | ||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | | <span title="assignable peripheral" style="font-size:21px">☐</span> |
Revision as of 10:27, 9 November 2023
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the FMC peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The FMC peripheral includes two memory controllers:
- The NOR/PSRAM memory controller
- The NAND memory controller.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
2.1. NOR/PSRAM memory controller (or external bus interface controller)[edit | edit source]
The FMC NOR/PSRAM memory controller is used to interface static memory devices, but it is also used to interface Ethernet devices, LCD devices, and so on.
The FMC NOR/PSRAM controller generates the appropriate signal timings to drive the following types of memories:
- Asynchronous SRAM, FRAM and ROM
- 8 bits
- 16 bits
- PSRAM (CellularRAM™)
- Asynchronous mode
- Burst mode for synchronous accesses with configurable option to split burst access when crossing boundary page for CRAM 1.5.
- Multiplexed or non-multiplexed
- NOR Flash memory
- Asynchronous mode
- Burst mode for synchronous accesses
- Multiplexed or non-multiplexed
The FMC NOR/PSRAM controller supports a wide range of devices through programmable timings.
Among those programmable timings, there are:
- Programmable wait states (up to 15)
- Programmable bus turnaround cycles (up to 15)
- Programmable output enable and write enable delays (up to 15)
- Independent read and write timings and protocol to support the widest variety of memories and timings
- Programmable continuous clock output.
The FMC NOR/PSRAM controller also supports up to four external devices.
2.2. NAND Flash controller[edit | edit source]
The FMC NAND Flash controller is used to interface STM32 MPU with SLC 8-bit or 16-bit NAND Flash memory devices.
The FMC NAND Flash controller supports:
- Programmable error correction capability (ECC) using BCH8 code, BCH4 code or Hamming code
- Programmable page size of 2048, 4096 and 8192 bytes
- Programmable memory timings
- Multiple dice per package.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP1 series[edit | edit source]
The FMC NAND Flash controller is the boot device that supports serial boot for Flash programming with STM32CubeProgrammer.
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Mass storage | FMC | FMC | ☐ | ☐ | ☐ |
3.1.2. On STM32MP2 series[edit | edit source]
STM32MP2 internal peripherals assignment table template
| rowspan="1" | Mass storage
| rowspan="1" | FMC
| FMC
| ☐
| ☐
| ☐
| Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
|-
|}
The below table shows the possible boot time allocations for the features of the FMC instance. STM32MP2 internal peripherals assignment table template | FMC_CFGR | ☐ | ☐ | ☐ | |- | FMC_NOR/PSRAM1 | | ⬚ | ☐ | |- | FMC_NOR/PSRAM2 | | ⬚ | ☐ | |- | FMC_NOR/PSRAM3 | | ⬚ | ☐ | |- | FMC_NOR/PSRAM4 | | ⬚ | ☐ | |- | FMC_NAND | ☐ | ☐ | ☐ | |- |}
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Mass storage | FMC | FMC | ⬚ | ☐ | Assignment (single choice) |
3.2.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Mass storage | FMC | FMC | ☐ | ☐ | Assignment (single choice) |
3.2.3. On STM32MP25x lines
[edit | edit source]
STM32MP2 internal peripherals assignment table template
| rowspan="1" | Mass storage
| rowspan="1" | FMC
| FMC
| ☐OP-TEE
| ☐
| ☐
| ☐
| ☐
| Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
|-
|}
The below table shows the possible runtime allocations for the features of the FMC instance. STM32MP2 internal peripherals assignment table template | FMC_CFGR | ☐OP-TEE | ☐ | ☐ | ☐ | | |- | FMC_NOR/PSRAM1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | | |- | FMC_NOR/PSRAM2 | ⬚OP-TEE | ☐ | ⬚ | ☐ | | |- | FMC_NOR/PSRAM3 | ⬚OP-TEE | ☐ | ⬚ | ☐ | | |- | FMC_NOR/PSRAM4 | ⬚OP-TEE | ☐ | ⬚ | ☐ | | |- | FMC_NAND | ⬚OP-TEE | ☐ | ⬚ | ⬚ | | |- |}
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the FMC peripheral for the embedded software components listed in the above tables.
- Linux®: MTD framework and drivers (drivers/mtd/nand/raw/stm32_fmc2_nand.c , drivers/memory/stm32-fmc2-ebi.c )
- STM32Cube: FMC HAL driver
- TF-A BL2: MTD framework (drivers/mtd/nand/ ) and driver (drivers/st/fmc/stm32_fmc2_nand.c )
- U-Boot: MTD framework (drivers/mtd/nand/raw/ ) and drivers (drivers/mtd/nand/raw/stm32_fmc2_nand.c , drivers/memory/stm32-fmc2-ebi.c )
- OP-TEE: driver (core/drivers/stm32_fmc.c )
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
For Linux kernel configuration, please refer to FMC device tree configuration.