Registered User (Merge articles) |
Registered User m (→Overview) |
||
(32 intermediate revisions by 2 users not shown) | |||
Line 7: | Line 7: | ||
== Overview == | == Overview == | ||
To load and execute U-Boot (the programming service) in DDR with [[STM32CubeProgrammer]], you need first to follow the steps described in [[ | To load and execute U-Boot (the programming service) in DDR with [[STM32CubeProgrammer]], you need first to follow the steps described in [[STM32_MPU_resources#AN5275|AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders]]: | ||
# Download phase {{Highlight|0x1}} by ROM code, the FSBL = [[TF-A_overview|TF-A]] BL2 | # Download phase {{Highlight|0x1}} by ROM code, the FSBL = [[TF-A_overview|TF-A]] BL2 | ||
# Download phase {{Highlight|0x3}} by FSBL, the FIP file including the SSBL image: [[U-Boot_overview|U-Boot]] | # Download phase {{Highlight|0x3}} by FSBL, the FIP file including the SSBL image: [[U-Boot_overview|U-Boot]] | ||
Line 25: | Line 24: | ||
To access to U-Boot console when U-Boot is loaded with STM32CubeProgrammer: | To access to U-Boot console when U-Boot is loaded with STM32CubeProgrammer: | ||
* For USB boot, you can easily interrupt this command <code>stm32prog usb 0</code>by pressing <code> | * For USB boot, you can easily interrupt this command <code>stm32prog usb 0</code>by pressing <code>Ctrl</code> + <code>C</code> in the console without U-Boot modification. | ||
* For UART boot, the U-Boot console is deactivated to execute the <code>stm32prog serial ${boot_instance}</code> command in the [[U-Boot_overview#bootcmd|bootcmd]].<br/>To use the U-Boot console after STM32CubeProgrammer load, you can deactivate this behavior by: | * For UART boot, the U-Boot console is deactivated to execute the <code>stm32prog serial ${boot_instance}</code> command in the [[U-Boot_overview#bootcmd|bootcmd]].<br/>To use the U-Boot console after STM32CubeProgrammer load, you can deactivate this behavior by: | ||
** deactivate CONFIG_CMD_STM32PROG_SERIAL using one of the following method: | ** deactivate CONFIG_CMD_STM32PROG_SERIAL using one of the following method: | ||
Line 32: | Line 31: | ||
** [[U-Boot_overview#U-Boot_build|recompile U-Boot]] | ** [[U-Boot_overview#U-Boot_build|recompile U-Boot]] | ||
== Load U-Boot using Flashlayout.tsv file == | |||
You can use a minimal [[STM32CubeProgrammer_flashlayout#Flashlayout-tsv_file_to_load_and_start_U-Boot|"FlashLayout.tsv"]] files for {{Highlight|<dev>}} serial boot, {{Highlight|<dev>}}=usb or uart (see [[STM32CubeProgrammer_flashlayout]] for file format details): | |||
You can use a minimal [[STM32CubeProgrammer_flashlayout# | |||
#Opt id Name Type IP Offset Binary | #Opt id Name Type IP Offset Binary | ||
Line 77: | Line 66: | ||
For serial USB boot, {{Highlight|<dev>}}={{Highlight|usb}} device with port={{HighlightParam|usb1}}. | For serial USB boot, {{Highlight|<dev>}}={{Highlight|usb}} device with port={{HighlightParam|usb1}}. | ||
{{PC$}} STM32_Programmer_CLI -c port={{HighlightParam|usb1}} \ | {{PC$}} STM32_Programmer_CLI -c port={{HighlightParam|usb1}} \ | ||
-d tf-a_{{Highlight|usb}}.stm32 {{Highlight|0x1}} -s {{Highlight|0x1}} \ | -d tf-a_{{Highlight|usb}}.stm32 {{Highlight|0x1}} -s {{Highlight|0x1}} \ | ||
-d fip.bin {{Highlight|0x3}} -s {{Highlight|0x3}} | -d fip.bin {{Highlight|0x3}} -s {{Highlight|0x3}} | ||
It is the same for serial UART boot with {{Highlight|<dev>}}={{Highlight|uart}} and {{HighlightParam|port}}= the UART Interface identifier. | It is the same for serial UART boot with {{Highlight|<dev>}}={{Highlight|uart}} and {{HighlightParam|port}}= the UART Interface identifier. | ||
When U-Boot is loaded, the <code>stm32prog</code> command is executed and it is waiting a .stm32 file {{HighlightParam|flashlayout.stm32}} in phase {{Highlight|0x0}}. | |||
This command can be interrupted by enter a<code>Ctrl</code> + <code>C</code> on the U-Boot console. | |||
== Load U-Boot script using CLI == | == Load U-Boot script using CLI == | ||
When | When U-Boot receives in phase {{Highlight|0x0}} a U-Boot script {{HighlightParam|script.bin}} with U-Boot image header added by <code>mkimage</code> U-Boot tool, this script will be executed automatically by U-Boot. | ||
Example for a simple script to start U-Boot in dfu mode and then reset : | Example for a simple script to start U-Boot in dfu mode and then reset: | ||
dfu 0 | dfu 0 | ||
Line 107: | Line 86: | ||
{{PC$}} echo "dfu 0; reset" > script.cmd | {{PC$}} echo "dfu 0; reset" > script.cmd | ||
{{PC$}} mkimage -C none -A arm -T script -d script.cmd | {{PC$}} mkimage -C none -A arm -T script -d script.cmd {{HighlightParam|script.bin}} | ||
{{PC$}} STM32_Programmer_CLI -c port={{HighlightParam|usb1}} \ | {{PC$}} STM32_Programmer_CLI -c port={{HighlightParam|usb1}} \ | ||
-d tf-a_{{Highlight|usb}}.stm32 {{Highlight|0x1}} -s {{Highlight|0x1}} \ | -d tf-a_{{Highlight|usb}}.stm32 {{Highlight|0x1}} -s {{Highlight|0x1}} \ | ||
-d fip.bin {{Highlight|0x3}} -s {{Highlight|0x3}} \ | -d fip.bin {{Highlight|0x3}} -s {{Highlight|0x3}} \ | ||
-d {{HighlightParam|script. | -d {{HighlightParam|script.bin}} {{Highlight|0x0}} -s {{Highlight|0x0}} --detach | ||
<noinclude> | <noinclude> | ||
[[Category:U-Boot]] | [[Category:U-Boot|U-Boot - 9]] | ||
{{PublicationRequestId | 1900 | 2021-02-16}} | {{PublicationRequestId | 1900 | 2021-02-16}} | ||
</noinclude> | </noinclude> |
Revision as of 18:18, 30 June 2022
This page explains how to load and start U-Boot with STM32CubeProgrammer over a UART or USB port.
1. Overview[edit | edit source]
To load and execute U-Boot (the programming service) in DDR with STM32CubeProgrammer, you need first to follow the steps described in AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders:
- Download phase 0x1 by ROM code, the FSBL = TF-A BL2
- Download phase 0x3 by FSBL, the FIP file including the SSBL image: U-Boot
The FSBL, SSBL and FIP definitions can be found in the Boot chain overview (FIP includes the required SSBL).
This feature can be used to debug U-Boot features required for the programming service (USB support, Flash device support, and so on) during board bring-up.
See FAQ of STM32CubeProgrammer for answers to questions specific to this tool.
For information, the required DFU detach is automatically managed by STM32CubeProgrammer when flashlayout is used or with start command in CLI mode.
2. Prepare U-Boot to use the console[edit | edit source]
By default in the STM32 boot command the stm32prog
command is executed when the boot device is UART or USB to allow U-Boot (the programming service) to communicate with STM32CubeProgrammer.
To access to U-Boot console when U-Boot is loaded with STM32CubeProgrammer:
- For USB boot, you can easily interrupt this command
stm32prog usb 0
by pressingCtrl
+C
in the console without U-Boot modification. - For UART boot, the U-Boot console is deactivated to execute the
stm32prog serial ${boot_instance}
command in the bootcmd.
To use the U-Boot console after STM32CubeProgrammer load, you can deactivate this behavior by:- deactivate CONFIG_CMD_STM32PROG_SERIAL using one of the following method:
- use
make menuconfig
as explained in Kbuild - add the line
# CONFIG_CMD_STM32PROG_SERIAL is not set
in your defconfig (for example stm32mp15_trusted_defconfig)
- use
- recompile U-Boot
- deactivate CONFIG_CMD_STM32PROG_SERIAL using one of the following method:
3. Load U-Boot using Flashlayout.tsv file[edit | edit source]
You can use a minimal "FlashLayout.tsv" files for <dev> serial boot, <dev>=usb or uart (see STM32CubeProgrammer_flashlayout for file format details):
0x01 fsbl Binary none 0x00000000 tf-a_<dev>.stm32 - 0x03 fip Binary none 0x00000000 fip.bin#Opt id Name Type IP Offset Binary -
You can then use this with STM32CubeProgrammer command:
<dev_port> -w FlashLayout.tsvPC $> STM32_Programmer_CLI -c port=
With
- For USB: <dev> = usb and <dev_port>=usb1
- For UART: <dev> =uart and <dev_port>= UART Interface identifier (ex COM1, /dev/ttyS0,...)
4. Load U-Boot using CLI[edit | edit source]
You can also use the CLI interface with the options -d and -s to load and start U-Boot.
MPU: .. -s, --start -g, --go : Run the code at the specified partition ID. [<partitionID>] : Partition ID If not specified, last loaded partition will be started .. -d, --download : Download the content of a file into device memory <file_path> : File path name to be downloaded: (bin, stm32 file <partition_id> : Partition ID to be downloadedPC $> STM32_Programmer_CLI --help Available commands for STM32
For serial USB boot, <dev>=usb device with port=usb1.
usb1 \ -d tf-a_usb.stm32 0x1 -s 0x1 \ -d fip.bin 0x3 -s 0x3PC $> STM32_Programmer_CLI -c port=
It is the same for serial UART boot with <dev>=uart and port= the UART Interface identifier.
When U-Boot is loaded, the stm32prog
command is executed and it is waiting a .stm32 file flashlayout.stm32 in phase 0x0.
This command can be interrupted by enter aCtrl
+ C
on the U-Boot console.
5. Load U-Boot script using CLI[edit | edit source]
When U-Boot receives in phase 0x0 a U-Boot script script.bin with U-Boot image header added by mkimage
U-Boot tool, this script will be executed automatically by U-Boot.
Example for a simple script to start U-Boot in dfu mode and then reset:
dfu 0
reset
script.binPC $> echo "dfu 0; reset" > script.cmd PC $> mkimage -C none -A arm -T script -d script.cmd
usb1 \ -d tf-a_usb.stm32 0x1 -s 0x1 \ -d fip.bin 0x3 -s 0x3 \ -d script.bin 0x0 -s 0x0 --detachPC $> STM32_Programmer_CLI -c port=