Registered User mNo edit summary |
Registered User m (Text replacement - "st_table" to "st-table") |
||
(11 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | ||
}}</noinclude> | }} | ||
The | <noinclude></noinclude> | ||
The STM32 Key Generator tool (KeyGen) generates three "key" files: | |||
* a public Key file. | * a public Key file. | ||
* a private Key file. | * a private Key file. | ||
* a Hash public key file. | * a Hash public key file. | ||
* a Hash table binary file (for Header version greater than 1) | |||
More information can be found in the detailed release notes referenced later in this article. | More information can be found in the detailed release notes referenced later in this article. | ||
==KeyGen - Version v2. | ==KeyGen - Version v2.18.0 == | ||
{| class=" | {| class="st-table" | ||
|- | |- | ||
!colspan="3" | KeyGen for Linux<sup>®</sup> and Windows<sup>®</sup> host PC | !colspan="3" | KeyGen for Linux<sup>®</sup> and Windows<sup>®</sup> host PC | ||
Line 16: | Line 18: | ||
| '''Download''' | | '''Download''' | ||
|colspan="2" | | |colspan="2" | | ||
'''Version v2. | '''Version v2.18.0''' | ||
* KeyGen is integrated in [[STM32CubeProgrammer]] package, available [https://www.st.com/en/development-tools/stm32cubeprog.html here] | * KeyGen is integrated in [[STM32CubeProgrammer]] package, available [https://www.st.com/en/development-tools/stm32cubeprog.html here] | ||
|- | |- | ||
| '''Installing the KeyGen tool''' | | '''Installing the KeyGen tool''' | ||
|colspan="2" | | |colspan="2" | | ||
* To use | * To use STM32 KeyGen Tool, the installation of [[STM32CubeProgrammer]] is needed. | ||
* '''The installation is then complete'''. To use this tool, follow the instruction given in [[KeyGen tool]]. | * '''The installation is then complete'''. To use this tool, follow the instruction given in [[KeyGen tool]]. | ||
|- | |- |
Latest revision as of 12:34, 12 March 2025
The STM32 Key Generator tool (KeyGen) generates three "key" files:
- a public Key file.
- a private Key file.
- a Hash public key file.
- a Hash table binary file (for Header version greater than 1)
More information can be found in the detailed release notes referenced later in this article.
1. KeyGen - Version v2.18.0[edit | edit source]
KeyGen for Linux® and Windows® host PC | ||
---|---|---|
Download |
Version v2.18.0
| |
Installing the KeyGen tool |
| |
Detailed release note |
|