deleted>Frq08988 mNo edit summary |
Registered User m (Text replacement - "st_table" to "st-table") |
||
(28 intermediate revisions by 10 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
{{ | |MPUs list=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | |||
}} | }} | ||
</noinclude> | <noinclude></noinclude> | ||
The STM32 Key Generator tool (KeyGen) generates three "key" files: | |||
The | |||
* a public Key file. | * a public Key file. | ||
* a private Key file. | * a private Key file. | ||
* a Hash public key file. | * a Hash public key file. | ||
* a Hash table binary file (for Header version greater than 1) | |||
More information can be found in the detailed release notes referenced later in this article. | More information can be found in the detailed release notes referenced later in this article. | ||
==KeyGen - Version v2.18.0 == | |||
{| class="st-table" | |||
==KeyGen - Version | |||
{| class=" | |||
|- | |- | ||
! | !colspan="3" | KeyGen for Linux<sup>®</sup> and Windows<sup>®</sup> host PC | ||
|- | |- | ||
| '''Download''' | | '''Download''' | ||
|| | |colspan="2" | | ||
'''Version | '''Version v2.18.0''' | ||
* KeyGen is integrated in [[STM32CubeProgrammer]] package, available [https://www.st.com/en/development-tools/stm32cubeprog.html here] | |||
* | |||
[ | |||
[https:// | |||
|- | |- | ||
| ''' | | '''Installing the KeyGen tool''' | ||
|| | |colspan="2" | | ||
* To use STM32 KeyGen Tool, the installation of [[STM32CubeProgrammer]] is needed. | |||
* | |||
* '''The installation is then complete'''. To use this tool, follow the instruction given in [[KeyGen tool]]. | * '''The installation is then complete'''. To use this tool, follow the instruction given in [[KeyGen tool]]. | ||
|- | |- | ||
| '''Detailed release note''' | | '''Detailed release note''' | ||
| colspan="2" | | | colspan="2" | | ||
* Full details about the content of this tool release are available | * Full details about the content of this tool release are available [https://www.st.com/en/development-tools/stm32cubeprog.html here]. | ||
|} | |} | ||
<noinclude> | |||
[[Category:Release notes]] | |||
[[Category:KeyGen tool]] | |||
{{PublicationRequestId | 7993 | 2018-06-28 | AnneJ}} | |||
{{UpdateNeededForNewRelease| | |||
* Copy the current release (first chapter) in the "Archives" chapter | |||
* Change the version of the tool | |||
* Change the name of the archive file | |||
* Change the download URLs | |||
}} | |||
</noinclude> | </noinclude> |
Latest revision as of 12:34, 12 March 2025
The STM32 Key Generator tool (KeyGen) generates three "key" files:
- a public Key file.
- a private Key file.
- a Hash public key file.
- a Hash table binary file (for Header version greater than 1)
More information can be found in the detailed release notes referenced later in this article.
1. KeyGen - Version v2.18.0[edit | edit source]
KeyGen for Linux® and Windows® host PC | ||
---|---|---|
Download |
Version v2.18.0
| |
Installing the KeyGen tool |
| |
Detailed release note |
|