Last edited 3 months ago

X-LINUX-AWS Starter package: Difference between revisions


Latest revision as of 17:13, 19 December 2024



1. Install from the OpenSTLinux X-LINUX-AWS package repository[edit | edit source]

All the generated X-LINUX-AWS packages are available from the OpenSTLinux X-LINUX-AWS package repository service hosted at the non-browsable URL http://extra.packages.openstlinux.st.com/AWS.

This repository contains X-LINUX-AWS packages that can be simply installed using apt-* utilities, which are the same as those used on a Debian® system:

  • The main group contains the selection of X-LINUX-AWS packages, the installation of which is automatically tested by STMicroelectronics.
  • The updates group is reserved for future uses such as package revision update.

You can install them individually or by package group.

1.1. Prerequisites[edit | edit source]

  • Your board has a direct (no proxy) connection to the Internet, either through the network cable or through a Wi-Fi® connection.

1.2. Configure the X-LINUX-AWS OpenSTLinux package repository[edit | edit source]

Once the board is booted, execute the following command in the console to configure the X-LINUX-AWS OpenSTLinux package repository:

For ecosystem release unknown revision 6.0.0 Warning.png :

Update the apt database:

apt-get update

Install the package with the apt configuration to access the X-LINUX-AWS packages

apt-get install apt-openstlinux-x-linux-aws

Update the apt database to access the X-LINUX-AWS package repository:

apt-get update


1.3. Install X-LINUX-AWS packages[edit | edit source]

1.3.1. Install all X-LINUX-AWS packages[edit | edit source]

Command Description
apt-get install packagegroup-x-linux-aws
Install all the X-LINUX-AWS packages (Greengrass-bin, Corretto-11, PKCS#11 implementation for OP-TEE, demonstration application)

Then, restart the demo launcher:

systemctl restart weston-graphical-session.service

2. How to use the X-LINUX-AWS Expansion Package[edit | edit source]

Go to X-LINUX-AWS package software setup.

3. Main software modifications[edit | edit source]

Through the Starter Package, the OpenSTLinux image is changed at the user space level by bringing the necessary libraries and tools to use AWS Greengrass and OP-TEE.

List of main modifications:

  • greengrass-bin package
    • Installation of Greengrass core software into directory /opt/greengrass/v2/
    • Installation of AmazonRootCA1 certificate
    • Installation of Pkcs11Provider 2.0.6 to use (soft) Security Module at first connection
    • Installation of modified configuration file
  • pkcs11-provider package
    • Installation of PKCS#11 provider for OpenSSL 3.x
    • Installation of OpenSSL PKCS#11 provider configuration file
  • demo-application-aws package
    • Grant user weston the right to perform some operations
    • Installation of a demonstration application to:
      • Visualize current Greengrass Core Device configuration
      • Show Greengrass component status
      • Interact with an MQTT network by subscribing and publishing to topics