Registered User mNo edit summary |
Registered User mNo edit summary Tag: 2017 source edit |
||
(11 intermediate revisions by 5 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | {{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x, STM32MP25x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}} | }} | ||
==Peripheral overview== | ==Peripheral overview== | ||
The '''HASH''' peripheral is used to compute a message digest. <br /> | The '''HASH''' peripheral is used to compute a message digest. <br /> | ||
The '''HASH''' peripheral is also able to give the HMAC<ref>https://en.wikipedia.org/wiki/HMAC</ref> used for authentication using the same algorithm support. | The '''HASH''' peripheral is also able to give the HMAC<ref>https://en.wikipedia.org/wiki/HMAC</ref> used for authentication using the same algorithm support. | ||
====On {{MicroprocessorDevice | device=13}} and {{MicroprocessorDevice | device= | ====On {{MicroprocessorDevice | device=13}} and {{MicroprocessorDevice | device=2}}==== | ||
Secure Hash algorithms supports: | Secure Hash algorithms supports: | ||
* SHA-1 <ref name=SHA>https://en.wikipedia.org/wiki/Secure_Hash_Algorithms</ref> | * SHA-1 <ref name=SHA>https://en.wikipedia.org/wiki/Secure_Hash_Algorithms</ref> | ||
Line 26: | Line 24: | ||
* HMAC support for all supported algorithm | * HMAC support for all supported algorithm | ||
Refer to the [[ | Refer to the [[STM32 MPU resources#Reference manuals|STM32 MPU reference manuals]] for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented. | ||
====On {{MicroprocessorDevice | device=15}}==== | ====On {{MicroprocessorDevice | device=15}}==== | ||
Line 43: | Line 41: | ||
===Boot time assignment=== | ===Boot time assignment=== | ||
The HASH instance is used as boot device to support binary authentication. | The HASH instance is used as boot device to support binary authentication when device is in [[Device life cycle|secured locked]] state. | ||
====On {{MicroprocessorDevice | device=13}}==== | ====On {{MicroprocessorDevice | device=13}}==== | ||
{{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp1_boottime}} | {{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp1_boottime}} | ||
Line 78: | Line 76: | ||
|} | |} | ||
====On {{MicroprocessorDevice | device= | ====On {{MicroprocessorDevice | device=21}}==== | ||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp2_a35_boottime}} | |||
<section begin=stm32mp21_a35_boottime /> | |||
| rowspan="1" | Security | |||
| rowspan="1" | [[HASH internal peripheral | HASH]] | |||
| HASH1 | |||
| <span title="system peripheral" style="font-size:21px">✓</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| | |||
|- | |||
<section end=stm32mp21_a35_boottime /> | |||
|} | |||
====On {{MicroprocessorDevice | device=23}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp2_a35_boottime}} | |||
<section begin=stm32mp23_a35_boottime /> | |||
| rowspan="1" | Security | |||
| rowspan="1" | [[HASH internal peripheral | HASH]] | |||
| HASH | |||
| <span title="system peripheral" style="font-size:21px">✓</span> | |||
| <span title="assigned peripheral" style="font-size:21px">☑</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| | |||
|- | |||
<section end=stm32mp23_a35_boottime /> | |||
|} | |||
====On {{MicroprocessorDevice | device=25}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp2_a35_boottime}} | {{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp2_a35_boottime}} | ||
<section begin=stm32mp25_a35_boottime /> | <section begin=stm32mp25_a35_boottime /> | ||
Line 124: | Line 153: | ||
|- | |- | ||
<section end=stm32mp15_runtime /> | <section end=stm32mp15_runtime /> | ||
|} | |||
====On {{MicroprocessorDevice | device=21}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp21_runtime}} | |||
<section begin=stm32mp21_a35_runtime /> | |||
| rowspan="2" | Security | |||
| rowspan="2" | [[HASH internal peripheral | HASH]] | |||
| HASH1 | |||
| <span title="assigned peripheral" style="font-size:21px">☐</span><sup>OP-TEE</sup> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| | |||
|- | |||
| HASH2 | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span><sup>OP-TEE</sup> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| | |||
|- | |||
<section end=stm32mp21_a35_runtime /> | |||
|} | |||
====On {{MicroprocessorDevice | device=23}}==== | |||
{{#lst:STM32MP2_internal_peripherals_assignment_table_template|stm32mp23_runtime}} | |||
<section begin=stm32mp23_a35_runtime /> | |||
| rowspan="1" | Security | |||
| rowspan="1" | [[HASH internal peripheral | HASH]] | |||
| HASH | |||
| <span title="assigned peripheral" style="font-size:21px">☐</span><sup>OP-TEE</sup> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| | |||
|- | |||
<section end=stm32mp23_a35_runtime /> | |||
|} | |} | ||
Line 145: | Line 211: | ||
Below are listed the software frameworks and drivers managing the HASH peripheral for the embedded software components listed in the above tables. | Below are listed the software frameworks and drivers managing the HASH peripheral for the embedded software components listed in the above tables. | ||
* '''Linux<sup>®</sup>''': [[Crypto_API_overview|crypto framework]] | *'''Linux<sup>®</sup>''': [[Crypto_API_overview|crypto framework]] | ||
* '''OP-TEE''': [[OP-TEE_overview|HASH driver]] and {{CodeSource | OP-TEE_OS | core/include/crypto/crypto.h | Cryptographic Provider API (CP API)}} | * '''OP-TEE''': [[STM32 MPU OP-TEE_overview|HASH driver]] and {{CodeSource | OP-TEE_OS | core/include/crypto/crypto.h | Cryptographic Provider API (CP API)}} | ||
* '''STM32Cube''': [[STM32CubeMP15 Package architecture|HASH HAL driver]] and {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_HAL_Driver/Inc/stm32mp1xx_hal_hash.h | header file of HASH HAL module}} | *'''STM32Cube''': [[STM32CubeMP15 Package architecture|HASH HAL driver]] and {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_HAL_Driver/Inc/stm32mp1xx_hal_hash.h | header file of HASH HAL module}} | ||
* '''TF-A BL2''': [[TF-A_overview|HASH driver]] | *'''TF-A BL2''': [[TF-A_overview|HASH driver]] | ||
==How to assign and configure the peripheral== | ==How to assign and configure the peripheral== | ||
The peripheral assignment can be done via the [[STM32CubeMX]] graphical tool (and manually completed if needed).<br /> | The peripheral assignment can be done via the [[STM32CubeMX]] graphical tool (and manually completed if needed).<br /> | ||
This tool also helps to configure the peripheral: | This tool also helps to configure the peripheral: | ||
* partial device trees (pin control and clock tree) generation for the OpenSTLinux software components, | *partial device trees (pin control and clock tree) generation for the OpenSTLinux software components, | ||
* HAL initialization code generation for the STM32CubeMPU Package. | *HAL initialization code generation for the STM32CubeMPU Package. | ||
The configuration is applied by the firmware running in the context in which the peripheral is assigned. | The configuration is applied by the firmware running in the context in which the peripheral is assigned. | ||
==References== | ==References== | ||
<references/> | <references /> | ||
<noinclude> | <noinclude> |
Latest revision as of 11:18, 7 November 2024
1. Peripheral overview[edit | edit source]
The HASH peripheral is used to compute a message digest.
The HASH peripheral is also able to give the HMAC[1] used for authentication using the same algorithm support.
1.1. On STM32MP13x lines
and STM32MP2 series[edit | edit source]
Secure Hash algorithms supports:
- SHA-1 [2]
- SHA-2 [3]:
- SHA-224
- SHA-256
- SHA-384
- SHA-512
- Truncated output SHA-512/224, SHA512/256
- SHA-3 [4]:
- SHA3-224
- SHA3-256
- SHA3-384
- SHA3-512
- SHAKE128 and 256
- Keccak-based functions
- HMAC support for all supported algorithm
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
1.2. On STM32MP15x lines
[edit | edit source]
Secure Hash algorithms supports:
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
2. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
2.1. Boot time assignment[edit | edit source]
The HASH instance is used as boot device to support binary authentication when device is in secured locked state.
2.1.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Security | HASH | HASH | ✓ | ☑ |
2.1.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
Security | HASH | HASH1 | ✓ | ☑ | ||
HASH2 | not used at boot time. |
2.1.3. On STM32MP21 unknown microprocessor device[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Security | HASH | HASH1 | ✓ | ☑ | ☐ |
2.1.4. On STM32MP23 unknown microprocessor device[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Security | HASH | HASH | ✓ | ☑ | ☐ |
2.1.5. On STM32MP25x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Security | HASH | HASH | ✓ | ☑ | ☐ |
2.2. Runtime assignment[edit | edit source]
2.2.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Security | HASH | HASH | ☐ | ☐ | Assignment (single choice) |
2.2.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Security | HASH | HASH1 | ☐ | ☐ | Assignment (single choice) | |
HASH2 | ☐ |
2.2.3. On STM32MP21 unknown microprocessor device[edit | edit source]
| rowspan="2" | Security | rowspan="2" | HASH | HASH1 | ☐OP-TEE | ☐ | ☐ | ☐ | |- | HASH2 | ☐OP-TEE | ☐ | ☐ | ☐ | |-
|}
2.2.4. On STM32MP23 unknown microprocessor device[edit | edit source]
| rowspan="1" | Security | rowspan="1" | HASH | HASH | ☐OP-TEE | ☐ | ☐ | ☐ | |-
|}
2.2.5. On STM32MP25x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Security | HASH | HASH | ☐OP-TEE | ☐ | ☐ | ☐ |
3. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the HASH peripheral for the embedded software components listed in the above tables.
- Linux®: crypto framework
- OP-TEE: HASH driver and Cryptographic Provider API (CP API)
- STM32Cube: HASH HAL driver and header file of HASH HAL module
- TF-A BL2: HASH driver
4. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
5. References[edit | edit source]