Registered User mNo edit summary |
Registered User No edit summary |
||
(20 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | |||
}} | |||
<noinclude></noinclude> | |||
==Article purpose== | ==Article purpose== | ||
The purpose of this article is to | The purpose of this article is to: | ||
* briefly introduce the USBPHYC | * briefly introduce the USBPHYC peripheral and its main features, | ||
* indicate the | * indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts), | ||
* list the software frameworks and drivers managing the peripheral, | |||
* explain | * explain how to configure the peripheral. | ||
==Peripheral overview== | ==Peripheral overview== | ||
The '''USBPHYC''' peripheral is a block that contains a dual port USB high-speed UTMI+ PHY and a UTMI switch. It makes the interface between: | The '''USBPHYC ''' peripheral is a block that contains a dual port USB high-speed UTMI+ PHY and a UTMI switch. It makes the interface between: | ||
* the internal USB controllers ([[USBH_internal_peripheral|USBH]] and [[OTG_internal_peripheral|OTG]]) | * the internal USB controllers ([[USBH_internal_peripheral|USBH]] and [[OTG_internal_peripheral|OTG]]) | ||
* the external USB physical lines (DP, DM) | * the external USB physical lines (DP, DM) | ||
The USBPHYC peripheral: | |||
The | |||
* controls a two port high-speed PHY: | * controls a two port high-speed PHY: | ||
** Port1 connected to the [[USBH_internal_peripheral|USBH]] controller | ** Port1 connected to the [[USBH_internal_peripheral|USBH]] controller | ||
Line 21: | Line 26: | ||
[[File:USBPHYC.png|link=]] | [[File:USBPHYC.png|link=]] | ||
Refer to [[ | Refer to the [[STM32 MPU resources#Reference manuals|STM32 MPU reference manuals]] for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented. | ||
== | ==Peripheral usage== | ||
This chapter is applicable in the scope of the '''OpenSTLinux BSP''' running on the Arm<sup>®</sup> Cortex<sup>®</sup>-A processor(s), and the '''STM32CubeMPU Package''' running on the Arm<sup>®</sup> Cortex<sup>®</sup>-M processor. | |||
== | ===Boot time assignment=== | ||
=== | ====On {{MicroprocessorDevice | device=1}}==== | ||
USBPHYC instances are boot devices that support Flash programming with [[STM32CubeProgrammer]]. | USBPHYC instances are boot devices that support Flash programming with [[STM32CubeProgrammer]]. | ||
The USBPHYC peripheral is used by [[ | The USBPHYC peripheral is used by [[STM32 MPU ROM code overview|ROM code]], [[Boot chain overview|FSBL]] and [[Boot chain overview|SSBL]] when using [[OTG_internal_peripheral|OTG]] in Device mode (DFU).<br> | ||
The [[Boot | {{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp1_boottime}} | ||
<section begin=stm32mp13_boottime /><section begin=stm32mp15_boottime /> | |||
| rowspan="1" | High speed interface | |||
| rowspan="1" | [[USBPHYC internal peripheral|USBPHYC (USB HS PHY controller)]] | |||
| USBPHYC (USB HS PHY controller) | |||
| <span title="system peripheral" style="font-size:21px">✓</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| The USBPHYC can be used by [[STM32 MPU ROM code overview|ROM code]], [[Boot chain overview|FSBL]] and [[Boot chain overview|SSBL]] in DFU mode to support serial boot.</br> It can be used also in U-boot by [[OTG_internal_peripheral|OTG]] and [[USBH_internal_peripheral|USBH]] with command line tools. | |||
|- | |||
<section end=stm32mp13_boottime /><section end=stm32mp15_boottime /> | |||
|} | |||
===Runtime=== | ===Runtime assignment=== | ||
==== | ====On {{MicroprocessorDevice | device=13}}==== | ||
{{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp13_runtime}} | |||
<section begin=stm32mp13_runtime /> | |||
| rowspan="1" | High speed interface | |||
| rowspan="1" | [[USBPHYC internal peripheral|USBPHYC (USB HS PHY controller)]] | |||
| USBPHYC (USB HS PHY controller) | |||
| <span title="assignable peripheral but not supported" style="font-size:21px">⬚</span> | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| Assignment (single choice) | |||
|- | |||
<section end=stm32mp13_runtime /> | |||
|} | |||
====On {{MicroprocessorDevice | device=15}}==== | |||
{{#lst:STM32MP1_internal_peripherals_assignment_table_template|stm32mp15_runtime}} | |||
<section begin=stm32mp15_runtime /> | |||
| rowspan="1" | High speed interface | |||
| rowspan="1" | [[USBPHYC internal peripheral|USBPHYC (USB HS PHY controller)]] | |||
| USBPHYC (USB HS PHY controller) | |||
| | |||
| <span title="assignable peripheral" style="font-size:21px">☐</span> | |||
| <span title="assignable peripheral but not supported" style="font-size:21px">⬚</span> | |||
| | |||
|- | |||
<section end=stm32mp15_runtime /> | |||
|} | |||
==Software frameworks and drivers== | |||
Below are listed the software frameworks and drivers managing the USBPHYC peripheral for the embedded software components listed in the above tables. | |||
* '''Linux<sup>®</sup>''': [[PHY overview | PHY framework]] | |||
* '''U-Boot''': PHY uclass ({{CodeSource | U-Boot | drivers/phy/phy-uclass.c}}) and driver ({{CodeSource | U-Boot | drivers/phy/phy-stm32-usbphyc.c}}) | |||
==How to assign and configure the peripheral== | |||
The peripheral assignment can be done via the [[STM32CubeMX]] graphical tool (and manually completed if needed).<br /> | |||
This tool also helps to configure the peripheral: | |||
* partial device trees (pin control and clock tree) generation for the OpenSTLinux software components, | |||
* HAL initialization code generation for the STM32CubeMPU Package. | |||
The configuration is applied by the firmware running in the context in which the peripheral is assigned. | |||
For U-boot and Linux kernel configuration, please refer to [[USBPHYC device tree configuration|USBPHYC device tree configuration]]. | |||
<noinclude> | <noinclude> | ||
[[Category:High speed interface peripherals]] | [[Category:High speed interface peripherals]] | ||
{{ArticleBasedOnModel | Internal peripheral article model}} | |||
{{PublicationRequestId | 10276 | 2019-01-14 | AnneJ}} | {{PublicationRequestId | 10276 | 2019-01-14 | AnneJ}} | ||
</noinclude> | </noinclude> |
Latest revision as of 07:24, 24 October 2024
1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the USBPHYC peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The USBPHYC peripheral is a block that contains a dual port USB high-speed UTMI+ PHY and a UTMI switch. It makes the interface between:
The USBPHYC peripheral:
- controls a two port high-speed PHY:
- sets the PLL values
- performs other controls (and monitoring) on the PHY.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
3.1.1. On STM32MP1 series[edit | edit source]
USBPHYC instances are boot devices that support Flash programming with STM32CubeProgrammer.
The USBPHYC peripheral is used by ROM code, FSBL and SSBL when using OTG in Device mode (DFU).
Click on to expand or collapse the legend...
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (ROM code) |
Cortex-A7 secure (TF-A BL2) |
Cortex-A7 non-secure (U-Boot) | |||
High speed interface | USBPHYC (USB HS PHY controller) | USBPHYC (USB HS PHY controller) | ✓ | ☐ | ☐ | The USBPHYC can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot. It can be used also in U-boot by OTG and USBH with command line tools. |
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP13x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
High speed interface | USBPHYC (USB HS PHY controller) | USBPHYC (USB HS PHY controller) | ⬚ | ☐ | Assignment (single choice) |
3.2.2. On STM32MP15x lines
[edit | edit source]
Click on to expand or collapse the legend...
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
High speed interface | USBPHYC (USB HS PHY controller) | USBPHYC (USB HS PHY controller) | ☐ | ⬚ |
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the USBPHYC peripheral for the embedded software components listed in the above tables.
- Linux®: PHY framework
- U-Boot: PHY uclass (drivers/phy/phy-uclass.c ) and driver (drivers/phy/phy-stm32-usbphyc.c )
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
For U-boot and Linux kernel configuration, please refer to USBPHYC device tree configuration.