| Recommended setup: Native Linux® PC |
1. Purpose[edit | edit source]
This article explains and describes the host PC hardware and software configuration required to activate and run the STM32 MPU platforms.
2. Recommended PC configurations[edit | edit source]
The PC requirements depend on the Package you want to use.
The table below guides through the selection and configuration of the host PC environment according the targeted Package:
| Host environment | Starter Package | Developer Package | Distribution Package |
|---|---|---|---|
| Windows® (64 bits) Tested with Windows 10 and Windows 11 Preferred version is Windows 11 |
native | Virtual machine | Virtual Machine |
| Linux (64 bits) Tested with Ubuntu®24.04, 22.04 and 26.04 |
Native | Native + additional packages (see Linux PC chapter ) | native + additional packages (see Linux PC chapter ) |
There are no absolute minimal requirements regarding the PC hardware configuration. However ST recommends to meet or exceed the following hardware requirements when using theDeveloper Package or Distribution Package.
The table below corresponds to the minimal validated configuration:
| Hardware item | Minimal validated configuration | Comments / Recommendations |
|---|---|---|
| CPU | core i5-2540M @ 2.6 GHz 2 cores (4 threads) 3-Mbyte cache |
64-bit instruction set is mandatory 8 cores/threads or more is a good configuration for Developer Package and Distribution Package. |
| RAM | 8 Gbytes | 16 Gbytes or more are recommended especially for Virtual machine setup, Developer Package and Distribution Package. |
| Hard drive | 320 Gbytes | 1 Tbytes is the best suited configuration for Distribution Package |
3. Linux® PC[edit | edit source]
A Linux PC with recent Ubuntu LTS (24.04, 22.04 or 26.04) is the recommended setup. Other Ubuntu revisions could also supported (refer to Yocto reference manual[1]) .
| ST solutions are tested and validated on a Linux PC running Ubuntu 24.04 LTS. |
3.1. Checking Internet access[edit | edit source]
- Internet access through http and https protocols
Required at least for Developer Package and Distribution Package.
The command below enables checking internet access through http/https protocols:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You might need to set up a proxy."
If an 'OK' message is returned, the network is well configured. In such case, skip the rest of this section and jump to Installing extra packages.
Any other situation likely indicates that a proxy is required for http/https protocols. The best solution to set a proxy for http/https protocols is via the shell variables http_proxy and https_proxy:
export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
Since your password (<MyProxyPassword>) might contain "special characters", translate it into ASCII hexacode. To do this, use the command below:
echo -n " <MyProxyPassword>" | od -A n -t x1 -w128 | head -1 | tr " " "%"
Check again the Internet access by using the following command:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You might need to set up a proxy."
- Internet access for sudo commands
Required for Distribution Package.
By default, sudo commands are executed in the root user environment; no Internet proxy settings are applied for root users.
Root users must be able to browse Internet after having created an alias passing the proxy settings on sudo commands:
alias sudo='sudo http_proxy=$http_proxy'
Check that the sudo commands are successful (requires Internet access):
sudo apt-get update
- Internet over git://, ssh:// and others specifics protocols
Required for Distribution Package.
In addition to http/https protocols (used in 90% of the Internet traffic), other protocols such as git:// or ssh:// might be required.
For example, in the context of the Distribution Package, some "git fetch" commands might require "git:// protocols".
To support these protocols through a proxy, directly setup the proxy in the $HOME/.gitconfig file (core.gitproxy) and use a tool such as cockscrew[2] to tunnel the git:// flow into the http flow:
sudo apt-get update sudo apt-get install corkscrew git config --replace-all --global core.gitproxy "$HOME/bin/git-proxy.sh" git config --add --global core.gitproxy "none for <MyPrivateNetworkDomain>" (optional, for example .st.com or localhost) echo 'exec corkscrew <MyProxyServerUrl> <MyProxyPort> $* $HOME/.git-proxy.auth' > $HOME/bin/git-proxy.sh chmod 700 $HOME/bin/git-proxy.sh echo '<MyProxyLogin>:<MyProxyPassword>' > $HOME/.git-proxy.auth chmod 600 $HOME/.git-proxy.auth
Use the command below to test the proxy settings:
git ls-remote git://git.openembedded.org/openembedded-core > /dev/null && echo OK || echo KO
The command returns 'OK' if the proxy settings are correct.
3.2. Installing extra packages[edit | edit source]
Required for Developer Package and Distribution Package.
Additional Ubuntu packages must be installed to perform basic development tasks, basic cross-compilation (via Developer Package) or more complex cross-compilation such as OpenEmbedded does (via Distribution Package):
- Packages required by OpenEmbedded/Yocto (details here):
sudo apt-get update sudo apt-get install gawk wget git git-lfs diffstat unzip texinfo gcc-multilib chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libsdl1.2-dev pylint xterm bsdmainutils libusb-1.0-0 bison flex sudo apt-get install libssl-dev libgmp-dev libmpc-dev lz4 zstd (Ubuntu 22.04 only) sudo apt install libegl1-mesa
- Packages needed for some "Developer Package" use cases:
sudo apt-get install build-essential libncurses-dev libyaml-dev libssl-dev
- Package for repo (used to download the "Distribution Package" source code):
First set python3 as default: sudo apt install python-is-python3
export REPO=$(mktemp /tmp/repo.XXXXXXXXX)
curl -o ${REPO} https://storage.googleapis.com/git-repo-downloads/repo
gpg --recv-keys 8BB9AD793E8E6153AF0F9A4416530D5E920F5C65
curl -s https://storage.googleapis.com/git-repo-downloads/repo.asc | gpg --verify - ${REPO} && install -m 755 ${REPO} ~/bin/repo
- Useful tools:
sudo apt-get install coreutils bsdmainutils sed curl bc lrzsz corkscrew cvs subversion mercurial nfs-common nfs-kernel-server libarchive-zip-perl dos2unix texi2html libxml2-utils
3.2.1. Installing extra packages for AndroidTM[edit | edit source]
| Below information is related to the Android™ distribution Here after are the list of packages which can be useful to work with the OpenSTDroid distribution: Before downloading and building the OpenSTDroid distribution, make sure your system meets the following requirements:
For more details, refer to the requirements page of the AOSP website. Use the following commands to install the packages required to setup your environment (Distribution Package): sudo apt-get install build-essential gcc-multilib cmake ant bison flex chrpath pahole bc rustfmt sudo apt-get install libssl-dev libgmp-dev libmpc-dev libncurses-dev libyaml-dev libelf-dev libsdl1.2-dev libncurses5 sudo apt-get install git gitk git-gui git-doc git-lfs cvs subversion mercurial sudo apt-get install python3 python3-pip python3-pexpect python-is-python3 python3-pyelftools python3-cbor2 python3-intelhex python3-pycryptodome python3-sepolgen pylint python3-git sudo apt-get install wget curl unzip cpio lz4 zstd pv dos2unix lrzsz libarchive-zip-perl sudo apt-get install gawk sed diffstat coreutils bsdmainutils texinfo texi2html libxml2-utils sudo apt-get install socat connect-proxy corkscrew picocom nfs-common nfs-kernel-server sudo apt-get install meld gitk git-gui Depending on the Ubuntu version you use, you may need to adapt the list. If any error occurs during installation, remove the package from the list and rerun the command to avoid an incomplete installation.
At this stage: Your environment is ready for Android build, debug and test.
|
3.3. Additional configurations[edit | edit source]
- disable appamor (requiered for 24.04)
At least on Ubuntu 24.04, in combination with the apparmor package, the Ubuntu kernel now restricts the use of unprivileged user namespaces. This affects all programs on the system that are unprivileged and unconfined. You can disable this restriction by running
sudo apparmor_parser -R /etc/apparmor.d/unprivileged_userns
- Allowing up to 16 partitions per MMC
By default a maximum of 8 MMC partitions are allowed on Linux systems. All Packages (such as Starter Package) need more than 10 partitons for the storage device. To extend the number of partitions per device to 16, the following options must be added to modprobe:
echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf
- Checking for locale setup
Required for Distribution Package.
The locale setting is used by some applications/commands (including by Distribution Package applications/commands).
Verify that the locale settings are as follows:
locale LANG=en-US.UTF-8
If the locale command returns a different configuration than the one shown above, reconfigure it as follows:
sudo update-locale LANG=en_US.UTF-8
- Adding users in basics groups
The user login must belong to the basic Linux groups such as disk, tty, dialout or plugdev
Use the groups command to list groups for the current user:
groups
If needed, add user to the missing <groups>:
sudo adduser $USER <group>
Then reboot the PC.
3.4. Setting up Git user information[edit | edit source]
Required for Developer Package and Distribution Package.
The user Information are needed by git[3] if commit and/or push commands are used:
git config --global user.name "Your Name" git config --global user.email "you@example.com"
4. Windows PC[edit | edit source]
Starter Package may run on Windows.
Developer Package and Distribution Package require a Linux environment.
There are several ways to run Linux system on top of a Windows host PC. ST recommends to use a Virtual Machine System:
- Install a virtual machine such as VirtualBox [4]
- Setup a 64-bit Ubuntu image compatible with your virtual machine
ST, in an experimental way, has also run Developer Package and Distribution Package on WSL2 (Windows Subsystem for Linux 2). Refer to WSL2 chapter.
4.1. Virtual machine system[edit | edit source]
4.1.1. Installing the virtual machine[edit | edit source]
Please proceed with the installation of the virtual machine.
Before running the virtual machine, make sure the virtualization is activated in the BIOS (it should be activated by default for any retail PC).
4.1.2. Downloading the Ubuntu image for the virtual machine[edit | edit source]
The "osboxes.org" [6] website provides virtual machine images compatible with VirtualBox(*.ova).
ecosystem release v7.0.0
: Setup have been validated and tested on Ubuntu 24.04 (64bits).
Download the 64-bit Ubuntu image available at [7], then:
- Unzip the downloaded file
- In VirtualBox, create a virtual machine using the Ubuntu virtual disk downloaded from osboxes.org.
The recommended usage is to dedicate, at least, half of the host machine to the virtual machine:
- CPU: 2 cores at least, - RAM: 8 Gbytes or more is a good choice (the more RAM allocated to Virtual Machine the better - the RAM allocated to Virtual Machine must be at least 4 Gbytes), - Network: NAT is a good easy way to benefit from a network connection within the virtual machine.
The virtual size of the virtual disk downloaded from osboxes.org is about 500 Gbytes. Even if, at beginning, the real size of the file of the virtual disk is less, the size can grow up to 500 Gbytes over distribution package compiling or package development.
| First load the just downloaded image (*.ova) via the menu "File->Import Appliance" and the update the RAM and CPU if needed. |
4.1.3. Launching Ubuntu image[edit | edit source]
Default 'Ubuntu Credentials' are set to "osboxes.org" for both login and password.
For a better experience with the VirtualBox machine have a look in the settings of the image to adjust some settings or turn on the clipboard or drag-and-drop and copy/paste files between VirtualBox and Windows. Then enable this features by installing VirtualBox Guest Additional tool:
- First mount the VBoxGuestAdditions.iso from image "settings->storage" then add "optical drive" and choose "VBoxGuestAdditions.iso" image
- Then go inside image through a bash terminal and run the sh ./VBoxLinuxAdditions.run:
- sudo apt install bzip2 tar gcc make perl
- cd /media/osboxes/VBox_GAs*
- sudo ./VBoxLinuxAdditions.run
- then reboot the image
The virtual machine is now up and running!
The Ubuntu setup must be finalized according recommendations provided in Linux PC chapter
4.2. WSL2 (experimental)[edit | edit source]
Even if STMicroelectronics strongly recommends to use a Linux® environment, the Developer Package and Distribution Package work on WSL2 (Windows Sub-system Linux 2) environment. WSL is a feature provided by Windows 10®.
WSL2 is a new version of the architecture that powers the Windows subsystem for Linux to run ELF64 Linux binaries on Windows (more details on aka.ms/wsl2). It is available on Windows 10 since build 18917.
The Developer Package successfully runs on WSL2 but unsuccessfully on WSL.
- Installing WSL2 :
- To install WSL2, read https://docs.microsoft.com/fr-fr/windows/wsl/wsl2-install
- Once WSL2 is installed, jump to #Linux-C2-AE_PC to make your WSL2 ready to run Developer Package and/or Distribution Package.
- WSL2 limitations :
- Up to now (March 2021), WSL2 does not support hardware such as USB or serial devices (more details).
- This means that STM32CubeProgrammer must be used through native Windows.
- WSL2 files are not browsable from Windows native file explorer.
- To share files between WSL2 and Windows, it is recommend to use the mount point /mnt/c from WSL2 and perform copies.
- Up to now (March 2021), WSL2 does not support hardware such as USB or serial devices (more details).
- Tips for using WSL2 :
- Launching graphical application : on wiki.ubuntu.com, go to WSL page and read the chapter Running Graphical Applications.
4.3. References[edit | edit source]
- ↑ Supported Linux Distributions
- ↑ https://en.wikipedia.org/wiki/Corkscrew_(program)
- ↑ Git
- ↑ https://www.virtualbox.org
- ↑ http://flow.st.com/st/UP/LVM/Lists/RequestList/NewForm.aspx
- ↑ http://osboxes.org
- ↑ https://sourceforge.net/projects/osboxes/files/v/vb/55-U-u/OVA-Versions/24.04/Ubuntu-24.04-64bit-VB.ova/download