1. Article purpose[edit | edit source]
This article explains how to configure the DDRCTRL and DDRPHYC internal peripherals from the first stage bootloader.
The configuration is performed using the device tree mechanism that provides a hardware description of the DDR subsystem (DDR controler and DDR PHY peripheral), and embeds the configuration used by the first stage bootloader to initialize the DDR before loading the second stage bootloader.
The DDR settings are stored in the device tree of the boot chain FSBL, that is, in the TF-A device tree for OpenSTLinux official delivery.
2. DT bindings documentation[edit | edit source]
The DDR subsystem is a 'memory-controller' device represented by the device tree bindings documented below:
- TF-A: docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt"[1] on STM32MP1 series
- TF-A: docs/devicetree/bindings/memory-controllers/st,stm32mp2-ddr.txt"[2] on STM32MP2 series
3. DT configuration[edit | edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file split.
STM32CubeMX can be used to generate this DDR board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit | edit source]
The STM32MP DDR node is located
- for STM32MP13x lines
in stm32mp131.dtsi [3]
- for STM32MP15x lines
in stm32mp151.dtsi [4]
- for STM32MP21x lines
in stm32mp211.dtsi [5]
- for STM32MP23x lines
in stm32mp231.dtsi [6]
- for STM32MP25x lines
in stm32mp251.dtsi [7]
see Device tree for further explanation.
For example (STM32MP15x lines ):
ddr: ddr@5a003000{
compatible = "st,stm32mp1-ddr";
reg = <0x5A003000 0x550 0x5A004000 0x234>;
clocks = <&rcc AXIDCG>,
<&rcc DDRC1>,
<&rcc DDRC2>,
<&rcc DDRPHYC>,
<&rcc DDRCAPB>,
<&rcc DDRPHYCAPB>;
clock-names = "axidcg",
"ddrc1",
"ddrc2",
"ddrphyc",
"ddrcapb",
"ddrphycapb";
status = "okay";
};
3.2. DT configuration (board level)[edit | edit source]
The next attributes provide the DDR information and DDR settings; the values are used by the FSBL to initialize the registers of the DDR subsystem (the DDR controller and the DDR PHY).
These value are generated by DDR tools included in STM32CubeMX.
The board configuration defines each configuration needed (DDR_...) and includes the STM32-level device tree.
3.2.1. DDR supply attributes[edit | edit source]
For cold boot and depending of the DDR type, the DDR supply must respect the expected sequence:
- for DDR3:
VREF / VTT / VDD - for DDR4:
VPP / VREF / VTT / VDD - for LPPPR2, LPDDR3 and LPDDR4:
VDD1 / VDD2 / VDDQ
The required supply are defined in the define tree, with parameters of ddr node:
- For DDR3:
- vdd-supply: phandle to the VDD/VDDQ regulator device tree node.
- vref-supply: phandle to the VREFCA/VREFDQ regulator device tree node.
- vtt-supply: phandle to the VTT regulator device tree node.
- For DDR4:
- vdd-supply: phandle to the VDD/VDDQ regulator device tree node.
- vref-supply: phandle to the VREFCA regulator device tree node.
- vpp-supply: phandle to the VPP regulator device tree node.
- vtt-supply: phandle to the VTT regulator device tree node.
- For LPDDR2/LPDDR3/LPDDR4:
- vdd1-supply: phandle to the VDD1 regulator device tree node.
- vdd2-supply: phandle to the VDD2/VDDCA regulator device tree node.
- vddq-supply: phandle to the VDDQ regulator device tree node.
The supply are used during the DDR power-on sequence and they can provided, according the board design, by:
- PMIC regulators
- GPIO regulators
- fixed regulators
See regulator page for generic binding details.
Two properties can used for customized the power-on sequence in TF-A:
- regulator-always-on: force the regulator ON
- regulator-enable-ramp-delay: define the waiting time, in microseconds, for the supply rail to reach the target voltage.
it should be explicitly initialized to zero (regulator-enable-ramp-delay = <0>) for disabling ramp delay.
The DDR driver doesn't use delay for power on sequence, so the delay needed to have the correct voltage must be managed in each regulator driver:
- it is managed in the STPMIC driver with a default delay of 1ms for each regulator, regulator-enable-ramp-delay is optional
- it must be defined for gpio regulator in the device tree, regulator-enable-ramp-delay is mandatory.
3.2.2. On STM32MP1 series[edit | edit source]
3.2.2.1. Information[edit | edit source]
- st,mem-name: name for the DDR configuration, a simple string for information
- st,mem-speed: DDR expected speed in kHz
- st,mem-size: DDR mem size in bytes (used in SSBL and FSBL)
3.2.2.2. Controller register values[edit | edit source]
- st,ctl-reg: controller values depending on the DDR type (DDR3/LPDDR2/LPDDR3):
- st,ctl-timing: controller values depending on the DDR frequency and timing parameters:
- st,ctl-map: controller values depending on the address mapping:
- st,ctl-perf: controller values depending on performance and scheduling:
- for STM32MP13x lines
11 values are requested in this order: (SCHED SCHED1 PERFHPR1 PERFLPR1 PERFWR1 PCFGR_0 PCFGW_0 PCFGQOS0_0 PCFGQOS1_0 PCFGWQOS0_0 PCFGWQOS1_0)
- for STM32MP15x lines
17 values are requested in this order: (SCHED SCHED1 PERFHPR1 PERFLPR1 PERFWR1 PCFGR_0 PCFGW_0 PCFGQOS0_0 PCFGQOS1_0 PCFGWQOS0_0 PCFGWQOS1_0 PCFGR_1 PCFGW_1 PCFGQOS0_1 PCFGQOS1_1 PCFGWQOS0_1 PCFGWQOS1_1)
- for STM32MP13x lines
3.2.2.3. phy register values[edit | edit source]
- st,phy-reg: phy values depending on the DDR type: (DDR3/LPDDR2/LPDDR3):
- st,phy-timing: phy values depending on the DDR frequency and timing parameters:
- st,phy-cal: phy cal depending on the DDR calibration or tuning. This parameter is optional: when it is absent, the built-in PHY calibration is done (see the next chapter for details); when it is present:
3.2.2.4. st,phy-cal value and DDR tuning[edit | edit source]
By default, the st,phy-cal property is absent in device tree and the built-in PHY calibration is executed by the DDR driver to determine DXnDQTR and DXnDQSTR register values (with n = byte id, 0 to 3).
When st,phy-cal is present in device tree (e.g. when DDR_PHY_CAL_SKIP is defined), the built-in PHY calibration is skipped and the driver use the DXnDQTR and DXnDQSTR values defined in the device tree: they described the fine step delays used for DQ/DQS pin deskew and for eye centering.
See #How to configure the DT using STM32CubeMX and the dedicated application note[8] for further information.
3.2.3. On STM32MP2 series[edit | edit source]
3.2.3.1. Information[edit | edit source]
- st,mem-name: name for the DDR configuration, a simple string for information
- st,mem-speed: DDR expected speed in kHz
- st,mem-size: DDR mem size in bytes, 2 cells (32 bits) for 64 bit size
3.2.3.2. Controller register values[edit | edit source]
- st,ctl-reg: controller values depending on the DDR type (DDR3/DDR4/LPDDR4):
- 48 values are requested in this order: (MSTR MRCTRL0 MRCTRL1 MRCTRL2 DERATEEN DERATEINT DERATECTL PWRCTL PWRTMG HWLPCTL RFSHCTL0 RFSHCTL1 RFSHCTL3 CRCPARCTL0 CRCPARCTL1 INIT0 INIT1 INIT2 INIT3 INIT4 INIT5 INIT6 INIT7 DIMMCTL RANKCTL RANKCTL1 ZQCTL0 ZQCTL1 ZQCTL2 DFITMG0 DFITMG1 DFILPCFG0 DFILPCFG1 DFIUPD0 DFIUPD1 DFIUPD2 DFIMISC DFITMG2 DFITMG3 DBICTL DFIPHYMSTR DBG0 DBG1 DBGCMD SWCTL SWCTLSTATIC POISONCFG PCCFG)
- st,ctl-timing: controller values depending on the DDR frequency and timing parameters:
- 20 values are requested in this order: (RFSHTMG RFSHTMG1 DRAMTMG0 DRAMTMG1 DRAMTMG2 DRAMTMG3 DRAMTMG4 DRAMTMG5 DRAMTMG6 DRAMTMG7 DRAMTMG8 DRAMTMG9 DRAMTMG10 DRAMTMG11 DRAMTMG12 DRAMTMG13 DRAMTMG14 DRAMTMG15 ODTCFG ODTMAP)
- st,ctl-map: controller values depending on the address mapping:
- 12 values are requested in this order: (ADDRMAP0 ADDRMAP1 ADDRMAP2 ADDRMAP3 ADDRMAP4 ADDRMAP5 ADDRMAP6 ADDRMAP7 ADDRMAP8 ADDRMAP9 ADDRMAP10 ADDRMAP11)
- st,ctl-perf: controller values depending on performance and scheduling:
- 21 values are requested in this order: (SCHED SCHED1 PERFHPR1 PERFLPR1 PERFWR1 SCHED3 SCHED4 PCFGR_0 PCFGW_0 PCTRL_0 PCFGQOS0_0 PCFGQOS1_0 PCFGWQOS0_0 PCFGWQOS1_0 PCFGR_1 PCFGW_1 PCTRL_1 PCFGQOS0_1 PCFGQOS1_1 PCFGWQOS0_1 PCFGWQOS1_1)
3.2.3.3. phy attributes[edit | edit source]
Following values correspond to user input parameters of the DDR PHY software driver.
It configures the IP and runs the DDR training sequence by loading and executing the DDR Firmware binary.
Binary path <ddr_type>_pmu_train.bin is present in TF-A directory drivers/st/ddr/phy/firmware/bin/stm32mp2/ .
The DDR Firmware can also be downloaded from https://github.com/STMicroelectronics/stm32-ddr-phy-binary with git.
- st,phy-basic: basic entry values for the PHYINIT driver:
- 19 values are requested in this order: (UIB_DRAMTYPE UIB_DIMMTYPE UIB_LP4XMODE UIB_NUMDBYTE UIB_NUMACTIVEDBYTEDFI0 UIB_NUMACTIVEDBYTEDFI1 UIB_NUMANIB UIB_NUMRANK_DFI0 UIB_NUMRANK_DFI1 UIB_DRAMDATAWIDTH UIB_NUMPSTATES UIB_FREQUENCY_0 UIB_PLLBYPASS_0 UIB_DFIFREQRATIO_0 UIB_DFI1EXISTS UIB_TRAIN2D UIB_HARDMACROVER UIB_READDBIENABLE_0 UIB_DFIMODE)
- st,phy-advanced: advanced entry values for the PHYINIT driver:
- 43 values are requested in this order: (UIA_LP4RXPREAMBLEMODE_0 UIA_LP4POSTAMBLEEXT_0 UIA_D4RXPREAMBLELENGTH_0 UIA_D4TXPREAMBLELENGTH_0 UIA_EXTCALRESVAL UIA_IS2TTIMING_0 UIA_ODTIMPEDANCE_0 UIA_TXIMPEDANCE_0 UIA_ATXIMPEDANCE UIA_MEMALERTEN UIA_MEMALERTPUIMP UIA_MEMALERTVREFLEVEL UIA_MEMALERTSYNCBYPASS UIA_DISDYNADRTRI_0 UIA_PHYMSTRTRAININTERVAL_0 UIA_PHYMSTRMAXREQTOACK_0 UIA_WDQSEXT UIA_CALINTERVAL UIA_CALONCE UIA_LP4RL_0 UIA_LP4WL_0 UIA_LP4WLS_0 UIA_LP4DBIRD_0 UIA_LP4DBIWR_0 UIA_LP4NWR_0 UIA_LP4LOWPOWERDRV UIA_DRAMBYTESWAP UIA_RXENBACKOFF UIA_TRAINSEQUENCECTRL UIA_SNPSUMCTLOPT UIA_SNPSUMCTLF0RC5X_0 UIA_TXSLEWRISEDQ_0 UIA_TXSLEWFALLDQ_0 UIA_TXSLEWRISEAC UIA_TXSLEWFALLAC UIA_DISABLERETRAINING UIA_DISABLEPHYUPDATE UIA_ENABLEHIGHCLKSKEWFIX UIA_DISABLEUNUSEDADDRLNS UIA_PHYINITSEQUENCENUM UIA_ENABLEDFICSPOLARITYFIX UIA_PHYVREF UIA_SEQUENCECTRL_0)
- st,phy-mr: mode register entry values for the PHYINIT driver:
- 12 values are requested in this order: (UIM_MR0_0 UIM_MR1_0 UIM_MR2_0 UIM_MR3_0 UIM_MR4_0 UIM_MR5_0 UIM_MR6_0 UIM_MR11_0 UIM_MR12_0 UIM_MR13_0 UIM_MR14_0 UIM_MR22_0)
- st,phy-swizzle swizzling (i.e. signal/ball multiplexing) entry values for the PHYINIT driver:
- 44 values are requested in this order: (UIS_SWIZZLE_0 UIS_SWIZZLE_1 UIS_SWIZZLE_2 UIS_SWIZZLE_3 UIS_SWIZZLE_4 UIS_SWIZZLE_5 UIS_SWIZZLE_6 UIS_SWIZZLE_7 UIS_SWIZZLE_8 UIS_SWIZZLE_9 UIS_SWIZZLE_10 UIS_SWIZZLE_11 UIS_SWIZZLE_12 UIS_SWIZZLE_13 UIS_SWIZZLE_14 UIS_SWIZZLE_15 UIS_SWIZZLE_16 UIS_SWIZZLE_17 UIS_SWIZZLE_18 UIS_SWIZZLE_19 UIS_SWIZZLE_20 UIS_SWIZZLE_21 UIS_SWIZZLE_22 UIS_SWIZZLE_23 UIS_SWIZZLE_24 UIS_SWIZZLE_25 UIS_SWIZZLE_26 UIS_SWIZZLE_27 UIS_SWIZZLE_28 UIS_SWIZZLE_29 UIS_SWIZZLE_30 UIS_SWIZZLE_31 UIS_SWIZZLE_32 UIS_SWIZZLE_33 UIS_SWIZZLE_34 UIS_SWIZZLE_35 UIS_SWIZZLE_36 UIS_SWIZZLE_37 UIS_SWIZZLE_38 UIS_SWIZZLE_39 UIS_SWIZZLE_40 UIS_SWIZZLE_41 UIS_SWIZZLE_42 UIS_SWIZZLE_43)
See #How to configure the DT using STM32CubeMX for further information.
3.3. DT configuration examples[edit | edit source]
3.3.1. DDR supply examples[edit | edit source]
DDR3 example in fdts/stm32mp135f-dk.dts or fdts/stm32mp15xx-dkx.dtsi :
&ddr {
vdd-supply = <&vdd_ddr>;
vref-supply = <&vref_ddr>;
};
DDR4 example in fdts/stm32mp257f-ev1.dts
&ddr {
vdd-supply = <&vdd_ddr>;
vtt-supply = <&vtt_ddr>;
vpp-supply = <&vpp_ddr>;
vref-supply = <&vref_ddr>;
};
And you can optimized the delay DDR boot sequence on cold boot:
&vdd_ddr {
regulator-enable-ramp-delay = <1000>;
};
&vtt_ddr {
regulator-enable-ramp-delay = <50>;
};
&vpp_ddr {
regulator-enable-ramp-delay = <440>;
};
&vref_ddr {
regulator-enable-ramp-delay = <0>;
};
LPDDR4 example in fdts/stm32mp257f-dk.dts :
&ddr {
vdd1-supply = <&vdd1_ddr>;
vdd2-supply = <&vdd2_ddr>;
vddq-supply = <&vdd2_ddr>;
};
Example with fixed regulator, for board without PMIC:
/ {
vdd_ddr: vdd-ddr {
compatible = "regulator-fixed";
regulator-name = "vdd_ddr";
regulator-min-microvolt = <1350000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
};
vref_ddr: vref-ddr {
compatible = "regulator-fixed";
regulator-name = "vref_ddr";
regulator-min-microvolt = <675000>;
regulator-max-microvolt = <675000>;
regulator-always-on;
};
vtt_ddr: vtt-ddr {
compatible = "regulator-fixed";
regulator-name = "vtt_ddr";
regulator-min-microvolt = <675000>;
regulator-max-microvolt = <675000>;
regulator-always-on;
};
vpp_ddr: vpp-ddr {
compatible = "regulator-fixed";
regulator-name = "vpp_ddr";
regulator-min-microvolt = <2500000>;
regulator-max-microvolt = <2500000>;
regulator-always-on;
};
};
&ddr {
vdd-supply = <&vdd_ddr>;
vtt-supply = <&vtt_ddr>;
vpp-supply = <&vpp_ddr>;
vref-supply = <&vref_ddr>;
};
3.3.2. On STM32MP1 series[edit | edit source]
3.3.2.1. Simple example[edit | edit source]
You can add the DDR configuration node with (STM32MP15x lines example):
&ddr {
st,mem-name = "DDR3 2x4Gb 533MHz";
st,mem-speed = <533000>;
st,mem-size = <0x40000000>;
st,ctl-reg = <
0x00040401 /*MSTR*/
0x00000010 /*MRCTRL0*/
0x00000000 /*MRCTRL1*/
0x00000000 /*DERATEEN*/
0x00800000 /*DERATEINT*/
0x00000000 /*PWRCTL*/
0x00400010 /*PWRTMG*/
0x00000000 /*HWLPCTL*/
0x00210000 /*RFSHCTL0*/
0x00000000 /*RFSHCTL3*/
0x00000000 /*CRCPARCTL0*/
0xC2000040 /*ZQCTL0*/
0x02050105 /*DFITMG0*/
0x00000202 /*DFITMG1*/
0x07000000 /*DFILPCFG0*/
0xC0400003 /*DFIUPD0*/
0x00000000 /*DFIUPD1*/
0x00000000 /*DFIUPD2*/
0x00000000 /*DFIPHYMSTR*/
0x00000001 /*ODTMAP*/
0x00000000 /*DBG0*/
0x00000000 /*DBG1*/
0x00000000 /*DBGCMD*/
0x00000000 /*POISONCFG*/
0x00000010 /*PCCFG*/
>;
st,ctl-timing = <
0x0080008A /*RFSHTMG*/
0x121B2414 /*DRAMTMG0*/
0x000D041B /*DRAMTMG1*/
0x0607080E /*DRAMTMG2*/
0x0050400C /*DRAMTMG3*/
0x07040407 /*DRAMTMG4*/
0x06060303 /*DRAMTMG5*/
0x02020002 /*DRAMTMG6*/
0x00000202 /*DRAMTMG7*/
0x00001005 /*DRAMTMG8*/
0x000D041B /*DRAMTMG14*/
0x06000600 /*ODTCFG*/
>;
st,ctl-map = <
0x00080808 /*ADDRMAP1*/
0x00000000 /*ADDRMAP2*/
0x00000000 /*ADDRMAP3*/
0x00001F1F /*ADDRMAP4*/
0x07070707 /*ADDRMAP5*/
0x0F070707 /*ADDRMAP6*/
0x00000000 /*ADDRMAP9*/
0x00000000 /*ADDRMAP10*/
0x00000000 /*ADDRMAP11*/
>;
st,ctl-perf = <
0x00001201 /*SCHED*/
0x00001201 /*SCHED*/1
0x01000001 /*PERFHPR1*/
0x08000200 /*PERFLPR1*/
0x08000400 /*PERFWR1*/
0x00010000 /*PCFGR_0*/
0x00000000 /*PCFGW_0*/
0x02100B03 /*PCFGQOS0_0*/
0x00800100 /*PCFGQOS1_0*/
0x01100B03 /*PCFGWQOS0_0*/
0x01000200 /*PCFGWQOS1_0*/
0x00010000 /*PCFGR_1*/
0x00000000 /*PCFGW_1*/
0x02100B03 /*PCFGQOS0_1*/
0x00800000 /*PCFGQOS1_1*/
0x01100B03 /*PCFGWQOS0_1*/
0x01000200 /*PCFGWQOS1_1*/
>;
st,phy-reg = <
0x01442E02 /*PGCR*/
0x10400812 /*ACIOCR*/
0x00000C40 /*DXCCR*/
0xF200001F /*DSGCR*/
0x0000000B /*DCR*/
0x00010000 /*ODTCR*/
0x0000007B /*ZQ0CR1*/
0x0000CE81 /*DX0GCR*/
0x0000CE81 /*DX1GCR*/
0x0000CE81 /*DX2GCR*/
0x0000CE81 /*DX3GCR*/
>;
st,phy-timing = <
0x0022A41B /*PTR0*/
0x047C0740 /*PTR1*/
0x042D9C80 /*PTR2*/
0x369477D0 /*DTPR0*/
0x098A00D8 /*DTPR1*/
0x10023600 /*DTPR2*/
0x00000830 /*MR0*/
0x00000000 /*MR1*/
0x00000208 /*MR2*/
0x00000000 /*MR3*/
>;
status = "okay";
};
The optional node st,phy-cal allows to use a calibration result when it is present, for example:
&ddr {
...
st,phy-cal = <
0x40000000 /*DX0DLLCR*/
0xFFFFFFFF /*DX0DQTR*/
0x3DB02000 /*DX0DQSTR*/
0x40000000 /*DX1DLLCR*/
0xFFFFFFFF /*DX1DQTR*/
0x3DB02000 /*DX1DQSTR*/
0x40000000 /*DX2DLLCR*/
0xFFFFFFFF /*DX2DQTR*/
0x3DB02000 /*DX2DQSTR*/
0x40000000 /*DX3DLLCR*/
0xFFFFFFFF /*DX3DQTR*/
0x3DB02000 /*DX3DQSTR*/
>;
...
};
3.3.2.2. STM32CubeMX configuration file[edit | edit source]
STM32CubeMX generates a .dtsi file with the needed values as defines (named DDR_...), and includes the #Generic DDR dtsi file for STM32MP1 series: as this dtsi file is preprocessed during FSBL compilation, it generates a correct device tree.
For example the file fdts/stm32mp15-ddr3-1x4Gb-1066-binG.dtsi is:
/ SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause
/*
* File generated by STMicroelectronics STM32CubeMX DDR Tool for MPUs
* DDR type: DDR3 / DDR3L
* DDR width: 16bits
* DDR density: 4Gb
* System frequency: 533000Khz
* Relaxed Timing Mode: false
* Address mapping type: RBC
*
* Save Date: 2020.02.20, save Time: 18:45:20
*/
#define DDR_MEM_NAME "DDR3-DDR3L 16bits 533000kHz"
#define DDR_MEM_SPEED 533000
#define DDR_MEM_SIZE 0x20000000
#define DDR_MSTR 0x00041401
#define DDR_MRCTRL0 0x00000010
#define DDR_MRCTRL1 0x00000000
#define DDR_DERATEEN 0x00000000
#define DDR_DERATEINT 0x00800000
.....
#define DDR_DX2DQSTR 0x3DB02000
#define DDR_DX3GCR 0x0000CE80
#define DDR_DX3DLLCR 0x40000000
#define DDR_DX3DQTR 0xFFFFFFFF
#define DDR_DX3DQSTR 0x3DB02000
#include "stm32mp15-ddr.dtsi"
NB: the calibration values (DXnDLLCR, DXnDQTR, DXnDQSTR, with n in 1...3) are not used when DDR_PHY_CAL_SKIP is not defined, only the built-in calibration is done.
3.3.2.3. Generic DDR dtsi file for STM32MP1 series[edit | edit source]
The dtsi file used with DDR_ defines is
For example, stm32mp15-ddr.dtsi is:
// SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause
/*
* Copyright (C) 2018-2021, STMicroelectronics - All Rights Reserved
*/
&ddr {
st,mem-name = DDR_MEM_NAME;
st,mem-speed = <DDR_MEM_SPEED>;
st,mem-size = <DDR_MEM_SIZE>;
st,ctl-reg = <
DDR_MSTR
DDR_MRCTRL0
DDR_MRCTRL1
DDR_DERATEEN
DDR_DERATEINT
DDR_PWRCTL
DDR_PWRTMG
DDR_HWLPCTL
DDR_RFSHCTL0
DDR_RFSHCTL3
DDR_CRCPARCTL0
DDR_ZQCTL0
DDR_DFITMG0
DDR_DFITMG1
DDR_DFILPCFG0
DDR_DFIUPD0
DDR_DFIUPD1
DDR_DFIUPD2
DDR_DFIPHYMSTR
DDR_ODTMAP
DDR_DBG0
DDR_DBG1
DDR_DBGCMD
DDR_POISONCFG
DDR_PCCFG
>;
st,ctl-timing = <
DDR_RFSHTMG
DDR_DRAMTMG0
DDR_DRAMTMG1
DDR_DRAMTMG2
DDR_DRAMTMG3
DDR_DRAMTMG4
DDR_DRAMTMG5
DDR_DRAMTMG6
DDR_DRAMTMG7
DDR_DRAMTMG8
DDR_DRAMTMG14
DDR_ODTCFG
>;
st,ctl-map = <
DDR_ADDRMAP1
DDR_ADDRMAP2
DDR_ADDRMAP3
DDR_ADDRMAP4
DDR_ADDRMAP5
DDR_ADDRMAP6
DDR_ADDRMAP9
DDR_ADDRMAP10
DDR_ADDRMAP11
>;
st,ctl-perf = <
DDR_SCHED
DDR_SCHED1
DDR_PERFHPR1
DDR_PERFLPR1
DDR_PERFWR1
DDR_PCFGR_0
DDR_PCFGW_0
DDR_PCFGQOS0_0
DDR_PCFGQOS1_0
DDR_PCFGWQOS0_0
DDR_PCFGWQOS1_0
DDR_PCFGR_1
DDR_PCFGW_1
DDR_PCFGQOS0_1
DDR_PCFGQOS1_1
DDR_PCFGWQOS0_1
DDR_PCFGWQOS1_1
>;
st,phy-reg = <
DDR_PGCR
DDR_ACIOCR
DDR_DXCCR
DDR_DSGCR
DDR_DCR
DDR_ODTCR
DDR_ZQ0CR1
DDR_DX0GCR
DDR_DX1GCR
DDR_DX2GCR
DDR_DX3GCR
>;
st,phy-timing = <
DDR_PTR0
DDR_PTR1
DDR_PTR2
DDR_DTPR0
DDR_DTPR1
DDR_DTPR2
DDR_MR0
DDR_MR1
DDR_MR2
DDR_MR3
>;
#ifdef DDR_PHY_CAL_SKIP
st,phy-cal = <
DDR_DX0DLLCR
DDR_DX0DQTR
DDR_DX0DQSTR
DDR_DX1DLLCR
DDR_DX1DQTR
DDR_DX1DQSTR
DDR_DX2DLLCR
DDR_DX2DQTR
DDR_DX2DQSTR
DDR_DX3DLLCR
DDR_DX3DQTR
DDR_DX3DQSTR
>;
#endif
};
3.3.3. On STM32MP2 series[edit | edit source]
3.3.3.1. Simple example[edit | edit source]
You can add the DDR configuration node with (STM32MP25x lines example):
&ddr {
st,mem-name = "DDR4 2x16Gbits 2x16bits 1200MHz";
st,mem-speed = <1200000>;
st,mem-size = <(0x100000000 >> 32) (0x100000000 & 0xFFFFFFFF)>;
st,ctl-reg = <
0x01040010 /* DDR_MSTR */
0x00000030 /* DDR_MRCTRL0 */
0x00000000 /* DDR_MRCTRL1 */
0x00000000 /* DDR_MRCTRL2 */
0x00000000 /* DDR_DERATEEN */
0x00000000 /* DDR_DERATEINT */
0x00000000 /* DDR_DERATECTL */
0x00000000 /* DDR_PWRCTL */
0x00130001 /* DDR_PWRTMG */
0x00000002 /* DDR_HWLPCTL */
0x00210010 /* DDR_RFSHCTL0 */
0x00000000 /* DDR_RFSHCTL1 */
0x00000000 /* DDR_RFSHCTL3 */
0x00000000 /* DDR_CRCPARCTL0 */
0x00001000 /* DDR_CRCPARCTL1 */
0xC0020002 /* DDR_INIT0 */
0x00010002 /* DDR_INIT1 */
0x00000D00 /* DDR_INIT2 */
0x09400103 /* DDR_INIT3 */
0x00180000 /* DDR_INIT4 */
0x00100004 /* DDR_INIT5 */
0x00080460 /* DDR_INIT6 */
0x00000C0F /* DDR_INIT7 */
0x00000000 /* DDR_DIMMCTL */
0x0000066F /* DDR_RANKCTL */
0x0000000D /* DDR_RANKCTL1 */
0x01000040 /* DDR_ZQCTL0 */
0x2000493E /* DDR_ZQCTL1 */
0x00000000 /* DDR_ZQCTL2 */
0x038F8209 /* DDR_DFITMG0 */
0x00080303 /* DDR_DFITMG1 */
0x07004111 /* DDR_DFILPCFG0 */
0x00000000 /* DDR_DFILPCFG1 */
0xC0300018 /* DDR_DFIUPD0 */
0x005700B4 /* DDR_DFIUPD1 */
0x80000000 /* DDR_DFIUPD2 */
0x00000041 /* DDR_DFIMISC */
0x00000F09 /* DDR_DFITMG2 */
0x00000000 /* DDR_DFITMG3 */
0x00000001 /* DDR_DBICTL */
0x80000000 /* DDR_DFIPHYMSTR */
0x00000000 /* DDR_DBG0 */
0x00000000 /* DDR_DBG1 */
0x00000000 /* DDR_DBGCMD */
0x00000000 /* DDR_SWCTL */
0x00000000 /* DDR_SWCTLSTATIC */
0x00000000 /* DDR_POISONCFG */
0x00000000 /* DDR_PCCFG */
>;
st,ctl-timing = <
0x0092014A /* DDR_RFSHTMG */
0x008C0000 /* DDR_RFSHTMG1 */
0x11152815 /* DDR_DRAMTMG0 */
0x0004051E /* DDR_DRAMTMG1 */
0x0609060D /* DDR_DRAMTMG2 */
0x0050400C /* DDR_DRAMTMG3 */
0x0904050A /* DDR_DRAMTMG4 */
0x06060403 /* DDR_DRAMTMG5 */
0x02020005 /* DDR_DRAMTMG6 */
0x00000202 /* DDR_DRAMTMG7 */
0x0606100B /* DDR_DRAMTMG8 */
0x0002040A /* DDR_DRAMTMG9 */
0x001C180A /* DDR_DRAMTMG10 */
0x4408021C /* DDR_DRAMTMG11 */
0x0C020010 /* DDR_DRAMTMG12 */
0x1C200004 /* DDR_DRAMTMG13 */
0x000000A0 /* DDR_DRAMTMG14 */
0x00000000 /* DDR_DRAMTMG15 */
0x06000618 /* DDR_ODTCFG */
0x00000001 /* DDR_ODTMAP */
>;
st,ctl-map = <
0x0000001F /* DDR_ADDRMAP0 */
0x003F0909 /* DDR_ADDRMAP1 */
0x00000000 /* DDR_ADDRMAP2 */
0x00000000 /* DDR_ADDRMAP3 */
0x00001F1F /* DDR_ADDRMAP4 */
0x070F0707 /* DDR_ADDRMAP5 */
0x07070707 /* DDR_ADDRMAP6 */
0x00000F07 /* DDR_ADDRMAP7 */
0x00003F08 /* DDR_ADDRMAP8 */
0x07070707 /* DDR_ADDRMAP9 */
0x07070707 /* DDR_ADDRMAP10 */
0x00000007 /* DDR_ADDRMAP11 */
>;
st,ctl-perf = <
0x80001B0C /* DDR_SCHED */
0x00000000 /* DDR_SCHED1 */
0x04000200 /* DDR_PERFHPR1 */
0x08000020 /* DDR_PERFLPR1 */
0x08000400 /* DDR_PERFWR1 */
0x04040208 /* DDR_SCHED3 */
0x08400810 /* DDR_SCHED4 */
0x00704100 /* DDR_PCFGR_0 */
0x00004100 /* DDR_PCFGW_0 */
0x00000000 /* DDR_PCTRL_0 */
0x0021000C /* DDR_PCFGQOS0_0 */
0x01000080 /* DDR_PCFGQOS1_0 */
0x01100C07 /* DDR_PCFGWQOS0_0 */
0x04000200 /* DDR_PCFGWQOS1_0 */
0x00704100 /* DDR_PCFGR_1 */
0x00004100 /* DDR_PCFGW_1 */
0x00000000 /* DDR_PCTRL_1 */
0x00100007 /* DDR_PCFGQOS0_1 */
0x01000080 /* DDR_PCFGQOS1_1 */
0x01100C07 /* DDR_PCFGWQOS0_1 */
0x04000200 /* DDR_PCFGWQOS1_1 */
>;
st,phy-basic = <
0x00000000 /* DDR_UIB_DRAMTYPE */
0x00000004 /* DDR_UIB_DIMMTYPE */
0x00000000 /* DDR_UIB_LP4XMODE */
0x00000004 /* DDR_UIB_NUMDBYTE */
0x00000004 /* DDR_UIB_NUMACTIVEDBYTEDFI0 */
0x00000000 /* DDR_UIB_NUMACTIVEDBYTEDFI1 */
0x00000008 /* DDR_UIB_NUMANIB */
0x00000001 /* DDR_UIB_NUMRANK_DFI0 */
0x00000001 /* DDR_UIB_NUMRANK_DFI1 */
0x00000010 /* DDR_UIB_DRAMDATAWIDTH */
0x00000001 /* DDR_UIB_NUMPSTATES */
0x000004B0 /* DDR_UIB_FREQUENCY_0 */
0x00000000 /* DDR_UIB_PLLBYPASS_0 */
0x00000001 /* DDR_UIB_DFIFREQRATIO_0 */
0x00000001 /* DDR_UIB_DFI1EXISTS */
0x00000000 /* DDR_UIB_TRAIN2D */
0x00000003 /* DDR_UIB_HARDMACROVER */
0x00000000 /* DDR_UIB_READDBIENABLE_0 */
0x00000000 /* DDR_UIB_DFIMODE */
>;
st,phy-advanced = <
0x00000000 /* DDR_UIA_LP4RXPREAMBLEMODE_0 */
0x00000000 /* DDR_UIA_LP4POSTAMBLEEXT_0 */
0x00000000 /* DDR_UIA_D4RXPREAMBLELENGTH_0 */
0x00000000 /* DDR_UIA_D4TXPREAMBLELENGTH_0 */
0x00000000 /* DDR_UIA_EXTCALRESVAL */
0x00000000 /* DDR_UIA_IS2TTIMING_0 */
0x00000050 /* DDR_UIA_ODTIMPEDANCE_0 */
0x0000001E /* DDR_UIA_TXIMPEDANCE_0 */
0x0000001E /* DDR_UIA_ATXIMPEDANCE */
0x00000000 /* DDR_UIA_MEMALERTEN */
0x00000000 /* DDR_UIA_MEMALERTPUIMP */
0x00000000 /* DDR_UIA_MEMALERTVREFLEVEL */
0x00000000 /* DDR_UIA_MEMALERTSYNCBYPASS */
0x00000001 /* DDR_UIA_DISDYNADRTRI_0 */
0x00000000 /* DDR_UIA_PHYMSTRTRAININTERVAL_0 */
0x00000000 /* DDR_UIA_PHYMSTRMAXREQTOACK_0 */
0x00000000 /* DDR_UIA_WDQSEXT */
0x00000009 /* DDR_UIA_CALINTERVAL */
0x00000000 /* DDR_UIA_CALONCE */
0x00000000 /* DDR_UIA_LP4RL_0 */
0x00000000 /* DDR_UIA_LP4WL_0 */
0x00000000 /* DDR_UIA_LP4WLS_0 */
0x00000000 /* DDR_UIA_LP4DBIRD_0 */
0x00000000 /* DDR_UIA_LP4DBIWR_0 */
0x00000000 /* DDR_UIA_LP4NWR_0 */
0x00000000 /* DDR_UIA_LP4LOWPOWERDRV */
0x00000000 /* DDR_UIA_DRAMBYTESWAP */
0x00000000 /* DDR_UIA_RXENBACKOFF */
0x00000000 /* DDR_UIA_TRAINSEQUENCECTRL */
0x00000000 /* DDR_UIA_SNPSUMCTLOPT */
0x00000000 /* DDR_UIA_SNPSUMCTLF0RC5X_0 */
0x0000000F /* DDR_UIA_TXSLEWRISEDQ_0 */
0x0000000F /* DDR_UIA_TXSLEWFALLDQ_0 */
0x0000000F /* DDR_UIA_TXSLEWRISEAC */
0x0000000F /* DDR_UIA_TXSLEWFALLAC */
0x00000001 /* DDR_UIA_DISABLERETRAINING */
0x00000000 /* DDR_UIA_DISABLEPHYUPDATE */
0x00000000 /* DDR_UIA_ENABLEHIGHCLKSKEWFIX */
0x00000001 /* DDR_UIA_DISABLEUNUSEDADDRLNS */
0x00000000 /* DDR_UIA_PHYINITSEQUENCENUM */
0x00000000 /* DDR_UIA_ENABLEDFICSPOLARITYFIX */
0x00000058 /* DDR_UIA_PHYVREF */
0x0000031F /* DDR_UIA_SEQUENCECTRL_0 */
>;
st,phy-mr = <
0x00000940 /* DDR_UIM_MR0_0 */
0x00000103 /* DDR_UIM_MR1_0 */
0x00000018 /* DDR_UIM_MR2_0 */
0x00000000 /* DDR_UIM_MR3_0 */
0x00000008 /* DDR_UIM_MR4_0 */
0x00000460 /* DDR_UIM_MR5_0 */
0x00000C0B /* DDR_UIM_MR6_0 */
0x00000000 /* DDR_UIM_MR11_0 */
0x00000000 /* DDR_UIM_MR12_0 */
0x00000000 /* DDR_UIM_MR13_0 */
0x00000000 /* DDR_UIM_MR14_0 */
0x00000000 /* DDR_UIM_MR22_0 */
>;
st,phy-swizzle = <
0x0000000C /* DDR_UIS_SWIZZLE_0 */
0x00000005 /* DDR_UIS_SWIZZLE_1 */
0x00000013 /* DDR_UIS_SWIZZLE_2 */
0x0000001A /* DDR_UIS_SWIZZLE_3 */
0x00000009 /* DDR_UIS_SWIZZLE_4 */
0x00000003 /* DDR_UIS_SWIZZLE_5 */
0x00000001 /* DDR_UIS_SWIZZLE_6 */
0x00000019 /* DDR_UIS_SWIZZLE_7 */
0x00000007 /* DDR_UIS_SWIZZLE_8 */
0x00000004 /* DDR_UIS_SWIZZLE_9 */
0x0000000A /* DDR_UIS_SWIZZLE_10 */
0x0000000D /* DDR_UIS_SWIZZLE_11 */
0x00000014 /* DDR_UIS_SWIZZLE_12 */
0x00000000 /* DDR_UIS_SWIZZLE_13 */
0x00000000 /* DDR_UIS_SWIZZLE_14 */
0x00000000 /* DDR_UIS_SWIZZLE_15 */
0x00000000 /* DDR_UIS_SWIZZLE_16 */
0x00000000 /* DDR_UIS_SWIZZLE_17 */
0x00000006 /* DDR_UIS_SWIZZLE_18 */
0x0000000B /* DDR_UIS_SWIZZLE_19 */
0x00000000 /* DDR_UIS_SWIZZLE_20 */
0x00000000 /* DDR_UIS_SWIZZLE_21 */
0x00000000 /* DDR_UIS_SWIZZLE_22 */
0x00000008 /* DDR_UIS_SWIZZLE_23 */
0x00000002 /* DDR_UIS_SWIZZLE_24 */
0x00000018 /* DDR_UIS_SWIZZLE_25 */
0x1A13050C /* DDR_UIS_SWIZZLE_26 */
0x19010309 /* DDR_UIS_SWIZZLE_27 */
0x0D0A0407 /* DDR_UIS_SWIZZLE_28 */
0x00000014 /* DDR_UIS_SWIZZLE_29 */
0x000B0600 /* DDR_UIS_SWIZZLE_30 */
0x02080000 /* DDR_UIS_SWIZZLE_31 */
0x00000018 /* DDR_UIS_SWIZZLE_32 */
0x00000000 /* DDR_UIS_SWIZZLE_33 */
0x00000000 /* DDR_UIS_SWIZZLE_34 */
0x00000000 /* DDR_UIS_SWIZZLE_35 */
0x00000000 /* DDR_UIS_SWIZZLE_36 */
0x00000000 /* DDR_UIS_SWIZZLE_37 */
0x00000000 /* DDR_UIS_SWIZZLE_38 */
0x00000000 /* DDR_UIS_SWIZZLE_39 */
0x00000000 /* DDR_UIS_SWIZZLE_40 */
0x00000000 /* DDR_UIS_SWIZZLE_41 */
0x00000000 /* DDR_UIS_SWIZZLE_42 */
0x00000000 /* DDR_UIS_SWIZZLE_43 */
>;
status = "okay";
};
3.3.3.2. STM32CubeMX configuration file[edit | edit source]
STM32CubeMX generates a .dtsi file with the needed values as defines (named DDR_...), and includes the #Generic DDR dtsi file for STM32MP2 series: as this dtsi file is preprocessed during FSBL compilation, it generates a correct device tree.
For example the file fdts/stm32mp25-ddr4-2x16Gbits-2x16bits-1200MHz.dtsi is:
/*
* Copyright (C) 2015-2018, STMicroelectronics - All Rights Reserved
*
* SPDX-License-Identifier: GPL-2.0-or-later BSD-3-Clause
*
*/
/*
* File generated by STMicroelectronics STM32CubeMX DDR Tool for MPUs
* DDR type: DDR4
* DDR width: 32 bits
* DDR density: 32Gb
* System frequency: 1200000kHz
* Address mapping type: RBC
*
* Save Date: 2023.10.13, save Time: 16:12:09
*/
#define DDR_MEM_NAME "DDR4 32 bits 933000kHz"
#define DDR_MEM_SPEED 933000
#define DDR_MEM_SIZE 0x100000000
#define DDR_MSTR 0x01040010
#define DDR_MRCTRL0 0x00000030
#define DDR_MRCTRL1 0x00000000
#define DDR_MRCTRL2 0x00000000
#define DDR_DERATEEN 0x00000000
.....
#define DDR_UIS_SWIZZLE_39 0x00000000
#define DDR_UIS_SWIZZLE_40 0x00000000
#define DDR_UIS_SWIZZLE_41 0x00000000
#define DDR_UIS_SWIZZLE_42 0x00000000
#define DDR_UIS_SWIZZLE_43 0x00000000
#include "stm32mp25-ddr.dtsi"
3.3.3.3. Generic DDR dtsi file for STM32MP2 series[edit | edit source]
The dtsi file used with DDR_ defines is
- stm32mp25-ddr.dtsi[11] for STM32MP25x lines
For example, stm32mp25-ddr.dtsi is:
// SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause
/*
* Copyright (C) 2023, STMicroelectronics - All Rights Reserved
*/
&ddr{
st,mem-name = DDR_MEM_NAME;
st,mem-speed = <DDR_MEM_SPEED>;
st,mem-size = <(DDR_MEM_SIZE >> 32) (DDR_MEM_SIZE & 0xFFFFFFFF)>;
st,ctl-reg = <
DDR_MSTR
DDR_MRCTRL0
DDR_MRCTRL1
DDR_MRCTRL2
DDR_DERATEEN
DDR_DERATEINT
DDR_DERATECTL
DDR_PWRCTL
DDR_PWRTMG
DDR_HWLPCTL
DDR_RFSHCTL0
DDR_RFSHCTL1
DDR_RFSHCTL3
DDR_CRCPARCTL0
DDR_CRCPARCTL1
DDR_INIT0
DDR_INIT1
DDR_INIT2
DDR_INIT3
DDR_INIT4
DDR_INIT5
DDR_INIT6
DDR_INIT7
DDR_DIMMCTL
DDR_RANKCTL
DDR_RANKCTL1
DDR_ZQCTL0
DDR_ZQCTL1
DDR_ZQCTL2
DDR_DFITMG0
DDR_DFITMG1
DDR_DFILPCFG0
DDR_DFILPCFG1
DDR_DFIUPD0
DDR_DFIUPD1
DDR_DFIUPD2
DDR_DFIMISC
DDR_DFITMG2
DDR_DFITMG3
DDR_DBICTL
DDR_DFIPHYMSTR
DDR_DBG0
DDR_DBG1
DDR_DBGCMD
DDR_SWCTL
DDR_SWCTLSTATIC
DDR_POISONCFG
DDR_PCCFG
>;
st,ctl-timing = <
DDR_RFSHTMG
DDR_RFSHTMG1
DDR_DRAMTMG0
DDR_DRAMTMG1
DDR_DRAMTMG2
DDR_DRAMTMG3
DDR_DRAMTMG4
DDR_DRAMTMG5
DDR_DRAMTMG6
DDR_DRAMTMG7
DDR_DRAMTMG8
DDR_DRAMTMG9
DDR_DRAMTMG10
DDR_DRAMTMG11
DDR_DRAMTMG12
DDR_DRAMTMG13
DDR_DRAMTMG14
DDR_DRAMTMG15
DDR_ODTCFG
DDR_ODTMAP
>;
st,ctl-map = <
DDR_ADDRMAP0
DDR_ADDRMAP1
DDR_ADDRMAP2
DDR_ADDRMAP3
DDR_ADDRMAP4
DDR_ADDRMAP5
DDR_ADDRMAP6
DDR_ADDRMAP7
DDR_ADDRMAP8
DDR_ADDRMAP9
DDR_ADDRMAP10
DDR_ADDRMAP11
>;
st,ctl-perf = <
DDR_SCHED
DDR_SCHED1
DDR_PERFHPR1
DDR_PERFLPR1
DDR_PERFWR1
DDR_SCHED3
DDR_SCHED4
DDR_PCFGR_0
DDR_PCFGW_0
DDR_PCTRL_0
DDR_PCFGQOS0_0
DDR_PCFGQOS1_0
DDR_PCFGWQOS0_0
DDR_PCFGWQOS1_0
DDR_PCFGR_1
DDR_PCFGW_1
DDR_PCTRL_1
DDR_PCFGQOS0_1
DDR_PCFGQOS1_1
DDR_PCFGWQOS0_1
DDR_PCFGWQOS1_1
>;
st,phy-basic = <
DDR_UIB_DRAMTYPE
DDR_UIB_DIMMTYPE
DDR_UIB_LP4XMODE
DDR_UIB_NUMDBYTE
DDR_UIB_NUMACTIVEDBYTEDFI0
DDR_UIB_NUMACTIVEDBYTEDFI1
DDR_UIB_NUMANIB
DDR_UIB_NUMRANK_DFI0
DDR_UIB_NUMRANK_DFI1
DDR_UIB_DRAMDATAWIDTH
DDR_UIB_NUMPSTATES
DDR_UIB_FREQUENCY_0
DDR_UIB_PLLBYPASS_0
DDR_UIB_DFIFREQRATIO_0
DDR_UIB_DFI1EXISTS
DDR_UIB_TRAIN2D
DDR_UIB_HARDMACROVER
DDR_UIB_READDBIENABLE_0
DDR_UIB_DFIMODE
>;
st,phy-advanced = <
DDR_UIA_LP4RXPREAMBLEMODE_0
DDR_UIA_LP4POSTAMBLEEXT_0
DDR_UIA_D4RXPREAMBLELENGTH_0
DDR_UIA_D4TXPREAMBLELENGTH_0
DDR_UIA_EXTCALRESVAL
DDR_UIA_IS2TTIMING_0
DDR_UIA_ODTIMPEDANCE_0
DDR_UIA_TXIMPEDANCE_0
DDR_UIA_ATXIMPEDANCE
DDR_UIA_MEMALERTEN
DDR_UIA_MEMALERTPUIMP
DDR_UIA_MEMALERTVREFLEVEL
DDR_UIA_MEMALERTSYNCBYPASS
DDR_UIA_DISDYNADRTRI_0
DDR_UIA_PHYMSTRTRAININTERVAL_0
DDR_UIA_PHYMSTRMAXREQTOACK_0
DDR_UIA_WDQSEXT
DDR_UIA_CALINTERVAL
DDR_UIA_CALONCE
DDR_UIA_LP4RL_0
DDR_UIA_LP4WL_0
DDR_UIA_LP4WLS_0
DDR_UIA_LP4DBIRD_0
DDR_UIA_LP4DBIWR_0
DDR_UIA_LP4NWR_0
DDR_UIA_LP4LOWPOWERDRV
DDR_UIA_DRAMBYTESWAP
DDR_UIA_RXENBACKOFF
DDR_UIA_TRAINSEQUENCECTRL
DDR_UIA_SNPSUMCTLOPT
DDR_UIA_SNPSUMCTLF0RC5X_0
DDR_UIA_TXSLEWRISEDQ_0
DDR_UIA_TXSLEWFALLDQ_0
DDR_UIA_TXSLEWRISEAC
DDR_UIA_TXSLEWFALLAC
DDR_UIA_DISABLERETRAINING
DDR_UIA_DISABLEPHYUPDATE
DDR_UIA_ENABLEHIGHCLKSKEWFIX
DDR_UIA_DISABLEUNUSEDADDRLNS
DDR_UIA_PHYINITSEQUENCENUM
DDR_UIA_ENABLEDFICSPOLARITYFIX
DDR_UIA_PHYVREF
DDR_UIA_SEQUENCECTRL_0
>;
st,phy-mr = <
DDR_UIM_MR0_0
DDR_UIM_MR1_0
DDR_UIM_MR2_0
DDR_UIM_MR3_0
DDR_UIM_MR4_0
DDR_UIM_MR5_0
DDR_UIM_MR6_0
DDR_UIM_MR11_0
DDR_UIM_MR12_0
DDR_UIM_MR13_0
DDR_UIM_MR14_0
DDR_UIM_MR22_0
>;
st,phy-swizzle = <
DDR_UIS_SWIZZLE_0
DDR_UIS_SWIZZLE_1
DDR_UIS_SWIZZLE_2
DDR_UIS_SWIZZLE_3
DDR_UIS_SWIZZLE_4
DDR_UIS_SWIZZLE_5
DDR_UIS_SWIZZLE_6
DDR_UIS_SWIZZLE_7
DDR_UIS_SWIZZLE_8
DDR_UIS_SWIZZLE_9
DDR_UIS_SWIZZLE_10
DDR_UIS_SWIZZLE_11
DDR_UIS_SWIZZLE_12
DDR_UIS_SWIZZLE_13
DDR_UIS_SWIZZLE_14
DDR_UIS_SWIZZLE_15
DDR_UIS_SWIZZLE_16
DDR_UIS_SWIZZLE_17
DDR_UIS_SWIZZLE_18
DDR_UIS_SWIZZLE_19
DDR_UIS_SWIZZLE_20
DDR_UIS_SWIZZLE_21
DDR_UIS_SWIZZLE_22
DDR_UIS_SWIZZLE_23
DDR_UIS_SWIZZLE_24
DDR_UIS_SWIZZLE_25
DDR_UIS_SWIZZLE_26
DDR_UIS_SWIZZLE_27
DDR_UIS_SWIZZLE_28
DDR_UIS_SWIZZLE_29
DDR_UIS_SWIZZLE_30
DDR_UIS_SWIZZLE_31
DDR_UIS_SWIZZLE_32
DDR_UIS_SWIZZLE_33
DDR_UIS_SWIZZLE_34
DDR_UIS_SWIZZLE_35
DDR_UIS_SWIZZLE_36
DDR_UIS_SWIZZLE_37
DDR_UIS_SWIZZLE_38
DDR_UIS_SWIZZLE_39
DDR_UIS_SWIZZLE_40
DDR_UIS_SWIZZLE_41
DDR_UIS_SWIZZLE_42
DDR_UIS_SWIZZLE_43
>;
};
4. How to configure the DT using STM32CubeMX[edit | edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX supports all the defines described in the above DT bindings documentation paragraph with a generated included file "stm32mpXX-mx.dtsi"; it is included in the mx dts file before the Generic DDR dtsi file. Refer to the STM32CubeMX user manual and the dedicated application note[8] (only on STM32MP1 series) for further information.
On STM32MP1 series, If you want to use the STM32CubeMX DDR Tuning Tool calibration result, add in the generated files "stm32mp13-mx.dtsi" or "stm32mp15-mx.dtsi" the line:
#define DDR_PHY_CAL_SKIP
5. References[edit | edit source]
Please refer to the following links for additional information:
- ↑ docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt TF-A DDR binding information file
- ↑ docs/devicetree/bindings/memory-controllers/st,stm32mp2-ddr.txt TF-A DDR binding information file
- ↑ stm32mp131.dtsi (for TF-A)
- ↑ stm32mp151.dtsi (for TF-A)
- ↑ stm32mp211.dtsi (for TF-A)
- ↑ stm32mp231.dtsi (for TF-A)
- ↑ stm32mp251.dtsi (for TF-A)
- ↑ Jump up to: 8.0 8.1 AN5168 - DDR configuration on STM32MP1 series MPU
- ↑ fdts/stm32mp13-ddr.dtsi (for TF-A): STM32MP13x DDR device tree file
- ↑ fdts/stm32mp15-ddr.dtsi (for TF-A): STM32MP15x DDR device tree file
- ↑ fdts/stm32mp25-ddr.dtsi (for TF-A): STM32MP25x DDR device tree file