This article introduces the structure and the content of the STM32CubeMP15 Package / STM32CubeMP1 Package (a.k.a., STM32CubeMP15 / STM32CubeMP1) , the embedded software part of STM32Cube™, running on the Arm® Cortex®-M4 processor. It references also other interesting wiki articles to better understand and use the STM32CubeMP15 Package.
1. What is the STM32CubeMP15 Package?[edit | edit source]
STM32CubeMP15 Package, running on the Arm® Cortex®-M4 processor, consists of:
- The hardware abstraction layer (HAL), enabling portability between different STM32 devices via standardized API calls
- The low-layer API (LL), a light-weight, optimized, expert oriented set of APIs designed for runtime efficiency and so enhanced performance
- The board support package drivers (BSP), based on HAL drivers, an API set for the evaluation board and third-party components.
- A collection of middleware components (such as FreeRTOS)
- A collection of examples, running on an MPU board and allowing demonstration of a basic implementation of features from a set of IPs
The STM32CubeMP15 Package is based on the STM32CubeMCU Package and has been adapted to a Linux framework (OpenSTLinux).
STM32CubeMP15 Package introduces new components such as OpenAMP and ResourceManager that allow easy communication and resource sharing between main processors running with Linux on Arm® Cortex®-A7, and MCU processors running on Arm® Cortex®-M4.
- OpenAMP is a library implementing the remote processor service framework (RPMsg) which is a virtio-based messaging bus that allows a local processor to communicate with remote processors available on the system.
- ResourceManager is a utility that handles peripheral-accessibility requests and system-resource configuration.
![]() |
Note:
|
2. Software architecture overview[edit | edit source]
Software architecture overview is described in STM32CubeMP15 Package architecture.
3. STM32CubeMP15 Package structure[edit | edit source]
This chapter describes the structure of the STM32CubeMP15 Package (drivers, middleware components...).
STM32CubeMP15 Package offers a highly portable Hardware Abstraction Layer (HAL), built around a generic and modular architecture.
This HAL allows the upper layers, middleware and application, to implement functions whatever the STM32MP1 device used. This improves the library code re-usability and guarantees easy portability from one device to another.
STM32CubeMP15 Package also offers a highly portable Low Layer interface (LL), which allows a quick, simple and optimized API to access the STM32MP15 registers.
The STM32CubeMP15 Package is provided with the structure shown below.
4. STM32CubeMP15 Package content[edit | edit source]
This chapter describes the content of the STM32CubeMP15 Package (drivers, middleware components...).
4.1. Drivers[edit | edit source]
The Drivers folder contains all the STM32Cube Drivers, including BSP and HAL drivers.
The STM32CubeMP15 Package provides all driver user manuals:
- The BSP user manual for STM32MP157x-EV1 Evaluation board
is available in Drivers/BSP/STM32MP15xx_EVAL/STM32MP15xx_EVAL_BSP_User_Manual.chm
- The BSP user manual for STM32MP157x-DK2 Discovery kit
is available in Drivers/BSP/STM32MP15xx_DISCO/STM32MP15xx_DISCO_BSP_User_Manual.chm
- The HAL user manual is available in Drivers/STM32MP1xx_HAL_Driver/STM32MP157Cxx_CM4_User_Manual.chm
Chapters, here after, give the list of available BSP, HAL and LL drivers.
4.1.1. HAL drivers[edit | edit source]
STM32CubeMP15 HAL Driver items | Description |
---|---|
ADC |
ADC) * peripheral: * + Initialization and de-initialization functions * ++ Initialization and Configuration of ADC * + Operation functions * ++ Start, stop, get result of conversions of regular * group, using 3 possible modes: polling, interruption or DMA. * + Control functions * ++ Channels configuration on regular group * ++ Analog Watchdog configuration * + State functions * ++ ADC state machine management * ++ Interrupts and flags management * + Operation functions * ++ Start, stop, get result of conversions of ADC group injected, * using 2 possible modes: polling, interruption. * ++ Calibration * +++ ADC automatic self-calibration * +++ Calibration factors get or set * ++ Multimode feature when available * + Control functions * ++ Channels configuration on ADC group injected * + State functions * ++ ADC group injected contexts queue management* This driver provides firmware functions to manage the following * functionalities of the Analog to Digital Convertor ( |
CEC |
CEC). * + Initialization and de-initialization function * + IO operation function * + Peripheral Control function* This driver provides firmware functions to manage the following * functionalities of the High Definition Multimedia Interface * Consumer Electronics Control Peripheral ( |
CRC |
CRC) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral State functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Cyclic Redundancy Check ( |
CORTEX |
MPU, Cache, …): * + Initialization and de-initialization functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the CORTEX ( |
CRYP |
CRYP) peripheral: * + Initialization and de-initialization functions * + AES processing functions * + DES processing functions * + TDES processing functions * + DMA callback functions * + CRYP IRQ handler management * + Peripheral State functions * + Extended AES processing functions* This driver provides firmware functions to manage the following * functionalities of the Cryptography ( |
DAC |
DAC) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Digital to Analog Converter ( |
DCMI |
DCMI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions* This driver provides firmware functions to manage the following * functionalities of the Digital Camera Interface ( |
DFSDM |
DFSDM) peripherals: * + Initialization and configuration of channels and filters * + Regular channels configuration * + Injected channels configuration * + Regular/Injected Channels DMA Configuration * + Interrupts and flags management * + Analog watchdog feature * + Short-circuit detector feature * + Extremes detector feature * + Clock absence detector feature * + Break generation on analog watchdog or short-circuit event * + Set and get pulses skipping on channel.* This driver provides firmware functions to manage the following * functionalities of the Digital Filter for Sigma-Delta Modulators * ( |
DMA |
DMA) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and errors functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access ( |
EXTI |
EXTI) peripheral: * + Initialization and de-initialization functions * + IO operation functions* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output ( |
FDCAN |
IO operation functions * + Peripheral Configuration and Control functions * + Peripheral State and Error functions* This driver provides firmware functions to manage the following * functionalities of the Flexible DataRate Controller Area Network * (FDCAN) peripheral: * + Initialization and de-initialization functions * + |
FMC_SRAM |
* This driver provides a generic firmware to drive SRAM memories
* mounted as external device.
|
GPIO |
GPIO) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Extended Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output ( |
HAL |
HAL, Tick, SYSCFG, DBGMCU: * + Initialization and de-initialization functions * + HAL Initialization and de-initialization functions * + Configure the source of the time base * + HAL Control functions * + Tick management (get/set/inc/priority/suspend/resume) * + Get HAL revision, the device revision identifier, the device identifier * + Enable/Disable DBG wake up on AIEC * + Enable/Disable the Debug Module during Domain1 SLEEP mode * + Enable/Disable the Debug Module during Domain1 STOP mode * + Enable/Disable the Debug Module during Domain1 STANDBY mode * + Configure the internal voltage reference buffer voltage scale * + Configure the internal voltage reference buffer high impedance mode * + Tune the Internal Voltage Reference buffer (VREFBUF) * + Enable/Disable the Internal Voltage Reference buffer (VREFBUF) * + Ethernet PHY Interface Selection either MII or RMII * + Analog Switch control for dual analog pads * + Enable/Disable the booster to reduce the total harmonic distortion of the analog * + Enable/Power-down the I/O Compensation Cell * + To Enable/Disable optimize the I/O speed when the product voltage is low * + Code selection for the I/O Compensation cell* This driver provides firmware functions to manage the following * functionalities of |
HASH |
HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * + Peripheral State methods * + HASH or HMAC processing suspension/resumption * Additionally, this driver provides functions to manage HMAC * multi-buffer DMA-based processing for MD-5, SHA-1, SHA-224 * and SHA-256.* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral: * + Initialization and de-initialization methods * + HASH or |
HSEM |
* This driver provides firmware functions to manage the following
* functionalities of the semaphore peripheral:
* + Semaphore Take function (2-Step Procedure) , non blocking
* + Semaphore FastTake function (1-Step Procedure) , non blocking
* + Semaphore Status check
* + Semaphore Clear Key Set and Get
* + Release and release all functions
* + Semaphore notification enabling and disabling and callnack functions
* + IRQ handler management
|
I2C |
IO operation functions * + Peripheral State and Errors functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Inter Integrated Circuit (I2C) peripheral: * + Initialization and de-initialization functions * + |
IPCC |
IPCC). * + Initialization and de-initialization functions * + Configuration, notification and interrupts handling * + Peripheral State and Error functions* This driver provides firmware functions to manage the following * functionalities of the Inter-Processor communication controller * peripherals ( |
LPTIM |
LPTIM) peripheral: * + Initialization and de-initialization functions. * + Start/Stop operation functions in polling mode. * + Start/Stop operation functions in interrupt mode. * + Reading operation functions. * + Peripheral State functions.* This driver provides firmware functions to manage the following * functionalities of the Low Power Timer ( |
MDIOS |
IO operation functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the MDIOS Peripheral. * + Initialization and de-initialization functions * + |
MDMA |
* This driver provides firmware functions to manage the following
* functionalities of the Master Direct Memory Access (MDMA) peripheral:
* + Initialization/de-initialization functions
* + I/O operation functions
* + Peripheral State and errors functions
|
PWR |
* This driver provides firmware functions to manage the following
* functionalities of the Power Controller (PWR) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Peripheral Extended features functions
|
QUADSPI |
* This driver provides firmware functions to manage the following
* functionalities of the QuadSPI interface (QSPI).
* + Initialization and de-initialization functions
* + Indirect functional mode management
* + Memory-mapped functional mode management
* + Auto-polling functional mode management
* + Interrupts and flags management
* + MDMA channel configuration for indirect functional mode
* + Errors management and abort functionality
|
RCC |
RCC) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Extended Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the Reset and Clock Control ( |
RNG |
RNG) peripheral: * + Initialization and configuration functions * + Peripheral Control functions * + Peripheral State functions* This driver provides firmware functions to manage the following * functionalities of the Random Number Generator ( |
RTC |
RTC) peripheral: * + Initialization/de-initialization functions * + Calendar (Time and Date) configuration * + Alarms (Alarm A and Alarm B) configuration * + WakeUp Timer configuration * + TimeStamp configuration * + Tampers configuration * + Backup Data Registers configuration * + RTC Tamper and TimeStamp Pins Selection * + Interrupts and flags management* This driver provides firmware functions to manage the following * functionalities of the Real-Time Clock ( |
SAI |
SAI) peripheral: * + Initialization/de-initialization functions * + I/O operation functions * + Peripheral Control functions * + Peripheral State functions * + Modify PDM microphone delays.* This driver provides firmware functions to manage the following * functionalities of the Serial Audio Interface ( |
SD |
SD) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Secure Digital ( |
SMARTCARD |
IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the SMARTCARD peripheral: * + Initialization and de-initialization functions * + |
SMBUS |
SMBus) peripheral, * based on I2C principles of operation : * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions* This driver provides firmware functions to manage the following * functionalities of the System Management Bus ( |
SPDIFRX |
DMA transfers management * + Interrupts and flags management* This driver provides firmware functions to manage the following * functionalities of the SPDIFRX audio interface: * + Initialization and Configuration * + Data transfers functions * + |
SPI |
SPI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + IO operation functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the Serial Peripheral Interface ( |
TIMER |
DMA * + Time Output Compare/PWM Initialization * + Time Output Compare/PWM Channel Configuration * + Time Output Compare/PWM Start * + Time Output Compare/PWM Start Interruption * + Time Output Compare/PWM Start DMA * + Time Input Capture Initialization * + Time Input Capture Channel Configuration * + Time Input Capture Start * + Time Input Capture Start Interruption * + Time Input Capture Start DMA * + Time One Pulse Initialization * + Time One Pulse Channel Configuration * + Time One Pulse Start * + Time Encoder Interface Initialization * + Time Encoder Interface Start * + Time Encoder Interface Start Interruption * + Time Encoder Interface Start DMA * + Commutation Event configuration with Interruption and DMA * + Time OCRef clear configuration * + Time External Clock configuration * + Time Hall Sensor Interface Initialization * + Time Hall Sensor Interface Start * + Time Complementary signal bread and dead time configuration * + Time Master and Slave synchronization configuration * + Time Output Compare/PWM Channel Configuration (for channels 5 and 6) * + Time OCRef clear configuration * + Timer remapping capabilities configuration* This driver provides firmware functions to manage the following * functionalities of the Timer (TIM) peripheral: * + Time Base Initialization * + Time Base Start * + Time Base Start Interruption * + Time Base Start |
U(S)ART |
ART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the Universal (Synchronous) Asynchronous Receiver Transmitter * Peripheral (U(S) |
WWDG |
IO operation functions* This driver provides firmware functions to manage the following * functionalities of the Window Watchdog (WWDG) peripheral: * + Initialization and Configuration functions * + |
4.1.2. LL drivers[edit | edit source]
STM32CubeMP15 LL Driver items | Description |
---|---|
ADC |
ADC peripheral: * + Initialization/de-initialization functions * + Configuration functions (ADC instance, group regular, group injected, * channels, analog watchdog, oversampling, multimode) * + IT/FLAGS management functions* This driver provides firmware functions to manage the following * functionalities of the |
BUS |
* This driver provides firmware functions to manage the following
* functionalities of the BUS peripheral:
* + Enable/disable/reset clocks for all system BUS (AHB2, AHB3, AHB4, AHB5, AHB6,
* AXI, MLAHB, APB1, APB2, APB3, APB4, APB5)
|
CORTEX |
SYSTICK configuration used by @ref LL_mDelay and @ref LL_Init1msTick functions * + Low power mode configuration (SCB register of Cortex®-MCU) * + API to access to MCU info (CPUID register)* This driver contains a set of generic APIs that can be used by user: * + |
DMA |
DMA peripheral: * + Initialization/de-initialization functions * + Configuration functions * + IT/FLAGS management functions* This driver provides firmware functions to manage the following * functionalities of the |
DMAMUX |
* This driver provides firmware functions to manage the following
* functionalities of the DMAMUX peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS management functions
|
EXTI |
EXTI peripheral: * + Initialization/de-initialization functions * + IT/FLAGS/Trigger management functions * + Configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
FMC_SRAM |
* This driver provides firmware functions to manage the following
* functionalities of the PSRAM peripheral:
* + Initialization/de-initialization functions
* + Timing management functions
* + Configuration functions
|
GPIO |
GPIO peripheral: * + Initialization/de-initialization functions * + Data access functions * + Port configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
HSEM |
HSEM peripheral: * + IT/FLAGS management functions * +Data management functions* This driver provides firmware functions to manage the following * functionalities of the |
I2C |
* This driver provides firmware functions to manage the following
* functionalities of the I2C peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS management functions
* +Data management functions
* + Configuration functions
|
IPCC |
IPCC peripheral: * + IT/FLAGS management functions * + Enable/disable transmit and receive channels functions* This driver provides firmware functions to manage the following * functionalities of the |
LPTIM |
LPTIM peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Configuration (Trigger / Clock / Encoder / LPTIM) functions* This driver provides firmware functions to manage the following * functionalities of the |
PWR |
* This driver provides firmware functions to manage the following
* functionalities of the PWR peripheral:
* + Initialization/de-initialization functions
* + FLAGS management functions
* + Configuration functions
|
RCC |
RCC peripheral: * + Clocks management functions (HSE/HSI/CSI/LSE/LSI/MCO/PLL) * + RTC/TIMERS functions * + IT/FLAGS management functions * + De-initialization functions * + Get system and peripherals clocks frequency functions* This driver provides firmware functions to manage the following * functionalities of the |
RTC |
RTC peripheral: * + Initialization/de-initialization functions * + TIME/DATE/ALM functions * + Configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
SPI |
SPI peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Data / DMA management functions * + Configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
SYSTEM |
SYSCFG and DBGMCU functions* This driver provides firmware functions to manage the following * functionalities of the SYSTEM peripheral: * + |
TIM |
DMA Burst Mode ) * + Counter clock selection functions * + Timer input remapping functions * + IT/FLAGS management functions * + DMA management functions * + Event management functions* This driver provides firmware functions to manage the following * functionalities of the TIM peripheral: * + Initialization/de-initialization functions * + Configuration functions (Time base, Capture Compare, Output and Input Channel, * Timer Synchro, Break, |
USART |
USART peripheral: * + Initialization/de-initialization functions * + Configuration functions (Irda, Smartcard, Half duplex, * SPI Slave, LIN, Driver enable) * + Advanced configurations services functions * + IT/FLAGS management functions * + DMA management functions * + Data management functions * + Execution functions* This driver provides firmware functions to manage the following * functionalities of the |
UTILS |
* This driver provides firmware functions to manage the following
* functionalities of the UTILS peripheral:
* + Device Electronic Signature functions
* + DELAY functions
* + SYSTEM functions
|
WWDG |
* This driver provides firmware functions to manage the following
* functionalities of the WWDG peripheral:
* + Enable / Disable functions
* + Configuration functions
* + IT/FLAGS management functions
|
4.1.3. BSP drivers[edit | edit source]
The BSP drivers offer a set of APIs relative to the hardware components available in the hardware boards (LEDs, Buttons and COM port).
DISCO │ ├── bumpversion.cfg │ ├── Release_Notes.html │ ├── STM32MP15xx_DISCO_BSP_User_Manual.chm │ ├── stm32mp15xx_disco_bus.c │ ├── stm32mp15xx_disco_bus.h │ ├── stm32mp15xx_disco.c │ ├── stm32mp15xx_disco_conf_template.h │ ├── stm32mp15xx_disco_errno.h │ ├── stm32mp15xx_disco.h │ ├── stm32mp15xx_disco_stpmic1.c │ └── stm32mp15xx_disco_stpmic1.h └── STM32MP15xx_EVAL │ ├── bumpversion.cfg │ ├── Release_Notes.html │ ├── STM32MP15xx_EVAL_BSP_User_Manual.chm │ ├── stm32mp15xx_eval_bus.c │ ├── stm32mp15xx_eval_bus.h │ ├── stm32mp15xx_eval.c │ ├── stm32mp15xx_eval_conf_template.h │ ├── stm32mp15xx_eval_errno.h │ ├── stm32mp15xx_eval.h │ ├── stm32mp15xx_eval_stpmic1.c │ └── stm32mp15xx_eval_stpmic1.h├── STM32MP15xx_
4.2. Middlewares[edit | edit source]
The Middlewares folder contains all available STM32Cube Middlewares including:
- FreeRTOS
- OpenAMP
![]() |
Note:
|
4.3. Projects[edit | edit source]
The "Projects" folder contains all STM32Cube examples that are classified in 3 levels as described below :
- Level 0 : Examples. It uses only the HAL drivers without any middleware component. They are available in directory Firmware/Projects/<board_name>/Examples.
- Level 1 : Applications. It provides typical use cases of each middleware component. They are available in directory Firmware/Projects/<board_name>/Applications.
- Level 2 : Demonstrations. It involves all the HAL, BSP and middleware components. They are available in directory Firmware/Projects/<board_name>/Demonstrations.
ATemplate folder is available in Firmware/Projects/<board_name>/Templates and allows quick creation and building of any firmware application on a given board.
All examples respect the same structure :
OpenAMP_TTY_echo │ ├── readme.txt describes the example behavior and the setup required to make it work │ ├── Inc contains all header files │ ├── Remoteproc (optional): contains specific files related to the use of Linux® remote processor framework to load STM32Cube Cortex-M4 firmware │ ├── Src contains all the sources code files │ └── STM32CubeIDE contains the preconfigured project for Eclipse IDE├──
You will find below a list of examples, applications and demonstrations available for STM32MP157x-EV1 Evaluation board and STM32MP157x-DK2 Discovery kit
:
Find below, the list of available projects for those boards:
Legend:
- (*) : List of STM32MP157x-DK2
and STM32MP157x-EV1
examples available with 3 IDEs ( STM32CubeIDE, IARTM, KEIL®), the others are only available with STM32CubeIDE.
- Examples, applications and demonstrations for STM32MP157C-EV1
FreeRTOS │ │ ├── FreeRTOS_ThreadCreation │ │ └── OpenAMP │ │ ├── OpenAMP_Dynamic_ResMgr │ │ ├── OpenAMP_for_signed_fw │ │ ├── OpenAMP_FreeRTOS_echo │ │ ├── OpenAMP_raw │ │ ├── OpenAMP_TTY_echo │ │ └── OpenAMP_TTY_echo_wakeup │ ├── Demonstrations │ │ └── AI_Character_Recognition │ ├── Examples │ │ ├── ADC │ │ │ └── ADC_AnalogWatchdog │ │ │ └── ADC_MultiChannelSingleConversion │ │ │ └── ADC_OverSampler │ │ │ └── ADC_SingleConversion_TriggerTimer_DMA │ │ ├── Cortex │ │ │ └── CORTEXM_MPU │ │ ├── CRC │ │ │ └── CRC_UserDefinedPolynomial │ │ ├── CRYP │ │ │ └── CRYP_AES_DMA │ │ ├── DAC │ │ │ └── DAC_SimpleConversion │ │ ├── DMA │ │ │ └── DMA_FIFOMode │ │ ├── FDCAN │ │ │ └── FDCAN_Loopback │ │ ├── GPIO │ │ │ └── GPIO_EXTI │ │ ├── HASH │ │ │ └── HASH_SHA224SHA256_DMA │ │ ├── I2C │ │ │ ├── I2C_TwoBoards_ComDMA │ │ │ └── I2C_TwoBoards_ComIT │ │ ├── LPTIM │ │ │ └── LPTIM_PulseCounter │ │ │ └── LPTIM_PWM_LSE │ │ ├── PWR │ │ │ └── PWR_STOP_CoPro │ │ ├── QSPI │ │ │ └── QSPI_ReadWrite_IT │ │ ├── SPI │ │ │ ├── SPI_FullDuplex_ComDMA_Master │ │ │ └── SPI_FullDuplex_ComDMA_Slave │ │ ├── TIM │ │ │ └── TIM_DMABurst │ │ │ └── TIM_OnePulse │ │ │ └──TIM_PWMOutput │ │ │ └── TIM_Synchronization │ │ │ └── TIM_TimeBase │ │ ├── UART │ │ │ └── UART_Receive_Transmit_Console │ │ │ └── UART_TwoBoards_ComIT │ │ └── WWDG │ │ └── WWDG_Example├── STM32MP157C-EV1 │ ├── Applications │ │ ├── CoproSync │ │ ├── CoproSync_ShutDown │ │ ├──
- Examples, applications and demonstrations for STM32MP157C-DK2
- Examples, applications and demonstrations for STM32MP157C-DK2
FreeRTOS │ │ ├── FreeRTOS_ThreadCreation │ │ └── OpenAMP │ │ ├── OpenAMP_for_signed_fw │ │ ├── OpenAMP_FreeRTOS_echo │ │ ├── OpenAMP_raw │ │ ├── OpenAMP_TTY_echo │ │ └── OpenAMP_TTY_echo_wakeup │ ├── Demonstrations │ │ └── AI_Character_Recognition │ ├── Examples │ │ ├── ADC │ │ │ └── ADC_SingleConversion_TriggerTimer_DMA │ │ ├── Cortex │ │ │ └── CORTEXM_MPU │ │ ├── CRC │ │ │ └── CRC_UserDefinedPolynomial │ │ ├── CRYP │ │ │ └── CRYP_AES_DMA │ │ ├── DMA │ │ │ └── DMA_FIFOMode │ │ ├── FDCAN │ │ │ └── FDCAN_Loopback │ │ ├── GPIO │ │ │ └── GPIO_EXTI │ │ ├── HASH │ │ │ └── HASH_SHA224SHA256_DMA │ │ ├── I2C │ │ │ └── I2C_TwoBoards_ComIT │ │ ├── LPTIM │ │ │ └── LPTIM_PulseCounter │ │ ├── PWR │ │ │ └── PWR_STOP_CoPro │ │ ├── SPI │ │ │ ├── SPI_FullDuplex_ComDMA_Master │ │ │ ├── SPI_FullDuplex_ComDMA_Slave │ │ │ ├── SPI_FullDuplex_ComIT_Master │ │ │ └── SPI_FullDuplex_ComIT_Slave │ │ ├── TIM │ │ │ └── TIM_DMABurst │ │ ├── UART │ │ │ └── UART_Receive_Transmit_Console │ │ │ ├── UART_TwoBoards_ComDMA │ │ │ └── UART_TwoBoards_ComIT │ │ └── WWDG │ │ └── WWDG_Example├── STM32MP157C-DK2 │ ├── Applications │ │ ├── CoproSync │ │ ├── CoproSync_ShutDown │ │ ├──
5. Get started with STM32CubeMP15 Package[edit | edit source]
The STM32CubeMP15 Package is available through the three packages (starter, developer, and distribution). To know how to get them, read STM32CubeMP15_Package_-_Getting_started article.