STM32MP135x-DK - software distributions

Revision as of 15:13, 18 November 2022 by Registered User (→‎Supported software distribution)
Applicable for STM32MP13x lines

The STM32MP135x-DK Discovery kit More info green.png (STM32MP135F-DK More info green.png) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP135 line More info.png microprocessor devices.

All useful information to start with the STM32MP135x-DK Discovery kit More info green.png is accessible through the links provided below.

1. Supported software distribution[edit source]

Only one software distribution is supported with STM32MP135x-DK Discovery kit More info green.png:

  • The STM32MPU Embedded Software distribution[1].

Take also a look at the latest STM32 MPU ecosystem release note for complementary information.

For this distribution, three software Packages are delivered:

  • the Starter Package
  • the Developer Package
  • the Distribution Package

Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.

These Packages provide you with the software packages (image, source code) and the tools that are needed to start using the STM32MP135x-DK More info green.png Discovery Kits boards.

ST logo.png STM32MPU Embedded Software distribution[1]
Starter Package Developer Package Distribution Package
  • to evaluate the board capabilities
  • to run examples
  • to modify the pieces of software delivered as source code in this Package (for example the Linux® kernel)
  • to add custom applications in the user space (delivered as binary in this Package)

Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE

  • to create a custom distribution

2. Hardware description[edit source]

A brief article (see link below) describes the board, and provides indications on how to:

  • assemble the board
  • configure the hardware switches
  • connect the board to external material

It also contains a short introduction of the board hardware components and connectors.

Board description
STM32MP135x-DK - hardware description
STM32MP135x-DK - hardware description

3. References[edit source]