Template:ArticleMainWriter
Template:ArticleApprovedVersion
1. Article purpose[edit source]
The purpose of this article is to
- briefly introduce the CRC peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain how to configure the CRC peripheral.
2. Peripheral overview[edit source]
The CRC peripheral is used to verify data transmission or storage integrity.
2.1. Features[edit source]
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2. Security support[edit source]
CRC1 and CRC2 are non secure peripherals.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
CRC instances are not used at boot time.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
CRC instances can be allocated to:
- the Arm® Cortex®-A7 non-secure for using in Linux® with Linux Crypto framework
or
- the Arm® Cortex®-M4 for using in STM32Cube with STM32Cube CRC driver
Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.
3.2.2. Software frameworks[edit source]
Internal peripherals software table template
| rowspan="9" | Security | rowspan="9" | CRC |- | | Linux Crypto framework | STM32Cube CRC driver |- |}
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
3.2.4. Peripheral assignment[edit source]
Internal peripherals assignment table template
| rowspan="2" | Security | rowspan="2" | CRC | CRC1 | | ☐ | | |- | CRC2 | | | ☐ | |-
|}
4. How to go further[edit source]
Not applicable.