Last edited 2 months ago

STM32CubeMP2 Package release note


This article aims to describe the content of the software release included in the STM32CubeMP2 package, version v1.1.0, which is part of the STM32 MPU ecosystem release note v6.0.0.

1. Delivery purpose and scope[edit | edit source]

The STM32CubeMP2 package is a software package running on the Arm® Cortex®-M33 processor and is a fundamental part of the Yocto-based OpenSTLinux embedded software distribution.

This release includes:

  • The STM32Cube HAL: STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
  • Low-layer APIs (LL APIs): Offering a fast, lightweight, expert-oriented layer that is closer to the hardware than the HAL. LL APIs are only available for a limited set of peripherals.
  • A consistent set of middleware components: such as FreeRTOS™ and OpenAMP.
  • All embedded software utilities: delivered with a full set of examples.

It also includes:

  • BSP for the STM32MP257F-EV1 Evaluation board More info green.png, STM32MP257F-DK Discovery kit More info green.png, and STM32MP257F-DK Discovery kit More info green.png for STM32MP23x lines evaluation Info.png (LED, button, STPMIC25 and COM ports)
  • Multi-core components
  • Projects: several projects (examples, applications) are implemented in IDE delivered by ST
  • STM32CubeIDE delivered by ST
  • All the STM32MP257F-EV1 More info green.png, STM32MP257F-DK More info green.png, STM32MP257F-DK More info green.png for STM32MP23x lines evaluation Info.png projects are available on STM32CubeIDE.

2. Intended Audience[edit | edit source]

The targeted audience is STM32 MPU customers and partners.

3. Licensing[edit | edit source]

All licenses applicable to STM32CubeMP2 package are available here.

4. Supported devices[edit | edit source]

The drivers provided within this package support all STM32MP23x lines More info.png and STM32MP25x lines More info.png.

5. Supported hardware[edit | edit source]

The software examples and the drivers delivered in this package are applicable for the following boards:

6. Release content[edit | edit source]

This is a maintenance release of the STM32CubeMP2 software package running on Arm® Cortex®-M33 core. The full content is available in STM32CubeMP2 Package content.

6.1. Main changes[edit | edit source]

  • Support for STM32MP235/3/1 (including BSP, ResourceManager and Examples)
  • Support for STM32MP257/5/3/1 16x16 package
  • Support for STM32MP25 Cortex-M0+
  • Low power modes demonstration
  • Support to run encrypted firmware
  • Resource manager improvements
  • CMSIS version v5.9.0 - Updated

6.1.1. HAL drivers[edit | edit source]

  • This is a maintenance release of the STM32CubeMP2 package HAL drivers. Added Register callback support and some MISRA fixes.
  • All HAL drivers have been checked for MISRA 2012 compliance, and most warnings have been resolved. The last remaining warnings could be solved by customers if needed.
  • Check the overview and all available HAL drivers in HAL drivers.

6.1.2. LL drivers[edit | edit source]

  • This is a maintenance release of the STM32CubeMP2 package LL drivers. There are some driver fixes for support of Arm® Cortex®-M0+ and a few MISRA fixes.
  • All LL drivers have been checked for MISRA 2012 compliance, and most warnings have been resolved. The last remaining warnings could be solved by customers if needed.
  • Check the overview and all available LL drivers here: LL drivers.

6.1.3. BSP[edit | edit source]

  • This is a maintenance release of the STM32CubeMP2 package BSP drivers.
  • Refer to the BSP Drivers section here: BSP drivers.
  • BSP has been added for the DK board with STM32MP23x lines More info.png.

6.1.4. CMSIS[edit | edit source]

  • Bit and register definitions for STM32MP25x lines More info.png and STM32MP23x lines More info.png.
  • Support for System, Startup, and Linker files.
  • For more details, refer to CMSIS.

6.1.5. Middleware[edit | edit source]

6.1.6. Projects[edit | edit source]

  • Check project section here Projects for details about implemented projects .

6.2. Main restrictions[edit | edit source]

  • A compilation issue is observed when developing a project using the I3C LL API and any other internal peripheral using the HAL API.
  • There is python package issue observed when using the script to sign the firmware.
    • A Python package issue is observed when using the script to sign the firmware. This issue is resolved by using the following solution available on GitHub : Fix python package issue in signing script. This solution should also be applied on top of the Yocto-based Linux embedded software.

6.3. Released components[edit | edit source]

6.3.1. Drivers[edit | edit source]

Component Version Notes
Cortex®-M CMSIS V5.9.0 -
STM32MP2xx CMSIS V1.1.0 -
STM32MP2xx HAL V1.1.0 -
BSP STM32MP257F_EV1 V1.1.0 -
BSP STM32MP257F_DK V1.1.0 -
BSP STM32MP235F_DK V1.1.0 -

Find here the list of available HAL , LL and BSP drivers.

6.3.2. Middleware[edit | edit source]

Component Version Notes
FreeRTOSTM v10.5.1_231117 -
OpenAMP v2022.10_20230315 -
STM32_USBPD_Library - Core v5.2.0_rc4
STM32_USBPD_Library - Device v1.0.0_rc2


6.3.3. Utilities[edit | edit source]

Component Version Notes
ResourceManager V1.1.0 -

6.4. Released projects[edit | edit source]

The STM32CubeMP2 package comes with a rich set of examples running on STMicroelectronics boards, organized by board and provided with preconfigured projects. The main supported development environment is STM32CubeIDE (works on multiple operating systems) and uses the GNU toolchain.

  • All STM32MP257F-EV1 More info green.png and STM32MP257F-DK More info green.png projects are available with STM32CubeIDE.

Find in this article STM32MP257x Projects, the exhaustive list of available projects for STM32MP257F-EV1 Evaluation board More info green.png, STM32MP257F-DK Discovery kit More info green.png, and STM32MP257F-DK Discovery kit More info green.png for STM32MP23x lines evaluation Info.png

The recommended supported toolchain for STM32MP2 is now STM32CubeIDE (all-in-one multi-OS development tool).

7. How to get started with STM32CubeMP2 Package[edit | edit source]

Refer to How to get software and start with this release article.

8. References[edit | edit source]