This article introduces the structure and the content of the STM32CubeMP15 Package / STM32CubeMP1 Package (a.k.a., STM32CubeMP15 / STM32CubeMP1) , the embedded software part of STM32Cube™, running on the Arm® Cortex®-M4 coprocessor. It references also other interesting wiki articles to better understand and use the STM32CubeMP13 Package.
1. What is the STM32CubeMP15 Package?[edit | edit source]
STM32CubeMP15 Package, running on the Arm® Cortex®-M4 coprocessor, consists of:
- The hardware abstraction layer (HAL), enabling portability between different STM32 devices via standardized API calls
- The low-layer API (LL), a light-weight, optimized, expert oriented set of APIs designed for runtime efficiency and so enhanced performance
- The board support package drivers (BSP), based on HAL drivers, an API set for the evaluation board and third-party components.
- A collection of middleware components (such as FreeRTOS)
- A collection of examples, running on an MPU board and allowing demonstration of a basic implementation of features from a set of IPs
The STM32CubeMP15 Package is based on the STM32CubeMCU Package and has been adapted to a Linux framework (OpenSTLinux).
STM32CubeMP15 Package introduces new components such as OpenAMP and ResourceManager that allow easy communication and resource sharing between main processors running with Linux on Arm® Cortex®-A7, and MCU coprocessors running on Arm® Cortex®-M4.
- OpenAMP is a library implementing the remote processor service framework (RPMsg) which is a virtio-based messaging bus that allows a local processor to communicate with remote processors available on the system.
- ResourceManager is a utility that handles peripheral-accessibility requests and system-resource configuration.
Information |
Note:
|
2. Software architecture overview[edit | edit source]
Software architecture overview is described in STM32CubeMP15 Package architecture.
3. STM32CubeMP15 Package structure[edit | edit source]
This chapter describes the structure of the STM32CubeMP15 Package (drivers, middleware components...).
STM32CubeMP15 Package offers a highly portable Hardware Abstraction Layer (HAL), built around a generic and modular architecture.
This HAL allows the upper layers, middleware and application, to implement functions whatever the STM32MP1 device used. This improves the library code re-usability and guarantees easy portability from one device to another.
STM32CubeMP15 Package also offers a highly portable Low Layer interface (LL), which allows a quick, simple and optimized API to access the STM32MP15 registers.
The STM32CubeMP15 Package is provided with the structure shown below.
4. STM32CubeMP15 Package content[edit | edit source]
This chapter describes the content of the STM32CubeMP15 Package (drivers, middleware components...).
4.1. Drivers[edit | edit source]
The Drivers folder contains all the STM32Cube Drivers, including BSP and HAL drivers.
The STM32CubeMP15 Package provides all driver user manuals:
- The BSP user manual for STM32MP157x-EV1Â Evaluation board is available in Drivers/BSP/STM32MP15xx_EVAL/STM32MP15xx_EVAL_BSP_User_Manual.chm
- The BSP user manual for STM32MP157x-DK2Â Discovery kit is available in Drivers/BSP/STM32MP15xx_DISCO/STM32MP15xx_DISCO_BSP_User_Manual.chm
- The HAL user manual is available in Drivers/STM32MP1xx_HAL_Driver/STM32MP157Cxx_CM4_User_Manual.chm
Chapters, here after, give the list of available BSP, HAL and LL drivers.
4.1.1. HAL drivers[edit | edit source]
STM32CubeMP15 HAL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the Analog to Digital Convertor (ADC) * peripheral: * + Initialization and de-initialization functions * ++ Initialization and Configuration of ADC * + Operation functions * ++ Start, stop, get result of conversions of regular * group, using 3 possible modes: polling, interruption or DMA. * + Control functions * ++ Channels configuration on regular group * ++ Analog Watchdog configuration * + State functions * ++ ADC state machine management * ++ Interrupts and flags management * + Operation functions * ++ Start, stop, get result of conversions of ADC group injected, * using 2 possible modes: polling, interruption. * ++ Calibration * +++ ADC automatic self-calibration * +++ Calibration factors get or set * ++ Multimode feature when available * + Control functions * ++ Channels configuration on ADC group injected * + State functions * ++ ADC group injected contexts queue management |
CEC |
* This driver provides firmware functions to manage the following * functionalities of the High Definition Multimedia Interface * Consumer Electronics Control Peripheral (CEC). * + Initialization and de-initialization function * + IO operation function * + Peripheral Control function |
CRC |
* This driver provides firmware functions to manage the following
* functionalities of the Cyclic Redundancy Check (CRC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Peripheral State functions
* + Extended features functions
|
CORTEX |
* This driver provides firmware functions to manage the following
* functionalities of the CORTEX (MPU, Cache, …):
* + Initialization and de-initialization functions
* + Peripheral Control functions
|
CRYP |
* This driver provides firmware functions to manage the following * functionalities of the Cryptography (CRYP) peripheral: * + Initialization and de-initialization functions * + AES processing functions * + DES processing functions * + TDES processing functions * + DMA callback functions * + CRYP IRQ handler management * + Peripheral State functions * + Extended AES processing functions |
DAC |
* This driver provides firmware functions to manage the following * functionalities of the Digital to Analog Converter (DAC) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions * + Extended features functions |
DCMI |
* This driver provides firmware functions to manage the following * functionalities of the Digital Camera Interface (DCMI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DFSDM |
* This driver provides firmware functions to manage the following * functionalities of the Digital Filter for Sigma-Delta Modulators * (DFSDM) peripherals: * + Initialization and configuration of channels and filters * + Regular channels configuration * + Injected channels configuration * + Regular/Injected Channels DMA Configuration * + Interrupts and flags management * + Analog watchdog feature * + Short-circuit detector feature * + Extremes detector feature * + Clock absence detector feature * + Break generation on analog watchdog or short-circuit event * + Set and get pulses skipping on channel. |
DMA |
* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access (DMA) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and errors functions * + Extended features functions |
EXTI |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (EXTI) peripheral: * + Initialization and de-initialization functions * + IO operation functions |
FDCAN |
* This driver provides firmware functions to manage the following
* functionalities of the Flexible DataRate Controller Area Network
* (FDCAN) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Configuration and Control functions
* + Peripheral State and Error functions
|
FMC_SRAM |
* This driver provides a generic firmware to drive SRAM memories * mounted as external device. |
GPIO |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (GPIO) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Extended Peripheral Control functions |
HAL |
* This driver provides firmware functions to manage the following * functionalities of HAL, Tick, SYSCFG, DBGMCU: * + Initialization and de-initialization functions * + HAL Initialization and de-initialization functions * + Configure the source of the time base * + HAL Control functions * + Tick management (get/set/inc/priority/suspend/resume) * + Get HAL revision, the device revision identifier, the device identifier * + Enable/Disable DBG wake up on AIEC * + Enable/Disable the Debug Module during Domain1 SLEEP mode * + Enable/Disable the Debug Module during Domain1 STOP mode * + Enable/Disable the Debug Module during Domain1 STANDBY mode * + Configure the internal voltage reference buffer voltage scale * + Configure the internal voltage reference buffer high impedance mode * + Tune the Internal Voltage Reference buffer (VREFBUF) * + Enable/Disable the Internal Voltage Reference buffer (VREFBUF) * + Ethernet PHY Interface Selection either MII or RMII * + Analog Switch control for dual analog pads * + Enable/Disable the booster to reduce the total harmonic distortion of the analog * + Enable/Power-down the I/O Compensation Cell * + To Enable/Disable optimize the I/O speed when the product voltage is low * + Code selection for the I/O Compensation cell |
HASH |
* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral: * + Initialization and de-initialization methods * + HASH or HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * + Peripheral State methods * + HASH or HMAC processing suspension/resumption * Additionally, this driver provides functions to manage HMAC * multi-buffer DMA-based processing for MD-5, SHA-1, SHA-224 * and SHA-256. |
HSEM |
* This driver provides firmware functions to manage the following * functionalities of the semaphore peripheral: * + Semaphore Take function (2-Step Procedure) , non blocking * + Semaphore FastTake function (1-Step Procedure) , non blocking * + Semaphore Status check * + Semaphore Clear Key Set and Get * + Release and release all functions * + Semaphore notification enabling and disabling and callnack functions * + IRQ handler management |
I2C |
* This driver provides firmware functions to manage the following
* functionalities of the Inter Integrated Circuit (I2C) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral State and Errors functions
* + Extended features functions
|
IPCC |
* This driver provides firmware functions to manage the following
* functionalities of the Inter-Processor communication controller
* peripherals (IPCC).
* + Initialization and de-initialization functions
* + Configuration, notification and interrupts handling
* + Peripheral State and Error functions
|
LPTIM |
* This driver provides firmware functions to manage the following
* functionalities of the Low Power Timer (LPTIM) peripheral:
* + Initialization and de-initialization functions.
* + Start/Stop operation functions in polling mode.
* + Start/Stop operation functions in interrupt mode.
* + Reading operation functions.
* + Peripheral State functions.
|
MDIOS |
* This driver provides firmware functions to manage the following
* functionalities of the MDIOS Peripheral.
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Control functions
|
MDMA |
* This driver provides firmware functions to manage the following * functionalities of the Master Direct Memory Access (MDMA) peripheral: * + Initialization/de-initialization functions * + I/O operation functions * + Peripheral State and errors functions |
PWR |
* This driver provides firmware functions to manage the following * functionalities of the Power Controller (PWR) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral Extended features functions |
QUADSPI |
* This driver provides firmware functions to manage the following * functionalities of the QuadSPI interface (QSPI). * + Initialization and de-initialization functions * + Indirect functional mode management * + Memory-mapped functional mode management * + Auto-polling functional mode management * + Interrupts and flags management * + MDMA channel configuration for indirect functional mode * + Errors management and abort functionality |
RCC |
* This driver provides firmware functions to manage the following
* functionalities of the Reset and Clock Control (RCC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Extended Peripheral Control functions
|
RNG |
* This driver provides firmware functions to manage the following
* functionalities of the Random Number Generator (RNG) peripheral:
* + Initialization and configuration functions
* + Peripheral Control functions
* + Peripheral State functions
|
RTC |
* This driver provides firmware functions to manage the following * functionalities of the Real-Time Clock (RTC) peripheral: * + Initialization/de-initialization functions * + Calendar (Time and Date) configuration * + Alarms (Alarm A and Alarm B) configuration * + WakeUp Timer configuration * + TimeStamp configuration * + Tampers configuration * + Backup Data Registers configuration * + RTC Tamper and TimeStamp Pins Selection * + Interrupts and flags management |
SAI |
* This driver provides firmware functions to manage the following
* functionalities of the Serial Audio Interface (SAI) peripheral:
* + Initialization/de-initialization functions
* + I/O operation functions
* + Peripheral Control functions
* + Peripheral State functions
* + Modify PDM microphone delays.
|
SD |
* This driver provides firmware functions to manage the following * functionalities of the Secure Digital (SD) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + Extended features functions |
SMARTCARD |
* This driver provides firmware functions to manage the following
* functionalities of the SMARTCARD peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Control functions
* + Peripheral State and Error functions
* + Extended features functions
|
SMBUS |
* This driver provides firmware functions to manage the following * functionalities of the System Management Bus (SMBus) peripheral, * based on I2C principles of operation : * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
SPDIFRX |
* This driver provides firmware functions to manage the following
* functionalities of the SPDIFRX audio interface:
* + Initialization and Configuration
* + Data transfers functions
* + DMA transfers management
* + Interrupts and flags management
|
SPI |
* This driver provides firmware functions to manage the following * functionalities of the Serial Peripheral Interface (SPI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + IO operation functions * + Peripheral Control functions |
TIMER |
* This driver provides firmware functions to manage the following * functionalities of the Timer (TIM) peripheral: * + Time Base Initialization * + Time Base Start * + Time Base Start Interruption * + Time Base Start DMA * + Time Output Compare/PWM Initialization * + Time Output Compare/PWM Channel Configuration * + Time Output Compare/PWM Start * + Time Output Compare/PWM Start Interruption * + Time Output Compare/PWM Start DMA * + Time Input Capture Initialization * + Time Input Capture Channel Configuration * + Time Input Capture Start * + Time Input Capture Start Interruption * + Time Input Capture Start DMA * + Time One Pulse Initialization * + Time One Pulse Channel Configuration * + Time One Pulse Start * + Time Encoder Interface Initialization * + Time Encoder Interface Start * + Time Encoder Interface Start Interruption * + Time Encoder Interface Start DMA * + Commutation Event configuration with Interruption and DMA * + Time OCRef clear configuration * + Time External Clock configuration * + Time Hall Sensor Interface Initialization * + Time Hall Sensor Interface Start * + Time Complementary signal bread and dead time configuration * + Time Master and Slave synchronization configuration * + Time Output Compare/PWM Channel Configuration (for channels 5 and 6) * + Time OCRef clear configuration * + Timer remapping capabilities configuration |
U(S)ART |
* This driver provides firmware functions to manage the following * functionalities of the Universal (Synchronous) Asynchronous Receiver Transmitter * Peripheral (U(S)ART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Peripheral Control functions |
WWDG |
* This driver provides firmware functions to manage the following
* functionalities of the Window Watchdog (WWDG) peripheral:
* + Initialization and Configuration functions
* + IO operation functions
|
4.1.2. LL drivers[edit | edit source]
STM32CubeMP15 LL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the ADC peripheral: * + Initialization/de-initialization functions * + Configuration functions (ADC instance, group regular, group injected, * channels, analog watchdog, oversampling, multimode) * + IT/FLAGS management functions |
BUS |
* This driver provides firmware functions to manage the following * functionalities of the BUS peripheral: * + Enable/disable/reset clocks for all system BUS (AHB2, AHB3, AHB4, AHB5, AHB6, * AXI, MLAHB, APB1, APB2, APB3, APB4, APB5) |
CORTEX |
* This driver contains a set of generic APIs that can be used by user: * + SYSTICK configuration used by @ref LL_mDelay and @ref LL_Init1msTick functions * + Low power mode configuration (SCB register of Cortex®-MCU) * + API to access to MCU info (CPUID register) |
DMA |
* This driver provides firmware functions to manage the following
* functionalities of the DMA peripheral:
* + Initialization/de-initialization functions
* + Configuration functions
* + IT/FLAGS management functions
|
DMAMUX |
* This driver provides firmware functions to manage the following * functionalities of the DMAMUX peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions |
EXTI |
* This driver provides firmware functions to manage the following
* functionalities of the EXTI peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS/Trigger management functions
* + Configuration functions
|
FMC_SRAM |
* This driver provides firmware functions to manage the following * functionalities of the PSRAM peripheral: * + Initialization/de-initialization functions * + Timing management functions * + Configuration functions |
GPIO |
* This driver provides firmware functions to manage the following
* functionalities of the GPIO peripheral:
* + Initialization/de-initialization functions
* + Data access functions
* + Port configuration functions
|
HSEM |
* This driver provides firmware functions to manage the following
* functionalities of the HSEM peripheral:
* + IT/FLAGS management functions
* +Data management functions
|
I2C |
* This driver provides firmware functions to manage the following * functionalities of the I2C peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * +Data management functions * + Configuration functions |
IPCC |
* This driver provides firmware functions to manage the following
* functionalities of the IPCC peripheral:
* + IT/FLAGS management functions
* + Enable/disable transmit and receive channels functions
|
LPTIM |
* This driver provides firmware functions to manage the following * functionalities of the LPTIM peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Configuration (Trigger / Clock / Encoder / LPTIM) functions |
PWR |
* This driver provides firmware functions to manage the following * functionalities of the PWR peripheral: * + Initialization/de-initialization functions * + FLAGS management functions * + Configuration functions |
RCC |
* This driver provides firmware functions to manage the following * functionalities of the RCC peripheral: * + Clocks management functions (HSE/HSI/CSI/LSE/LSI/MCO/PLL) * + RTC/TIMERS functions * + IT/FLAGS management functions * + De-initialization functions * + Get system and peripherals clocks frequency functions |
RTC |
* This driver provides firmware functions to manage the following
* functionalities of the RTC peripheral:
* + Initialization/de-initialization functions
* + TIME/DATE/ALM functions
* + Configuration functions
|
SPI |
* This driver provides firmware functions to manage the following * functionalities of the SPI peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Data / DMA management functions * + Configuration functions |
SYSTEM |
* This driver provides firmware functions to manage the following
* functionalities of the SYSTEM peripheral:
* + SYSCFG and DBGMCU functions
|
TIM |
* This driver provides firmware functions to manage the following * functionalities of the TIM peripheral: * + Initialization/de-initialization functions * + Configuration functions (Time base, Capture Compare, Output and Input Channel, * Timer Synchro, Break, DMA Burst Mode ) * + Counter clock selection functions * + Timer input remapping functions * + IT/FLAGS management functions * + DMA management functions * + Event management functions |
USART |
* This driver provides firmware functions to manage the following * functionalities of the USART peripheral: * + Initialization/de-initialization functions * + Configuration functions (Irda, Smartcard, Half duplex, * SPI Slave, LIN, Driver enable) * + Advanced configurations services functions * + IT/FLAGS management functions * + DMA management functions * + Data management functions * + Execution functions |
UTILS |
* This driver provides firmware functions to manage the following * functionalities of the UTILS peripheral: * + Device Electronic Signature functions * + DELAY functions * + SYSTEM functions |
WWDG |
* This driver provides firmware functions to manage the following * functionalities of the WWDG peripheral: * + Enable / Disable functions * + Configuration functions * + IT/FLAGS management functions |
4.1.3. BSP drivers[edit | edit source]
The BSP drivers offer a set of APIs relative to the hardware components available in the hardware boards (LEDs, Buttons and COM port).
├── STM32MP15xx_DISCO │  ├── bumpversion.cfg │  ├── Release_Notes.html │  ├── STM32MP15xx_DISCO_BSP_User_Manual.chm │  ├── stm32mp15xx_disco_bus.c │  ├── stm32mp15xx_disco_bus.h │  ├── stm32mp15xx_disco.c │  ├── stm32mp15xx_disco_conf_template.h │  ├── stm32mp15xx_disco_errno.h │  ├── stm32mp15xx_disco.h │  ├── stm32mp15xx_disco_stpmic1.c │  └── stm32mp15xx_disco_stpmic1.h └── STM32MP15xx_EVAL │  ├── bumpversion.cfg │  ├── Release_Notes.html │  ├── STM32MP15xx_EVAL_BSP_User_Manual.chm │  ├── stm32mp15xx_eval_bus.c │  ├── stm32mp15xx_eval_bus.h │  ├── stm32mp15xx_eval.c │  ├── stm32mp15xx_eval_conf_template.h │  ├── stm32mp15xx_eval_errno.h │  ├── stm32mp15xx_eval.h │  ├── stm32mp15xx_eval_stpmic1.c │  └── stm32mp15xx_eval_stpmic1.h
4.2. Middlewares[edit | edit source]
The Middlewares folder contains all available STM32Cube Middlewares including:
- FreeRTOS
- OpenAMP
Information |
Note:
|
4.3. Projects[edit | edit source]
The "Projects" folder contains all STM32Cube examples that are classified in 3 levels as described below :
- Level 0Â : Examples. It uses only the HAL drivers without any middleware component. They are available in directory Firmware/Projects/<board_name>/Examples.
- Level 1Â : Applications. It provides typical use cases of each middleware component. They are available in directory Firmware/Projects/<board_name>/Applications.
- Level 2Â : Demonstrations. It involves all the HAL, BSP and middleware components. They are available in directory Firmware/Projects/<board_name>/Demonstrations.
A Template folder is available in Firmware/Projects/<board_name>/Templates and allows quick creation and building of any firmware application on a given board.
All examples respect the same structure :
├── OpenAMP_TTY_echo │  ├── readme.txt describes the example behavior and the setup required to make it work │  ├── Inc contains all header files │  ├── Remoteproc (optional): contains specific files related to the use of Linux® remote processor framework to load STM32Cube Cortex-M4 firmware │  ├── Src contains all the sources code files │  └── STM32CubeIDE contains the preconfigured project for Eclipse IDE
You will find below a list of examples, applications and demonstrations available for STM32MP157C-EV1Â Evaluation board and STM32MP157C-DK2Â Discovery kit :
Find below, the list of available projects for those boards:
Legend:
- (*) : List of STM32MP157C-DK2 and STM32MP157C-EV1 examples available with 3 IDEs ( STM32CubeIDE, IARTM, KEIL®), the others are only available with STM32CubeIDE.
- Examples, applications and demonstrations for STM32MP157C-EV1
├── STM32MP157C-EV1 │  ├── Applications │  │  ├── CoproSync │  │  ├── CoproSync_ShutDown │  │  ├── FreeRTOS │  │  ├── FreeRTOS_ThreadCreation │  │  └── OpenAMP │  │  ├── OpenAMP_Dynamic_ResMgr │  │    ├── OpenAMP_for_signed_fw │  │  ├── OpenAMP_FreeRTOS_echo │  │  ├── OpenAMP_raw │  │  ├── OpenAMP_TTY_echo │  │  └── OpenAMP_TTY_echo_wakeup │  ├── Demonstrations │  │  └── AI_Character_Recognition │  ├── Examples │  │  ├── ADC │  │  │  └── ADC_AnalogWatchdog │  │  │  └── ADC_MultiChannelSingleConversion │  │  │  └── ADC_OverSampler │  │  │  └── ADC_SingleConversion_TriggerTimer_DMA │  │  ├── Cortex │  │  │  └── CORTEXM_MPU │  │  ├── CRC │  │  │  └── CRC_UserDefinedPolynomial │  │  ├── CRYP │  │  │  └── CRYP_AES_DMA │  │  ├── DAC │  │  │  └── DAC_SimpleConversion │  │  ├── DMA │  │  │  └── DMA_FIFOMode │  │  ├── FDCAN │  │  │  └── FDCAN_Loopback │  │  ├── GPIO │  │  │  └── GPIO_EXTI │  │  ├── HASH │  │  │  └── HASH_SHA224SHA256_DMA │  │  ├── I2C │  │  │  ├── I2C_TwoBoards_ComDMA │  │  │  └── I2C_TwoBoards_ComIT │  │  ├── LPTIM │  │  │  └── LPTIM_PulseCounter │  │  │  └── LPTIM_PWM_LSE │  │  ├── PWR │  │  │  └── PWR_STOP_CoPro │  │  ├── QSPI │  │  │  └── QSPI_ReadWrite_IT │  │  ├── SPI │  │  │  ├── SPI_FullDuplex_ComDMA_Master │  │  │  └── SPI_FullDuplex_ComDMA_Slave │  │  ├── TIM │  │  │  └── TIM_DMABurst │  │  │  └── TIM_OnePulse │  │  │  └──TIM_PWMOutput │  │  │  └── TIM_Synchronization │  │  │  └── TIM_TimeBase │  │  ├── UART │  │  │  └── UART_Receive_Transmit_Console │  │  │  └── UART_TwoBoards_ComIT │  │  └── WWDG │  │  └── WWDG_Example
- Examples, applications and demonstrations for STM32MP157C-DK2
├── STM32MP157C-DK2 │  ├── Applications │  │  ├── CoproSync │  │  ├── CoproSync_ShutDown │  │  ├── FreeRTOS │  │  ├── FreeRTOS_ThreadCreation │  │  └── OpenAMP │  │    ├── OpenAMP_for_signed_fw │  │  ├── OpenAMP_FreeRTOS_echo │  │  ├── OpenAMP_raw │  │  ├── OpenAMP_TTY_echo │  │  └── OpenAMP_TTY_echo_wakeup │  ├── Demonstrations │  │  └── AI_Character_Recognition │  ├── Examples │  │  ├── ADC │  │  │  └── ADC_SingleConversion_TriggerTimer_DMA │  │  ├── Cortex │  │  │  └── CORTEXM_MPU │  │  ├── CRC │  │  │  └── CRC_UserDefinedPolynomial │  │  ├── CRYP │  │  │  └── CRYP_AES_DMA │  │  ├── DMA │  │  │  └── DMA_FIFOMode │  │  ├── FDCAN │  │  │  └── FDCAN_Loopback │  │  ├── GPIO │  │  │  └── GPIO_EXTI │  │  ├── HASH │  │  │  └── HASH_SHA224SHA256_DMA │  │  ├── I2C │  │  │  └── I2C_TwoBoards_ComIT │  │  ├── LPTIM │  │  │  └── LPTIM_PulseCounter │  │  ├── PWR │  │  │  └── PWR_STOP_CoPro │  │  ├── SPI │  │  │  ├── SPI_FullDuplex_ComDMA_Master │  │  │  ├── SPI_FullDuplex_ComDMA_Slave │  │  │  ├── SPI_FullDuplex_ComIT_Master │  │  │  └── SPI_FullDuplex_ComIT_Slave │  │  ├── TIM │  │  │  └── TIM_DMABurst │  │  ├── UART │  │  │  └── UART_Receive_Transmit_Console │  │  │  ├── UART_TwoBoards_ComDMA │  │  │  └── UART_TwoBoards_ComIT │  │  └── WWDG │  │  └── WWDG_Example
5. Get started with STM32CubeMP15 Package[edit | edit source]
The STM32CubeMP15 Package is available through the three packages (starter, developer, and distribution). To know how to get them, read STM32CubeMP15_Package_-_Getting_started article.