Registered User mNo edit summary |
Registered User m (https://wiki.st.com/stm32mp25-beta-v4.1/wiki/U-Boot) |
||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | ||
}}</noinclude> | }}</noinclude> | ||
Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the | Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the | ||
Line 20: | Line 20: | ||
|- | |- | ||
| {{MicroprocessorDevice | device=15}}|| [[STM32MP15 U-Boot]] | | {{MicroprocessorDevice | device=15}}|| [[STM32MP15 U-Boot]] | ||
|- | |||
| {{MicroprocessorDevice | device=25}}|| [[STM32MP25 U-Boot]] | |||
|} | |} | ||
Revision as of 14:59, 12 July 2023
Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the platform and load the Linux® kernel.
See U-Boot overview for generic information.
Information about U-Boot depends on the microprocessor device.
Several articles have been created to manage STM32 MPU diversity and provide the relevant level of information. Browse the one corresponding to the STM32 MPU you use.
STM32 MPU devices | Associated articles |
---|---|
STM32MP13x lines | STM32MP13 U-Boot |
STM32MP15x lines | STM32MP15 U-Boot |
STM32MP25x lines | STM32MP25 U-Boot |