Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 4: | Line 4: | ||
}}</noinclude> | }}</noinclude> | ||
==Starting, stopping and restarting Weston== | ==Starting, stopping and restarting Weston== | ||
Weston has its own '''systemd''' service (/lib/systemd/system/weston.service) to easily start, stop and restart Weston. | Weston has its own '''systemd''' service (/lib/systemd/system/weston-launch.service) to easily start, stop and restart Weston. | ||
The following command stops the Weston service: | The following command stops the Weston service: | ||
{{board$}} systemctl stop weston | {{board$}} systemctl stop weston-launch | ||
The following command starts the Weston service: | The following command starts the Weston service: | ||
{{board$}} systemctl start weston | {{board$}} systemctl start weston-launch | ||
The following command stops and then restarts the Weston service: | The following command stops and then restarts the Weston service: | ||
{{board$}} systemctl restart weston | {{board$}} systemctl restart weston-launch | ||
==Preventing Weston from automatically starting on boot== | ==Preventing Weston from automatically starting on boot== | ||
Line 24: | Line 24: | ||
To re-enable this service, rename this file according to the udev rules of your system. | To re-enable this service, rename this file according to the udev rules of your system. | ||
=== Weston service with systemd | === Weston service with systemd === | ||
During the development process, when udev rules are not fully configured, the Weston service can be automatically started on boot as specified in '''/lib/systemd/system/weston*'''. | During the development process, when udev rules are not fully configured, the Weston service can be automatically started on boot as specified in '''/lib/systemd/system/weston*'''. | ||
In this case, the following command disables the automatic start of the Weston service: | In this case, the following command disables the automatic start of the Weston service: | ||
{{board$}} systemctl disable weston | {{board$}} systemctl disable weston-launch | ||
The following command enables the automatic start of the Weston service: | |||
{{board$}} systemctl enable weston | {{board$}} systemctl enable weston-launch | ||
Depending on your systemd configuration, it may be required to mask/unmask the Weston service with the following commands: | |||
{{board$}} systemctl mask weston-launch | |||
{{board$}} systemctl unmask weston-launch | |||
You can check the status of the Weston service with the following command: | |||
{{board$}} systemctl list-unit-files | grep -i weston | |||
Please refer to the '''systemctl manpage'''<ref name="systemctl">[https://www.freedesktop.org/software/systemd/man/systemctl.html systemctl man page]</ref> to know more about it. | |||
== References == | |||
<references /> | |||
<noinclude> | <noinclude> |
Revision as of 14:28, 9 June 2022
1. Starting, stopping and restarting Weston
Weston has its own systemd service (/lib/systemd/system/weston-launch.service) to easily start, stop and restart Weston.
The following command stops the Weston service:
systemctl stop weston-launch
The following command starts the Weston service:
systemctl start weston-launch
The following command stops and then restarts the Weston service:
systemctl restart weston-launch
2. Preventing Weston from automatically starting on boot
2.1. Weston service with udev rules
The Weston service is automatically started on boot thanks to an udev rules file, most of the time located in /etc/udev/rules.d/*weston*, for instance /etc/udev/rules.d/71-weston-drm.rules.
To disable this service, rename this file (by changing its extension for instance), then restart your board.
To re-enable this service, rename this file according to the udev rules of your system.
2.2. Weston service with systemd
During the development process, when udev rules are not fully configured, the Weston service can be automatically started on boot as specified in /lib/systemd/system/weston*.
In this case, the following command disables the automatic start of the Weston service:
systemctl disable weston-launch
The following command enables the automatic start of the Weston service:
systemctl enable weston-launch
Depending on your systemd configuration, it may be required to mask/unmask the Weston service with the following commands:
systemctl mask weston-launch
systemctl unmask weston-launch
You can check the status of the Weston service with the following command:
systemctl list-unit-files | grep -i weston
Please refer to the systemctl manpage[1] to know more about it.
3. References