Last edited 3 months ago

STM32MP15 OTP mapping: Difference between revisions


Latest revision as of 17:33, 10 December 2024


1. Memory mapping

The table below gives an overview of the BSEC OTP memory mapping with useful information in the context of this Wiki reading.
OTP words 0 to 31 are called lower OTP and words 32 to 95 are called upper OTP.
Further information for the words and fields that are not explicitly described here can be found in the reference manual.

OTP word Bit field (size) Name Description
0 31-7 (25 bits) reserved
6 (1 bit) is closed
5-0 (6 bits) reserved
1-2 - - See the reference manual
3 31-30 (2 bits) HSE value
29-27 (3 bits) primary boot source
26-24 (3 bits) secondary boot source
23-16 (8 bits) boot source disable If it is different from zero, each bit disables a boot source.
15 (1 bit) data cache disabling
14-7 (8 bits) UART instances boot source disabling If it is different from zero, then each bit disables an UART instance.
6 (1 bit) USB DP pullup disabling
5 (1 bit) PLL disabling
4-3 (2 bits) SD card memory interface
2-1 (2 bits) e•MMC™ memory interface
0 (1 bit) QSPI non default AFmux
4 31-0 (32 bits) monotonic counter This is an anti rollback monotonic counter. On closed devices, the ROM code checks if it is less or equal to the version stored in the loaded image header.
5-7 31-28 (4 bits) AFmux configuration - port1[3:0] Bank id
27-24 (4 bits) AFmux configuration - pin1[3:0] Pin id
23-20 (4 bits) AFmux configuration - afmux1[3:0] AFmux value
19-16 (4 bits) AFmux configuration - mode1[3:0] Pin mode
15-12 (4 bits) AFmux configuration - port0[3:0] Bank id
11-8 (4 bits) AFmux configuration - pin0[3:0] Pin id
7-4 (4 bits) AFmux configuration - afmux0[3:0] AFmux value
3-0 (4 bits) AFmux configuration - mode0[3:0] Pin mode
8 31-10 (22 bits) reserved
9 (1 bit) SSP success
8 (1 bit) SSP request
7-0 (8 bits) reserved
9 31 (1 bit) nand param stored in otp FMC NAND parameters storage flag

Notes:

  • serial NAND parameters must always be stored in OTP. This bit shall be set to 1 for serial NAND.
30-29 (2 bits) nand page size[1:0] FMC or serial NAND page size
28-27 (2 bits) nand block size[1:0] FMC or serial NAND block size
26-19 (8 bits) nand block nb[7:0] FMC or serial NAND number of blocks in unit of 256 blocks (nb blocks = N * 256)
18 (1 bit) fmc nand width FMC NAND width
17-15 (3 bits) fmc ecc bit nb[2:0] FMC NAND number of ECC bits
14 (1 bit) spinand needs plane select Serial NAND needs plane select.
13-5 (9 bits) reserved
4 (1 bit) eMMC 128KB boot partition support
3 (1 bit) disable ddr power optim Disable DDR PLL switch off sequence
2 (1 bit) disable HSE bypass detection
1 (1 bit) disable HSE frequency autodetection
0 (1 bit) disable ROM code traces
10-23 - - See the reference manual.
24 31-0 (32 bits) PKH1 The Public Key Hash (PKH) is the SHA256 hash of ECDSA public key used for the Secure boot.

If hash = 01 02 03 04 05 06 07 08… then PKH1 = 0x01020304, PKH2 = 0x05060708, etc,…

25 31-0 (32 bits) PKH2
26 31-0 (32 bits) PKH3
27 31-0 (32 bits) PKH4
28 31-0 (32 bits) PKH5
29 31-0 (32 bits) PKH6
30 31-0 (32 bits) PKH7
31 31-0 (32 bits) PKH8
32-55 - - See the reference manual.
56 31-30 (2 bits) reserved
29-15 (15 bits) rma relock passwd A password is required for RMA relock request.
14-0 (15 bits) rma unlock passwd A password is required for RMA unlock request.
57 31-0 mac[4 first octets] ETH MAC address for STMicroelectronics boards
58 15-0 mac[2 last octets]
59-95 - - See the reference manual.