Registered User mNo edit summary Tag: 2017 source edit |
Registered User m (Text replacement - "arch/arm/boot/dts/stm32" to "arch/arm/boot/dts/st/stm32") |
||
Line 79: | Line 79: | ||
====adv7533 device tree example==== | ====adv7533 device tree example==== | ||
<div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | <div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | ||
Devicetree example with the B-LCDAD-HDMI1<ref name="B-LCDAD-HDMI1"/> board connected to the [[STM32MP157x-EV1_-_hardware_description | STM32MP157 evaluation board]]: {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c-ev1.dts}} | Devicetree example with the B-LCDAD-HDMI1<ref name="B-LCDAD-HDMI1"/> board connected to the [[STM32MP157x-EV1_-_hardware_description | STM32MP157 evaluation board]]: {{CodeSource | Linux kernel | arch/arm/boot/dts/st/stm32mp157c-ev1.dts}} | ||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
<syntaxhighlight lang="dts"> | <syntaxhighlight lang="dts"> | ||
Line 287: | Line 287: | ||
<div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | <div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | ||
Devicetree example: {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xx-dkx.dtsi}} | Devicetree example: {{CodeSource | Linux kernel | arch/arm/boot/dts/st/stm32mp15xx-dkx.dtsi}} | ||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
<syntaxhighlight lang="dts"> | <syntaxhighlight lang="dts"> | ||
Line 352: | Line 352: | ||
<div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | <div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | ||
Devicetree pin control bindings example: {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15-pinctrl.dtsi}} | Devicetree pin control bindings example: {{CodeSource | Linux kernel | arch/arm/boot/dts/st/stm32mp15-pinctrl.dtsi}} | ||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
<syntaxhighlight lang="dts"> | <syntaxhighlight lang="dts"> | ||
Line 464: | Line 464: | ||
<div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | <div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | ||
Devicetree example: {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xx-dhcor-avenger96.dtsi}} | Devicetree example: {{CodeSource | Linux kernel | arch/arm/boot/dts/st/stm32mp15xx-dhcor-avenger96.dtsi}} | ||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
<syntaxhighlight lang="dts"> | <syntaxhighlight lang="dts"> | ||
Line 561: | Line 561: | ||
<div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | <div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | ||
Devicetree pin control bindings example: {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15-pinctrl.dtsi}} | Devicetree pin control bindings example: {{CodeSource | Linux kernel | arch/arm/boot/dts/st/stm32mp15-pinctrl.dtsi}} | ||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
<syntaxhighlight lang="dts"> | <syntaxhighlight lang="dts"> |
Latest revision as of 13:48, 8 October 2024
1. Article purpose
The purpose of this article is to:
- List the display bridge hardware components that might be integrated in the different boards.
- Link these components to the corresponding software framework(s).
- Point to the appropriate component datasheets.
- Explain, when necessary, how to configure these components.
![]() |
Some of these hardware components are part of the accessories for STM32 boards like the B-LCDAD-HDMI1 for instance. |
2. Software frameworks
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Visual | Analog Devices adv7533 & adv7535 | DRM/KMS framework | MIPI® DSI to HDMI transmitter | ||
Visual | Silab sil9022 | DRM/KMS framework | Parallel RGB (DPI) to HDMI transmitter | ||
Visual | Toshiba tc358762 | DRM/KMS framework | MIPI® DSI to Parallel RGB (DPI) | ||
Visual | Analog Devices adv7513 | DRM/KMS framework | Parallel RGB (DPI) to HDMI transmitter |
3. Analog Devices adv7533 & adv7535
The adv7533 and adv7535 (adv753x) DSI to HDMI transmitter support the HDMI® Specification on a wide range of mobile products.
For details and the datasheet please contact the adv753x HDMI transmitter provider.
The adv753x transmitter does not support DSI burst mode. Check the pixel clock constraints in non-burst mode.
![]() |
The adv7533 HDMI transmitter can be found on the adapter board B-LCDAD-HDMI1[1]. It is compatible with the STM32MP157 evaluation boards and can be plugged in place of the display. But note that:
|
![]() |
The adv7535 HDMI transmitter can be found on: |
3.3. Linux driver
Bindings: Documentation/devicetree/bindings/display/bridge/adi,adv7533.yaml (for both adv7533 & adv7535)
Sources: drivers/gpu/drm/bridge/adv7511/
Configuration:
- DRM_I2C_ADV7511
- DRM_I2C_ADV7511_AUDIO
- DRM_I2C_ADV7511_CEC
3.3.1. adv7533 device tree example
Devicetree example with the B-LCDAD-HDMI1[1] board connected to the STM32MP157 evaluation board: arch/arm/boot/dts/st/stm32mp157c-ev1.dts
3.3.2. adv7535 device tree example
Devicetree example based on STM32MP25 Discovery kit: arch/arm64/boot/dts/st/stm32mp257f-dk.dts
4. Silab sil9022
The SiI9022A HDMI transmitter supports the HDMI® Specification on a wide range of mobile products.
For details and the datasheet please contact the SiI9022A HDMI transmitter provider.
![]() |
This HDMI transmitter can be found on some STM32MP1 Discovery kits. |
4.1. Linux driver
Bindings: Documentation/devicetree/bindings/display/bridge/sil,sii9022.yaml
Sources: drivers/gpu/drm/bridge/sii902x.c
Configuration: DRM_SII902X
Devicetree example: arch/arm/boot/dts/st/stm32mp15xx-dkx.dtsi
Devicetree pin control bindings example: arch/arm/boot/dts/st/stm32mp15-pinctrl.dtsi
5. Toshiba tc358762
The tc358762 is a DSI de-serializer to parallel DPI or DBI. Only DPI output is supported in current Linux driver.
For details and the datasheet please contact the tc358762 device provider.
5.1. Linux driver
Bindings: Documentation/devicetree/bindings/display/bridge/toshiba,tc358762.yaml
Sources: drivers/gpu/drm/bridge/tc358762.c
Configuration:
- DRM_TOSHIBA_TC358762
Devicetree example: check the complete example for the Raspberry Pi 7" Touch Display.
6. Analog Devices adv7513
The Analog Devices adv7513 Parallel RGB (DPI) to HDMI transmitter supports the HDMI® Specification on a wide range of mobile products.
For details and the datasheet please contact the adv7513 HDMI transmitter provider.
![]() |
This HDMI transmitter can be found on some dh-electronics AVENGER 96Boards compliant consumer edition boards. |
6.1. Linux driver
Bindings: Documentation/devicetree/bindings/display/bridge/adi,adv7511.yaml
Sources: drivers/gpu/drm/bridge/adv7511
Configuration:
- DRM_I2C_ADV7511
- DRM_I2C_ADV7511_AUDIO
- DRM_I2C_ADV7511_CEC
Devicetree example: arch/arm/boot/dts/st/stm32mp15xx-dhcor-avenger96.dtsi
Devicetree pin control bindings example: arch/arm/boot/dts/st/stm32mp15-pinctrl.dtsi
7. References