Last edited one month ago

STM32MP15 V4L2 camera overview: Difference between revisions


Revision as of 15:53, 24 October 2023


This article gives information about the Linux® V4L2 camera framework.

1. Framework purpose[edit | edit source]

The V4L2 Linux kernel framework[1] allows to control both an external camera sensor and the camera interface in order to capture raw frames in various pixel formats or encoded stream data such as JPEG.

This could be typically used, with the help of other Linux multimedia frameworks and applications, to take snapshot, to make preview, to make a video recording or even remotely stream images from the camera sensor.

2. System overview[edit | edit source]

CAMERAOverview.png

2.1. Component description[edit | edit source]

  • Application (User space)

Any application relying on V4L2 Linux kernel interface or libv4l abstraction layer. GStreamer framework provides such application.

  • V4L2 utilities (User space)

A set of tools to test, configure and use the whole camera subsystem, including the external camera sensor and the camera interface. V4l2-ctl is one of the most usefull utility.

  • V4L2 libraries (libv4l) (User space)

A set of libraries on top of the V4L2 Linux kernel interface which abstract the kernel interface in order to simplify, keep compatibility or add some hooks between V4L-based applications and the V4L2 kernel interface.

  • yavta (User space)

Yavta is a test tool which relies on the V4L2 Linux kernel interface.

  • V4L2 core (Kernel space)

This layer represents the standard Linux kernel V4L2 Framework.

  • stm32-dcmi (Kernel space)

This V4L2 DCMI Linux device driver handles the DCMI hardware block.

  • Camera sensor X driver (Kernel space)

This V4L2 Linux device driver handles the camera sensor X external peripheral, handles some GPIOs lines and potentially power supplies to power-up/down the camera sensor. The communication with camera sensor is done through the i2c bus.

  • DCMI (Hardware)

The Digital Camera Memory Interface hardware block.

  • Camera sensor X (Hardware)

The camera sensor external peripheral.

2.2. APIs description[edit | edit source]

The V4L2 userland API is documented in the Linux Media subsystem documentation[2]

The V4L2 kernel framework internal API is documented in the V4L2 Kernel Support section of the Linux Kernel documentation[3]

3. Configuration[edit | edit source]

3.1. Kernel configuration[edit | edit source]

The STM32 camera interface and OV5640 camera sensor are enabled by default in STMicroelectronics deliveries.

Nevertheless this is not the case when using upstream kernel version. In this case, the DCMI V4L2 driver can be enabled using Linux kernel menuconfig tool:

[*] Device Drivers --->
    [*] Multimedia support --->
        [*] V4L platform devices  ---> 
            [*] STM32 Digital Camera Memory Interface (DCMI) support

The external camera sensor connected to the camera interface must also be enabled, here is an example with the OV5640 Omnivision camera sensor located on the MB1379 camera daughter board[4] connected to the CN7 camera connector[5] of the STM32MP15 evaluation board[6]:

[*] Device Drivers --->
    [*] Multimedia support --->
        I2C Encoders, decoders, sensors and other helper chips  ---> 
            [*] OmniVision OV5640 sensor support

3.2. Device tree configuration[edit | edit source]

Refer to DCMI device tree configuration article for a complete view of DCMI & sensor configuration thanks to Linux kernel device tree mechanism.

4. How to use the framework[edit | edit source]

The use cases described here are enabled using V4l2-ctl, gst-launch or gst-play command line utilities.

4.1. List the video devices and their capabilities[edit | edit source]

List all the available video devices using --list-devices option:

 v4l2-ctl --list-devices
STM32 Camera Memory Interface (platform:dcmi):
        /dev/video0

If several devices are available, use -d option after any V4l2-ctl commands to target a specific device. If -d option is not specified, /dev/video0 is targeted by default.

In order to have information on a specific device, use -D option:

 v4l2-ctl -d /dev/video0 -D
Driver Info (not using libv4l2):
        Driver name   : stm32-dcmi
        Card type     : STM32 Camera Memory Interface
        Bus info      : platform:dcmi
        Driver version: X.Y.Z
        Capabilities  : 0x85200001
                Video Capture
                Read/Write
                Streaming
                Extended Pix Format
                Device Capabilities
        Device Caps   : 0x05200001
                Video Capture
                Read/Write
                Streaming
                Extended Pix Format



4.2. Controlling camera[edit | edit source]

Use V4l2-ctl with -L option to get the list of supported controls:

 v4l2-ctl -L
User Controls

                       contrast (int)    : min=0 max=255 step=1 default=0 value=0 flags=slider
                     saturation (int)    : min=0 max=255 step=1 default=64 value=64 flags=slider
                            hue (int)    : min=0 max=359 step=1 default=0 value=0 flags=slider
        white_balance_automatic (bool)   : default=1 value=1 flags=update
                    red_balance (int)    : min=0 max=4095 step=1 default=0 value=128 flags=inactive, slider
                   blue_balance (int)    : min=0 max=4095 step=1 default=0 value=128 flags=inactive, slider
                       exposure (int)    : min=0 max=65535 step=1 default=0 value=885 flags=inactive, volatile
                 gain_automatic (bool)   : default=1 value=1 flags=update
                           gain (int)    : min=0 max=1023 step=1 default=0 value=32 flags=inactive, volatile
                horizontal_flip (bool)   : default=0 value=0
                  vertical_flip (bool)   : default=0 value=0

Camera Controls

                  auto_exposure (menu)   : min=0 max=1 default=0 value=0 flags=update
                                0: Auto Mode
                                1: Manual Mode

Image Processing Controls

                   test_pattern (menu)   : min=0 max=1 default=0 value=0
                                0: Disabled
                                1: Color bars

The control value can be changed thanks to --set-ctrl option, for example:

 v4l2-ctl --set-ctrl test_pattern=1

The control value can be changed dynamically. In the following example, the color bar is enabled/disabled while preview is running:

  • Start preview in background
 gst-launch-1.0 v4l2src ! "video/x-raw, width=1280, height=720, framerate=(fraction)15/1" ! queue ! autovideosink -e &
  • Then alternate the color bar activation or not
 v4l2-ctl --set-ctrl test_pattern=1;sleep 1;v4l2-ctl --set-ctrl test_pattern=0;sleep 1;v4l2-ctl --set-ctrl test_pattern=1;sleep 1;v4l2-ctl --set-ctrl test_pattern=0;killall gst-launch-1.0
  • Horizontal/vertical flip can also be changed while preview is running:
 v4l2-ctl --set-ctrl horizontal_flip=1;sleep 2;v4l2-ctl --set-ctrl horizontal_flip=0;sleep 2;v4l2-ctl --set-ctrl vertical_flip=1;sleep 2;v4l2-ctl --set-ctrl vertical_flip=0;killall gst-launch-1.0


4.3. Set the pixel format, resolution and framerate[edit | edit source]

Use --list-formats-ext option to get the supported pixel format, resolution and framerate:

 v4l2-ctl --list-formats-ext
ioctl: VIDIOC_ENUM_FMT
        Index       : 0
        Type        : Video Capture
        Pixel Format: 'JPEG' (compressed)
        Name        : JFIF JPEG
                Size: Discrete 176x144
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 320x240
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 640x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x576
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1024x768
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1280x720
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1920x1080
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 2592x1944
                        Interval: Discrete 0.067s (15.000 fps)

        Index       : 1
        Type        : Video Capture
        Pixel Format: 'UYVY'
        Name        : UYVY 4:2:2
                Size: Discrete 176x144
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 320x240
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 640x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x576
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1024x768
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1280x720
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1920x1080
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 2592x1944
                        Interval: Discrete 0.067s (15.000 fps)

        Index       : 2
        Type        : Video Capture
        Pixel Format: 'YUYV'
        Name        : YUYV 4:2:2
                Size: Discrete 176x144
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 320x240
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 640x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x576
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1024x768
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1280x720
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1920x1080
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 2592x1944
                        Interval: Discrete 0.067s (15.000 fps)

        Index       : 3
        Type        : Video Capture
        Pixel Format: 'RGBP'
        Name        : 16-bit RGB 5-6-5
                Size: Discrete 176x144
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 320x240
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 640x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x480
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 720x576
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1024x768
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1280x720
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 1920x1080
                        Interval: Discrete 0.067s (15.000 fps)
                        Interval: Discrete 0.033s (30.000 fps)
                Size: Discrete 2592x1944
                        Interval: Discrete 0.067s (15.000 fps)

In order to change the camera configuration, select first the framerate using --set-parm option:

 v4l2-ctl --set-parm=30

Then select the wanted resolution and/or pixel format using --set-fmt-video option:

 v4l2-ctl --set-fmt-video=width=320,height=240,pixelformat=RGBP

4.4. Set the framerate[edit | edit source]

  • With V4l2-ctl, use --set-parm option giving the framerate numerator only, the denominator is fixed to 1 (only integer framerate values are allowed):
 v4l2-ctl --set-parm=<framerate numerator>

Take 100 VGA pictures at 30fps:

 v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=100 --stream-to=pics@30fps.jpeg

Replay at 30fps using gst-play:

 gst-play-1.0 pics@30fps.jpeg --videosink="videorate ! video/x-raw, framerate=(fraction)30/1 ! autovideosink" 

Take 100 VGA pictures at 15fps:

 v4l2-ctl --set-parm=15;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=100 --stream-to=pics@15fps.jpeg

Replay at 15fps using gst-play:

 gst-play-1.0 pics@15fps.jpeg --videosink="videorate ! video/x-raw, framerate=(fraction)15/1 ! autovideosink" 


 gst-launch-1.0 v4l2src ! "video/x-raw, ... framerate=(fraction)<numerator>/<denominator>" ! ...

Preview VGA@30fps

 gst-launch-1.0 v4l2src ! "video/x-raw, width=640, height=480, framerate=(fraction)30/1" ! queue ! autovideosink -e

Preview VGA@15fps

 gst-launch-1.0 v4l2src ! "video/x-raw, width=640, height=480, framerate=(fraction)15/1" ! queue ! autovideosink -e

4.5. Grab a raw frame[edit | edit source]

Capture a QVGA RGB565 raw frame on disk:

 v4l2-ctl --set-fmt-video=width=320,height=240,pixelformat=RGBP --stream-mmap --stream-count=1 --stream-to=grab-320x240-rgb565.raw

In order to display it, this raw frame must be converted first to JPEG:

 gst-launch-1.0 filesrc location= grab-320x240-rgb565.raw blocksize=153600 ! "video/x-raw, format=(string)RGB16, width=(int)320, height=(int)240, framerate=(fraction)30/1" ! videoconvert ! jpegenc ! filesink location=grab-320x240-rgb565.jpeg

Then weston-image utility can be used to display this JPEG file:

 weston-image grab-320x240-rgb565.jpeg

4.6. Fullscreen preview[edit | edit source]

 gst-launch-1.0 v4l2src ! "video/x-raw, width=1280, height=720, framerate=(fraction)15/1" ! queue ! autovideosink -e

4.7. Take a picture[edit | edit source]

Capture a 5Mp JPEG:

 v4l2-ctl --set-parm=15; v4l2-ctl --set-fmt-video=width=2592,height=1944,pixelformat=JPEG --stream-mmap --stream-count=1 --stream-skip=3 --stream-to=pic-5Mp.jpeg; v4l2-ctl --set-parm=30

Then display it:

 weston-image pic-5Mp.jpeg

You can check the picture resolution using gst-typefind:

 gst-typefind-1.0 pic-5Mp.jpeg
pic-5Mp.jpeg - image/jpeg, width=(int)2592, height=(int)1944, sof-marker=(int)0

4.8. Pictures streaming over network[edit | edit source]

Refer to How to stream camera over network article to get some examples on how to stream camera content over network.

5. How to trace and debug[edit | edit source]

5.1. How to monitor[edit | edit source]

5.1.1. Check of devicetree configuration[edit | edit source]

Here are some commands to verify that DCMI is enabled, check which camera sensor is used and log other details about devicetree settings:

 rm devicetree.txt
 echo "[devicetree]" >> devicetree.txt
 echo "|-[dcmi]" >> devicetree.txt
 find /proc/device-tree/soc | grep dcmi | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt
 echo "|" >> devicetree.txt
 echo "|-[camera:" | tr -d "\n" >> devicetree.txt
 cat /proc/device-tree/soc/i2c*/camera*/compatible >> devicetree.txt
 echo "]" >> devicetree.txt
 find /proc/device-tree/soc | grep camera | sed 's/\/proc\/device-tree\/soc\//  |-/' >> devicetree.txt
 echo "" >> devicetree.txt
 cat devicetree.txt
[devicetree]
|-[dcmi]
| |-dcmi@4c006000
| |-dcmi@4c006000/compatible
| |-dcmi@4c006000/clocks
| |-dcmi@4c006000/resets
| |-dcmi@4c006000/pinctrl-1
| |-dcmi@4c006000/port
| |-dcmi@4c006000/port/endpoint
| |-dcmi@4c006000/port/endpoint/hsync-active
| |-dcmi@4c006000/port/endpoint/vsync-active
| |-dcmi@4c006000/port/endpoint/remote-endpoint
| |-dcmi@4c006000/port/endpoint/bus-width
| |-dcmi@4c006000/port/endpoint/pclk-sample
| |-dcmi@4c006000/port/endpoint/phandle
| |-dcmi@4c006000/port/endpoint/linux,phandle
| |-dcmi@4c006000/port/endpoint/name
| |-dcmi@4c006000/port/name
| |-dcmi@4c006000/clock-names
| |-dcmi@4c006000/status
| |-dcmi@4c006000/interrupts
| |-dcmi@4c006000/dma-names
| |-dcmi@4c006000/phandle
| |-dcmi@4c006000/reg
| |-dcmi@4c006000/pinctrl-0
| |-dcmi@4c006000/dmas
| |-dcmi@4c006000/linux,phandle
| |-dcmi@4c006000/name
| |-dcmi@4c006000/pinctrl-names
| |-pin-controller/dcmi-sleep@0
| |-pin-controller/dcmi-sleep@0/pins
| |-pin-controller/dcmi-sleep@0/pins/pinmux
| |-pin-controller/dcmi-sleep@0/pins/name
| |-pin-controller/dcmi-sleep@0/phandle
| |-pin-controller/dcmi-sleep@0/linux,phandle
| |-pin-controller/dcmi-sleep@0/name
| |-pin-controller/dcmi@0
| |-pin-controller/dcmi@0/pins
| |-pin-controller/dcmi@0/pins/pinmux
| |-pin-controller/dcmi@0/pins/bias-disable
| |-pin-controller/dcmi@0/pins/name
| |-pin-controller/dcmi@0/phandle
| |-pin-controller/dcmi@0/linux,phandle
| |-pin-controller/dcmi@0/name
|
|-[camera:ovti,ov5640]
  |-i2c@40013000/camera@3c
  |-i2c@40013000/camera@3c/compatible
  |-i2c@40013000/camera@3c/powerdown-gpios
  |-i2c@40013000/camera@3c/DOVDD-supply
  |-i2c@40013000/camera@3c/clocks
  |-i2c@40013000/camera@3c/rotation
  |-i2c@40013000/camera@3c/port
  |-i2c@40013000/camera@3c/port/endpoint
  |-i2c@40013000/camera@3c/port/endpoint/hsync-active
  |-i2c@40013000/camera@3c/port/endpoint/vsync-active
  |-i2c@40013000/camera@3c/port/endpoint/remote-endpoint
  |-i2c@40013000/camera@3c/port/endpoint/bus-width
  |-i2c@40013000/camera@3c/port/endpoint/pclk-sample
  |-i2c@40013000/camera@3c/port/endpoint/phandle
  |-i2c@40013000/camera@3c/port/endpoint/data-shift
  |-i2c@40013000/camera@3c/port/endpoint/linux,phandle
  |-i2c@40013000/camera@3c/port/endpoint/name
  |-i2c@40013000/camera@3c/port/name
  |-i2c@40013000/camera@3c/clock-names
  |-i2c@40013000/camera@3c/status
  |-i2c@40013000/camera@3c/reset-gpios
  |-i2c@40013000/camera@3c/phandle
  |-i2c@40013000/camera@3c/reg
  |-i2c@40013000/camera@3c/linux,phandle
  |-i2c@40013000/camera@3c/name

5.2. How to trace[edit | edit source]

5.2.1. V4L2 userland API tracing[edit | edit source]

Tracing of V4L2 userland API[2] can be enabled using command:

 echo 0x3 >  /sys/devices/platform/soc/*.dcmi/video4linux/video*/dev_debug 

Traces are output in kernel log buffer:

 dmesg
[10130.641469] video0: VIDIOC_TRY_FMT: type=vid-cap, width=640, height=480, pixelformat=YUYV, field=none, bytesperline=
1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_func=2
[10130.641550] video0: VIDIOC_S_FMT: type=vid-cap, width=640, height=480, pixelformat=YUYV, field=none, bytesperline=12
80, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_func=2
[10130.641597] video0: VIDIOC_G_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode
=0, readbuffers=2
[10130.641638] video0: VIDIOC_G_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode
=0, readbuffers=2
[10130.641681] video0: VIDIOC_S_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode
=0, readbuffers=2
[10130.641740] video0: VIDIOC_G_CTRL: error -22: id=0x980927, value=0
[10130.642770] video0: VIDIOC_REQBUFS: count=0, type=vid-cap, memory=mmap
[10130.642819] video0: VIDIOC_CREATE_BUFS: index=0, count=0, memory=mmap, type=vid-cap, width=640, height=480, pixelfor
mat=YUYV, field=none, bytesperline=1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_f
unc=2
[10130.658541] video0: VIDIOC_G_CTRL: error -22: id=0x980927, value=0
[10130.662770] video0: VIDIOC_REQBUFS: count=3, type=vid-cap, memory=mmap
[10130.662852] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=0, type=vid-cap, flags=0x00002000, field=any, sequence=
0, memory=mmap, bytesused=0, offset/userptr=0x0, length=614400
[10130.662892] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[10130.662917] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=1, type=vid-cap, flags=0x00002000, field=any, sequence=
0, memory=mmap, bytesused=0, offset/userptr=0x96000, length=614400
[10130.662952] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[10130.662967] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=2, type=vid-cap, flags=0x00002000, field=any, sequence=
0, memory=mmap, bytesused=0, offset/userptr=0x12c000, length=614400
[10130.663002] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[10130.666880] video0: VIDIOC_STREAMON: type=vid-cap
[10130.857484] video0: VIDIOC_CREATE_BUFS: index=3, count=1, memory=mmap, type=vid-cap, width=640, height=480, pixelfor
mat=YUYV, field=none, bytesperline=1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_f
unc=2
[10130.857585] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=3, type=vid-cap, flags=0x00002000, field=any, sequence=
0, memory=mmap, bytesused=0, offset/userptr=0x1c2000, length=614400
[10130.857627] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[10131.022069] video0: VIDIOC_STREAMOFF: type=vid-cap

5.2.2. V4L2 core framework tracing[edit | edit source]

Tracing of the V4L2 core framework[3] can be enabled using commands:

 echo 0x3 > /sys/module/videobuf2_core/parameters/debug
 echo 0x3 > /sys/module/videobuf2_v4l2/parameters/debug

Traces are output in kernel log buffer:

 dmesg
[11875.487933] vb2-core: __setup_offsets: buffer 0, plane 0 offset 0x00000000
[11875.501731] vb2-core: __setup_offsets: buffer 1, plane 0 offset 0x001fb000
[11875.514901] vb2-core: __setup_offsets: buffer 2, plane 0 offset 0x003f6000
[11875.532298] vb2-core: __setup_offsets: buffer 3, plane 0 offset 0x005f1000
[11875.540019] vb2-core: __vb2_queue_alloc: allocated 4 buffers, 1 plane(s) each
[11875.563689] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb4f05000, size 2076672
[11875.571174] vb2-core: vb2_mmap: buffer 0, plane 0 successfully mapped
[11875.589656] vb2-core: vb2_core_qbuf: qbuf of buffer 0 succeeded
[11875.595684] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb4d0a000, size 2076672
[11875.603062] vb2-core: vb2_mmap: buffer 1, plane 0 successfully mapped
[11875.609668] vb2-core: vb2_core_qbuf: qbuf of buffer 1 succeeded
[11875.615642] vb2_dc_mmap: mapped dma addr 0xf1d00000 at 0xb4b0f000, size 2076672
[11875.623016] vb2-core: vb2_mmap: buffer 2, plane 0 successfully mapped
[11875.629628] vb2-core: vb2_core_qbuf: qbuf of buffer 2 succeeded
[11875.635617] vb2_dc_mmap: mapped dma addr 0xf1f00000 at 0xb4914000, size 2076672
[11875.642952] vb2-core: vb2_mmap: buffer 3, plane 0 successfully mapped
[11875.649715] vb2-core: vb2_core_qbuf: qbuf of buffer 3 succeeded
[11875.734058] vb2-core: vb2_core_streamon: successful
[11875.961291] vb2-core: vb2_buffer_done: done processing on buffer 0, state: 6
[11875.967036] vb2-core: vb2_core_dqbuf: returning done buffer
[11875.972437] vb2-core: vb2_core_dqbuf: dqbuf of buffer 0, with state 0
[11876.094639] vb2-core: vb2_buffer_done: done processing on buffer 1, state: 6
[11876.100367] vb2-core: vb2_core_dqbuf: returning done buffer
[11876.105788] vb2-core: vb2_core_dqbuf: dqbuf of buffer 1, with state 0

5.2.3. DCMI V4L2 kernel driver tracing[edit | edit source]

DCMI dynamic debug traces[7] can be enabled using command:

 echo "module stm32_dcmi +p" > /sys/kernel/debug/dynamic_debug/control

Here is an example with a 5Mp jpeg capture:

 gst-launch-1.0 v4l2src ! image/jpeg, width=2592, height=1944 ! fakesink
 dmesg
[12706.715949] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944
[12706.721548] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944
[12707.365947] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944
[12707.371551] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944
[12707.437537] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944
[12707.443042] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944
[12707.459767] stm32-dcmi 4c006000.dcmi: Setup queue, count=4, size=5038848
[12707.518914] stm32-dcmi 4c006000.dcmi: buffer[0] phy=0xf1900000 size=5038848
[12707.526068] stm32-dcmi 4c006000.dcmi: buffer[1] phy=0xf1e00000 size=5038848
[12707.533299] stm32-dcmi 4c006000.dcmi: buffer[2] phy=0xf2300000 size=5038848
[12707.541456] stm32-dcmi 4c006000.dcmi: buffer[3] phy=0xf2800000 size=5038848
[12707.551443] stm32-dcmi 4c006000.dcmi: Start streaming, starting capture
[12707.820885] stm32-dcmi 4c006000.dcmi: buffer[0] done seq=0, bytesused=499936
[12708.087436] stm32-dcmi 4c006000.dcmi: buffer[1] done seq=1, bytesused=447472
[12708.306415] stm32-dcmi 4c006000.dcmi: Stop streaming, errors=0 (overrun=0), buffers=2
[12708.319095] stm32-dcmi 4c006000.dcmi: Start streaming, starting capture
[12708.333571] stm32-dcmi 4c006000.dcmi: Stop streaming, errors=0 (overrun=0), buffers=0

5.3. How to debug[edit | edit source]

5.3.1. Errors[edit | edit source]

Errors are unconditionnaly traced in kernel log:

 dmesg
[   87.233672] stm32-dcmi 4c006000.dcmi: Some errors found while streaming: errors=1 (overrun=1), buffers=24

5.3.2. Memory tracking[edit | edit source]

Frames require large chunks of contiguous memory, they are allocated by V4L2 framework through DMA backend. Those allocations can be traced using:

 echo "module dma_contiguous +p" > /sys/kernel/debug/dynamic_debug/control
 echo "module videobuf2_dma_contig +p" > /sys/kernel/debug/dynamic_debug/control

Here is the trace after a VGA preview

[11311.617688] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb3b6a000, size 614400
[11311.617986] vb2_dc_mmap: mapped dma addr 0xf1a00000 at 0xb3ad4000, size 614400
[11311.618071] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb3a3e000, size 614400
[11311.764146] vb2_dc_mmap: mapped dma addr 0xf1c00000 at 0xb307c000, size 614400

4 frames of VGA YUV422 frames: 640x480x2=614400 bytes

6. Source code location[edit | edit source]

6.1. User space[edit | edit source]

6.2. Kernel space[edit | edit source]

7. References[edit | edit source]