Registered User mNo edit summary |
Registered User mNo edit summary |
||
(7 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | |||
|MPUs list=STM32MP13x,STM32MP15x | |||
|MPUs checklist=STM32MP13x, STM32MP15x | |||
}}</noinclude> | |||
== Introduction == | == Introduction == | ||
The blue and red [[LEDs and buttons on STM32 MPU boards|LEDs on | The blue and red [[LEDs and buttons on STM32 MPU boards|LEDs on STM32 MPU boards]] are used to notify the user in case of boot failure during the [[Boot chain overview|boot chain]] execution and at runtime.<br /> | ||
== Description and debug == | == Description and debug == | ||
The statuses of blue and red LEDs allow to see at which stage the execution failed: the diagram below shows how each boot component uses these LEDs while the table gives more information on the way to interpret the LED statuses when the boot fails. Among the boot components, the FSBL | The statuses of blue and red LEDs allow to see at which stage the execution failed: the diagram below shows how each boot component uses these LEDs while the table gives more information on the way to interpret the LED statuses when the boot fails. Among the boot components, the FSBL is TF-A and the SSBL is U-Boot, as explained in the [[Boot chain overview|boot chain overview]]. | ||
<br /><br /> | <br /><br /> | ||
Line 17: | Line 21: | ||
| Off | | Off | ||
| Blinking | | Blinking | ||
| The execution failed during [[ | | The execution failed during [[STM32 MPU ROM code overview|ROM code]] execution | ||
| Check that:<br /> | | Check that:<br /> | ||
* your microSD card is properly inserted in the board | * your microSD card is properly inserted in the board | ||
* the [[ | * the [[STM32 MPU ROM code overview#Boot device selection|boot pins]] configuration selects the boot device | ||
* your boot memory was well programmed with [[STM32CubeProgrammer]] | * your boot memory was well programmed with [[STM32CubeProgrammer]] | ||
|- | |- | ||
Line 34: | Line 38: | ||
# After the SSBL execution but before the heartbeat (blue LED) started | # After the SSBL execution but before the heartbeat (blue LED) started | ||
| <br /> | | <br /> | ||
# See [[TF-A | # See [[How to debug TF-A BL2]] to investigate the failure | ||
# See [[U-Boot - How to debug]] and [[:Category:How_to_trace_and_debug|how to trace and debug]] to investigate the failure | # See [[U-Boot - How to debug]] and [[:Category:How_to_trace_and_debug|how to trace and debug]] to investigate the failure | ||
|- | |- |
Latest revision as of 18:49, 24 January 2023
1. Introduction[edit | edit source]
The blue and red LEDs on STM32 MPU boards are used to notify the user in case of boot failure during the boot chain execution and at runtime.
2. Description and debug[edit | edit source]
The statuses of blue and red LEDs allow to see at which stage the execution failed: the diagram below shows how each boot component uses these LEDs while the table gives more information on the way to interpret the LED statuses when the boot fails. Among the boot components, the FSBL is TF-A and the SSBL is U-Boot, as explained in the boot chain overview.
Blue LED | Red LED | System state | Action |
---|---|---|---|
Off | Blinking | The execution failed during ROM code execution | Check that:
|
On | Blinking | The execution failed during the second stage bootloader (SSBL) | See U-Boot - How to debug to investigate the failure |
Off | Off | The execution may have failed:
|
|
Off or on | Off | The execution may have failed during Linux® kernel execution between two heartbeat pulses (blue LED): a fatal error leading to a kernel panic might have occurred... | See Dmesg and Linux kernel log to investigate the failure |
Blinking | Off | Your platform is alive | Enjoy ! |