Registered User mNo edit summary |
Registered User m (Text replacement - "st_table" to "st-table") |
||
(44 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP23x, STM32MP25x | ||
}}</noinclude> | }} | ||
The STM32PRGFW-UTIL is an STMicroelectronics original initiative to manage the One-time Programmable (OTP) memories. | Support of STPMIC automatic detection on ST boards</noinclude> | ||
The STM32PRGFW-UTIL is an STMicroelectronics original initiative to manage the One-time Programmable (OTP) memories and also supports STPMIC programming. | |||
More information can be found in the detailed release notes referenced later in this article. | More information can be found in the detailed release notes referenced later in this article. | ||
==STM32PRGFW-UTIL - | ==STM32PRGFW-UTIL - version 1.1.2 == | ||
{| class=" | {{Important| It is mandatory to use STM32PRGFW-UTIL version v1.1.1 and above, to avoid bricking of your device. | ||
'''This new version v1.1.2 has some dependencies with STM32CubeIDE 1.16.1 (and higher version) and STM32CubeProgrammer v2.18.0 for PMIC NVM programming, it is mandatory to update also those 2 other ST tools''' <br>}} | |||
===Main changes=== | |||
* Support of STPMIC automatic detection on ST boards | |||
* Support of {{MicroprocessorDevice | device=23}} through {{MicroprocessorDevice | device=2}} binary | |||
===Main restrictions=== | |||
* {{MicroprocessorDevice | device=15}} boards fail sometimes to connect to STM32CubeProgrammer via UART (reset the board and try again) | |||
===How to get STM32PRGFW-UTIL=== | |||
{| class="st-table" | |||
|- | |- | ||
!colspan="3" | STM32PRGFW-UTIL for Linux<sup>®</sup> and Windows<sup>®</sup> host PC | !colspan="3" | STM32PRGFW-UTIL for Linux<sup>®</sup> and Windows<sup>®</sup> host PC | ||
Line 14: | Line 25: | ||
| '''Download''' | | '''Download''' | ||
|colspan="2" | | |colspan="2" | | ||
'''Version | '''Version 1.1.2''' | ||
* STM32PRGFW-UTIL firmware package is available | * [[STM32PRGFW-UTIL| STM32PRGFW-UTIL firmware package]] is available {{CodeSource | STM32PRGFW-UTIL | / | here}}. | ||
|- | |- | ||
| '''Installing the STM32PRGFW-UTIL''' | | '''Installing the STM32PRGFW-UTIL''' | ||
|colspan="2" | | |colspan="2" | | ||
* To use STM32PRGFW-UTIL, unzip the package on computer | * To use STM32PRGFW-UTIL, unzip the package on computer. | ||
* Then refer to | * Then refer to {{CodeSource | STM32PRGFW-UTIL | /README.md | READMED.md}}, to use this tool. | ||
|- | |- | ||
| '''Detailed release note''' | | '''Detailed release note''' | ||
| colspan="2" | | | colspan="2" | | ||
* Full details about the content of this tool release are available | * Full details about the content of this tool release are available {{CodeSource | STM32PRGFW-UTILhtml | Release_Notes.html}}. | ||
|} | |} | ||
<noinclude> | <noinclude> | ||
[[Category:Release notes]] | [[Category:Release notes]] | ||
[[Category:STM32PRGFW-UTIL]] | [[Category:STM32PRGFW-UTIL]] | ||
{{PublicationRequestId | 24647 | 2022-09-26}} | |||
</noinclude> | </noinclude> |
Latest revision as of 12:27, 12 March 2025
Support of STPMIC automatic detection on ST boards The STM32PRGFW-UTIL is an STMicroelectronics original initiative to manage the One-time Programmable (OTP) memories and also supports STPMIC programming.
More information can be found in the detailed release notes referenced later in this article.
1. STM32PRGFW-UTIL - version 1.1.2[edit | edit source]
1.1. Main changes[edit | edit source]
- Support of STPMIC automatic detection on ST boards
- Support of STM32MP23x lines
through STM32MP2 series binary
1.2. Main restrictions[edit | edit source]
- STM32MP15x lines
boards fail sometimes to connect to STM32CubeProgrammer via UART (reset the board and try again)
1.3. How to get STM32PRGFW-UTIL[edit | edit source]
STM32PRGFW-UTIL for Linux® and Windows® host PC | ||
---|---|---|
Download |
Version 1.1.2
| |
Installing the STM32PRGFW-UTIL |
| |
Detailed release note |
|