Registered User mNo edit summary Tag: 2017 source edit |
Registered User m (→Kernel space) Tag: 2017 source edit |
||
Line 1,320: | Line 1,320: | ||
=== Kernel space === | === Kernel space === | ||
* {{CodeSource | Linux kernel | drivers/media/v4l2-core | V4L2 core source code}} | * {{CodeSource | Linux kernel | drivers/media/v4l2-core/ | V4L2 core source code}} | ||
* {{CodeSource | Linux kernel | drivers/media/platform/st/stm32/stm32-dcmipp/ | stm32-dcmipp V4L2 driver source code}} | * {{CodeSource | Linux kernel | drivers/media/platform/st/stm32/stm32-dcmipp/ | stm32-dcmipp V4L2 driver source code}} | ||
* {{CodeSource | Linux kernel | drivers/media/i2c | i2c camera sensor V4L2 drivers source code}} | * {{CodeSource | Linux kernel | drivers/media/i2c/ | i2c camera sensor V4L2 drivers source code}} | ||
==References== | ==References== |
Revision as of 18:55, 7 November 2024
This article gives information about the Linux® V4L2 camera framework.
1. Framework purpose[edit | edit source]
The V4L2 Linux kernel framework[1] allows the control of both an external camera sensor, and the camera interface. This allows the capture of raw frames in various pixel formats or encoded stream data such as JPEG.
This could be typically used, with the help of other Linux multimedia frameworks, and applications, to take snapshot, to make preview, to make a video recording or even remotely stream images from the camera sensor.
2. System overview[edit | edit source]
2.1. Component description[edit | edit source]
- media-ctl (User space)
A V4L2 utility relying on Media Controller Linux kernel interface[2] aiming to configure, and link each sub devices composing the camera subsystem in order to configure it.
- Application (User space)
Any application relying on V4L2 Linux kernel interface[3] or libv4l abstraction layer. GStreamer framework provides such application.
- V4L2 utilities (User space)
A set of tools to test, configure, and use the whole camera subsystem, including the external camera sensor, and the camera interface. v4l2-ctl is one of the most useful utility.
- V4L2 libraries (libv4l) (User space)
A set of libraries on top of the V4L2 Linux kernel interface[3] which abstract the kernel interface in order to simplify, keep compatibility or add some hooks between V4L-based applications, and the V4L2 kernel interface.
- V4L2 core (Kernel space)
This layer represents the standard Linux kernel V4L2 Framework.
- stm32-dcmipp (Kernel space)
This V4L2 DCMIPP Linux device driver handles the DCMIPP hardware block.
- Camera sensor X driver (Kernel space)
This V4L2 Linux device driver handles the camera sensor X external peripheral, handles some GPIOs lines, and potentially power supplies to power-up/down the camera sensor. The communication with camera sensor is done through the i2c bus.
- DCMIPP (Hardware)
The Digital Camera Memory Interface Pixel Processor hardware block.
- Camera sensor X (Hardware)
The camera sensor external peripheral.
2.2. APIs description[edit | edit source]
The V4L2 userland API is documented in the Linux Media subsystem documentation[3]
The V4L2 kernel framework internal API is documented in the V4L2 Kernel Support section of the Linux kernel documentation[4]
The Media Controller API is documented in the Linux Media subsystem documentation[2]
3. Configuration[edit | edit source]
3.1. Kernel configuration[edit | edit source]
The STM32 DCMIPP camera interface and the camera sensor are enabled by default in STMicroelectronics deliveries.
Nevertheless, this is not the case when using the upstream kernel version. In this case, the DCMIPP V4L2 driver can be enabled using Linux kernel menuconfig tool:
Device Drivers --->
<M> Multimedia support --->
Media drivers --->
[*] Media platform devices --->
<M> STM32 Digital Camera Memory Interface Pixel Processor (DCMIPP) support
The external camera sensor connected to the camera interface must also be enabled, here is an example with the GC2145 GalaxyCore camera sensor located on the MB1897 camera daughter board[5] connected to the CN1 camera connector[6] of the STM32MP135x-DK Discovery kit :
Device Drivers --->
<M> Multimedia support --->
Media ancillary drivers --->
Camera sensor devices --->
<M> GalaxyCore GC2145 sensor support
The external camera sensor connected to the camera interface must also be enabled, here is an example with the OV5640 Omnivision camera sensor located on the MB1723 camera daughter board connected to the CN1 camera connector[6] of the STM32MP135x-DK Discovery kit Device Drivers --->
<M> Multimedia support --->
Media ancillary drivers --->
Camera sensor devices --->
<M> OmniVision OV5640 sensor support
|
DCMIPP hardware block interconnects with the camera sensor connected on CN1 camera connector[6] of the STM32MP135x-DK Discovery kit through the MIPID02 CSI-2 to parallel bridge soldered on STM32MP13 discovery board. Hence, MIPID02 driver must be enabled too:
Device Drivers --->
<M> Multimedia support --->
Media ancillary drivers --->
Miscellaneous helper chips --->
<M> STMicroelectronics MIPID02 CSI-2 to PARALLEL bridge
3.2. Device tree configuration[edit | edit source]
Refer to DCMIPP device tree configuration article for a complete view of DCMIPP and sensor configuration thanks to Linux kernel device tree mechanism.
4. How to use the framework[edit | edit source]
The use cases described here are enabled using media-ctl, v4l2-ctl, gst-launch or gst-play command line utilities.
4.1. List the video devices and their capabilities[edit | edit source]
List all the available video devices using --list-devices option:
--list-devicesv4l2-ctl
dcmipp_bytecap (platform:dcmipp):
/dev/video0
/dev/media0
If several devices are available, use -d option after any v4l2-ctl commands to target a specific device. If -d option is not specified, /dev/video0 is targeted by default.
In order to have information on a specific device, use -D option:
-d /dev/video0 -Dv4l2-ctl
DCMIPP MDEV Serial : Bus info : platform:5a000000.dcmipp Media version : 6.6.48 Hardware revision: 0x00000010 (16) Driver version : 6.6.48 Interface Info: ID : 0x03000009 Type : V4L Video Entity Info: ID : 0x00000007 (7) Name : dcmipp_dump_capture Function : V4L2 I/O Pad 0x01000008 : 0: Sink Link 0x0200000d: from remote pad 0x1000006 of entity 'dcmipp_dump_postproc' (Video Scaler): Data, EnableeDriver Info: Driver name : dcmipp Card type : stm32_dcmipp Bus info : platform:5a000000.dcmipp Driver version : 6.6.48 Capabilities : 0xa4200001 Video Capture I/O MC Streaming Extended Pix Format Device Capabilities Device Caps : 0x24200001 Video Capture I/O MC Streaming Extended Pix Format Media Driver Info: Driver name : dcmipp Model :
4.2. Get the topology of camera subsystem[edit | edit source]
Print the topology of camera subsystem using -p media-ctl option:
-pmedia-ctl
API version 6.6.48 Media device information ------------------------ driver dcmipp model DCMIPP MDEV serial bus info platform:5a000000.dcmipp hw revision 0x10 driver version 6.6.48 Device topology - entity 1: dcmipp_input (2 pads, 2 links, 0 routes) type V4L2 subdev subtype Unknown flags 0 device node name /dev/v4l-subdev0 pad0: Sink [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:srgb] <- "st-mipid02 1-0014":2 [ENABLED,IMMUTABLE] pad1: Source [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:rec709] -> "dcmipp_dump_postproc":0 [ENABLED,IMMUTABLE] - entity 4: dcmipp_dump_postproc (2 pads, 2 links, 0 routes) type V4L2 subdev subtype Unknown flags 0 device node name /dev/v4l-subdev1 pad0: Sink [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:rec709 compose.bounds:(0,0)/640x480 compose:(0,0)/640x480] <- "dcmipp_input":1 [ENABLED,IMMUTABLE] pad1: Source [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:rec709 crop.bounds:(0,0)/640x480 crop:(0,0)/640x480] -> "dcmipp_dump_capture":0 [ENABLED,IMMUTABLE] - entity 7: dcmipp_dump_capture (1 pad, 1 link) type Node subtype V4L flags 0 device node name /dev/video0 pad0: Sink <- "dcmipp_dump_postproc":1 [ENABLED,IMMUTABLE] - entity 15: st-mipid02 1-0014 (3 pads, 2 links, 0 routes) type V4L2 subdev subtype Unknown flags 0 device node name /dev/v4l-subdev2 pad0: Sink [stream:0 fmt:RGB565_1X16/640x480 field:none colorspace:srgb] <- "gc2145 1-003c":0 [ENABLED,IMMUTABLE] pad1: Sink pad2: Source [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:srgb] -> "dcmipp_input":0 [ENABLED,IMMUTABLE] - entity 21: gc2145 1-003c (1 pad, 1 link, 0 routes) type V4L2 subdev subtype Sensor flags 0 device node name /dev/v4l-subdev3 pad0: Source [stream:0 fmt:RGB565_1X16/640x480 field:none colorspace:srgb crop.bounds:(0,0)/1600x1200 crop:(0,0)/640x480] -> "st-mipid02 1-0014":0 [ENABLED,IMMUTABLE]Media controller
This gives the current links between camera subdevices, and each subdevice current pads configuration such as, format, resolution, framerate.
Print the topology of camera subsystem using -p media-ctl option: -pmedia-ctl API version 6.6.48 Media device information ------------------------ driver dcmipp model DCMIPP MDEV serial bus info platform:5a000000.dcmipp hw revision 0x10 driver version 6.6.48 Device topology - entity 1: dcmipp_input (2 pads, 2 links, 0 routes) type V4L2 subdev subtype Unknown flags 0 device node name /dev/v4l-subdev0 pad0: Sink [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range] <- "st-mipid02 1-0014":2 [ENABLED,IMMUTABLE] pad1: Source [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:rec709] -> "dcmipp_dump_postproc":0 [ENABLED,IMMUTABLE] - entity 4: dcmipp_dump_postproc (2 pads, 2 links, 0 routes) type V4L2 subdev subtype Unknown flags 0 device node name /dev/v4l-subdev1 pad0: Sink [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:rec709 compose.bounds:(0,0)/640x480 compose:(0,0)/640x480] <- "dcmipp_input":1 [ENABLED,IMMUTABLE] pad1: Source [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:rec709 crop.bounds:(0,0)/640x480 crop:(0,0)/640x480] -> "dcmipp_dump_capture":0 [ENABLED,IMMUTABLE] - entity 7: dcmipp_dump_capture (1 pad, 1 link) type Node subtype V4L flags 0 device node name /dev/video0 pad0: Sink <- "dcmipp_dump_postproc":1 [ENABLED,IMMUTABLE] - entity 15: st-mipid02 1-0014 (3 pads, 2 links, 0 routes) type V4L2 subdev subtype Unknown flags 0 device node name /dev/v4l-subdev2 pad0: Sink [stream:0 fmt:RGB565_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range] <- "ov5640 1-003c":0 [ENABLED,IMMUTABLE] pad1: Sink pad2: Source [stream:0 fmt:RGB565_2X8_LE/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range] -> "dcmipp_input":0 [ENABLED,IMMUTABLE] - entity 21: ov5640 1-003c (1 pad, 1 link, 0 routes) type V4L2 subdev subtype Sensor flags 0 device node name /dev/v4l-subdev3 pad0: Source [stream:0 fmt:RGB565_1X16/640x480@1/30 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range crop.bounds:(0,0)/2624x1964 crop:(16,14)/2592x1944] -> "st-mipid02 1-0014":0 [ENABLED,IMMUTABLE]Media controller This gives the current links between camera subdevices, and each subdevice current pads configuration such as, format, resolution, framerate. |
This topology can also be displayed in a human readable graphical form thanks to --print-dot option:
--print-dot > graph.dotmedia-ctl
Retrieve then this .dot file into your host PC in order to convert it to .png:
dot -Tpng -Nfontname=Roboto -Nfontsize=10 -Efontname=Roboto -Efontsize=10 graph.dot > graph.png
|
4.3. Camera subsystem setup[edit | edit source]
In order to be able to capture frames from video device node with v4l2-ctl, GStreamer or any other V4L2 application, the camera subsystem must be first configured. To do so use media-ctl --set-v4l2 command giving the subdevice name & pad, the desired format, resolution and framerate:
--set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_2X8_BE/640x480 field:none]"media-ctl -d /dev/media0
The configuration must be done from source to sink. Below is a configuration allowing to capture RGB565 480x272 frames (the display size of the MP13 discovery board):
'gc2145 1-003c':0[fmt:RGB565_1X16/640x480 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(80,104)/480x272]"media-ctl -d /dev/media0 --set-v4l2 "
'ov5640 1-003c':0[fmt:RGB565_1X16/640x480 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(80,104)/480x272]"media-ctl -d /dev/media0 --set-v4l2 " |
Sensor is configured in 640x480 RGB565 at 30 fps, then DCMIPP is configured to crop area 480x272 in the middle of the 640x480 frame output by sensor. The configuration can be read back displaying the topology of graph, see #Get the topology of camera subsystem. Then, any application that read frames from V4L2 video device node can be executed:
RGB16, width=480,height=272, framerate=30/1 ! queue ! waylandsink fullscreen=truegst-launch-1.0 v4l2src ! video/x-raw, format=
4.4. Controlling camera sensor[edit | edit source]
In order to control camera sensor, its corresponding entity device node must be found in the topology. To do so, the first entity of the graph must be found, ie the entity having no sink pad:
V4L2 subdev subtype Sensor flags 0 device node name /dev/v4l-subdev3 pad0: Source [stream:0 fmt:RGB565_1X16/640x480@1/30 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range crop.bounds:(0,0)/2624x1964 crop:(16,14)/2592x1944] -> "st-mipid02 1-0014":0 [ENABLED,IMMUTABLE]- entity 21: ov5640 1-003c (1 pad, 1 link, 0 routes) type
Here it is /dev/v4l-subdev3.
Use then v4l2-ctl with -L option to get the list of supported controls:
-Lv4l2-ctl -d /dev/v4l-subdev3
User Controls
horizontal_flip 0x00980914 (bool) : default=0 value=0
vertical_flip 0x00980915 (bool) : default=0 value=0
Image Source Controls
vertical_blanking 0x009e0901 (int) : min=0 max=8191 step=1 default=12 value=12
horizontal_blanking 0x009e0902 (int) : min=0 max=4095 step=1 default=304 value=304
Image Processing Controls
link_frequency 0x009f0901 (intmenu): min=0 max=2 default=0 value=0 (120000000 0x7270e00) flags=read-only
0: 120000000 (0x7270e00)
1: 192000000 (0xb71b000)
2: 240000000 (0xe4e1c00)
pixel_rate 0x009f0902 (int64) : min=30000000 max=60000000 step=1 default=30000000 value=30000000 flags=read-only
test_pattern 0x009f0903 (menu) : min=0 max=8 default=0 value=0 (Disabled)
0: Disabled
1: Colored patterns
2: Uniform white
3: Uniform yellow
4: Uniform cyan
5: Uniform green
6: Uniform magenta
7: Uniform red
8: Uniform black
![]() |
"value=" field returns the current value of the control |
V4L2 subdev subtype Sensor flags 0 device node name /dev/v4l-subdev3 pad0: Source [stream:0 fmt:RGB565_1X16/640x480@1/30 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:full-range crop.bounds:(0,0)/2624x1964 crop:(16,14)/2592x1944] -> "st-mipid02 1-0014":0 [ENABLED,IMMUTABLE]- entity 21: ov5640 1-003c (1 pad, 1 link, 0 routes) type Here it is /dev/v4l-subdev3. Use then v4l2-ctl with -L option to get the list of supported controls: -Lv4l2-ctl -d /dev/v4l-subdev3
User Controls
contrast 0x00980901 (int) : min=0 max=255 step=1 default=0 value=0 flags=slider
saturation 0x00980902 (int) : min=0 max=255 step=1 default=64 value=64 flags=slider
hue 0x00980903 (int) : min=0 max=359 step=1 default=0 value=0 flags=slider
white_balance_automatic 0x0098090c (bool) : default=1 value=1 flags=update
red_balance 0x0098090e (int) : min=0 max=4095 step=1 default=0 value=0 flags=inactive, slider
blue_balance 0x0098090f (int) : min=0 max=4095 step=1 default=0 value=0 flags=inactive, slider
exposure 0x00980911 (int) : min=0 max=996 step=1 default=520 value=0 flags=inactive, volatile
gain_automatic 0x00980912 (bool) : default=1 value=1 flags=update
horizontal_flip 0x00980914 (bool) : default=0 value=0
vertical_flip 0x00980915 (bool) : default=0 value=0
power_line_frequency 0x00980918 (menu) : min=0 max=3 default=1 value=1 (50 Hz)
0: Disabled
1: 50 Hz
2: 60 Hz
3: Auto
Camera Controls
auto_exposure 0x009a0901 (menu) : min=0 max=1 default=0 value=0 (Auto Mode) flags=update
0: Auto Mode
1: Manual Mode
Image Source Controls
vertical_blanking 0x009e0901 (int) : min=24 max=2895 step=1 default=520 value=520
horizontal_blanking 0x009e0902 (int) : min=960 max=960 step=1 default=960 value=960 flags=read-only
analogue_gain 0x009e0903 (int) : min=0 max=1023 step=1 default=0 value=0 flags=inactive, volatile
Image Processing Controls
link_frequency 0x009f0901 (intmenu): min=0 max=22 default=13 value=19 (192000000 0xb71b000) flags=read-only
0: 992000000 (0x3b20b800)
1: 888000000 (0x34edce00)
2: 768000000 (0x2dc6c000)
3: 744000000 (0x2c588a00)
4: 672000000 (0x280de800)
5: 672000000 (0x280de800)
6: 592000000 (0x23493400)
7: 592000000 (0x23493400)
8: 576000000 (0x22551000)
9: 576000000 (0x22551000)
10: 496000000 (0x1d905c00)
11: 496000000 (0x1d905c00)
12: 384000000 (0x16e36000)
13: 384000000 (0x16e36000)
14: 384000000 (0x16e36000)
15: 336000000 (0x1406f400)
16: 296000000 (0x11a49a00)
17: 288000000 (0x112a8800)
18: 248000000 (0xec82e00)
19: 192000000 (0xb71b000)
20: 192000000 (0xb71b000)
21: 192000000 (0xb71b000)
22: 96000000 (0x5b8d800)
pixel_rate 0x009f0902 (int64) : min=48000000 max=168000000 step=1 default=48000000 value=48000000 flags=read-only
test_pattern 0x009f0903 (menu) : min=0 max=4 default=0 value=0 (Disabled)
0: Disabled
1: Color bars
2: Color bars w/ rolling bar
3: Color squares
4: Color squares w/ rolling bar
|
The control value can be changed thanks to --set-ctrl option, for example:
--set-ctrl test_pattern=1v4l2-ctl -d /dev/v4l-subdev3
The control value can be changed dynamically. In the following example, the color bar is enabled/disabled while preview is running:
- Start preview in background
gst-launch-1.0 v4l2src ! "video/x-raw, format=RGB16, width=480, height=272, framerate=(fraction)30/1" ! queue ! waylandsink fullscreen=true -e &
- Then alternate the color bar activation or not
--set-ctrl test_pattern=1;sleep 1;v4l2-ctl -d /dev/v4l-subdev3 --set-ctrl test_pattern=0;sleep 1;v4l2-ctl -d /dev/v4l-subdev3 --set-ctrl test_pattern=1;sleep 1;v4l2-ctl -d /dev/v4l-subdev3 --set-ctrl test_pattern=0;killall gst-launch-1.0v4l2-ctl -d /dev/v4l-subdev3
- Horizontal/vertical flip can also be changed while preview is running:
--set-ctrl horizontal_flip=1;sleep 2;v4l2-ctl -d /dev/v4l-subdev3 --set-ctrl horizontal_flip=0;sleep 2;v4l2-ctl -d /dev/v4l-subdev3 --set-ctrl vertical_flip=1;sleep 2;v4l2-ctl -d /dev/v4l-subdev3 --set-ctrl vertical_flip=0;killall gst-launch-1.0v4l2-ctl -d /dev/v4l-subdev3
4.5. Set the camera sensor pixel format, resolution and framerate[edit | edit source]
Camera sensor only supports a discrete set of formats, resolutions and framerates that can be get thanks to v4l2-ctl options --list-subdev-mbus-codes, --list-subdev-framesizes and --list-subdev-frameintervals:
--list-subdev-mbus-codesv4l2-ctl -d /dev/v4l-subdev3
ioctl: VIDIOC_SUBDEV_ENUM_MBUS_CODE (pad=0,stream=0)
0x200f: MEDIA_BUS_FMT_UYVY8_1X16
0x2010: MEDIA_BUS_FMT_VYUY8_1X16
0x2011: MEDIA_BUS_FMT_YUYV8_1X16
0x2012: MEDIA_BUS_FMT_YVYU8_1X16
0x1017: MEDIA_BUS_FMT_RGB565_1X16
0x3002: MEDIA_BUS_FMT_SGRBG8_1X8
0x3014: MEDIA_BUS_FMT_SRGGB8_1X8
0x3001: MEDIA_BUS_FMT_SBGGR8_1X8
0x3013: MEDIA_BUS_FMT_SGBRG8_1X8
ioctl: VIDIOC_SUBDEV_ENUM_MBUS_CODE (pad=0,stream=0)
0x4001: MEDIA_BUS_FMT_JPEG_1X8
0x200f: MEDIA_BUS_FMT_UYVY8_1X16
0x2011: MEDIA_BUS_FMT_YUYV8_1X16
0x1017: MEDIA_BUS_FMT_RGB565_1X16
0x1013: MEDIA_BUS_FMT_BGR888_1X24
0x3001: MEDIA_BUS_FMT_SBGGR8_1X8
0x3013: MEDIA_BUS_FMT_SGBRG8_1X8
0x3002: MEDIA_BUS_FMT_SGRBG8_1X8
0x3014: MEDIA_BUS_FMT_SRGGB8_1X8
|
Frame size might depend on frame format, so precise it when asking for frame size:
--list-subdev-framesizes pad=0,code=0x1017v4l2-ctl -d /dev/v4l-subdev3
ioctl: VIDIOC_SUBDEV_ENUM_FRAME_SIZE (pad=0,stream=0)
Size Range: 640x480 - 640x480
Size Range: 1280x720 - 1280x720
Size Range: 1600x1200 - 1600x1200
ioctl: VIDIOC_SUBDEV_ENUM_FRAME_SIZE (pad=0,stream=0)
Size Range: 160x120 - 160x120
Size Range: 176x144 - 176x144
Size Range: 320x240 - 320x240
Size Range: 640x480 - 640x480
Size Range: 720x480 - 720x480
Size Range: 720x576 - 720x576
Size Range: 1024x768 - 1024x768
Size Range: 1280x720 - 1280x720
Size Range: 1920x1080 - 1920x1080
Size Range: 2592x1944 - 2592x1944
|
Framerate depends on resolution and format, so precise them when asking for frame intervals:
--list-subdev-frameintervals pad=0,width=640,height=480,code=0x1007v4l2-ctl -d /dev/v4l-subdev3
ioctl: VIDIOC_SUBDEV_ENUM_FRAME_INTERVAL (pad=0)
Interval: 0.033s (30.000 fps)
ioctl: VIDIOC_SUBDEV_ENUM_FRAME_INTERVAL (pad=0,stream=0)
Interval: 0.067s (15.000 fps)
Interval: 0.033s (30.000 fps)
Interval: 0.017s (60.000 fps)
|
Now that camera sensor capabilities are known, the wanted configuration can be set following instructions described in chapter camera subsystem setup.
For example here to make a VGA preview at 30 fps:
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_1X16/640x480 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/640x480]"
gst-launch-1.0 v4l2src ! video/x-raw, format=RGB16, width=640,height=480, framerate=30/1 ! queue ! autovideosink
For example here to make a QVGA preview at 15 fps:
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:RGB565_1X16/320x240@1/15 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/320x240]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/320x240]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/320x480]"
gst-launch-1.0 v4l2src ! video/x-raw, format=RGB16, width=320,height=240, framerate=15/1 ! queue ! autovideosink
Here is another example to capture 100 QVGA JPEG files at 30 fps:
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:JPEG_1X8/320x240@1/30 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:JPEG_1X8/320x240]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:JPEG_1X8/320x240]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:JPEG_1X8/320x240]"
v4l2-ctl --set-fmt-video=width=320,height=240,pixelformat=JPEG --stream-mmap --stream-count=100 --stream-to=pics.jpeg
Replay using gst-play:
gst-play-1.0 pics.jpeg --videosink="videorate ! video/x-raw, framerate=30/1 ! autovideosink"
|
4.6. Downscale and crop[edit | edit source]
Two features of DCMIPP can help to reduce resolution: downsize and crop, these two features are configured on postproc subdev.
Downscale is basic and consists in skipping 1 pixel over 2 in width and/or height, allowing to divide by 2 in width and/or height. The wanted resolution must be set on postproc subdev using compose property of sink pad respecting /2 ratio. Here is an example to get 320x240 frames from 640x480 input frames:
640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[compose:(0,0)/320x240]"media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_1X16/640x480 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/
640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[compose:(0,0)/320x240]"media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:RGB565_1X16/@1/30 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/ |
gst-launch-1.0 v4l2src ! video/x-raw, format=RGB16, width=320,height=240, framerate=30/1 ! queue ! autovideosink
![]() |
Please note that (top,left) argument of compose property is ignored by driver |
Crop can be made at 16 pixels precision (output is rounded to 16 inferior multiple).
The wanted area must be set using crop property of postproc subdev source pad.
Here is an example to crop a 480x272 area centered inside the 640x480 input frame:
640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(80,104)/480x272]"media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_1X16/640x480 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/
640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(80,104)/480x272]"media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:RGB565_1X16/640x480@1/30 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/ |
gst-launch-1.0 v4l2src ! video/x-raw, format=RGB16, width=480,height=272, framerate=30/1 ! queue ! autovideosink
Downscale and crop can be combined together. Here is an example to get small 320x176 frames from 1280x720 input frames:
1280x720]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[compose:(0,0)/640x360]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(160,92)/320x176]"media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_1X16/1280x720 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/1280x720]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/1280x720]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/
1280x720]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[compose:(0,0)/640x360]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(160,92)/320x176]"media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:RGB565_1X16/1280x720@1/30 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/1280x720]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/1280x720]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/ |
gst-launch-1.0 v4l2src ! video/x-raw, format=RGB16, width=320,height=176, framerate=30/1 ! queue ! autovideosink
Refer to the selection chapter of the sub device interface documentation[7] to get more details on how to control scaling and crop.
4.7. Grab a raw frame[edit | edit source]
Capture a VGA RGB565 raw frame on disk:
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_1X16/640x480 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/640x480]"
v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=RGBP --stream-mmap --stream-count=1 --stream-to=grab-640x480-rgb565.raw
Capture a VGA RGB565 raw frame on disk:
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:RGB565_1X16/640x480@1/30 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/640x480]"
v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=RGBP --stream-mmap --stream-count=1 --stream-to=grab-640x480-rgb565.raw
|
In order to display it, this raw frame must be converted first to JPEG:
gst-launch-1.0 filesrc location= grab-640x480-rgb565.raw blocksize=614400 ! "video/x-raw, format=(string)RGB16, width=(int)640, height=(int)480, framerate=(fraction)30/1" ! videoconvert ! jpegenc ! filesink location=grab-640x480-rgb565.jpeg
Then weston-image utility can be used to display this JPEG file:
weston-image grab-640x480-rgb565.jpeg
4.8. Fullscreen preview[edit | edit source]
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_1X16/640x480 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(80,104)/480x272]"
gst-launch-1.0 v4l2src ! "video/x-raw, format=RGB16, width=480, height=272, framerate=(fraction)15/1" ! queue ! autovideosink -e
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:RGB565_1X16/640x480@1/15 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:RGB565_1X16/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(80,104)/480x272]"
gst-launch-1.0 v4l2src ! "video/x-raw, format=RGB16, width=480, height=272, framerate=(fraction)15/1" ! queue ! autovideosink -e
|
4.9. Take a picture in JPEG format[edit | edit source]
The GC2145 sensor doesn't support JPEG frame format natively.
Capture a 5Mp JPEG:
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:JPEG_1X8/640x480@1/15 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:JPEG_1X8/2592x1944@1/15 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:JPEG_1X8/2592x1944]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:JPEG_1X8/2592x1944]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:JPEG_1X8/2592x1944]"
v4l2-ctl --set-fmt-video=width=2592,height=1944,pixelformat=JPEG --stream-mmap --stream-count=1 --stream-skip=3 --stream-to=pic-5Mp.jpeg
Then display it:
weston-image pic-5Mp.jpeg
You can check the picture resolution using gst-typefind:
gst-typefind-1.0 pic-5Mp.jpeg
pic-5Mp.jpeg - image/jpeg, width=(int)2592, height=(int)1944, sof-marker=(int)0
|
4.10. Preview in YUV422[edit | edit source]
Capture VGA YUV422 frames and display them using GStreamer :
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:YUYV8_1X16/640x480 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:YUYV8_1X16/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':0[fmt:YUYV8_2X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:YUYV8_2X8/640x480]"
gst-launch-1.0 v4l2src ! "video/x-raw, format=YUY2, width=640,height=480, framerate=(fraction)15/1" ! queue ! videoconvert ! queue ! autovideosink
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:YUYV8_1X16/640x480@1/15 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:YUYV8_1X16/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:YUYV8_2X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:YUYV8_2X8/640x480]"
gst-launch-1.0 v4l2src ! "video/x-raw, format=YUY2, width=640,height=480, framerate=(fraction)15/1" ! queue ! videoconvert ! queue ! autovideosink
|
4.11. Grab a raw-bayer frame[edit | edit source]
Capture a 720p raw-bayer frame on disk. The GC2145 only currently support the RGGB format.
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:SRGGB8_1X8/1280x720 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:SRGGB8_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:SRGGB8_1X8/1280x720]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:SRGGB8_1X8/1280x720]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:SRGGB8_1X8/1280x720]"
v4l2-ctl --set-fmt-video=width=1280,height=720,pixelformat=BA81 --stream-mmap --stream-count=1 --stream-to=grab-1280x720-bayer.raw
In order to display it, this raw-bayer frame must be converted first to JPEG:
gst-launch-1.0 filesrc location= grab-1280x720-bayer.raw blocksize=921600 ! "video/x-bayer, format=(string)rggb, width=(int)1280, height=(int)720, framerate=(fraction)30/1" ! bayer2rgb ! videoconvert ! jpegenc ! filesink location=grab-1280x720-bayer.jpeg
Then weston-image utility can be used to display this JPEG file:
weston-image grab-1280x720-bayer.jpeg
Capture a 720p raw-bayer frame on disk:
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:SBGGR8_1X8/1280x720@1/15 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:SBGGR8_1X8/1280x720]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:SBGGR8_1X8/1280x720]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:SBGGR8_1X8/1280x720]"
v4l2-ctl --set-fmt-video=width=1280,height=720,pixelformat=BA81 --stream-mmap --stream-count=1 --stream-to=grab-1280x720-bayer.raw
In order to display it, this raw-bayer frame must be converted first to JPEG:
gst-launch-1.0 filesrc location= grab-1280x720-bayer.raw blocksize=921600 ! "video/x-bayer, format=(string)bggr, width=(int)1280, height=(int)720, framerate=(fraction)15/1" ! bayer2rgb ! videoconvert ! jpegenc ! filesink location=grab-1280x720-bayer.jpeg
Then weston-image utility can be used to display this JPEG file:
weston-image grab-1280x720-bayer.jpeg
|
4.12. Raw-bayer capture with preview[edit | edit source]
Camera subsystem is setup in order that VGA raw-bayer camera sensor output is reduced to 320x240 using crop (downscale is not possible with raw-bayer):
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:SRGGB8_1X8/640x480 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:SRGGB8_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:SRGGB8_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:SRGGB8_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(160,120)/320x240]"
Then GStreamer is used to grab frames on disk while previewing:
gst-launch-1.0 v4l2src num-buffers=100 ! "video/x-bayer, format=rggb, width=320,height=240, framerate=(fraction)30/1" ! queue ! tee name=tee ! queue ! fpsdisplaysink name="capturerate" sync=false text-overlay=false video-sink="multifilesink location=320x240_%d-bayer.raw max-files=10" tee. ! queue ! videorate max-rate=15 ! bayer2rgb ! queue ! videoconvert ! queue ! waylandsink sync=false -v
Raw-bayer frames are captured on disk looping over 10 files to not saturate the disk:
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_90-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_91-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_92-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_93-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_94-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_95-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_96-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_97-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_98-bayer.raw
-rw-r--r-- 1 root root 56320 Sep 20 12:38 320x240_99-bayer.raw
Note that capture occurs at 30 fps while preview is done at 15 fps to not overload system with software debayering, see trace below:
/GstPipeline:pipeline0/GstFPSDisplaySink:capturerate: last-message = rendered: 145, dropped: 0, current: 30.41, average: 30.63
/GstPipeline:pipeline0/GstFPSDisplaySink:capturerate: last-message = rendered: 161, dropped: 0, current: 30.41, average: 30.60
/GstPipeline:pipeline0/GstFPSDisplaySink:capturerate: last-message = rendered: 177, dropped: 0, current: 30.41, average: 30.59
Camera subsystem is setup in order that 720p raw-bayer camera sensor output is reduced to 320x176 using crop (downscale is not possible with raw-bayer):
media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:SBGGR8_1X8/1280x720@1/15 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'st-mipid02 1-0014':2[fmt:SBGGR8_1X8/1280x720]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':1[fmt:SBGGR8_1X8/1280x720]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:SBGGR8_1X8/1280x720]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(160,92)/320x176]"
Then GStreamer is used to grab frames on disk while previewing:
gst-launch-1.0 v4l2src num-buffers=100 ! "video/x-bayer, format=bggr, width=320,height=176, framerate=(fraction)30/1" ! queue ! tee name=tee ! queue ! fpsdisplaysink name="capturerate" sync=false text-overlay=false video-sink="multifilesink location=320x180_%d-bayer.raw max-files=10" tee. ! queue ! videorate max-rate=15 ! bayer2rgb ! queue ! videoconvert ! queue ! waylandsink sync=false -v
|
5. How to trace and debug[edit | edit source]
5.1. How to monitor[edit | edit source]
5.1.1. Check of devicetree configuration[edit | edit source]
Here are some commands to verify that DCMIPP is enabled, check which camera sensor is used and log other details about devicetree configuration:
cd ~ # go to $HOME directory
echo "#!/bin/bash" > dtdumpentry.sh;echo "hexdump -e '\"=\"' -e '20/1 \"%c\"\"\t\"' -e '20/1 \"%02x\"\"\n\"' \$1" >> dtdumpentry.sh;chmod +x dtdumpentry.sh
echo "#!/bin/bash" > dtdump.sh;echo "find \$1* -type f -print0 -exec ./dtdumpentry.sh {} \;" >> dtdump.sh;chmod +x dtdump.sh
cd ~ # go to $HOME directory
rm ~/devicetree.txt
echo "[devicetree]" >> ~/devicetree.txt
echo "|-[dcmipp]" >> devicetree.txt
./dtdump.sh /proc/device-tree/soc/bus@5c007000/dcmipp@5a000000 | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt
echo "|" >> devicetree.txt
echo "|-[camera:" | tr -d "\n" >> devicetree.txt
cat /proc/device-tree/soc/bus@5c007000/i2c*/camera*/compatible >> devicetree.txt
echo "]" >> devicetree.txt
./dtdump.sh /proc/device-tree/soc/bus@5c007000/i2c*/camera* -type f -print0 -exec ./dtdump.sh {} \; | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt
echo "|" >> devicetree.txt
echo "|-[mipi bridge:" | tr -d "\n" >> devicetree.txt
cat /proc/device-tree/soc/bus@5c007000/i2c*/*mipi*/compatible >> devicetree.txt
echo "]" >> devicetree.txt
./dtdump.sh /proc/device-tree/soc/bus@5c007000/i2c*/*mipi* -type f -print0 -exec ./dtdump.sh {} \; | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt
echo "" >> devicetree.txt
cat ~/devicetree.txt # or cat -t ~/devicetree.txt
[devicetree]
|-[dcmipp]
| |-bus@5c007000/dcmipp@5a000000/compatible=st,stm32mp13-dcmipp 73742c73746d33326d7031332d64636d69707000
| |-bus@5c007000/dcmipp@5a000000/clocks=�� 000000060000008f
| |-bus@5c007000/dcmipp@5a000000/access-controllers='� 0000002700000004
| |-bus@5c007000/dcmipp@5a000000/resets=�5� 00000006000035c1
| |-bus@5c007000/dcmipp@5a000000/pinctrl-1=` 00000060
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/hsync-active= 00000000
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/vsync-active= 00000000
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/remote-endpoint=a 00000061
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/pclk-max-frequency=' 07270e00
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/bus-width= 00000008
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/pclk-sample= 00000000
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/phandle=< 0000003c
| |-bus@5c007000/dcmipp@5a000000/port/endpoint/name=endpoint 656e64706f696e7400
| |-bus@5c007000/dcmipp@5a000000/port/name=port 706f727400
| |-bus@5c007000/dcmipp@5a000000/clock-names=kclk 6b636c6b00
| |-bus@5c007000/dcmipp@5a000000/status=okay 6f6b617900
| |-bus@5c007000/dcmipp@5a000000/interrupts=O� 000000000000004f00000004
| |-bus@5c007000/dcmipp@5a000000/phandle=� 000000cf
| |-bus@5c007000/dcmipp@5a000000/reg=Z� 5a00000000000400
| |-bus@5c007000/dcmipp@5a000000/pinctrl-0=_ 0000005f
| |-bus@5c007000/dcmipp@5a000000/name=dcmipp 64636d69707000
| |-bus@5c007000/dcmipp@5a000000/pinctrl-names=defaultsleep 64656661756c7400736c65657000
|
|-[camera:ovti,ov5640]
| |-bus@5c007000/i2c@4c006000/camera@3c/compatible=ovti,ov5640 6f7674692c6f763536343000
| |-bus@5c007000/i2c@4c006000/camera@3c/powerdown-gpios=3�� 000000330000000300000001
| |-bus@5c007000/i2c@4c006000/camera@3c/DOVDD-supply=% 00000025
| |-bus@5c007000/i2c@4c006000/camera@3c/clocks== 0000003d
| |-bus@5c007000/i2c@4c006000/camera@3c/port/endpoint/data-lanes=�� 0000000100000002
| |-bus@5c007000/i2c@4c006000/camera@3c/port/endpoint/clock-lanes= 00000000
| |-bus@5c007000/i2c@4c006000/camera@3c/port/endpoint/phandle=ϻ 000000bb
| |-bus@5c007000/i2c@4c006000/camera@3c/port/endpoint/name=endpoint 656e64706f696e7400
| |-bus@5c007000/i2c@4c006000/camera@3c/port/name=port 706f727400
| |-bus@5c007000/i2c@4c006000/camera@3c/clock-names=xclk 78636c6b00
| |-bus@5c007000/i2c@4c006000/camera@3c/status=disabled 64697361626c656400
| |-bus@5c007000/i2c@4c006000/camera@3c/reset-gpios=3�� 000000330000000400000001
| |-bus@5c007000/i2c@4c006000/camera@3c/phandle=� 000000ba
| |-bus@5c007000/i2c@4c006000/camera@3c/reg=< 0000003c
| |-bus@5c007000/i2c@4c006000/camera@3c/name=camera 63616d65726100
|
|-[mipi bridge:st,st-mipid02]
| |-bus@5c007000/i2c@4c006000/stmipi@14/compatible=st,st-mipid02 73742c73742d6d69706964303200
| |-bus@5c007000/i2c@4c006000/stmipi@14/clocks=9 00000039
| |-bus@5c007000/i2c@4c006000/stmipi@14/VDDIN-supply=: 0000003a
| |-bus@5c007000/i2c@4c006000/stmipi@14/clock-names=xclk 78636c6b00
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/#address-cells=� 00000001
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/#size-cells= 00000000
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/endpoint/hsync-active= 00000000
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/endpoint/vsync-active= 00000000
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/endpoint/remote-endpoint=< 0000003c
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/endpoint/bus-width=00000008
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/endpoint/pclk-sample= 00000000
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/endpoint/phandle=a 00000061
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/endpoint/name=endpoint 656e64706f696e7400
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/reg=� 00000002
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@2/name=port 706f727400
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@0/endpoint/remote-endpoint=; 0000003b
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@0/endpoint/data-lanes=�� 0000000100000002
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@0/endpoint/phandle=> 0000003e
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@0/endpoint/lane-polarities= 000000000000000000000000
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@0/endpoint/name=endpoint 656e64706f696e7400
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@0/reg= 00000000
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/port@0/name=port 706f727400
| |-bus@5c007000/i2c@4c006000/stmipi@14/ports/name=ports 706f72747300
| |-bus@5c007000/i2c@4c006000/stmipi@14/status=okay 6f6b617900
| |-bus@5c007000/i2c@4c006000/stmipi@14/reset-gpios=3�� 000000330000000200000001
| |-bus@5c007000/i2c@4c006000/stmipi@14/VDDE-supply=: 0000003a
| |-bus@5c007000/i2c@4c006000/stmipi@14/phandle=� 000000b8
| |-bus@5c007000/i2c@4c006000/stmipi@14/reg=� 00000014
| |-bus@5c007000/i2c@4c006000/stmipi@14/name=stmipi 73746d69706900
5.1.2. Camera subsystem configuration debugging[edit | edit source]
Refer to section #Get the topology of camera subsystem for basics on how to get and set camera subsystem configuration. Find below some debugging tips to help configuration handling.
5.1.2.1. subdevice configuration syntax error[edit | edit source]
media-ctl utility returns an error when a configuration syntax mistake is made. Example here with erroneous entity name:
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postpr':0[fmt:RGB565_2X8_LE/640x480]"
Unable to setup formats: Invalid argument (22)
In order to have details on the exact error, add -v option:
-v no such entity "dcmipp_dump_postpr" 'dcmipp_dump_postpr':0[fmt:RGB565_2X8_LE/640x480] ^media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postpr':0[fmt:RGB565_2X8_LE/640x480]"
Another example with pad number mistake (only pad number 0 or 1 are allowed):
-v No pad '4' on entity "dcmipp_dump_postproc". Maximum pad number is 1 'dcmipp_dump_postproc':4[fmt:RGB565_2X8_LE/640x480] ^media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':4[fmt:RGB565_2X8_LE/640x480]"
Example with format mistake (BA81 is a raw-bayer V4L2 pixel format while subdevice expects V4L2 mbus code such as SBGGR8_1X8):
-v Invalid pixel code 'BA81' 'dcmipp_dump_postproc':0[fmt:BA81/640x480] ^media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:BA81/640x480]"
5.1.2.2. subdevice negotiation[edit | edit source]
Requested configuration may not be fully accepted by the subdevice, in this case, the subdevice configures itself with the part of configuration it can handle. media-ctl -v option when setting configuration shows the effective subdevice configuration.
Here is an example with 5 fps framerate not accepted by the subdevice and 30 fps selected instead:
1/5 field:none]" -v Setting up format RGB565_2X8_BE 640x480 on pad gc2145 1-003c/0 Format set: RGB565_2X8_BE 640x480 Setting up frame interval 1/5 on pad gc2145 1-003c/0 Frame interval set: 1/30media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_2X8_BE/640x480@
Example with resolution negotiation (4000x4000 reduced to 2592x1944)
4000x4000@1/15 field:none]" -v Setting up format RGB565_2X8_BE 4000x4000 on pad gc2145 1-003c/0 Format set: RGB565_2X8_BE 1600x1200media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_2X8_BE/
Example with format negotiation (AYUV8_1X32 not supported, defaults to RGB565_2X8_LE):
AYUV8_1X32/640x480]" -v Setting up format AYUV8_1X32 640x480 on pad dcmipp_dump_postproc/0 Format set: RGB565_2X8_LEmedia-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:
5.2. How to trace[edit | edit source]
5.2.1. V4L2 userland API tracing[edit | edit source]
Tracing of V4L2 userland API[3] can be enabled using command:
echo 0x3 > devices/platform/soc/5c007000.etzpc/5a000000.dcmipp/video4linux/video0/dev_debug
Traces are output in kernel log buffer:
dmesg
[ 655.479016] video0: VIDIOC_QUERYCAP: driver=dcmipp, card=dcmipp_bytecap, bus=platform:dcmipp, version=0x00050f00, capabilities=0x852000011
[ 655.481591] video0: VIDIOC_G_FMT: type=vid-cap, width=640, height=480, pixelformat=RGBP little-endian (0x50424752), field=none, bytesperl0
[ 655.481656] video0: VIDIOC_ENUM_FMT: index=0, type=vid-cap, flags=0x0, pixelformat=RGBP little-endian (0x50424752), mbus_code=0x0000, des'
[ 655.481696] video0: VIDIOC_ENUM_FMT: index=1, type=vid-cap, flags=0x0, pixelformat=YUYV little-endian (0x56595559), mbus_code=0x0000, des'
[ 655.481732] video0: VIDIOC_ENUM_FMT: index=2, type=vid-cap, flags=0x0, pixelformat=YVYU little-endian (0x55595659), mbus_code=0x0000, des'
[ 655.481767] video0: VIDIOC_ENUM_FMT: index=3, type=vid-cap, flags=0x0, pixelformat=UYVY little-endian (0x59565955), mbus_code=0x0000, des'
[ 655.481802] video0: VIDIOC_ENUM_FMT: index=4, type=vid-cap, flags=0x0, pixelformat=VYUY little-endian (0x59555956), mbus_code=0x0000, des'
[ 655.481836] video0: VIDIOC_ENUM_FMT: index=5, type=vid-cap, flags=0x0, pixelformat=GREY little-endian (0x59455247), mbus_code=0x0000, des'
[ 655.481873] video0: VIDIOC_ENUM_FMT: index=6, type=vid-cap, flags=0x0, pixelformat=BA81 little-endian (0x31384142), mbus_code=0x0000, des'
[ 655.481909] video0: VIDIOC_ENUM_FMT: index=7, type=vid-cap, flags=0x0, pixelformat=GBRG little-endian (0x47524247), mbus_code=0x0000, des'
[ 655.481944] video0: VIDIOC_ENUM_FMT: index=8, type=vid-cap, flags=0x0, pixelformat=GRBG little-endian (0x47425247), mbus_code=0x0000, des'
[ 655.481981] video0: VIDIOC_ENUM_FMT: index=9, type=vid-cap, flags=0x0, pixelformat=RGGB little-endian (0x42474752), mbus_code=0x0000, des'
[ 655.482017] video0: VIDIOC_ENUM_FMT: index=10, type=vid-cap, flags=0x1, pixelformat=JPEG little-endian (0x4745504a), mbus_code=0x0000, de'
[ 655.482061] video0: VIDIOC_S_FMT: type=vid-cap, width=2592, height=1952, pixelformat=JPEG little-endian (0x4745504a), field=none, bytespe0
[ 655.526124] video0: VIDIOC_REQBUFS: count=4, type=vid-cap, memory=mmap
[ 655.526221] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=0, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4
[ 655.526272] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[ 655.526296] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=1, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4
[ 655.526339] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[ 655.526359] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=2, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4
[ 655.526401] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[ 655.526420] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=3, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4
[ 655.526462] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
[ 655.527192] video0: VIDIOC_G_FMT: type=vid-cap, width=2592, height=1952, pixelformat=JPEG little-endian (0x4745504a), field=none, bytespe0
[ 655.536625] video0: VIDIOC_STREAMON: type=vid-cap
[ 655.536701] video0: VIDIOC_G_FMT: type=vid-cap, width=2592, height=1952, pixelformat=JPEG little-endian (0x4745504a), field=none, bytespe0
[ 655.892309] video0: VIDIOC_STREAMOFF: type=vid-cap
[ 655.892435] video0: VIDIOC_STREAMOFF: type=vid-cap
[ 655.901481] video0: VIDIOC_REQBUFS: count=0, type=vid-cap, memory=mmap
5.2.2. V4L2 core framework tracing[edit | edit source]
Tracing of the V4L2 core framework[4] can be enabled using commands:
echo 0x3 > /sys/module/videobuf2_common/parameters/debug
echo 0x3 > /sys/module/videobuf2_v4l2/parameters/debug
Traces are output in kernel log buffer:
dmesg
[ 1218.626235] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 0, plane 0 offset 0x00000000
[ 1218.642445] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 1, plane 0 offset 0x004d4000
[ 1218.656398] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 2, plane 0 offset 0x009a8000
[ 1218.669843] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 3, plane 0 offset 0x00e7c000
[ 1218.677503] videobuf2_common: [cap-7b50f8bf] __vb2_queue_alloc: allocated 4 buffers, 1 plane(s) each
[ 1218.688361] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 0, plane 0 successfully mapped
[ 1218.696744] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 1, plane 0 successfully mapped
[ 1218.705291] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 2, plane 0 successfully mapped
[ 1218.712487] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 3, plane 0 successfully mapped
[ 1218.722474] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 0 succeeded
[ 1218.730528] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 1 succeeded
[ 1218.738153] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 2 succeeded
[ 1218.746012] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 3 succeeded
[ 1218.756237] videobuf2_common: [cap-7b50f8bf] vb2_core_streamon: successful
[ 1218.761969] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers
[ 1218.822167] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer
[ 1218.828383] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 0, state: dequeued
[ 1218.838812] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 0 succeeded
[ 1218.846549] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers
[ 1218.855624] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer
[ 1218.862118] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 1, state: dequeued
[ 1218.872406] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 1 succeeded
[ 1218.880029] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers
[ 1218.889460] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer
[ 1218.896756] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 2, state: dequeued
[ 1218.905383] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 2 succeeded
[ 1218.912309] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers
[ 1218.923080] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer
[ 1218.930392] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 3, state: dequeued
[ 1218.944499] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 3 succeeded
[ 1218.952210] videobuf2_common: [cap-7b50f8bf] vb2_core_streamoff: successful
[ 1218.959921] videobuf2_common: [cap-7b50f8bf] vb2_core_streamoff: successful
[ 1218.968800] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 0
[ 1218.978419] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 1
[ 1218.988204] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 2
[ 1218.997501] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 3
5.2.3. DCMIPP V4L2 kernel driver tracing[edit | edit source]
DCMIPP dynamic debug traces[8] can be enabled using command:
echo "module stm32_dcmipp +p" > /sys/kernel/debug/dynamic_debug/control
Here is an example with a 5Mp jpeg capture:
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_2X8_BE/640x480@1/30 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':0[fmt:RGB565_2X8_BE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_input':0[fmt:RGB565_2X8_LE/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:RGB565_2X8_LE/640x480]"
v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=RGBP --stream-mmap --stream-count=1 --stream-to=grab-640x480-rgb565.raw
dmesg
[ 6185.212240] dcmipp 5a000000.dcmipp: dcmipp_dump_capture: format update: old:480x272 (0x50424752, 8, 1, 2, 0) new:640x480 (0x50424752, 8, 1, 2, 0)
[ 6185.212629] dcmipp 5a000000.dcmipp: Setup queue, count=4, size=614400
[ 6185.216997] dcmipp 5a000000.dcmipp: Setup [0] phy=0xd8a00000 size=614400
[ 6185.217059] dcmipp 5a000000.dcmipp: Setup [1] phy=0xd8b00000 size=614400
[ 6185.217082] dcmipp 5a000000.dcmipp: Setup [2] phy=0xd8c00000 size=614400
[ 6185.217102] dcmipp 5a000000.dcmipp: Setup [3] phy=0xd8d00000 size=614400
[ 6185.217137] dcmipp 5a000000.dcmipp: Queue [0] d8b69f13 phy=0xd8a00000
[ 6185.217158] dcmipp 5a000000.dcmipp: Queue [1] b0942ca1 phy=0xd8b00000
[ 6185.217171] dcmipp 5a000000.dcmipp: Queue [2] 2d865547 phy=0xd8c00000
[ 6185.217183] dcmipp 5a000000.dcmipp: Queue [3] a70ff5be phy=0xd8d00000
[ 6185.217343] dcmipp 5a000000.dcmipp: CLR DCMIPP_P0FCTCR 0x00000003
[ 6185.217363] dcmipp 5a000000.dcmipp: WR DCMIPP_P0FCTCR 0x00000000
[ 6185.217374] dcmipp 5a000000.dcmipp: SET DCMIPP_P0FCTCR 0x00000000
[ 6185.217384] dcmipp 5a000000.dcmipp: WR DCMIPP_P0FCTCR 0x00000000
[ 6185.217395] dcmipp 5a000000.dcmipp: CLR DCMIPP_P0PPCR 0x00000180
[ 6185.217405] dcmipp 5a000000.dcmipp: WR DCMIPP_P0PPCR 0x00000000
[ 6185.217416] dcmipp 5a000000.dcmipp: CLR DCMIPP_P0PPCR 0x00000400
[ 6185.217426] dcmipp 5a000000.dcmipp: WR DCMIPP_P0PPCR 0x00000000
[ 6185.217436] dcmipp 5a000000.dcmipp: WR DCMIPP_P0SCSTR 0x00000000
[ 6185.217446] dcmipp 5a000000.dcmipp: WR DCMIPP_P0SCSZR 0x00000000
[ 6185.217457] dcmipp 5a000000.dcmipp: crop to 640x480
[ 6185.217468] dcmipp 5a000000.dcmipp: WR DCMIPP_P0SCSTR 0x00000000
[ 6185.217478] dcmipp 5a000000.dcmipp: WR DCMIPP_P0SCSZR 0x81e00140
[ 6185.217489] dcmipp 5a000000.dcmipp: "dcmipp_dump_postproc" is started
[ 6185.217502] dcmipp 5a000000.dcmipp: WR DCMIPP_PRCR 0x02220000
[ 6185.217513] dcmipp 5a000000.dcmipp: WR DCMIPP_CMCR 0x00000000
[ 6185.217524] dcmipp 5a000000.dcmipp: SET DCMIPP_PRCR 0x00004000
[ 6185.217535] dcmipp 5a000000.dcmipp: WR DCMIPP_PRCR 0x02224000
[ 6185.217545] dcmipp 5a000000.dcmipp: "dcmipp_input" is started
[ 6185.219357] dcmipp 5a000000.dcmipp: "st-mipid02 1-0014" is started
[ 6185.375507] dcmipp 5a000000.dcmipp: "gc2145 1-003c" is started
[ 6185.375543] dcmipp 5a000000.dcmipp: SET DCMIPP_P0FSCR 0x80000000
[ 6185.375560] dcmipp 5a000000.dcmipp: WR DCMIPP_P0FSCR 0x80000000
[ 6185.375572] dcmipp 5a000000.dcmipp: Start with next [0] d8b69f13 phy=0xd8a00000
[ 6185.375592] dcmipp 5a000000.dcmipp: WR DCMIPP_P0PPM0AR1 0xd8a00000
[ 6185.375602] dcmipp 5a000000.dcmipp: Write [0] d8b69f13 phy=0xd8a00000
[ 6185.375615] dcmipp 5a000000.dcmipp: WR DCMIPP_P0DCLMTR 0x80025800
[ 6185.375625] dcmipp 5a000000.dcmipp: SET DCMIPP_P0FCTCR 0x00000008
[ 6185.375635] dcmipp 5a000000.dcmipp: WR DCMIPP_P0FCTCR 0x00000008
[ 6185.375646] dcmipp 5a000000.dcmipp: SET DCMIPP_CMIER 0x00008600
[ 6185.375656] dcmipp 5a000000.dcmipp: WR DCMIPP_CMIER 0x00008600
[ 6185.626841] dcmipp 5a000000.dcmipp: RD DCMIPP_CMSR2 0x00000500
[ 6185.626890] dcmipp 5a000000.dcmipp: WR DCMIPP_CMFCR 0x00000400
[ 6185.626985] dcmipp 5a000000.dcmipp: WR DCMIPP_P0PPM0AR1 0xd8b00000
[ 6185.627012] dcmipp 5a000000.dcmipp: Write [1] b0942ca1 phy=0xd8b00000
[ 6185.660542] dcmipp 5a000000.dcmipp: RD DCMIPP_CMSR2 0x00000300
[ 6185.660591] dcmipp 5a000000.dcmipp: WR DCMIPP_CMFCR 0x00000200
[ 6185.660652] dcmipp 5a000000.dcmipp: RD DCMIPP_P0DCCNTR 0x00096000
[ 6185.660693] dcmipp 5a000000.dcmipp: Done [0] d8b69f13 phy=0xd8a00000
[ 6185.660821] dcmipp 5a000000.dcmipp: Queue [0] d8b69f13 phy=0xd8a00000
[ 6185.660953] dcmipp 5a000000.dcmipp: "dcmipp_dump_postproc" is stopped
[ 6185.660978] dcmipp 5a000000.dcmipp: CLR DCMIPP_PRCR 0x00004000
[ 6185.660998] dcmipp 5a000000.dcmipp: WR DCMIPP_PRCR 0x02220000
[ 6185.661014] dcmipp 5a000000.dcmipp: "dcmipp_input" is stopped
[ 6185.662357] dcmipp 5a000000.dcmipp: "st-mipid02 1-0014" is stopped
[ 6185.662419] dcmipp 5a000000.dcmipp: "gc2145 1-003c" is stopped
[ 6185.662454] dcmipp 5a000000.dcmipp: CLR DCMIPP_CMIER 0x00008600
[ 6185.662474] dcmipp 5a000000.dcmipp: WR DCMIPP_CMIER 0x00000000
[ 6185.662491] dcmipp 5a000000.dcmipp: CLR DCMIPP_P0FCTCR 0x00000008
[ 6185.662506] dcmipp 5a000000.dcmipp: WR DCMIPP_P0FCTCR 0x00000000
[ 6185.662523] dcmipp 5a000000.dcmipp: CLR DCMIPP_P0FSCR 0x80000000
[ 6185.662539] dcmipp 5a000000.dcmipp: WR DCMIPP_P0FSCR 0x00000000
[ 6185.662566] dcmipp 5a000000.dcmipp: RD DCMIPP_PRSR 0x00030000
[ 6185.662582] dcmipp 5a000000.dcmipp: [DCMIPP_PRSR] =0x00030000
[ 6185.662597] dcmipp 5a000000.dcmipp: RD DCMIPP_P0SR 0x00000007
[ 6185.662612] dcmipp 5a000000.dcmipp: [DCMIPP_P0SR] =0x00000007
[ 6185.662627] dcmipp 5a000000.dcmipp: RD DCMIPP_P0DCCNTR 0x00096000
[ 6185.662642] dcmipp 5a000000.dcmipp: [DCMIPP_P0DCCNTR]=0x00096000
[ 6185.662657] dcmipp 5a000000.dcmipp: RD DCMIPP_CMSR1 0x00000003
[ 6185.662672] dcmipp 5a000000.dcmipp: [DCMIPP_CMSR1] =0x00000003
[ 6185.662686] dcmipp 5a000000.dcmipp: RD DCMIPP_CMSR2 0x00000100
[ 6185.662701] dcmipp 5a000000.dcmipp: [DCMIPP_CMSR2] =0x00000100
[ 6185.662722] dcmipp 5a000000.dcmipp: Stop streaming, errors=0 (overrun=0, limit=0, nactive=0), underrun=0, vsync=1, frame=1, buffers=1, it=2
5.3. How to debug[edit | edit source]
5.3.1. Errors[edit | edit source]
Errors are unconditionally traced in kernel log:
dmesg
[ 1947.932915] dcmipp-bytecap dcmipp-bytecap.3.auto: Stop streaming, errors=1 (overrun=0, limit=0), vsync=2, frame=2, buffers=2, it=4
5.3.2. Memory tracking[edit | edit source]
Frames require large chunks of contiguous memory. They are allocated by V4L2 framework through DMA backend. Those allocations can be traced using:
echo "module dma_contiguous +p" > /sys/kernel/debug/dynamic_debug/control
echo "module videobuf2_dma_contig +p" > /sys/kernel/debug/dynamic_debug/control
Here is the trace after a VGA YUV422 capture.
[11311.617688] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb3b6a000, size 614400
[11311.617986] vb2_dc_mmap: mapped dma addr 0xf1a00000 at 0xb3ad4000, size 614400
[11311.618071] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb3a3e000, size 614400
[11311.764146] vb2_dc_mmap: mapped dma addr 0xf1c00000 at 0xb307c000, size 614400
4 frames of VGA YUV422 frames: 640x480x2=614400 bytes
6. Source code location[edit | edit source]
6.1. User space[edit | edit source]
6.2. Kernel space[edit | edit source]
- V4L2 core source code
- stm32-dcmipp V4L2 driver source code
- i2c camera sensor V4L2 drivers source code
7. References[edit | edit source]
- ↑ Information about V4L2 Linux kernel framework on wikipedia.
- ↑ Jump up to: 2.0 2.1 Linux Media Infrastructure userspace API » Part IV - Media Controller API
- ↑ Jump up to: 3.0 3.1 3.2 3.3 Linux Media Infrastructure userspace API » Part I - Video for Linux API
- ↑ Jump up to: 4.0 4.1 Media subsystem kernel internal API » 1. Video4Linux devices
- ↑ MB1897 camera daughter board
- ↑ Jump up to: 6.0 6.1 6.2 CN1 Camera sensor connector
- ↑ Linux Media Infrastructure userspace API » Part I - Video for Linux API » 4. Interfaces » 4.13. Sub-device Interface » 4.13.3.2. Selections: cropping, scaling and composition
- ↑ How to use the kernel dynamic debug