Registered User mNo edit summary |
Registered User mNo edit summary Tag: 2017 source edit |
||
(9 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x,STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}}</noinclude> | }} | ||
<noinclude></noinclude> | |||
== Article purpose == | == Article purpose == | ||
This article explains how to measure the overall DDR throughput generated during a Linux<sup>®</sup> user space command execution. | This article explains how to measure the overall DDR throughput generated during a Linux<sup>®</sup> user space command execution. | ||
Line 13: | Line 14: | ||
Once recorded, the '''stm32_ddr_pmu.py''' Python script is used to compute the corresponding DDR throughputs. | Once recorded, the '''stm32_ddr_pmu.py''' Python script is used to compute the corresponding DDR throughputs. | ||
Launching this script without any parameter returns the usage information: | Launching this script without any parameter returns the usage information (frequency, bursts length and word length are automatically detected on our platforms): | ||
{{Board$}} python3 /usr/bin/stm32_ddr_pmu.py | {{Board$}}python3 /usr/bin/stm32_ddr_pmu.py | ||
Found ddr frequency of 533.0 MHz | |||
Usage: | Usage: | ||
python stm32_ddr_pmu.py -f <perf_file> [-d <ddr_freq>] [-w <word_length>] [-l <burst_length>] | |||
-h: print this help | |||
-d ddr_freq: DDR frequency in MHz (533.0 MHz by default) | |||
-w word_length: width in bytes of DDR bus (4 by default) | |||
-l burst_length: length in cycles of DDR burst (8 by default) | |||
-f perf_file: text file containing the output of a perf stat command | |||
MP1: perf stat -e stm32_ddr_pmu/perf_op_is_rd/,\ | |||
stm32_ddr_pmu/perf_op_is_wr/,\ | |||
stm32_ddr_pmu/time_cnt/ -C 0 -o <perf_file> <command> | |||
MP2: perf stat -e stm32_ddr_pmu/dfi_is_rd/,\ | |||
stm32_ddr_pmu/dfi_is_wr/,\ | |||
stm32_ddr_pmu/dfi_is_rda/,\ | |||
stm32_ddr_pmu/dfi_is_wra/,\ | |||
stm32_ddr_pmu/dfi_is_mwra/,\ | |||
stm32_ddr_pmu/dfi_is_mwr/,\ | |||
stm32_ddr_pmu/time_cnt/ -C 0 -o <perf_file> <command> | |||
The script considers bursts of 8 words with 4 bytes per word. | |||
{{Info | The stm32_ddr_pmu driver is compiled as a kernel module (stm32_ddr_pmu.ko) that may not be automatically probed at startup. If 'lsmod' command does not show this module, then make sure that ddrperfm node is enabled in the device tree and run the command 'modprobe stm32_ddr_pmu' to get it properly loaded.}} | {{Info | The stm32_ddr_pmu driver is compiled as a kernel module (stm32_ddr_pmu.ko) that may not be automatically probed at startup. If 'lsmod' command does not show this module, then make sure that ddrperfm node is enabled in the device tree and run the command 'modprobe stm32_ddr_pmu' to get it properly loaded.}} | ||
== Example == | == Example == | ||
Let us see how to measure the DDR throughput generated during the 'sleep 1' command execution. | Let us see how to measure the DDR throughput generated during the 'sleep 1' command execution on a MP2 board. | ||
First, record the counters into 'perf.txt' file, providing the command to launch as parameter: | First, record the counters into 'perf.txt' file, providing the command to launch as parameter: | ||
{{Board$}} perf stat -e stm32_ddr_pmu/ | {{Board$}}perf stat -e stm32_ddr_pmu/dfi_is_rd/,\ | ||
stm32_ddr_pmu/dfi_is_wr/,\ | |||
stm32_ddr_pmu/dfi_is_rda/,\ | |||
stm32_ddr_pmu/dfi_is_wra/,\ | |||
stm32_ddr_pmu/dfi_is_mwra/,\ | |||
stm32_ddr_pmu/dfi_is_mwr/,\ | |||
stm32_ddr_pmu/time_cnt/ -C 0 -o '''perf.txt''' '''sleep 1''' | |||
Then, run the Python script to convert the result in throughput values: | Then, run the Python script to convert the result in throughput values: | ||
{{Board$}} python3 /usr/bin/stm32_ddr_pmu.py -f '''perf.txt''' | {{Board$}}python3 /usr/bin/stm32_ddr_pmu.py -f '''perf.txt''' | ||
R = 8 MB/s, W = 2 MB/s, R&W = 9 MB/s (DDR @ | R = 8 MB/s, W = 2 MB/s, R&W = 9 MB/s (DDR @ 800 MHz) | ||
== References == | == References == | ||
Line 40: | Line 61: | ||
<noinclude> | <noinclude> | ||
[[Category:How to trace and debug]] | [[Category:How to trace and debug]] | ||
{{PublicationRequestId | 20448| 2021-07-05}} | {{PublicationRequestId | 20448| 2021-07-05}} | ||
</noinclude> | </noinclude> |
Latest revision as of 11:19, 28 October 2024
1. Article purpose[edit | edit source]
This article explains how to measure the overall DDR throughput generated during a Linux® user space command execution.
2. Measurement flow[edit | edit source]
The DDR throughput measurement is done via counters provided by the DDRPERFM internal peripheral and controlled by stm32_ddr_pmu[1] performance monitoring unit driver that is registered to the Linux kernel perf framework.
From user land side, the perf tool is used to interact with the perf framework in order to record given events (such as stm32_ddr_pmu) during a command execution.
Once recorded, the stm32_ddr_pmu.py Python script is used to compute the corresponding DDR throughputs.
Launching this script without any parameter returns the usage information (frequency, bursts length and word length are automatically detected on our platforms):
DDR frequency in MHz (533.0 MHz by default) -w word_length: width in bytes of DDR bus (4 by default) -l burst_length: length in cycles of DDR burst (8 by default) -f perf_file: text file containing the output of a perf stat command MP1: perf stat -e stm32_ddr_pmu/perf_op_is_rd/,\ stm32_ddr_pmu/perf_op_is_wr/,\ stm32_ddr_pmu/time_cnt/ -C 0 -o <perf_file> <command> MP2: perf stat -e stm32_ddr_pmu/dfi_is_rd/,\ stm32_ddr_pmu/dfi_is_wr/,\ stm32_ddr_pmu/dfi_is_rda/,\ stm32_ddr_pmu/dfi_is_wra/,\ stm32_ddr_pmu/dfi_is_mwra/,\ stm32_ddr_pmu/dfi_is_mwr/,\ stm32_ddr_pmu/time_cnt/ -C 0 -o <perf_file> <command> The script considers bursts of 8 words with 4 bytes per word.Board $>python3 /usr/bin/stm32_ddr_pmu.py Found ddr frequency of 533.0 MHz Usage: python stm32_ddr_pmu.py -f <perf_file> [-d <ddr_freq>] [-w <word_length>] [-l <burst_length>] -h: print this help -d ddr_freq:
3. Example[edit | edit source]
Let us see how to measure the DDR throughput generated during the 'sleep 1' command execution on a MP2 board.
First, record the counters into 'perf.txt' file, providing the command to launch as parameter:
Board $>perf stat -e stm32_ddr_pmu/dfi_is_rd/,\
stm32_ddr_pmu/dfi_is_wr/,\
stm32_ddr_pmu/dfi_is_rda/,\
stm32_ddr_pmu/dfi_is_wra/,\
stm32_ddr_pmu/dfi_is_mwra/,\
stm32_ddr_pmu/dfi_is_mwr/,\
stm32_ddr_pmu/time_cnt/ -C 0 -o perf.txt sleep 1
Then, run the Python script to convert the result in throughput values:
DDR @ 800 MHz)Board $>python3 /usr/bin/stm32_ddr_pmu.py -f perf.txt R = 8 MB/s, W = 2 MB/s, R&W = 9 MB/s (
4. References[edit | edit source]