Registered User mNo edit summary |
Registered User m (→Compilation) Tag: 2017 source edit |
||
(4 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude>{{ApplicableFor | ||
|MPUs list=STM32MP13x | |MPUs list=STM32MP13x | ||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}}</noinclude> | }}</noinclude> | ||
This article briefly describes the {{MicroprocessorDevice | device=13}} support in [[U-Boot_overview|U-Boot]]. | This article briefly describes the {{MicroprocessorDevice | device=13}} support in [[U-Boot_overview|U-Boot]]. | ||
Line 46: | Line 46: | ||
For {{Board | type=135F-DK}}, the device tree is already selected in defconfig {{HighlightParam|stm32mp13_defconfig}} | For {{Board | type=135F-DK}}, the device tree is already selected in defconfig {{HighlightParam|stm32mp13_defconfig}} | ||
{{PC$}} make {{HighlightParam|stm32mp13_defconfig}} | {{PC$}}make {{HighlightParam|stm32mp13_defconfig}} | ||
{{PC$}} make all | {{PC$}}make all | ||
For other boards, you need to select the correct device tree | For other boards, you need to select the correct device tree | ||
{{PC$}} make {{HighlightParam|stm32mp13_defconfig}} | {{PC$}}make {{HighlightParam|stm32mp13_defconfig}} | ||
{{PC$}} make DEVICE_TREE={{HighlightParam|<Device tree>}} all | {{PC$}}make DEVICE_TREE={{HighlightParam|<Device tree>}} all | ||
The supported variables are: | The supported variables are: | ||
Line 58: | Line 58: | ||
* '''KBUILD_OUTPUT''': change the destination directory for the build | * '''KBUILD_OUTPUT''': change the destination directory for the build | ||
* '''EXT_DTB''': select external device tree. | * '''EXT_DTB''': select external device tree. | ||
* '''EXT_DTS''': select PATH of external device tree source, by default the sub-directory "arch/arm/dts/external-dt" is used to allow sub-module. | |||
The output files {{Highlight|'''u-boot.dtb'''}} and {{Highlight|'''u-boot-nodtb.bin'''}} are integrated in [[#U- | The output files {{Highlight|'''u-boot.dtb'''}} and {{Highlight|'''u-boot-nodtb.bin'''}} are integrated in [[U-Boot_overview#U-Boot_integration_in_FIP|TF-A FIP]]. | ||
Note: All the compiled devices trees are available in $KBUILD_OUTPUT/arch/arm/dts/*.dtb.<br/>You can select them instead of {{Highlight|u-boot.dtb}} without U-Boot recompilation. | Note: All the compiled devices trees are available in $KBUILD_OUTPUT/arch/arm/dts/*.dtb.<br/>You can select them instead of {{Highlight|u-boot.dtb}} without U-Boot recompilation. | ||
== Examples == | == Examples == | ||
=== {{Board | type=135F-DK}} === | === {{Board | type=135F-DK}} === | ||
{{PC$}} make {{HighlightParam|stm32mp13_defconfig}} | {{PC$}}make {{HighlightParam|stm32mp13_defconfig}} | ||
{{PC$}} make all | {{PC$}}make all | ||
or | or | ||
{{PC$}} make {{HighlightParam|stm32mp13_defconfig}} | {{PC$}}make {{HighlightParam|stm32mp13_defconfig}} | ||
{{PC$}} make DEVICE_TREE={{HighlightParam|stm32mp135f-dk}} all | {{PC$}}make DEVICE_TREE={{HighlightParam|stm32mp135f-dk}} all | ||
and | and | ||
{{PC$}} fiptool --verbose update {{HighlightParam|--nt-fw}} {{Highlight|u-boot-nodtb.bin}} {{HighlightParam|--hw-config}} {{Highlight|u-boot.dtb}} \ | {{PC$}}fiptool --verbose update {{HighlightParam|--nt-fw}} {{Highlight|u-boot-nodtb.bin}} {{HighlightParam|--hw-config}} {{Highlight|u-boot.dtb}} \ | ||
'''fip-{{HighlightParam|stm32mp135f-dk}}.bin''' | '''fip-{{HighlightParam|stm32mp135f-dk}}.bin''' | ||
=== {{Board | type=135F-DK}} with export === | === {{Board | type=135F-DK}} with export === | ||
{{PC$}} export KBUILD_OUTPUT=../build/stm32mp13 | {{PC$}}export KBUILD_OUTPUT=../build/stm32mp13 | ||
{{PC$}} export DEVICE_TREE={{HighlightParam|stm32mp135f-dk}} | {{PC$}}export DEVICE_TREE={{HighlightParam|stm32mp135f-dk}} | ||
{{PC$}} make {{HighlightParam|stm32mp13_defconfig}} | {{PC$}}make {{HighlightParam|stm32mp13_defconfig}} | ||
{{PC$}} make all | {{PC$}}make all | ||
{{PC$}} fiptool --verbose update {{HighlightParam|--nt-fw}} {{Highlight|$KBUILD_OUTPUT/u-boot-nodtb.bin}} \ | {{PC$}}fiptool --verbose update {{HighlightParam|--nt-fw}} {{Highlight|$KBUILD_OUTPUT/u-boot-nodtb.bin}} \ | ||
{{HighlightParam|--hw-config}} {{Highlight|$KBUILD_OUTPUT/u-boot.dtb}} \ | {{HighlightParam|--hw-config}} {{Highlight|$KBUILD_OUTPUT/u-boot.dtb}} \ | ||
'''fip-{{HighlightParam|stm32mp135f-dk}}.bin''' | '''fip-{{HighlightParam|stm32mp135f-dk}}.bin''' | ||
Line 111: | Line 93: | ||
=== Custom board with external device tree === | === Custom board with external device tree === | ||
{{PC$}} make {{HighlightParam|stm32mp13_defconfig}} | {{PC$}}make {{HighlightParam|stm32mp13_defconfig}} | ||
{{PC$}} make EXT_DTB={{HighlightParam|stm32mp131a-myboard.dtb}} all | {{PC$}}make EXT_DTB={{HighlightParam|stm32mp131a-myboard.dtb}} all | ||
{{PC$}} fiptool --verbose update {{HighlightParam|--nt-fw}} {{Highlight|u-boot-nodtb.bin}} \ | {{PC$}}fiptool --verbose update {{HighlightParam|--nt-fw}} {{Highlight|u-boot-nodtb.bin}} \ | ||
{{HighlightParam|--hw-config}} {{Highlight|u-boot.dtb}} \ | {{HighlightParam|--hw-config}} {{Highlight|u-boot.dtb}} \ | ||
'''fip-{{HighlightParam|stm32mp131a-myboard}}.bin''' | '''fip-{{HighlightParam|stm32mp131a-myboard}}.bin''' |
Latest revision as of 13:34, 18 October 2024
This article briefly describes the STM32MP13x lines support in U-Boot.
1. STM32MP13x lines
support[edit | edit source]
For detailed information, read the file in the delivered U-Boot code = doc/board/st/stm32mp1.rst or the documentation generated by make htlmdocs
: board/st/stm32mp1.html.
Code:
- arch/arm/mach-stm32mp : arch specific code for STM32 Arm® Cortex® MPUs
- arch/arm/mach-stm32mp/Kconfig : generic configuration for STM32 Arm® Cortex® MPUs
- arch/arm/mach-stm32mp/Kconfig.13x : specific configuration for STM32MP13x lines
- arch/arm/mach-stm32mp/Kconfig : generic configuration for STM32 Arm® Cortex® MPUs
- board/st/common : STMicroelectronics common code
- board/st/stm32mp1 : STMicroelectronics boards support for STM32MP1 series
- drivers/*/*stm32* : drivers
Configuration files:
- defconfig file
- config files
- include/configs/stm32mp13_common.h : generic for STM32MP13x lines
- include/configs/stm32mp13_st_common.h : STMicroelectronics board for STM32MP13x lines
- include/configs/stm32mp13_common.h : generic for STM32MP13x lines
- STM32_MPU_device_tree in arch/arm/dts : stm32mp13*.dts*
- <Device tree>.dts: same as kernel
- <Device tree>-u-boot.dtsi: addition for u-boot automatically included in build process
- stm32mp13-u-boot.dtsi : SoC add-on file included in <Device tree>-u-boot.dtsi
2. Selecting targets: choose defconfig and device tree[edit | edit source]
The U-Boot configuration with defconfig is stm32mp13_defconfig.
The STM32MP13 boards are supported with the associated device tree (same name as kernel):
Board part number | Device tree | Description |
---|---|---|
STM32MP135F-DK Discovery kit ![]() |
stm32mp135f-dk | MB1635 |
3. Compilation[edit | edit source]
see U-Boot_overview#U-Boot_build
For STM32MP135F-DK Discovery kit , the device tree is already selected in defconfig stm32mp13_defconfig
stm32mp13_defconfig make allmake
For other boards, you need to select the correct device tree
stm32mp13_defconfig make DEVICE_TREE=<Device tree> allmake
The supported variables are:
- DEVICE_TREE: select in arch/arm/dts the device tree that is used.
- KBUILD_OUTPUT: change the destination directory for the build
- EXT_DTB: select external device tree.
- EXT_DTS: select PATH of external device tree source, by default the sub-directory "arch/arm/dts/external-dt" is used to allow sub-module.
The output files u-boot.dtb and u-boot-nodtb.bin are integrated in TF-A FIP.
Note: All the compiled devices trees are available in $KBUILD_OUTPUT/arch/arm/dts/*.dtb.
You can select them instead of u-boot.dtb without U-Boot recompilation.
4. Examples[edit | edit source]
4.1. STM32MP135F-DK Discovery kit
[edit | edit source]
stm32mp13_defconfig make allmake
or
stm32mp13_defconfig make DEVICE_TREE=stm32mp135f-dk allmake
and
--nt-fw u-boot-nodtb.bin --hw-config u-boot.dtb \ fip-stm32mp135f-dk.binfiptool --verbose update
4.2. STM32MP135F-DK Discovery kit
with export[edit | edit source]
stm32mp135f-dk make stm32mp13_defconfig make allexport KBUILD_OUTPUT=../build/stm32mp13 export DEVICE_TREE=
--nt-fw $KBUILD_OUTPUT/u-boot-nodtb.bin \ --hw-config $KBUILD_OUTPUT/u-boot.dtb \ fip-stm32mp135f-dk.binfiptool --verbose update
4.3. Custom board with external device tree[edit | edit source]
stm32mp13_defconfig make EXT_DTB=stm32mp131a-myboard.dtb allmake
--nt-fw u-boot-nodtb.bin \ --hw-config u-boot.dtb \ fip-stm32mp131a-myboard.binfiptool --verbose update