Registered User m (→References) |
Registered User mNo edit summary Tag: 2017 source edit |
||
(23 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
<noinclude>{{ApplicableFor | <noinclude> | ||
|MPUs list=STM32MP25x | {{ApplicableFor | ||
|MPUs checklist=STM32MP13x,STM32MP15x,STM32MP25x | |MPUs list=STM32MP23x, STM32MP25x | ||
}}</noinclude> | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}} | |||
</noinclude> | |||
== Article purpose == | == Article purpose == | ||
Line 10: | Line 12: | ||
The device tree binding documents are stored, either in the given applicable components listed below, or in the Linux kernel repository: <br> | The device tree binding documents are stored, either in the given applicable components listed below, or in the Linux kernel repository: <br> | ||
* Linux<sup>®</sup> OS : | * Linux<sup>®</sup> OS : | ||
** | ** {{CodeSource | Linux kernel | Documentation/devicetree/bindings/display/st,stm32-lvds.yaml | st,stm32-lvds.yaml}}: STM32 LVDS device tree bindings. | ||
** {{CodeSource | Linux kernel | Documentation/devicetree/bindings/display/panel/panel-lvds.yaml | panel/panel-lvds.yaml}}: Description of properties for a '''<code>panel-lvds</code>''': '''<code>data-mapping</code>''', '''<code>width-mm</code>''', '''<code>height-mm</code>''', '''<code>panel-timing</code>''', '''<code>port</code>'''... | |||
** [https://elixir.bootlin.com/linux/latest/source/Documentation/devicetree/bindings/display/panel/panel-simple-lvds-dual-ports.yaml panel/panel-simple-lvds-dual-ports.yaml]: Description of the '''<code>dual-lvds-odd-pixels</code>''' and '''<code>dual-lvds-even-pixels</code>''' properties for "dual ports" (also named "dual links" or "dual channels") LVDS display panel. | |||
** [https://elixir.bootlin.com/linux/latest/source/Documentation/devicetree/bindings/display/lvds-data-mapping.yaml lvds-data-mapping.yaml]: Description of the '''<code>data-mapping</code>''' property with the following possible values: '''<code>jeida-18</code>''', '''<code>jeida-24</code>''' and '''<code>vesa-24</code>'''. | |||
** {{CodeSource | Linux kernel | Documentation/devicetree/bindings/display/lvds.yaml | lvds.yaml}}: Description of the '''<code>data-mirror</code>''' property. If set, reverse the bit order described in the data mappings on all data lanes, transmitting bits for slots 6 to 0 instead of 0 to 6. | |||
{{Warning|The '''<code>data-mirror</code>''' and '''<code>jeida-18</code>''' properties are not yet available in current {{EcosystemRelease | revision=latest}}.}} | |||
== DT configuration == | == DT configuration == | ||
Line 20: | Line 28: | ||
The LVDS node is located in the [[STM32 MPU device_tree#Device tree structure|device tree file]] for the software components, supporting the peripheral and listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. | The LVDS node is located in the [[STM32 MPU device_tree#Device tree structure|device tree file]] for the software components, supporting the peripheral and listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. | ||
The | The LVDSdevice tree node is declared in: | ||
< | <div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | ||
* {{CodeSource | Linux kernel | arch/arm64/boot/dts/st/stm32mp235.dtsi}} on {{MicroprocessorDevice | device=23}} | |||
<div class="mw-collapsible-content"> | |||
The declaration (shown below) defines the hardware register base address, the clocks, and the reset. | |||
<syntaxhighlight lang="dts"> | |||
... | |||
&rifsc { | |||
... | |||
lvds: lvds@48060000 { | |||
#clock-cells = <0>; | |||
compatible = "st,stm32mp25-lvds"; | |||
reg = <0x48060000 0x2000>; | |||
clocks = <&rcc CK_BUS_LVDS>, <&rcc CK_KER_LVDSPHY>, <&syscfg 0>; | |||
</ | clock-names = "pclk", "ref", "pixclk"; | ||
resets = <&rcc LVDS_R>; | |||
access-controllers = <&rifsc 84>; | |||
power-domains = <&CLUSTER_PD>; | |||
status = "disabled"; | |||
}; | |||
... | |||
</syntaxhighlight> | |||
</div> | |||
</div> | |||
<div class="mw-collapsible mw-collapsed" data-expandtext="Click here to show the example" data-collapsetext="Click here to hide the example"> | |||
* {{CodeSource | Linux kernel | arch/arm64/boot/dts/st/stm32mp255.dtsi}} on {{MicroprocessorDevice | device=25}} | |||
<div class="mw-collapsible-content"> | |||
The declaration (shown below) defines the hardware register base address, the clocks, and the reset. | |||
<syntaxhighlight lang="dts"> | |||
... | |||
&rifsc { | |||
... | |||
lvds: lvds@48060000 { | |||
#clock-cells = <0>; | |||
compatible = "st,stm32mp25-lvds"; | |||
reg = <0x48060000 0x2000>; | |||
clocks = <&rcc CK_BUS_LVDS>, <&rcc CK_KER_LVDSPHY>, <&syscfg 0>; | |||
clock-names = "pclk", "ref", "pixclk"; | |||
resets = <&rcc LVDS_R>; | |||
access-controllers = <&rifsc 84>; | |||
power-domains = <&CLUSTER_PD>; | |||
status = "disabled"; | |||
}; | |||
... | |||
</syntaxhighlight> | |||
</div> | |||
</div> | |||
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} | {{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} | ||
=== DT configuration (board level) === | === DT configuration (board level) === | ||
When configuring the board device tree, it is important to know the kind of the used LVDS display panel: | |||
* Number of links, '''Single-Link''' or '''Dual-Link''' (also named '''Single-Port & Dual-Port''' or '''Single-Channel & Dual-Channel'''): | |||
** '''Single-Link''' case: Only one '''<code>port</code>''' node is used. | |||
** '''Dual-Link''' case: 2 '''<code>port</code>''' nodes are used with the '''<code>dual-lvds-odd-pixels</code>''' and '''<code>dual-lvds-even-pixels</code>''' properties in each port nodes. | |||
** '''2x Single-Link''' case: 2 '''<code>port</code>''' nodes are used. | |||
* Bit-mapping: '''<code>data-mapping</code>''' property is set to '''<code>jeida-18</code>''', '''<code>jeida-24</code>''' or '''<code>vesa-24</code>'''. | |||
* Bit-ordering: '''<code>data-mirror</code>''' property is set if the reversed bit ordering is needed. | |||
{{Info | Only {{MicroprocessorDevice | device=25}} support '''Dual-Link''' and '''2x Single-Link''' cases.}} | |||
{{Warning|The '''<code>data-mirror</code>''' and '''<code>jeida-18</code>''' properties are not yet available in current {{EcosystemRelease | revision=latest}}.}} | |||
Below examples present some of these possibilities. | |||
==== Single-Link LVDS display panel ==== | |||
Depending on the board hardware, the LVDS device tree related to a particular board may have the following nodes: | Depending on the board hardware, the LVDS device tree related to a particular board may have the following nodes: | ||
* '''lvds''' node: it contains the in/out port descriptions. | * '''lvds''' node: it contains the in/out port descriptions. | ||
Line 44: | Line 101: | ||
* '''panel_lvds''' node: it contains the LVDS panel description. | * '''panel_lvds''' node: it contains the LVDS panel description. | ||
* '''panel_lvds_backlight''' node: it is related to the panel node. | * '''panel_lvds_backlight''' node: it is related to the panel node. | ||
A full example of the [[STM32MP257x-EV1 - hardware description | STM32MP257 Evaluation board]] device tree is available in stm32mp257f-ev1.dts <ref name="stm32mp257f_ev1_dts">{{CodeSource | Linux kernel | arch/arm64/boot/dts/st/stm32mp257f-ev1.dts | Linux kernel STM32MP257 Evaluation board device tree (stm32mp257f-ev1.dts)}}</ref>. | A full example of the [[STM32MP257x-EV1 - hardware description | STM32MP257 Evaluation board]] device tree is available in stm32mp257f-ev1.dts <ref name="stm32mp257f_ev1_dts">{{CodeSource | Linux kernel | arch/arm64/boot/dts/st/stm32mp257f-ev1.dts | Linux kernel STM32MP257 Evaluation board device tree (stm32mp257f-ev1.dts)}}</ref>. | ||
< | <syntaxhighlight lang="dts" line start="20" highlight="3, 4, 11, 25-29, 32, 43, 64, 81-86"> | ||
/ { | |||
... | |||
panel_lvds: panel-lvds { | |||
compatible = "edt,etml0700z9ndha", "panel-lvds"; | |||
enable-gpios = <&gpiog 15 GPIO_ACTIVE_HIGH>; | |||
backlight = <&panel_lvds_backlight>; | |||
status = "okay"; | |||
width-mm = <156>; | |||
height-mm = <92>; | |||
data-mapping = "vesa-24"; | |||
panel-timing { | |||
clock-frequency = <54000000>; | |||
hactive = <1024>; | |||
vactive = <600>; | |||
hfront-porch = <150>; | |||
hback-porch = <150>; | |||
hsync-len = <21>; | |||
vfront-porch = <24>; | |||
vback-porch = <24>; | |||
vsync-len = <21>; | |||
}; | |||
port { | |||
lvds_panel_in: endpoint { | |||
remote-endpoint = <&lvds_out0>; | |||
}; | |||
}; | |||
}; | |||
panel_lvds_backlight: panel-lvds-backlight { | |||
compatible = "gpio-backlight"; | |||
gpios = <&gpioi 5 GPIO_ACTIVE_HIGH>; | |||
default-on; | |||
default-brightness-level = <1>; | |||
status = "okay"; | |||
}; | |||
... | |||
}; | |||
<dc { | <dc { | ||
default-on; | |||
rotation-memory = <<dc_sec_rotation>; | rotation-memory = <<dc_sec_rotation>; | ||
status = "okay"; | status = "okay"; | ||
Line 69: | Line 169: | ||
&lvds { | &lvds { | ||
default-on; | |||
vdd-supply = <&scmi_vddcore>; | |||
vdda18-supply = <&scmi_v1v8>; | |||
status = "okay"; | status = "okay"; | ||
Line 90: | Line 193: | ||
}; | }; | ||
}; | }; | ||
... | |||
</syntaxhighlight> | |||
{{Info|In the above example, the compatible is set to <code>compatible {{=}} "edt,etml0700z9ndha", "panel-lvds";</code>. It is important to keep <code>"panel-lvds"</code> but the part <code>"edt,etml0700z9ndha"</code> can be ''any string'' (most of the time, the panel name found in the board documentation).}} | |||
==== JEIDA or VESA Bit-Mapping ==== | |||
The LVDS display panels use typically only '''two types of bit-mapping''', defined in the '''VESA''' and '''JEIDA''' sub-standards: | |||
* The transmission of RGB666 requires three data lanes (+1 clock lane) while the transmission of RGB888 requires four data lanes (+1 clock lane). | |||
* VESA groups on its three first lanes the LSB of the RGB components, which results in a different pattern for RGB666 and for RGB888. | |||
* JEIDA groups on its three first lanes the MSB of the RGB components, which results in a same pattern for RGB666 and for RGB888: | |||
** the 6 MSB bits are transmitted onto a common three data lanes (+1 clock lane), which maps RGB666. | |||
** the additional bits for RGB888 are mapped into the additional 4th data lane. | |||
The two following figures illustrates the above description, with the here-named bit R7,G7,B7 are the component MSB, while the R0,G0,B0 are the LSB. | |||
[[File:lvds_vesa_jeida.png|center|800px|link=|alt=Alternate text|LVDS VESA and JEIDA data mappings (extracted from [[STM32 MPU resources#Reference manuals|STM32 MPU reference manuals]]]] | |||
{{Info|Note that some panel specifications mention the MSB as R5,G5,B5, while the two LSB are called R7 and R6 (same for G and B), which can create some confusion.}} | |||
The [https://elixir.bootlin.com/linux/latest/source/Documentation/devicetree/bindings/display/lvds-data-mapping.yaml lvds-data-mapping.yaml] device tree binding documentation describes the Linux kernel available '''<code>data-mapping</code>''' property with the following possible values: '''<code>jeida-18</code>''', '''<code>jeida-24</code>''' and '''<code>vesa-24</code>'''. | |||
For instance, use '''<code>data-mapping = "vesa-24";</code>''' for a LVDS '''VESA RGB888''' display panel like in the below example : | |||
<syntaxhighlight lang="dts" line start="20" highlight="9"> | |||
panel_lvds: panel-lvds { | panel_lvds: panel-lvds { | ||
compatible = "edt,etml0700z9ndha", "panel-lvds"; | compatible = "edt,etml0700z9ndha", "panel-lvds"; | ||
enable-gpios = <&gpiog 15 GPIO_ACTIVE_HIGH>; | enable-gpios = <&gpiog 15 GPIO_ACTIVE_HIGH>; | ||
backlight = <&panel_lvds_backlight>; | backlight = <&panel_lvds_backlight>; | ||
status = "okay"; | |||
width-mm = <156>; | |||
height-mm = <92>; | |||
data-mapping = "vesa-24"; | |||
panel-timing { | |||
clock-frequency = <54000000>; | |||
hactive = <1024>; | |||
vactive = <600>; | |||
... | |||
</syntaxhighlight> | |||
==== Dual-Link LVDS display panel ==== | |||
For '''Dual-Link''' LVDS display panels, two '''<code>port</code>''' nodes are used with the '''<code>dual-lvds-odd-pixels</code>''' and '''<code>dual-lvds-even-pixels</code>''' properties in each port nodes. | |||
{{Info | Only {{MicroprocessorDevice | device=25}} support '''Dual-Link''' and '''2x Single-Link''' cases.}} | |||
The below devicetree code can be used as example for a '''Dual-Link''' LVDS display panel: | |||
<syntaxhighlight lang="dts" line start="20" highlight="34-52, 84-96"> | |||
/ { | |||
... | |||
panel_backlight_8dl: panel-backlight-8dl { | |||
compatible = "gpio-backlight"; | |||
gpios = <&gpioi 5 GPIO_ACTIVE_HIGH>; | |||
default-on; | |||
default-brightness-level = <0>; | |||
status = "okay"; | |||
}; | |||
panel_lvds_8dl: panel-lvds-8dl { | |||
compatible = "ampire,amp19201200b5tzqw-t03", "panel-lvds"; | |||
enable-gpios = <&gpioi 9 GPIO_ACTIVE_HIGH>; | |||
backlight = <&panel_backlight_8dl>; | |||
status = "okay"; | |||
width-mm = <217>; | |||
height-mm = <136>; | |||
data-mapping = "vesa-24"; | |||
panel-timing { | |||
clock-frequency = <150000000>; | |||
hactive = <1920>; | |||
vactive = <1200>; | |||
hsync-len = <18>; | |||
hfront-porch = <60>; | |||
hback-porch = <60>; | |||
vsync-len = <2>; | |||
vfront-porch = <6>; | |||
vback-porch = <6>; | |||
hsync-active = <0>; | |||
}; | |||
ports { | |||
#address-cells = <1>; | |||
#size-cells = <0>; | |||
port@0 { | |||
reg = <0>; | |||
dual-lvds-odd-pixels; | |||
lvds_panel_8dl_in0: endpoint { | |||
remote-endpoint = <&lvds_out0>; | |||
}; | |||
}; | |||
port@1 { | |||
reg = <1>; | |||
dual-lvds-even-pixels; | |||
lvds_panel_8dl_in1: endpoint { | |||
remote-endpoint = <&lvds_out1>; | |||
}; | |||
}; | |||
}; | |||
}; | |||
... | |||
<dc { | |||
status = "okay"; | |||
port { | |||
ltdc_ep0_out: endpoint { | |||
remote-endpoint = <&lvds_in>; | |||
}; | |||
}; | |||
}; | |||
&lvds { | |||
vdd-supply = <&vddcore>; | |||
vdda18-supply = <&v1v8>; | |||
status = "okay"; | |||
ports { | |||
#address-cells = <1>; | |||
#size-cells = <0>; | |||
port@0 { | |||
reg = <0>; | |||
lvds_in: endpoint { | |||
remote-endpoint = <<dc_ep0_out>; | |||
}; | |||
}; | |||
port@1 { | |||
reg = <1>; | |||
lvds_out0: endpoint { | |||
remote-endpoint = <&lvds_panel_8dl_in0>; | |||
}; | |||
}; | |||
port@2 { | |||
reg = <2>; | |||
lvds_out1: endpoint { | |||
remote-endpoint = <&lvds_panel_8dl_in1>; | |||
}; | |||
}; | |||
}; | |||
}; | |||
... | |||
</syntaxhighlight> | |||
{{Info|Depending on the display panel hardware configuration, it may be necessary to permute '''<code>dual-lvds-odd-pixels</code>''' and '''<code>dual-lvds-even-pixels</code>''' properties in each port nodes.}} | |||
==== 2x Single-Link LVDS display panels (same content duplicated on both) ==== | |||
For '''2x Single-Link''' LVDS display panels (same content duplicated on both), two '''<code>port</code>''' nodes are used. | |||
{{Info | Only {{MicroprocessorDevice | device=25}} support '''Dual-Link''' and '''2x Single-Link''' cases.}} | |||
The below devicetree code can be used as example for a '''2x Single-Link''' LVDS display panels: | |||
<syntaxhighlight lang="dts" line start="20" highlight="29-41, 81-93"> | |||
/ { | |||
... | |||
panel_lvds: panel-lvds { | |||
compatible = "edt,etml0700z9ndha", "panel-lvds"; | |||
enable-gpios = <&gpioi 9 GPIO_ACTIVE_HIGH>; | |||
backlight = <&panel_backlight>; | |||
status = "okay"; | status = "okay"; | ||
Line 114: | Line 375: | ||
}; | }; | ||
port { | ports { | ||
#address-cells = <1>; | |||
#size-cells = <0>; | |||
port@0 { | |||
reg = <0>; | |||
panel_lvds_in0: endpoint { | |||
remote-endpoint = <&lvds_out0>; | |||
}; | |||
}; | |||
port@1 { | |||
reg = <1>; | |||
panel_lvds_in1: endpoint { | |||
remote-endpoint = <&lvds_out1>; | |||
}; | |||
}; | }; | ||
}; | }; | ||
}; | }; | ||
panel_backlight: panel-backlight { | |||
compatible = "gpio-backlight"; | compatible = "gpio-backlight"; | ||
gpios = <& | gpios = <&gpiod 13 GPIO_ACTIVE_HIGH>; | ||
default-on; | default-on; | ||
default-brightness-level = <0>; | default-brightness-level = <0>; | ||
status = "okay"; | status = "okay"; | ||
}; | }; | ||
... | |||
}; | |||
<dc { | |||
status = "okay"; | |||
port { | |||
ltdc_ep0_out: endpoint { | |||
remote-endpoint = <&lvds_in>; | |||
}; | |||
}; | |||
}; | |||
</ | &lvds { | ||
vdd-supply = <&vddcore>; | |||
vdda18-supply = <&v1v8>; | |||
status = "okay"; | |||
ports { | |||
#address-cells = <1>; | |||
#size-cells = <0>; | |||
port@0 { | |||
reg = <0>; | |||
lvds_in: endpoint { | |||
remote-endpoint = <<dc_ep0_out>; | |||
}; | |||
}; | |||
port@1 { | |||
reg = <1>; | |||
lvds_out0: endpoint { | |||
remote-endpoint = <&panel_lvds_in0>; | |||
}; | |||
}; | |||
port@2 { | |||
reg = <2>; | |||
lvds_out1: endpoint { | |||
remote-endpoint = <&panel_lvds_in1>; | |||
}; | |||
}; | |||
}; | |||
}; | |||
... | |||
</syntaxhighlight> | |||
==How to configure the DT using STM32CubeMX== | ==How to configure the DT using STM32CubeMX== |
Latest revision as of 15:24, 14 October 2024
1. Article purpose
The purpose of this article is to explain how to configure the LVDS internal peripheral using the device tree mechanism, relying on the bindings documentation. The latter corresponds to the description of the required and optional device-tree properties.
2. DT bindings documentation
The device tree binding documents are stored, either in the given applicable components listed below, or in the Linux kernel repository:
- Linux® OS :
- st,stm32-lvds.yaml : STM32 LVDS device tree bindings.
- panel/panel-lvds.yaml : Description of properties for a
panel-lvds
:data-mapping
,width-mm
,height-mm
,panel-timing
,port
... - panel/panel-simple-lvds-dual-ports.yaml: Description of the
dual-lvds-odd-pixels
anddual-lvds-even-pixels
properties for "dual ports" (also named "dual links" or "dual channels") LVDS display panel. - lvds-data-mapping.yaml: Description of the
data-mapping
property with the following possible values:jeida-18
,jeida-24
andvesa-24
. - lvds.yaml : Description of the
data-mirror
property. If set, reverse the bit order described in the data mappings on all data lanes, transmitting bits for slots 6 to 0 instead of 0 to 6.
3. DT configuration
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and the board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file organization.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32/SoC level)
The LVDS node is located in the device tree file for the software components, supporting the peripheral and listed in the above DT bindings documentation paragraph.
The LVDSdevice tree node is declared in:
- arch/arm64/boot/dts/st/stm32mp235.dtsi on STM32MP23x lines
- arch/arm64/boot/dts/st/stm32mp255.dtsi on STM32MP25x lines
3.2. DT configuration (board level)
When configuring the board device tree, it is important to know the kind of the used LVDS display panel:
- Number of links, Single-Link or Dual-Link (also named Single-Port & Dual-Port or Single-Channel & Dual-Channel):
- Single-Link case: Only one
port
node is used. - Dual-Link case: 2
port
nodes are used with thedual-lvds-odd-pixels
anddual-lvds-even-pixels
properties in each port nodes. - 2x Single-Link case: 2
port
nodes are used.
- Single-Link case: Only one
- Bit-mapping:
data-mapping
property is set tojeida-18
,jeida-24
orvesa-24
. - Bit-ordering:
data-mirror
property is set if the reversed bit ordering is needed.
Below examples present some of these possibilities.
3.2.1. Single-Link LVDS display panel
Depending on the board hardware, the LVDS device tree related to a particular board may have the following nodes:
- lvds node: it contains the in/out port descriptions.
- ltdc node: it contains the in/out port description related to the lvds node.
- panel_lvds node: it contains the LVDS panel description.
- panel_lvds_backlight node: it is related to the panel node.
A full example of the STM32MP257 Evaluation board device tree is available in stm32mp257f-ev1.dts [1].
/ {
...
panel_lvds: panel-lvds {
compatible = "edt,etml0700z9ndha", "panel-lvds";
enable-gpios = <&gpiog 15 GPIO_ACTIVE_HIGH>;
backlight = <&panel_lvds_backlight>;
status = "okay";
width-mm = <156>;
height-mm = <92>;
data-mapping = "vesa-24";
panel-timing {
clock-frequency = <54000000>;
hactive = <1024>;
vactive = <600>;
hfront-porch = <150>;
hback-porch = <150>;
hsync-len = <21>;
vfront-porch = <24>;
vback-porch = <24>;
vsync-len = <21>;
};
port {
lvds_panel_in: endpoint {
remote-endpoint = <&lvds_out0>;
};
};
};
panel_lvds_backlight: panel-lvds-backlight {
compatible = "gpio-backlight";
gpios = <&gpioi 5 GPIO_ACTIVE_HIGH>;
default-on;
default-brightness-level = <1>;
status = "okay";
};
...
};
<dc {
default-on;
rotation-memory = <<dc_sec_rotation>;
status = "okay";
port {
#address-cells = <1>;
#size-cells = <0>;
ltdc_ep0_out: endpoint@0 {
reg = <0>;
remote-endpoint = <&dsi_in>;
};
ltdc_ep1_out: endpoint@1 {
reg = <1>;
remote-endpoint = <&lvds_in>;
};
};
};
&lvds {
default-on;
vdd-supply = <&scmi_vddcore>;
vdda18-supply = <&scmi_v1v8>;
status = "okay";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
lvds_in: endpoint {
remote-endpoint = <<dc_ep1_out>;
};
};
port@1 {
reg = <1>;
lvds_out0: endpoint {
remote-endpoint = <&lvds_panel_in>;
};
};
};
};
...
![]() |
In the above example, the compatible is set to compatible = "edt,etml0700z9ndha", "panel-lvds"; . It is important to keep "panel-lvds" but the part "edt,etml0700z9ndha" can be any string (most of the time, the panel name found in the board documentation).
|
3.2.2. JEIDA or VESA Bit-Mapping
The LVDS display panels use typically only two types of bit-mapping, defined in the VESA and JEIDA sub-standards:
- The transmission of RGB666 requires three data lanes (+1 clock lane) while the transmission of RGB888 requires four data lanes (+1 clock lane).
- VESA groups on its three first lanes the LSB of the RGB components, which results in a different pattern for RGB666 and for RGB888.
- JEIDA groups on its three first lanes the MSB of the RGB components, which results in a same pattern for RGB666 and for RGB888:
- the 6 MSB bits are transmitted onto a common three data lanes (+1 clock lane), which maps RGB666.
- the additional bits for RGB888 are mapped into the additional 4th data lane.
The two following figures illustrates the above description, with the here-named bit R7,G7,B7 are the component MSB, while the R0,G0,B0 are the LSB.

![]() |
Note that some panel specifications mention the MSB as R5,G5,B5, while the two LSB are called R7 and R6 (same for G and B), which can create some confusion. |
The lvds-data-mapping.yaml device tree binding documentation describes the Linux kernel available data-mapping
property with the following possible values: jeida-18
, jeida-24
and vesa-24
.
For instance, use data-mapping = "vesa-24";
for a LVDS VESA RGB888 display panel like in the below example :
panel_lvds: panel-lvds {
compatible = "edt,etml0700z9ndha", "panel-lvds";
enable-gpios = <&gpiog 15 GPIO_ACTIVE_HIGH>;
backlight = <&panel_lvds_backlight>;
status = "okay";
width-mm = <156>;
height-mm = <92>;
data-mapping = "vesa-24";
panel-timing {
clock-frequency = <54000000>;
hactive = <1024>;
vactive = <600>;
...
3.2.3. Dual-Link LVDS display panel
For Dual-Link LVDS display panels, two port
nodes are used with the dual-lvds-odd-pixels
and dual-lvds-even-pixels
properties in each port nodes.
The below devicetree code can be used as example for a Dual-Link LVDS display panel:
/ {
...
panel_backlight_8dl: panel-backlight-8dl {
compatible = "gpio-backlight";
gpios = <&gpioi 5 GPIO_ACTIVE_HIGH>;
default-on;
default-brightness-level = <0>;
status = "okay";
};
panel_lvds_8dl: panel-lvds-8dl {
compatible = "ampire,amp19201200b5tzqw-t03", "panel-lvds";
enable-gpios = <&gpioi 9 GPIO_ACTIVE_HIGH>;
backlight = <&panel_backlight_8dl>;
status = "okay";
width-mm = <217>;
height-mm = <136>;
data-mapping = "vesa-24";
panel-timing {
clock-frequency = <150000000>;
hactive = <1920>;
vactive = <1200>;
hsync-len = <18>;
hfront-porch = <60>;
hback-porch = <60>;
vsync-len = <2>;
vfront-porch = <6>;
vback-porch = <6>;
hsync-active = <0>;
};
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
dual-lvds-odd-pixels;
lvds_panel_8dl_in0: endpoint {
remote-endpoint = <&lvds_out0>;
};
};
port@1 {
reg = <1>;
dual-lvds-even-pixels;
lvds_panel_8dl_in1: endpoint {
remote-endpoint = <&lvds_out1>;
};
};
};
};
...
<dc {
status = "okay";
port {
ltdc_ep0_out: endpoint {
remote-endpoint = <&lvds_in>;
};
};
};
&lvds {
vdd-supply = <&vddcore>;
vdda18-supply = <&v1v8>;
status = "okay";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
lvds_in: endpoint {
remote-endpoint = <<dc_ep0_out>;
};
};
port@1 {
reg = <1>;
lvds_out0: endpoint {
remote-endpoint = <&lvds_panel_8dl_in0>;
};
};
port@2 {
reg = <2>;
lvds_out1: endpoint {
remote-endpoint = <&lvds_panel_8dl_in1>;
};
};
};
};
...
![]() |
Depending on the display panel hardware configuration, it may be necessary to permute dual-lvds-odd-pixels and dual-lvds-even-pixels properties in each port nodes.
|
3.2.4. 2x Single-Link LVDS display panels (same content duplicated on both)
For 2x Single-Link LVDS display panels (same content duplicated on both), two port
nodes are used.
The below devicetree code can be used as example for a 2x Single-Link LVDS display panels:
/ {
...
panel_lvds: panel-lvds {
compatible = "edt,etml0700z9ndha", "panel-lvds";
enable-gpios = <&gpioi 9 GPIO_ACTIVE_HIGH>;
backlight = <&panel_backlight>;
status = "okay";
width-mm = <156>;
height-mm = <92>;
data-mapping = "vesa-24";
panel-timing {
clock-frequency = <54000000>;
hactive = <1024>;
vactive = <600>;
hfront-porch = <150>;
hback-porch = <150>;
hsync-len = <21>;
vfront-porch = <24>;
vback-porch = <24>;
vsync-len = <21>;
};
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
panel_lvds_in0: endpoint {
remote-endpoint = <&lvds_out0>;
};
};
port@1 {
reg = <1>;
panel_lvds_in1: endpoint {
remote-endpoint = <&lvds_out1>;
};
};
};
};
panel_backlight: panel-backlight {
compatible = "gpio-backlight";
gpios = <&gpiod 13 GPIO_ACTIVE_HIGH>;
default-on;
default-brightness-level = <0>;
status = "okay";
};
...
};
<dc {
status = "okay";
port {
ltdc_ep0_out: endpoint {
remote-endpoint = <&lvds_in>;
};
};
};
&lvds {
vdd-supply = <&vddcore>;
vdda18-supply = <&v1v8>;
status = "okay";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
lvds_in: endpoint {
remote-endpoint = <<dc_ep0_out>;
};
};
port@1 {
reg = <1>;
lvds_out0: endpoint {
remote-endpoint = <&panel_lvds_in0>;
};
};
port@2 {
reg = <2>;
lvds_out1: endpoint {
remote-endpoint = <&panel_lvds_in1>;
};
};
};
};
...
4. How to configure the DT using STM32CubeMX
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in the DT binding files listed in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References
Refer to the following links for additional information: