Registered User mNo edit summary |
Registered User No edit summary |
||
(One intermediate revision by the same user not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
|MPUs list=STM32MP13x, STM32MP15x,STM32MP25x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x,STM32MP15x,STM32MP25x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}}</noinclude> | }} | ||
<noinclude></noinclude> | |||
Information about the Linux kernel depends on the microprocessor device. | Information about the Linux kernel depends on the microprocessor device. | ||
Line 16: | Line 17: | ||
|- | |- | ||
| {{MicroprocessorDevice | device=15}}|| [[STM32MP15 Linux kernel overview]] | | {{MicroprocessorDevice | device=15}}|| [[STM32MP15 Linux kernel overview]] | ||
|- | |||
| {{MicroprocessorDevice | device=21}}|| [[STM32MP21 Linux kernel overview]] | |||
|- | |||
| {{MicroprocessorDevice | device=23}}|| [[STM32MP23 Linux kernel overview]] | |||
|- | |- | ||
| {{MicroprocessorDevice | device=25}}|| [[STM32MP25 Linux kernel overview]] | | {{MicroprocessorDevice | device=25}}|| [[STM32MP25 Linux kernel overview]] |
Latest revision as of 18:33, 11 October 2024
Information about the Linux kernel depends on the microprocessor device.
Several articles have been created to manage STM32 MPU diversity and provide the relevant level of information.
Browse the one corresponding to the STM32 MPU you use.
STM32 MPU devices | Associated articles |
---|---|
STM32MP13x lines ![]() |
STM32MP13 Linux kernel overview |
STM32MP15x lines ![]() |
STM32MP15 Linux kernel overview |
STM32MP21 unknown microprocessor device | STM32MP21 Linux kernel overview |
STM32MP23 unknown microprocessor device | STM32MP23 Linux kernel overview |
STM32MP25x lines ![]() |
STM32MP25 Linux kernel overview |