Registered User No edit summary |
Registered User mNo edit summary Tag: 2017 source edit |
||
Line 1: | Line 1: | ||
<noinclude> | |||
{{ApplicableFor | {{ApplicableFor | ||
|MPUs list=STM32MP13x, STM32MP15x, STM32MP25x | |MPUs list=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP21x, STM32MP23x, STM32MP25x | ||
}} | }} | ||
</noinclude> | |||
==Starting, stopping and restarting Weston== | ==Starting, stopping and restarting Weston== | ||
Weston has its own | Weston has its own <code>systemd</code> service (/lib/systemd/system/weston-graphical-session.service) to easily start, stop and restart Weston. | ||
The following command stops the Weston service: | The following command stops the Weston service: | ||
Line 19: | Line 20: | ||
==Preventing Weston from automatically starting on boot== | ==Preventing Weston from automatically starting on boot== | ||
=== Weston service with udev rules === | === Weston service with udev rules === | ||
The Weston service is automatically started on boot thanks to an '''udev rules''' file, most of the time located in | The Weston service is automatically started on boot thanks to an '''udev rules''' file, most of the time located in <code>/etc/udev/rules.d/*weston*</code>, for instance <code>/etc/udev/rules.d/71-weston-drm.rules</code>. | ||
To disable this service, rename this file (by changing its extension for instance), then restart your board. | To disable this service, rename this file (by changing its extension for instance), then restart your board. | ||
Line 26: | Line 27: | ||
=== Weston service with systemd === | === Weston service with systemd === | ||
During the development process, when udev rules are not fully configured, the Weston service can be automatically started on boot as specified in | During the development process, when udev rules are not fully configured, the Weston service can be automatically started on boot as specified in <code>/lib/systemd/system/weston*</code>. | ||
In this case, the following command disables the automatic start of the Weston service: | In this case, the following command disables the automatic start of the Weston service: |
Latest revision as of 15:49, 8 October 2024
1. Starting, stopping and restarting Weston[edit | edit source]
Weston has its own systemd
service (/lib/systemd/system/weston-graphical-session.service) to easily start, stop and restart Weston.
The following command stops the Weston service:
systemctl stop weston-graphical-session
The following command starts the Weston service:
systemctl start weston-graphical-session
The following command stops and then restarts the Weston service:
systemctl restart weston-graphical-session
2. Preventing Weston from automatically starting on boot[edit | edit source]
2.1. Weston service with udev rules[edit | edit source]
The Weston service is automatically started on boot thanks to an udev rules file, most of the time located in /etc/udev/rules.d/*weston*
, for instance /etc/udev/rules.d/71-weston-drm.rules
.
To disable this service, rename this file (by changing its extension for instance), then restart your board.
To re-enable this service, rename this file according to the udev rules of your system.
2.2. Weston service with systemd[edit | edit source]
During the development process, when udev rules are not fully configured, the Weston service can be automatically started on boot as specified in /lib/systemd/system/weston*
.
In this case, the following command disables the automatic start of the Weston service:
systemctl disable weston-graphical-session
The following command enables the automatic start of the Weston service:
systemctl enable weston-graphical-session
Depending on your systemd configuration, it may be required to mask/unmask the Weston service with the following commands:
systemctl mask weston-graphical-session
systemctl unmask weston-graphical-session
You can check the status of the Weston service with the following command:
systemctl list-unit-files | grep -i weston
Please refer to the systemctl manpage[1] and to the Running Weston documentation[2] to know more about related details.
3. References[edit | edit source]