Registered User (Merge articles) |
Registered User (Merge articles) |
||
Line 3: | Line 3: | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x | ||
}}</noinclude> | }}</noinclude> | ||
{{:STM32CubeMP13 Package release note - v1.0.0 | {{:STM32CubeMP13 Package release note - v1.1.0}} | ||
==Archives [[File:Archive_box.png|25px|link=]]== | |||
{| class="st-table" | |||
! STM32CubeMP13 Package release !! Release note | |||
|- | |||
| STM32CubeMP13 Package release note - v1.0.0 ||[[STM32CubeMP13 Package release note - v1.0.0]] | |||
|} | |||
<noinclude> | <noinclude> |
Revision as of 13:01, 17 May 2024
This article aims to describe the content of the software release included in the STM32CubeMP13 Package, version v.1.1.0.
1. Delivery purpose and scope[edit | edit source]
The STM32CubeMP13 Package is a software package running on Arm® Cortex®-A7 processor.
This release includes:
- The STM32Cube HAL: STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
- Low-layer APIs (LL APIs) offering a fast lightweight expert-oriented layer that is closer to the hardware than the HAL.
LL APIs are only available for a limited set of peripherals. - A consistent set of middleware components such as AzureRTOS.
- All embedded software utilities delivered with a full set of examples.
It also includes:
- BSP for the STM32MP135F-DK Discovery kit
(LED, button, camera, LCD, SD card and COM ports)
- Projects: several projects (examples, applications, external loader and templates) are implemented in IDEs.
2. Intended audience[edit | edit source]
The targeted audience is STM32 MPU customers and partners.
3. Licensing[edit | edit source]
All licenses applicable to STM32CubeMP13 package are available here.
4. Supported devices[edit | edit source]
The drivers provided within this package support all STM32MP13x lines .
5. Supported hardware[edit | edit source]
The software examples and the drivers delivered in this package are applicable for the following boards:
- STM32MP135F-DK Discovery kit
, for information about those boards, read the article STM32MP135x-DK - hardware description.
6. Release content[edit | edit source]
This release is the 2nd release of the STM32CubeMP13 software package running in standalone on the Arm® Cortex®-A7 of STM32MP13x lines .
The full content is available in STM32CubeMP13 Package content. This STM32CubeMP13 package can be then used as any STM32Cube package running on STM32-MPU of STMicroelectronics.
6.1. Main changes[edit | edit source]
Main changes, compared to STM32CubeMP13-v1.0.0 package are
- support of eMMC as boot device
- addition of EWARM examples.
6.1.1. HAL drivers[edit | edit source]
- No major changes in HAL drivers.
- Check overview and all available HAL drivers in HAL drivers
6.1.2. LL drivers[edit | edit source]
- No major changes in LL drivers.
- Check overview and all available LL drivers here LL drivers
6.1.3. BSP[edit | edit source]
- GT911 BSP TouchScreen component support has been added at BSP.
- Refer to BSP Drivers section here BSP drivers.
6.1.4. CMSIS[edit | edit source]
- Bit and registers definition for STM32MP13x lines
.
- Support for IAR workbench has been added.
- For more details, refer main section CMSIS
6.1.5. Middleware[edit | edit source]
- AzureRTOS (ThreadX, LevelX, FileX, USBX, NetXDuo)
- USB Library (Device and Host)
- Check overview of middleware's in STM32CubeMP13 Package article
6.1.6. Projects[edit | edit source]
- Check project section here Projects for details of projects implemented.
6.2. Released components[edit | edit source]
6.2.1. Drivers[edit | edit source]
Component | Version | Notes |
---|---|---|
CMSIS CoreA | v5.8.0 | Unsupported domain! |
STM32MP13x CMSIS | v1.1.0 | Unsupported domain! |
STM32MP13x HAL | v1.1.0 | Unsupported domain! |
BSP STM32MP13x_DISCO | v1.1.0 | Unsupported domain! |
Find here the list of available HAL, LL and BSP drivers.
6.2.2. Middleware[edit | edit source]
Component | Version | Notes |
---|---|---|
ThreadX | v6.2.0 | - |
NetXduo | v6.2.0 | - |
USBX | v6.2.0 | - |
FileX | v6.2.0 | - |
LevelX | v6.2.0 | - |
cmsis_rtos_threadx | v1.1.0 | - |
STM32 USB Device Library | v2.10.0 | - |
STM32 USB Host Library | v3.5.1 | - |
6.3. Released projects[edit | edit source]
The STM32CubeMP13 Package comes with a rich set of examples running on STMicroelectronics boards, organized by board and provided with preconfigured projects. The main supported development environment is STM32CubeIDE (works on Multiple OS's) and uses the GNU toolchain.
IDE ready projects:
STM32MP135F-DK | |
---|---|
Number of projects | 70 |
Find in this article STM32CubeMP13_Package#Projects, the exhaustive list of available projects for STM32MP135F-DK Discovery kit :
The recommended supported toolchain for STM32MP13 is STM32CubeIDE (All-in-one multi-OS development tool).
7. Restrictions[edit | edit source]
- Source code for External Loader utility is not provided with this release.
8. How to get started with STM32CubeMP13 Package[edit | edit source]
Refer to STM32CubeMP13 Package - Getting started article.
9. Associated tools[edit | edit source]
Refer to Referenced tools release notes
10. Archives
[edit | edit source]
STM32CubeMP13 Package release | Release note |
---|---|
STM32CubeMP13 Package release note - v1.0.0 | STM32CubeMP13 Package release note - v1.0.0 |