Last edited 4 months ago

LPTIM Linux driver

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Article purpose

This article introduces the LPTIM Linux® driver for the LPTIM internal peripheral[1]:

  • Which LPTIM features are supported by the driver
  • How to configure, use and debug the driver
  • What is the driver structure, and where the source code can be found.


2. Short description

The LPTIM[1] Linux driver (kernel space) is based on the PWM, IIO and counter frameworks. It provides several functionalities:

MFD driver:

  • handles common resources (registers, clock)

PWM driver:

  • handles the PWM output channel (single channel)

IIO hardware trigger driver:

  • handles hardware trigger sources (synchronously with PWM) for other internal peripherals such as ADC[2], DAC[3], DFSDM[4]

Counter driver:

  • handles the quadrature encoder interface[5] as well as the external event counter.

Clocksource driver:


3. Configuration

3.1. Kernel configuration

Activate the LPTIM[1] Linux driver in the kernel configuration using the Linux Menuconfig tool: Menuconfig or how to configure kernel.

Enable the following configurations (as well as their dependencies):

  • CONFIG_MFD_STM32_LPTIMER
  • CONFIG_PWM_STM32_LP
  • CONFIG_IIO_STM32_LPTIMER_TRIGGER
  • CONFIG_STM32_LPTIMER_CNT
  • CONFIG_CLKSRC_STM32_LP
Device Drivers  --->
   -> Multifunction device drivers  --->
      <*> Support for STM32 Low-Power Timer
   -> Pulse-width modulation (PWM) support  --->
      <*> STMicroelectronics STM32 PWM LP
   -> Industrial I/O support  --->
      -> Triggers - standalone  --->
         <*> STM32 Low-Power Timer Trigger
   -> Counter support  --->
      <*> STM32 LP Timer encoder counter driver
   -> Clock Source drivers  --->
      <*> Low power clocksource for STM32 SoCs

3.2. Device tree

Refer to the LPTIM device tree configuration article when configuring the LPTIM Linux kernel driver.

4. How to use

How to use PWM with sysfs interface

How to set up a TIM or LPTIM trigger using the sysfs interface

How to use the quadrature encoder with the sysfs interface

LPTIM clocksource driver can be used as the Linux scheduling-clock during the low power modes, see timer documentation for details.

5. How to trace and debug

The LPTIM Linux driver can access LPTIM registers through REGMAP.

It comes with debugfs[6] entries, which allow dumping registers:

cd /sys/kernel/debug/regmap
ls
40004000.timer  40009000.timer

cd 40009000.timer
cat registers
000: 00000003
004: 00000000
008: 00000000
...

It also comes with tracepoints[7]:

cd /sys/kernel/debug/tracing
cat available_events | grep regmap
...
regmap:regmap_reg_read
regmap:regmap_reg_write

6. Source code location

The LPTIM Linux driver is composed of:

7. References